Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Examples of Use

This slide gives insights into further application examples, the function of the SiGe rectifier and its benefits. When power is converted, a boost or buck diode is used, like in Switch Mode Power Supplies. The key parameter of power conversion is efficiency. Therefore, power losses must be kept to an absolute minimum. Due to the low forward voltage drop, the SiGe diode is an ideal choice, even more, if high thermal stability is required and the circuit operates under high ambient temperatures. Another example is a SiGe diode used in an ORing application, in which an auxiliary battery is connected to the board net. The rectifier serves to minimize the superimposition of the board net battery voltage on the backup battery. That‘s why it is essential to keep the reverse leakage currents as low as possible. In addition, a low VF matters due to the limited battery capacity.

PTM פורסם ב: