Back to top

American Bright

- For over two decades, Bright LED has become one of the world's leading LED suppliers seeking unusual quality and service to the rapidly growing market for LEDs in the US market.

With the same philosophy that Bright has continually invested in the expansion of their research and development, manufacturing, and customer service capabilities, American Bright is capable of responding to the needs of the customers on a domestic basis. This response is achieved through a growing network of authorized sales representatives, applications staff, and qualified distributors. Leveraging its ability to communicate immediately with the factory and with customers and affiliates around the world, and through the further growth of its automated production lines, American Bright is positioned to answer the most demanding needs of its customers. American Bright's manufacturing techniques are highly proficient, assuring a level of quality and uniformity that the market has come to expect in such devices.

המוצרים החדשים ביותר הצג הכול (3)

Image of American Bright's E-Paper Displays

E-Paper Displays

American Bright's low power consumption E-Paper signage provides proficient software-driven solutions and more earth-friendly display alternatives.

קרא עוד
Image of American Bright's Opto-Coupler BPC-10xx Series

Opto-Coupler BPC-10xx Series

American Bright's BPC-10XX series are optically coupled isolators containing an infrared emitting diode and an NPN silicon phototransistor.

קרא עוד
Image of American Bright’s Smart RGB LED with built-in IC

Smart RGB LED with Built-In IC

American Bright’s smart RGB LED features an auto-detection signal for a continuous status of the R, G, B colors via the feedback signal from the built-in chip.

קרא עוד

אתר האינטרנט של היצרן