SHTxx Handling Instructions Datasheet by Sensirion AG
View All Related Products | Download PDF Datasheet
Preface
 
SENSIRION
THE sensor! commuv
organic compounds. i.e. high conceniration and long
volaiile
 
chemicals
cleaning agents
good vemilaiion fresh air suggly
 
www.sensirion.com  Rev. 5 – March 2018  1/7 
Handling Instructions 
For SHTxx Humidity and Temperature Sensors 
Applicability 
This  document  is  applicable  to  all  Sensirion  SHTxx 
humidity and temperature sensors. 
ESD protection 
The sensor shall be protected from ESD (Electrostatic 
Discharge) and only be handled in ESD protected areas 
(EPA) under protected and controlled conditions (ground 
all personnel with wrist-straps, ground all non-insulating 
and  conductive  objects,  exclude  insulating  materials 
from the EPA, operate only in grounded conductive floor, 
etc.).  Protect  sensor  outside  the  EPA  using  ESD 
protective packaging.   
Protection against ESD is mandatory. 
Exposure to Chemicals 
Humidity and Temperature sensors are highly accurate 
environmental sensors and as such they are not ordinary 
electronic  components.  The  opening  in  the  package 
exposes  the  sensor  to  the  environment  and  makes  it 
susceptible to pollutants. While applying sensors in the 
field in ambient environment is not critical, pollutants are 
known  to  occur  in  manufacturing  environments  and 
during storage. Please carefully follow the guidelines in 
this application note to ensure that you can benefit of the 
sensor’s outstanding performance. 
The  sensor shall  not  get  in  close  contact  with  volatile 
chemicals such as solvents or other organic compounds. 
Especially high concentration and long exposure must 
be  avoided.  Ketenes,  Acetone,  Ethanol,  Isopropyl 
Alcohol,  Toluene,  etc.  are  known  to  cause  drift  of  the 
humidity  reading  –  irreversibly  in  most  of  the  cases. 
Please  note  that  such  chemicals  are  integral  part  of 
epoxies, glues, adhesives, etc. and outgas during baking 
and  curing.  These  chemicals  are  also  added  as 
plasticisers into plastics, used for packaging materials, 
and do out-gas for some period. 
Acids and bases may affect the sensor irreversibly and 
shall  be  avoided:  HCl,  H2SO4,  HNO3,  NH3  etc.  Also 
Ozone  in  high  concentration  or  H2O2  have  the  same 
effect and therefore shall be avoided. Please note, that 
above examples represent no complete list of  harmful 
substances.  
The sensor shall not get in contact with cleaning agents 
(e.g. PCB board wash after soldering) or strong air blasts 
from  an  air-pistol  (not  oil-free  air).  Applying  cleaning 
agents to the sensor may lead to drift of the reading or 
complete breakdown of the sensor. 
Ensure good ventilation (fresh air supply) to avoid high 
concentrations  of  volatile  chemicals  (solvents,  e.g. 
ethanol,  isopropanol,  methanol,  acetone,  cleaning 
solutions, detergents…). 
Packing and Storage 
Prior  to  assembly  or  use  of  the  sensors  it  is  strongly 
recommended to store the sensors in the original sealed 
ESD bag at following conditions: Temperature shall be in 
the range of 10°C – 50°C (0 – 125°C for limited time) 
Preface 
Sensirion SHTxx are relative humidity and temperature 
sensors  of  high  quality.  For  taking  advantage  of  their 
outstanding  performance  some  precautions  must  be 
taken  during  storage,  assembly  and  packaging. 
Therefore, please read the following instructions carefully 
-  preferably  during  design-in  phase  and  before 
production  release  of  the  respective  device.  Special 
attention is required regarding the exposure to volatile 
organic  compounds,  i.e.  high  concentration  and  long 
exposure  time  to  respective  gases  shall  be  avoided. 
Such  conditions  are  known  to  occur  in  manufacturing 
environment  and/or  during  storage.  Therefore,  proper 
handling  and  choice  of  materials  are  crucial.  Applying 
sensors in the field in ambient environment is not critical.  
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
e sensors have been removed
we recommend to store the
devlces wih assemble
c shielded ESD bags
ended not to use any
reseal the sensor bag
 
 
 
 
 
Slroebel "Topshield" Bags
 
SENSIRION
YHE senson COMPANY
 
 
 
 
 
 
 
 
 
 
mu;
"V3.92"
2 131*
 
 
 
 
 
 
 
SENSIRION
 
 
 
 
 
 
 
soldering
older cycle. This
It is imponanl lh
no board wash
 
SHTxx Handling Instructions   
www.sensirion.com  Rev. 5 – March 2018  2/7 
and humidity at 20 – 60%RH (sensors that are not stored 
in ESD bags).  
Store sensors in original, unopened ESD bag. Place 
additional stickers only  on  the  outside of  the  ESD 
bag. 
Once sensors have been removed from the original ESD 
bag  we  recommend to store the  individual sensors as 
well  as  devices  with  assembled  sensors  in  metal-in 
antistatic  shielded  ESD  bags.  In  particular,  it  is 
recommended  not  to  use  any  adhesive  or  adhesive 
tapes to reseal the sensor bag after opening. Following 
ESD Bags can be recommended (no polluting effect on 
humidity sensor): 
ESD Bag 
Manufacturer 
Product 
Stroebel 
"Topshield" Bags 
Sensors  as  a  component  or  mounted  into  the  final 
product  shall  not  be  packaged  in  outgassing  plastic 
materials which could cause sensor pollution. Besides 
metal-in  antistatic  shielded  ESD  bags,  paper  or 
cardboards based packaging, deep drawn plastic trays 
(PE, PET, PP) may be considered. Do not use antistatic 
polyethylene bags (light blue, pink or rose color); be very 
careful with bubble foils and foams. 
Be careful about stickers present inside the packing (e.g. 
on the housing of the device). Sticker size should be kept 
to a minimum, and the sticky side shall fully adhere onto 
a surface.  
Please  note  that  many  packaging  materials  may  be 
provided with additives (plasticizers) which may have a 
polluting effect on  the sensor. Generally speaking, if a 
material  emits  a  strong  odor  you  should  not  use  it. 
Additives  may  also  be  added  to  materials  which  are 
listed  for  recommended  use.  For  high  safety,  device 
housing  and  shipment  packaging  must  be  qualified. 
Such  a  qualification  test  may  contain  exposure  of  the 
final  device  with  sensor  in  its  shipment  packaging  to 
temperature ≥65°C for at least 168 hours. (If shipping or 
storage  conditions  are  expected  to  be  harsh,  the 
qualification test conditions for the packing material have 
to be customized.) The sensor reading then shall show 
no changed deviation against a reference compared to 
same measurements before the exposure. 
Do not use polyethylene antistatic bags (light blue, 
pink or rose color). Do not use adhesive tapes inside 
packaging. 
For guidance on simple and straight-forward testing of 
humidity sensors please consult the  Testing Guide for 
humidity sensors. 
Assembly 
Sensors  in  SMT  packages  are  classified  as  Moisture 
Sensitivity  Level  1  (IPC/JEDEC  J-STD-020).  It  is 
recommended to process the sensors within 1 year after 
date of delivery. 
Before developing the assembly process please read the 
User’s  Guide  of  the  Datasheets  carefully.  In  the 
following,  crucial  items  are  underlined  plus  additional 
items are given:  
For soldering please read carefully the application note 
“Assembly of SMD Packages”. Make sure that maximum 
temperatures and exposure times are respected. In case 
the PCB passes through multiple solder cycles (as is the 
case for e.g. PCB that are assembled on top and bottom 
side), it is recommended to assemble the SHTxx only in 
the last solder cycle. This is to reduce risks of sensor 
pollution. It is  important that “no-clean” solder paste is 
used and no board wash is applied once the sensor is 
assembled to the PCB. 
SHT31 – 500pcs 
Inspected 
 
 
 
 
 
 
 
 
 
 
No mechanical force
SENSIRION
THE sensor: COMPANY
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
Perers Elpeguard Si. 1301 ECO-FLZ
Dow Corning 1-2577 Low Voc Conformal Coating
Electrolube AFA (Aromatic Free Acrylic Conformal
corrosive environment
conformal coatlnqs rpoltinq materials
spray coating Iechnigues
3M Elemrical Tape 92
 
 
 
 
 
 
adhesive tages
 
 
 
SHTxx Handling Instructions   
www.sensirion.com  Rev. 5 – March 2018  3/7 
Do not apply board wash. 
No mechanical force shall be applied to any part of the 
sensor during assembly or usage. 
For  application  in  corrosive  environment  –  such  as 
condensed  water  or  corrosive  gases  –  it  may  be 
necessary to protect the  electronic assembly including 
the soldered contacts of the sensor with a passivation. 
Such passivation may be achieved by conformal coating 
or by applying adhesive. 
Low viscose conformal coatings or potting materials may 
flow  into  the  inside  the  sensor  cap,  cover  the  sensor 
element and thus make the humidity sensor inoperative. 
Use  only  high  viscose  conformal  coatings  or  potting 
materials, or seal the interface between sensor cap and 
sensor PCB before applying conformal coating. Ensure 
good ventilation throughout the application, staging and 
curing to prevent sensor pollution. 
If conformal coating is applied, the top surface of the 
sensor must remain free of coating. 
In any case, covering the humidity sensor opening with 
any kind of coating must be avoided. Therefore, the top 
surface of the sensor should remain free of coating. 
The following table lists conformal coatings which have 
been tested regarding pollution of the humidity sensor 
and are known to be suitable if applied and fully cured 
under good ventilation (fresh air supply) and according 
to respective datasheet. 
Conformal Coatings 
Manufacturer 
Product 
Peters 
Elpeguard SL 1301 ECO-FLZ 
Dow Corning 
1-2577 Low Voc Conformal Coating 
Electrolube 
AFA (Aromatic Free Acrylic Conformal 
Coating) 
Do not apply spray to unprotected sensor. 
Whenever using spray coating techniques (e.g. to apply 
varnish  or  conformal  coating,  etc.)  the  SHT3x  with 
protective cover option can be used or the SHTxx sensor 
has  to  be  covered  by  the  adhesive  tape  to  prevent 
coating  of  the  humidity  sensor  opening.  The  following 
table  lists  adhesive  tapes  which  have  been  tested 
regarding pollution of the humidity sensor and are known 
to be suitable. 
Adhesive Tapes 
Manufacturer 
Product 
3M 
Electrical Tape 92 
Do not apply any other adhesive tapes such as Scotch 
Tape, Sello Tape, Tesa Film, etc. 
XXX 
SENSIRION
THE sewson (DMF'ANV
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
¢ Peters vu 4457-61
adhesives and encapsulants
Be par using strong cleaning
agents ohms
an
EFO-TEK H70E/S J
EFO-TEK T6067
EFO-TEK 93-86
Lord MD-130
Eccobond E35034
Ablebcnd 64-3
 
 
 
 
 
Slycasl 50300 I 50400 series
Hysol E01061/E01062
 
 
 
 
 
 
 
 
 
RTV 6424 (Momemive)
Dow Cormng 732
Slycasl S 7503
 
 
 
 
 
 
 
 
Loctile 401
 
 
SHTxx Handling Instructions   
www.sensirion.com  Rev. 5 – March 2018  4/7 
In  conjunction  with  the  sensor,  use  only 
recommended  Kapton®  tape  Electrical  Tape  92  by 
3M™. 
Regarding adhesives and encapsulants the material in 
the  following  tables  may  be  used  –  according  to 
respective  datasheets,  applied  and  fully  cured  in  well 
ventilated environment (fresh air supply). Materials and 
brands not listed in the following tables may be harmful 
and shall be tested carefully before applying. 
Epoxy Adhesives 
Manufacturer 
Product 
EPO-TEK 
H70E/S 
EPO-TEK  
T6067 
EPO-TEK  
93-86 
Lord  
MD-130 
Eccobond  
E3503-1 
Ablebond  
84-3 
Epoxy Glob Top Encapsulants 
Manufacturer 
Product 
Stycast  
50300 / 50400 series 
Hysol  
EO1061/EO1062 
Silicone Adhesives 
Manufacturer 
Product 
RTV  
6424 (Momentive) 
Dow Corning  
732 
Silicone Glob Top Encapsulants 
Manufacturer 
Product 
Stycast  
S 7503 
Instant Adhesives 
Manufacturer 
Product 
Loctite  
401 
PUR (Polyutherane) Casting Compounds 
Manufacturer 
Product 
Peters  
VU 4457-61 
Hot  melts  may  absorb  water  and  thus  may  have  an 
impact on the response time of the sensor in the device. 
Therefore, hot melt shall be applied sparingly. 
The sensor shall be mounted into the device, if possible, 
after all materials that are used in the assembly process 
have completely cured or dried  out.  Otherwise  ensure 
good ventilation (fresh air supply)  in curing ovens and 
assembly lines. 
Prevent any dust or  particles from entering the sensor 
opening (sensor performance may be affected). 
Wear  clean  gloves  or  finger  cots  while  handling  the 
sensor and avoid touching the sensor opening. 
Ensure  recommendations  in  this  application  note  are 
equally  considered  during  repair  and  rework  of 
assemblies  containing  sensors.  During  repair  and 
rework it  may  be  recommendable to cover  the  sensor 
with Kapton tape (specific recommendation see above). 
Be  particularly  careful  when  using  strong  cleaning 
agents  (e.g.  detergents,  alcohols,  brominated  or 
fluorinated  solvents).  Cleaning  any  part  of  a  product 
might lead to high concentration of cleaning agents on 
the  sensor.  Please  remove  any  sensors  or  devices 
containing sensors before cleaning the production area 
and tools.  Ensure good ventilation (fresh air supply) and 
that  any  solvents  have  evaporated  before  resuming 
production. 
Prevent sensor from exposure to cleaning agents. 
SENSIRION
YHE season COMPANY
clean air — gualification for use in harsh environment is
duty of the user of the sensor
For exposure to extreme
humidity and temgerature
volatile organic comgounds
acids or bases
Corrosive substances
 
SHTxx Handling Instructions   
www.sensirion.com  Rev. 5 – March 2018  5/7 
Application in extreme environment 
Some applications require the exposure of humidity and 
temperature sensors to harsh environments. In many of 
the cases the sensor is uncritical to be used. However, 
some precautions must be taken. 
For  exposure  to  extreme  conditions  with  regards  to 
humidity and temperature please consult the datasheet 
of respective product. Please make sure that exposure 
time  of  the  sensor  to  maximum  range  of  operating 
conditions is limited as given in datasheet. Exposure to 
volatile  organic  compounds  at  high  concentration  and 
long exposure time is critical not only in assembly but 
also in the field. Such application needs to be carefully 
tested and qualified. 
Exposure to acids or bases may be critical, too. In order 
to  be  critical,  the  concentration  must  be  such  that 
polymers are attacked. For bases there is a rule of thumb 
that  pH<9  are  uncritical.  Etching  substances  such  as 
H2O2, NH3, etc. at high concentrations are critical to the 
sensor, too. 
Corrosive substances at very low concentrations are not 
critical to the sensor itself. However, they may attack the 
solder  contacts.  Therefore,  the  contacts  must  be  well 
protected (passivated) in case of an application to such 
environment – compare also Section “Assembly”. 
Application  of  Sensirion  humidity  and  temperature 
sensors to harsh environment must be carefully tested 
and  qualified.  Sensirion  qualifies  its  humidity  and 
temperature  sensors  to  work  properly  within  ambient 
clean air – qualification for use in harsh environment is 
duty of the user of the sensor. 
Reconditioning Procedure 
As  stated  above  extreme  conditions  or  exposure  to 
solvent  vapors  may  offset  the  sensor.  The  following 
reconditioning procedure may bring the sensor back to 
calibration state:  
Baking:     100 – 105°C at < 5%RH for 10h  
Re-Hydration:    20 – 30°C at ~ 75%RH for 12h 
1
. 
Disclaimer 
The  above  given  restrictions,  recommendations, 
materials, etc. do not cover all possible cases and items. 
The material recommendations are given with regard to 
pollution  of  SHTxx  sensors  and  assume  optimal 
processing for avoiding VOC in process – the materials 
were not tested regarding other properties like reliability, 
performance,  usability  or  mechanical  properties.  The 
material recommendations have been compiled with our 
best knowledge at the time of writing. Manufacturers may 
change the compounds without notice, which can lead to 
reduced Sensor performance due to outgassing. 
This document is not to be considered complete and is 
subject to change without prior notice.  
1
   75%RH can conveniently be generated with saturated NaCl solution. 
SENSIRION
was sensor: COMPANY
 
 
 
 
 
 
 
 
Date Revision Changes
29 June 2007 0.1 (Preliminary) Initial revision
7 January 2009 1.0 Complete rework.
18 March 2010 1.1 New formal, implementation of pictograms.
28 June 2012 2.0 Moisture Sensitivity Level adapted.
18 November 2013 3 Document partially restructured and clarifications added.
22. May 2014 4 ESD bag recommendation changed, reconditioning procedure added
12. March 2018 5 ESD bag recommendation changed, Piclograms updated, conformal
 
 
 
 
 
SHTxx Handling Instructions   
www.sensirion.com  Rev. 5 – March 2018  6/7 
Revision History 
Date 
Revision 
Changes 
29 June  2007 
0.1 (Preliminary) 
Initial revision 
7 January 2009 
1.0 
Complete rework. 
18 March 2010 
1.1 
New format, implementation of pictograms. 
28 June 2012 
2.0 
Moisture Sensitivity Level adapted. 
18 November 2013 
3 
Document partially restructured and clarifications added. 
22. May 2014 
4 
ESD bag recommendation changed, reconditioning procedure added 
12. March 2018 
5 
ESD  bag  recommendation  changed,  Pictograms  updated,  conformal 
coating added 
SENSIRION AG
fax: +41 44 306
info@sensinon.com
www 9ensm0n.com
Sensirion Taiwan Co. Lxd.
info@sensirion.oom
SENSIRION
YHE senson COMPANY
Sensxrion \nc. USA Sensinon Korea Co. Ltd.
phone: +1 312 690 585 phone: +82 31 337 77
mfcrus@sensiricn.com info-kr@sensiricn.com
www.5ensirion com www.5ensirion.co.kr
phone: +81 3 3444 4 phone: +86 755 8252
mfcr'p@sensirion com info-en@sensirion.com
www.5ensirion 0032 www.5ensirion.com cn/
To find your ma‘ represenmwe, please visxt www sensinon.com/con1acl
 
SHTxx Handling Instructions   
www.sensirion.com  Rev. 5 – March 2018  7/7 
Important Notices 
Warning, Personal Injury
Do not use this product as safety or emergency stop devices 
or in any other application where failure of the product could 
result  in  personal  injury.  Do  not  use  this  product  for 
applications  other  than  its  intended  and  authorized  use. 
Before installing, handling, using or servicing this product, 
please consult the data sheet and application notes. Failure 
to comply with these instructions could result  in death or 
serious injury. 
If the Buyer shall purchase or use SENSIRION products for any 
unintended  or  unauthorized  application,  Buyer  shall  defend, 
indemnify  and  hold  harmless  SENSIRION  and  its  officers, 
employees,  subsidiaries,  affiliates  and  distributors  against  all 
claims, costs, damages and expenses, and reasonable attorney 
fees arising out of, directly or indirectly, any  claim of  personal 
injury or death associated with such unintended or unauthorized 
use, even if SENSIRION shall be allegedly negligent with respect 
to the design or the manufacture of the product. 
ESD Precautions 
The inherent design of this component causes it to be sensitive 
to  electrostatic  discharge  (ESD).  To  prevent  ESD-induced 
damage and/or degradation, take customary and statutory ESD 
precautions when handling this product. 
See  application  note  “ESD,  Latchup  and  EMC”  for  more 
information. 
Warranty 
SENSIRION  warrants  solely  to  the  original  purchaser  of  this 
product for a period of 12  months (one year) from the date  of 
delivery  that  this  product  shall  be  of  the  quality,  material  and 
workmanship defined in SENSIRION’s published specifications 
of  the  product.  Within  such  period,  if  proven  to  be  defective, 
SENSIRION  shall  repair  and/or  replace  this  product,  in 
SENSIRION’s discretion, free of charge to the Buyer, provided 
that: 
 notice in writing describing the defects shall be given to 
SENSIRION within fourteen (14) days after their 
appearance;  
 such defects shall be found, to SENSIRION’s reasonable 
satisfaction, to have arisen from SENSIRION’s faulty 
design, material, or workmanship;  
 the defective product shall be returned to SENSIRION’s 
factory at the Buyer’s expense; and 
 the warranty period for any repaired or replaced product 
shall be limited to the unexpired portion of the original 
period. 
This warranty does not apply to any equipment which has not 
been installed and used within the specifications recommended 
by  SENSIRION  for  the  intended  and  proper  use  of  the 
equipment.  EXCEPT  FOR  THE  WARRANTIES  EXPRESSLY 
SET FORTH HEREIN, SENSIRION MAKES NO WARRANTIES, 
EITHER  EXPRESS  OR  IMPLIED,  WITH  RESPECT  TO  THE 
PRODUCT.  ANY  AND  ALL  WARRANTIES,  INCLUDING 
WITHOUT  LIMITATION,  WARRANTIES  OF 
MERCHANTABILITY  OR  FITNESS  FOR  A  PARTICULAR 
PURPOSE, ARE EXPRESSLY EXCLUDED AND DECLINED. 
SENSIRION is only liable for defects of this product arising under 
the conditions of  operation provided for  in  the data  sheet and 
proper  use  of  the  goods.  SENSIRION  explicitly  disclaims  all 
warranties, express or implied, for any period during which the 
goods are operated or stored not in accordance with the technical 
specifications. 
SENSIRION  does  not  assume  any  liability  arising  out  of  any 
application  or  use  of  any  product  or  circuit  and  specifically 
disclaims  any  and  all  liability,  including  without  limitation 
consequential or incidental damages. All operating parameters, 
including without limitation recommended parameters, must be 
validated  for  each  customer’s  applications  by  customer’s 
technical experts. Recommended parameters can and do vary in 
different applications. 
SENSIRION  reserves  the  right,  without  further  notice,  (i)  to 
change the product specifications and/or the information in this 
document and (ii) to improve reliability, functions and design of 
this product. 
Copyright © 2018, by SENSIRION. 
CMOSens® is a trademark of Sensirion 
All rights reserved 
Headquarters and Subsidiaries 
SENSIRION AG 
Laubisruetistr. 50 
CH-8712 Staefa ZH 
Switzerland 
phone:  +41 44 306 40 00 
fax:  +41 44 306 40 30 
info@sensirion.com 
www.sensirion.com 
Sensirion Inc. USA 
phone:  +1 312 690 5858 
info-us@sensirion.com 
www.sensirion.com 
Sensirion Japan Co. Ltd.   
phone:  +81 3 3444 4940 
info-jp@sensirion.com 
www.sensirion.co.jp 
Sensirion Korea Co. Ltd. 
phone:  +82 31 337 7700~3 
info-kr@sensirion.com 
www.sensirion.co.kr 
Sensirion China Co. Ltd. 
phone:  +86 755 8252 1501 
info-cn@sensirion.com 
www.sensirion.com.cn/ 
Sensirion Taiwan Co. Ltd. 
phone:  +41 44 306 40 00 
info@sensirion.com 
To find your local representative, please visit www.sensirion.com/contact 
Products related to this Datasheet
SENSOR HUMI/TEMP 3V I2C 1.8% SMD
        
    SENSOR HUMID/TEMP 5V I2C 3% SMD
        
    SENSOR HUMI/TEMP 5V I2C 1.5% SMD
        
    SENSOR HUMID/TEMP 5V ANLG 2% SMD
        
    SENSOR HUMID/TEMP 5V DIGITAL MOD
        
    SENSOR HUMID/TEMP 3V I2C 2% SMD
        
    SENSOR HUMI/TEMP 1.8V I2C 3% SMD
        
    SENSOR HUMID/TEMP 5V I2C 2% SMD
        
    SENSOR HUMID/TEMP 5V I2C 2% SMD
        
    SENSOR HUMID/TEMP 5V I2C 2% SMD
        
    SENSOR HUMI/TEMP 5V I2C 1.5% SMD
        
    SENSOR HUMID/TEMP 3V I2C 3% SMD
        
    SENSOR HUMID/TEMP 5V ANLG 3% SMD
        
    SENSOR HUMID/TEMP 5V I2C 3% SMD
        
    SENSOR HUMID/TEMP 5V I2C 2% SMD
        
    SENSOR HUMID/TEMP 3V SDM 2% SMD
        
    SENSOR HUMI/TEMP 5V I2C 1.5% SMD
        
    SENSOR HUMID/TEMP 3V I2C 3% SMD
        
    SENSOR HUMID/TEMP 5V ANLG 3% SMD
        
    SENSOR HUMID/TEMP 5V I2C 3% SMD
        
    SENSOR HUMID/TEMP 5V I2C 2% SMD
        
    SENSOR HUMID/TEMP 5V I2C 2% SMD
        
    SENSOR HUMID/TEMP 5V I2C 3% SMD
        
    SENSOR HUMID/TEMP 5V I2C 3% SMD
        
    SENSOR HUMID/TEMP 3V PWM 2% SMD
        
    SENSOR HUMID/TEMP 3V PWM 2% SMD
        
    SENSOR HUMI/TEMP 3V I2C 1.8% SMD
        
    SENSOR HUMID/TEMP 3V I2C 2% SMD
        
    SENSOR HUMID/TEMP 3V SDM 2% SMD
        
    SENSOR HUMI/TEMP 1.8V I2C 3% SMD