Maker.io main logo

DIY addictive Arduino 1D Pong game

128

2024-07-15 | By Mirko Pavleski

License: General Public License Displays LEDs / Discrete / Modules Arduino

 

Pong is a table tennis–themed two-dimensional graphics arcade video game manufactured by Atari and originally released on 1972.

hjki

This time I will present you a simple way to make a 1D LED Pong game, an interesting project that simulates a Pong game on a single-dimensional array of LEDs. This can be done using an Arduino microcontroller board. The movement of the ball is simulated by the array of LEDs, and the paddles are the two buttons. The game is for 2 players, in which the "ball" travels down the length of the LED array and will bounce back if the button is pressed when the yellow LED is illuminated.

 

The result is displayed on the LCD screen. The movement of the ball, the winning of a point as well as the victory are accompanied by appropriate sounds The device is very simple to make and consists of several components:

- Arduino Nano microcontroller board

- 16x2 LCD Display

- 10 LEDs

- 12 resistors

- two buttons

- and Buzzer

vhj

The game starts by moving the ball from player 1 to player 2, and if player 2 fails to press the button while the yellow LED is on, the red LED will light up and it's a point for player 1. Each game is started by the winner of the previous one. The speed of the ball increases after every hit, making it more difficult to hit the ball in time. The match ends when one of the players wins 10 games, and at that moment the LEDs that are on the winner's side will flash.

fdgy

- The starting speed of movement of the LEDs is set in the row:const unsigned long initialMillisecondsPerLED = 400; The lower this number, the faster the movement speed

opo

- The degree of acceleration after each hit is adjusted in the rows: if (deltaMillisecondsPerLED > 50) { deltaMillisecondsPerLED -= 50;and the higher this number is, the higher the acceleration.

hjiohu

The game can be played by one or two players. In the case of two players, which is a natural option, it is preferable to use robust external arcade buttons.

jkl

For this purpose, I used these buttons that I made for the needs of one of my previous projects. They are large and have a precise, and audible click. Finally, a short conclusion. This is an interesting one-dimensional compact version of the classic "Pong" game made with a minimal number of components, yet extremely addictive, and can be played for hours before you get bored. The device is mounted in a suitable box made of PVC board and lined with self-adhesive wallpaper. For power, it is preferable to use a lithium battery for the sake of mobility

Code:

Copy Code
//#include <LiquidCrystal.h>

#include <Wire.h>

#include <LiquidCrystal_I2C.h>
LiquidCrystal_I2C lcd(0x27, 16, 2);


bool willTheBallGoTowardsPlayerTwo = true;
bool isInputAllowed = true;

const int playerOne = 12;
const int goalPlayerOne = 13;
const int buttonPlayerOne = 3;

const int playerTwo = 5;
const int goalPlayerTwo = 4;
const int buttonPlayerTwo = 2;

int scoreOfPlayerOne = 0;
int scoreOfPlayerTwo = 0;

const unsigned long initialMillisecondsPerLED = 400;
const unsigned long initialDeltaMillisecondsPerLED = 50;
unsigned long millisecondsPerLED = initialMillisecondsPerLED;
unsigned long deltaMillisecondsPerLED = initialDeltaMillisecondsPerLED;
unsigned long currentMillis = 0;
unsigned long previousMillis = 0;

int currentPosition = playerOne; //Player one starts the game.
int previousPosition = playerOne + 1;
int deltaPosition = 0;

int buttonStatePlayerOne = 0;
int lastButtonStatePlayerOne = 0;
int buttonStatePlayerTwo = 0;
int lastButtonStatePlayerTwo = 0;

void setup() {


lcd.backlight();
lcd.begin(16,2);
lcd.clear();
lcd.setCursor(2, 0);
lcd.print("1D-Pong Game");
lcd.setCursor(3, 1);
lcd.print("by mircemk");
delay(2000.);

lcd.clear();
lcd.setCursor(0, 0);
lcd.print("Player One: 0");
lcd.setCursor(0, 1);
lcd.print("Player Two: 0");



pinMode(4, 1);
pinMode(5, 1);
pinMode(6, 1);
pinMode(7, 1);
pinMode(8, 1);
pinMode(9, 1);
pinMode(10, 1);
pinMode(11, 1);
pinMode(12, 1);
pinMode(13, 1);
/*Connect pins 4 to 13 to 220ohm resistors, connect the LEDs' longer legs(+) to the resistors,
connect the other legs(-) of the LEDs' to ground.
I recommend red LEDs for 4 and 13(Goals), yellow LEDs for 5 and 12(Players), green LEDs for other pins(Field).
*/

pinMode(2, 0); //Pushbuttons for players. Pin 2 is for player two. Pin 3 is for player one.
pinMode(3, 0); //Connect pushbuttons following the instructions on this page: https://www.arduino.cc/en/Tutorial/DigitalReadSerial
}

void loop()
{
ListenForInput();
currentMillis = millis();
if (currentMillis - previousMillis >= millisecondsPerLED) //If you don't understand this, see: https://www.arduino.cc/en/Tutorial/BlinkWithoutDelay
{
CheckGoalConditions();
lcd.clear();
lcd.setCursor(0, 0); //(Column,Row)
lcd.print("Player One: ");
lcd.setCursor(12, 0);
lcd.print(scoreOfPlayerOne);

lcd.setCursor(0, 1); //(Column,Row)
lcd.print("Player Two: ");
lcd.setCursor(12, 1);
lcd.print(scoreOfPlayerTwo);
CheckEndGame();
DetermineNextPosition();
MoveBallToNextPosition();

previousMillis = currentMillis;

}
}

void ListenForInput() //If you don't understand this method. See: https://www.arduino.cc/en/Tutorial/StateChangeDetection
{
buttonStatePlayerOne = digitalRead(buttonPlayerOne);
buttonStatePlayerTwo = digitalRead(buttonPlayerTwo);

if (buttonStatePlayerOne != lastButtonStatePlayerOne && isInputAllowed)
{
if (buttonStatePlayerOne == 1)
{
if (currentPosition == playerOne)
{
ToggleBallDirection();
IncreaseSpeed();

}
else
{
ScoreForPlayer(2);

}
}
lastButtonStatePlayerOne = buttonStatePlayerOne;
}
if (buttonStatePlayerTwo != lastButtonStatePlayerTwo && isInputAllowed)
{
if (buttonStatePlayerTwo == 1)
{
if (currentPosition == playerTwo)
{
ToggleBallDirection();
IncreaseSpeed();

}
else
{
ScoreForPlayer(1);

}
}
lastButtonStatePlayerTwo = buttonStatePlayerTwo;
}
}

void ToggleBallDirection()
{
willTheBallGoTowardsPlayerTwo = !willTheBallGoTowardsPlayerTwo;
isInputAllowed = false; //Only one direction change per frame is allowed for consistent gameplay.
}

void IncreaseSpeed()
{
millisecondsPerLED -= deltaMillisecondsPerLED;
if (deltaMillisecondsPerLED > 50) //Because of this, it takes a little more time to reach to an insane speed. Adjust or remove this if rounds become too long.
{
deltaMillisecondsPerLED -= 50;
}
}

void MoveBallToNextPosition() //Moves the ball one spot.
{
previousPosition = currentPosition;
digitalWrite(previousPosition, 0);
currentPosition = currentPosition + deltaPosition;
digitalWrite(currentPosition, 1);
tone(1, 500, 50);
isInputAllowed = true;
}

void DetermineNextPosition()
{
if (willTheBallGoTowardsPlayerTwo)
{
deltaPosition = -1;
}
else
{
deltaPosition = 1;
}
}

void CheckGoalConditions()
{
if (currentPosition == goalPlayerTwo)
{
ScoreForPlayer(1);
}
else if (currentPosition == goalPlayerOne)
{
ScoreForPlayer(2);
}
}

void ScoreForPlayer(int playerWhoScored)
{
isInputAllowed = false;
FlashAllLEDs(1, 0);
if (playerWhoScored == 1)
{
scoreOfPlayerOne++;

Reset(1);
}
else if (playerWhoScored == 2)
{
scoreOfPlayerTwo++;

Reset(2);
}

}

void CheckEndGame()
{
if (scoreOfPlayerOne == 10)
{
lcd.clear();
lcd.setCursor(0, 0);
lcd.print("Player One Win");
EndGameCeremonyFor(1);

}
if (scoreOfPlayerTwo == 10)
{
lcd.clear();
lcd.setCursor(0, 0);
lcd.print("Player Two Win");
EndGameCeremonyFor(2);

}
}

void Reset(int playerCurrentlyScored)
{
if (playerCurrentlyScored == 1)
{
digitalWrite(playerOne, 1);
currentPosition = playerOne;
willTheBallGoTowardsPlayerTwo = true;
tone(1, 200 ,150 );
}
else if (playerCurrentlyScored == 2)
{
digitalWrite(playerTwo, 1);
currentPosition = playerTwo;
willTheBallGoTowardsPlayerTwo = false;
tone(1, 300 ,150 );

}

delay(1000); //Are three seconds enough for players to process the score?
millisecondsPerLED = initialMillisecondsPerLED; //Sets speed to initial value at the beginning of each round.
deltaMillisecondsPerLED = initialDeltaMillisecondsPerLED;
}


void EndGameCeremonyFor(int winner)
{
FlashAllLEDs(50, winner);
TurnOffAllLEDsForPlayer(0);
scoreOfPlayerOne = 0;
scoreOfPlayerTwo = 0;
delay(1000);
lcd.clear();
lcd.setCursor(4, 0);
lcd.print("Starting");
lcd.setCursor(4,1);
lcd.print("New Game");
delay(2000);
}

void TurnOnAllLEDsForPlayer(int player)
{
if (player != 1) //When this method is called with (2), only these pins(player two's) will turn on
{
digitalWrite(4, 1);
digitalWrite(5, 1);
digitalWrite(6, 1);
digitalWrite(7, 1);
digitalWrite(8, 1);
tone(1, 1000, 35);
}
if (player != 2) //When this method is called with (1), only these pins(player one's) will turn on
{
digitalWrite(9, 1);
digitalWrite(10, 1);
digitalWrite(11, 1);
digitalWrite(12, 1);
digitalWrite(13, 1);
tone(1, 1000, 35);
}
}

void TurnOffAllLEDsForPlayer(int player)
{
if (player != 1) //When this method is called with (2), only these pins(player two's) will turn off
{
digitalWrite(4, 0);
digitalWrite(5, 0);
digitalWrite(6, 0);
digitalWrite(7, 0);
digitalWrite(8, 0);
}
if (player != 2) //When this method is called with (1), only these pins(player one's) will turn off
{
digitalWrite(9, 0);
digitalWrite(10, 0);
digitalWrite(11, 0);
digitalWrite(12, 0);
digitalWrite(13, 0);
}
}

void FlashAllLEDs(int blinkCount, int player) //Second parameter(int player) is for when you want to flash only one player's LEDs. Use 1 for player one, use 2 for player two.
{
for (int i = 0; i < blinkCount; i++)
{
TurnOnAllLEDsForPlayer(player);
delay(35);
TurnOffAllLEDsForPlayer(player);
delay(35);
}
}

gh

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.