Maker.io main logo

Move a Stepper Motor NEMA 17 to an Exact Position With a Button

30

2026-05-27 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Motors Pushbutton Arduino

In this tutorial, we will learn how to move a NEMA 17 stepper motor for a certain number of steps and then, with a push of a button, repeat it again.

Watch the video!

Learn more about Visuino: What is Visuino

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

What You Will Need photo 8

What You Will Need photo 9

The Circuit

  • Arduino Digital Pin 2 will be used for the steps

  • Arduino Digital Pin 3 will be used for motor direction.

Connecting Button:

  • Connect Arduino Digital pin [7] to the button on the breadboard and to the Resistor

  • Connect the other side of the resistor to the breadboard pin [GND]

  • Connect the other pin of the button to the breadboard positive pin [5V]

  • Connect Arduino pin [5V] to breadboard positive pin [Red line]

  • Connect Arduino pin [GND] to breadboard negative pin [Black line]

If using a Stepper Motor Driver Shield:

  • Connect the Motor Shield GND pin to the Arduino negative pin [GND]

  • Connect the Motor Shield [5V] pin to the Arduino positive pin [5V]

  • Connect the Motor Shield GND pin to the power supply negative pin [GND]

  • Connect the motor shield [9V] pin to the power supply's positive pin [+]

  • Connect the Motor Shield pin[S] to the Arduino digital pin [2]

  • Connect the Motor Shield pin[D] to the Arduino digital pin [3]

  • Connect the stepper motor as shown in the picture.

If using a Stepper Motor Driver 8825:

  • Connect the DRV8825 GND pin to the Arduino negative pin [GND]

  • Connect the DRV8825 DIR pin to Arduino digital pin [3]

  • Connect the DRV8825 STEP pin to Arduino digital pin [2]

  • Connect the Power Supply for the motor to the DRV8825 VMOT and GND

  • Connect the Capacitor across VMOT and GND

  • Connect the stepper motor as shown in the picture.

The Circuit

The Circuit photo 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, Add Components

  • Add "Debounce Button" component

  • Add "Counter" component

  • Add "Pulse Generator" component

  • Add "Unsigned To Digital" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Set Components

  • Select "PulseGenerator1" and in the properties window set "Frequency" to 2000 << this will be the speed of the stepper motor; you can adjust it to your needs

  • Select "UnsignedToDigital1" and in the properties window set "Output Pins" to 1

  • Select "Counter1" and in the properties window, set "Initial Value" to 5000 << this will be the number of steps of the stepper motor; you can adjust it to your needs

  • Select "Counter1" and in the properties window, set "Max">"Value" to 5000 << this will be the number of steps of the stepper motor; you can adjust it to your needs

  • Select "Counter1" and in the properties window set "Max">"Roll Over" to False

  • Select "Counter1" and in the properties window set "Min">"Roll Over" to False

  • Select "Counter1" and in the properties window, set "Max">"Value" to 0

  • Double click on "Counter1" and in the Elements window, drag "Set Value" to the Left side

  • Close the Elements window

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Set Components photo 4

In Visuino Connect Components

  • Connect "PulseGenerator1" Pin[Out] to "Counter1" Pin [In]

  • Connect Arduino Board Digital Pin [7] to "Button1" Pin [In]

  • Connect "Button1" Pin [Out] to "Counter1" > 'Set Value 1" Pin [In]

  • Connect "Counter1" Pin [Out] to "UnsignedToDigital1" Pin [In]

  • Connect "UnsignedToDigital1" Pin [Out] to  Arduino Board Digital Pin [2]

In Visuino Connect Components

In Visuino Connect Components photo 2

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the Arduino module and press the button, the motor will start to run, and when it reaches a certain number of steps, it will stop. If you press the button again, it will run again for a certain number of steps.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.