Maker.io main logo

Raspberry Pi + Teachable Machine = Teachable Pi

569

2020-03-17 | By Adafruit Industries

License: See Original Project Raspberry Pi SBC

Courtesy of Adafruit

Guide by Andrew Reusch

Overview

In our previous demos, we got Google's Object Detection models running on a Raspberry Pi so that you could build your own smart camera! There's just one thing--what if you want to recognize something else besides coffee cups and people? Until recently, this was challenging; either it required a complex Collaboratory notebook or a long series of local commands to set up a local TensorFlow environment.

video_1

Google recently released a tool called Teachable Machine that automates the whole process for you! You bring some example images, configure a few parameters on their web page, and voila! Google produces a custom model trained against your own objects.

This guide walks you through the process of configuring Teachable Machine, downloading the generated model to Raspberry Pi 4, and running the model on your Pi.

You will need

You'll need the same equipment as used in our Running TensorFlow Lite Object Recognition on the Raspberry Pi 4 guide.

Visit Teachable Machine

Setting up Teachable Machine

To start with, visit the Teachable Machine page on your desktop or laptop (not the Pi--it's too slow).

Click Get Started, then choose Image Project from the first screen, and you'll be presented with this empty project screen:

setup_2

Now it's ready for you to input samples. Before you start, have a look at the guidelines for choosing and capturing samples below.

Choosing Samples

Now you need to find example images that include the objects you want to recognize. This can be the both the most important and most time-consuming part of retraining a machine learning model, so choose wisely!

Here are some tips for choosing example images:

  • Choose realistic images. Your model won't behave predictably in scenarios it hasn't seen before.

  • Choose varied images. It's really important that the only thing in common between the images is the thing you want to detect. As an example, if all of the images in one category have a blue background, the model might simply learn that a blue background indicates that category.

  • Choose representative images. Make sure you include images that show all different angles of the object you'd like to recognize.

  • Include an "empty" category. Try including a category that the machine can select when it isn't confident in any of the choices. This should have as much background variation as possible and shouldn't include any objects you want to recognize.

Create Categories

Now you need to create categories in the Teachable Machine UI to match the objects you've chosen. Usually, you should create one category for each distinct type of object you want to recognize--so, if you want to train your model to recognize different clothes, you might create categories for pants, dresses, shirts, and socks.

You can also try to train a smarter model, like one that looks for blue shirts or button-down shirts. But beware, this is advanced, and we don't suggest you start with this.

Also, be sure to create a nothing category--one that the machine can choose when it doesn't see anything. You'll need to find some example images that don't contain any of your chosen objects.

Adding Categories to your Teachable Machine project

Each box on the left of your page represents a different category. Change the name of each as follows:

Click the pencil icon, then name the category.

icon_4

Press Enter to accept the name. The box should look like this (e.g. for the transistor category).

transistor_5

Repeat these steps for each of the other objects you'd like to recognize. When you're finished, your screen should look like this:

machine_6

Use Computer Webcam

Capturing Samples

You can capture either from your computer's webcam or from the Pi's camera. When you use your computer's webcam, Teachable Machine captures the samples directly from the browser--super quick and easy! When you use the Pi camera, you'll need to run a script to generate the samples, transfer them to your computer, and upload them.

For best results, you should capture samples using the camera you want to use. But, a MacBook Pro webcam worked well enough for us, and it's much easier to use. So, we suggest you first try to use your computer webcam, and use the Pi camera if the model doesn't work well on the Pi.

Before you start

Be sure you've followed the steps in Create Categories first.

Though this method should work well enough, be warned that the model might not perform differently on the Pi because it uses a different camera. If this happens, you can try the next method to capture samples directly from the Pi camera.

Capturing the Samples

You should have Teachable Machine up on your laptop or desktop to a screen like this:

screen_7

Now, click the Webcam button. You might need to allow the page access to your computer camera.

webcam_8

Click and hold the Hold to Record button to capture samples!

 record_9

Samples will appear next to the webcam image.

sample_10

Try to capture as many unique samples as you can. Remember:

  • Try to capture around 200 samples per category

  • Capture different angles and light levels

  • Make sure the samples are as representative of the object as they can be

  • Try to move the camera around so that the only thing in common between all of the sample images for a given object is the object itself

Use Raspberry Pi Camera

Before you start

Be sure you've followed the steps in Create Categories first.

Setting up the Raspberry Pi

First, follow the instructions in Raspberry Pi Setup. This will load the software onto the Pi.

Launch the capture script

SSH to the pi or open a Terminal. Then, run these commands to set up the shell:

Copy Code
$ cd rpi-vision
$ sudo bash
# source .venv/bin/activate

Get ready to capture the first samples. Then, at the same shell, type:

Copy Code
# python3 tests/pitft_capture.py 
pygame 1.9.6
Hello from the pygame community. https://www.pygame.org/contribute.html

Ready. Press ENTER to toggle capture/standby. Press Ctrl+C to quit.    

You may need to adjust the focal distance of your Pi camera by rotating the lens. The Raspberry Pi Camera Board v2 includes a handy adjustment wheel.

At this point, the Raspberry Pi display should look like this.

mode_11

Record some data

At this point, the STANDBY text indicates that the Pi is not recording data. Make sure the camera is pointed at your object, then press ENTER to toggle between STANDBY and RECORD modes.

In RECORD mode, the script is capturing frames and saving them to the Pi's SD card. The display looks like this.

Press ENTER to toggle between STANDBY and RECORD modes.

standby_12

Be sure you see the frame count increasing. This means that the Pi is saving data to the SD card.

When finished, press CTRL + C to stop the process.

Copy images to your desktop/laptop computer

Here we show you how to use either samba or scp to copy the generated tar to your desktop/laptop for use with Teachable Machine.

Using Samba

The easiest way is to setup your Raspberry Pi as a file server using Samba. Follow these steps.

Now, copy the generated tarball into your samba share:

Copy Code
$ cp ~/rpi_vision/<<OBJECT_NAME>>.tar /share

On your local desktop, look for the RASPBERRYPI machine on your network. Connect to the share and copy the tar to your local machine.

tar_13

Using scp

On your local machine (i.e. not the raspberry pi), run:

Copy Code
$ scp pi@raspberrypi.local:~/rpi_vision/<<OBJECT_NAME>>.tar .

Be sure to change <<OBJECT_NAME>>.tar to the actual path you specified to your pitft_capture.py command above.

Upload images to Teachable Machine

Extract the tar by double-clicking it. On Windows, you may need a utility like 7-zip.

Now, in the Teachable Machine UI, follow these steps:

Click the Upload button next to the class box these images belong to.

upload_14

Now drag-n-drop the images from your file browser onto the dialog.

You can also click on the folder to find them from within the browser.

images_15

When done, the box looks like this.

box_16

Repeat this process for all categories in your project.

Training

When you've finished the last page (either Use Computer Webcam or Use Raspberry Pi Camera, your screen should look like the image below. Now you're ready to start training.

training_17

Run Training

Follow these steps to run the training process.

Now click Train and leave the tab open and visible. The training process happens in JavaScript on your own machine and will be slow or stalled if the browser window is left in the background.

model_18

You may see a dialog telling you that the page is running too slowly. Don't click Kill Page! You'll need to start over again.

While training is in progress, you'll see a progress bar. Training should take around 5 minutes or less using the default 50 epochs.

progress_19

Previewing

After training, you can use your computer's webcam to try out the model. You can also upload images taken from the Pi.

previewing_20

Tweaking advanced settings

Sometimes your model may not perform as well as you like on the first run. There are a couple of things you can do in this situation:

  • Run for more epochs. This is the easiest thing--just click the Advanced drop-down in the Training box and change the number of epochs. Your training time will increase more-or-less linearly with the number of epochs. Try 100 or 200 to start.

  • Use different samples. This will produce the most change in your results but takes more time.

Raspberry Pi Setup

If you already captured images from the Raspberry Pi camera, you don't need to do this page twice.

pi_21

Hardware

The camera and touchscreen display are attached to the Raspberry Pi. Plug in the camera first, then the touchscreen. Be sure the Pi is not powered while assembling hardware.

Here are the links to instructions for the hardware we use in this guide:

  • Camera Install Instructions

  • Touchscreen Installation: The PiTFT just needs to be attached to the 2x20 header so that the board is stacked directly on top of the Pi. The PiTFT module should fit snugly enough in the header port that you shouldn't need to attach any spacers.

Stabilizing the camera

Attach the camera to a larger, more stable object so that it doesn't bounce around on the cable. I taped the camera to the box it shipped in, like so:

camera_22

Software

Follow the Initial Setup and TensorFlow Lite 2.0 Setup steps. You can stop when you reach the Running the Graphic Labelling Demo section.

Running on the Pi

Exporting the SavedModel

The first step is to export your shiny new model in SavedModel format. This makes it easy to transfer all of the files needed to the Pi, since it comes in a zip file.

Click Export Model in the Preview box.

export_23

In the dialog that appears, choose TensorFlow and be sure the SavedModel button is selected, as shown below.

Then, click Download my model. After a minute or two, your browser will save a converted_savedmodel.zip file.

projects_24

Running the model on the Pi

When you clicked the Download my model button in the last step, your browser should have saved a file called converted_savedmodel.zip. Now you need to place this on your Raspberry Pi.

You can transfer the model to the Raspberry Pi using scp:

Copy Code
$ scp <<PATH_TO_DOWNLOADS>>/converted_savedmodel.zip pi@raspberrypi.local:~

NOTE: You might need to adjust the first path in the command above to point to your Downloads folder.

Now, SSH to your Pi and run:

Copy Code
$ cd rpi-vision
$ sudo bash
# source .venv/bin/activate
# python3 tests/pitft_teachablemachine.py ../converted_savedmodel.zip

It will take some time to load the model into memory. During this time, you'll see the BrainCraft logo appear on the display. Afterwards, point your rpi camera and try it out!

part_25

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.