Here are some of the advantages that CypherLinx® offers: The first advantage is that CypherLinx transmits in a truly serial fashion. Most competitive products use PWM to represent digital data. Because RF links introduce jitter, stretching, and contraction of the bits, this method is problematic and impacts range and reliability. Serial data is sampled at the center of each bit, so jitter at the edges does not have any effect on the interpretation of the bit. Experimental testing shows that this can improve performance by as much as 7dB to 9dB. The next advantage is excellent responsiveness. Responsiveness refers to the lag time between when a user pushes a button and something happens on the other end. This may be a concern because of the user’s perception or a more significant factor, such as safety.