When considering which cloud provider option to use with AE-CLOUD2, the chart shown here compares some of the key features and differences between each of the options. The Cloud Toolbox Demo supports the AE-CLOUD2 and AE-CLOUD1 kits. For visualizing the sensor data, a Renesas created dashboard is provided, which allows the user to quickly visualize their sensor data in as little as 10 minutes. For the Cloud Toolbox Demo, access to the AWS IoT, Microsoft Azure™ IoT Hub, and Google Cloud™ IoT Core services are managed using a master account created by Renesas that allows a single login account to switch between the cloud providers. The cost of the cloud accounts is also managed by Renesas. The Cloud Toolbox is suitable for demo only and it is not meant for production. The Cloud Application projects that connect to Amazon, Google, and Microsoft support the AE-CLOUD2 kit and PK-S5D9 board. Users are responsible for creating their own visualization tool such as a dashboard or website. Additionally users need to sign up and pay for any costs associated with using the services from the specific cloud provider. The Cloud Application projects serve as a great starting point for developers who want to create a production IoT design and need a starting point for their work. The Medium One IoT Prototyping Sandbox supports the AE-CLOUD2 and AE-CLOUD1 kits. Medium One provides a pre-built dashboard where users can customize their visualization from a selection of widgets. The users can create their own account free of charge that would be used to access the Medium One cloud environment. For developers who want to quickly build a prototype can start with the Medium One IoT Prototyping Sandbox and then easily convert their prototype into a production design.