Achieving RF Performance and Approvals
באדיבות ‎Convergence Promotions LLC
2011-03-03
Antenna design may seem to be as much art as science, but by following a few simple design rules you can reliably hit your performance and approval targets.
Before selecting the antenna or antenna design and defining the mechanical specifications for a wireless product the product designer must clearly understand the RF performance targets the product must reach in order to:
- Achieve good RF performance in the field to ensure market success and
- Pass all regulatory and operator approvals.
The basic concepts — TRP, TIS, and RSE
For cellular applications such as GSM or CDMA, basic RF performance is measured in terms of the product being able to transmit and receive reliably on a network. The scientific way to measure performance is in an anechoic chamber.
The measurements numbers used are outlined below:
- TRP – Total Radiated Power
This defines how much power is being radiated from the device and is measured in dBm. The higher this number, the better the device is able to transmit. - TIS – Total Isotropic Sensitivity
TIS – Total Isotropic Sensitivity This defines how low a signal the device can receive and demodulate. The lower this number (with a minus figure) the better the device can operate in weak signal environments. - RSE — Radiated Spurious Emissions
In practice this is the most difficult test for cellular products to pass, from Taoglas’ experience. These are radio waves output by the device which are above the power limit set by regulatory authorities to avoid interference. When a test confirms a radiated spurious emission over the limit either the device or the antenna must be modified to get it below the limit and thus pass certification. Otherwise the device cannot be sold in that country.
Wireless products are regulated in each country by slightly different standards. Taoglas, in co-operation with certified test labs, can advise on the exact regulations a product must conform to and provide a test plan.
In Table 1 are targets to reach for passing most but not all operator TRP/TIS approvals. Some operators have specific targets for certain products or applications so you need to confirm individually. In any case these are the numbers any designer should target for their device.
| Maximum Conducted Power |
TRP | Maximum Conducted Sensitivity |
TIS | |
| GSM 850 | 33 | 22 | -109 | -99 |
| GSM 900 | 33 | 23 | -109 | -100 |
| GSM 1800 | 30 | 24 | -109 | -101 |
| GSM 1900 | 30 | 24.5 | -109 | -101 |
| UMTS/HSPA/HSPA+/WCDMA 850 | 23 | 13 | -109 | -97 |
| UMTS/HSPA/HSPA+/WCDMA 1700 | 23 | 18.5 | -109 | -101 |
| UMTS/HSPA/HSPA+/WCDMA 1900 | 23 | 18.5 | -109 | -101 |
| UMTS/HSPA/HSPA+/WCDMA 2100 | 23 | 18.5 | -109 | -101 |
Table 1: TRP and TIS performance targets (all figures in dBm).
If your operator does not have a stated standard, or their standard is not mandatory, it is advisable to aim for these, or higher, numbers in order to accomplish the best industry standard.
Your product can in many cases still function normally below these values, there is no industry set cut-off for operation. It will depend on the actual application environment and your own conditions for what is acceptable in terms of reliability and the outcome of your own product field tests.
How are these TRP and TIS numbers calculated?
TRP
For TRP we have to work backwards from the maximum power allowed from a RF module. For most cellular modules this is capped by the FCC at 33 dBm for GSM 850 and 30 dBm for GSM 1900.
Let’s take a specific example. Usually the module will be set at a slightly lower power rating than maximum allowed. This would mean at GSM 850 with a power level of 32 dBm, this leaves us 10 dB of loss in the device to still pass the 22 dBm target. This sounds like plenty of margin but there are a lot of losses in the system.
As the RF signal passes down a cable or a transmission line on the device board it easily loses 4 dB or more. 4 dB loss is more than half the loss of the original power coming from the module.
- When the signal reaches the antenna and is radiated out into the air, it will also inevitably lose more.
- So 32 dBm – 4 dB = 28 dBm, meaning we need to reduce the loss from the antenna side to -6 dB or less.
- This -6 dB loss is equivalent to saying the antenna has an average gain of -6 dB.
- Therefore we need to design an antenna that has better than average gain of -6 dB for the device to reach the TRP performance required.
For TIS, a similar calculation can be done. For example, knowing that a network operator for GSM 850 has set a signal strength greater than -99 dBm, we can work backwards to what losses are allowed in the device for the device to still operate on the network.
The majority of cellular module sensitivity is around -109 dBM, therefore the device can sustain another 10 dB in loss on the antenna and transmission lines/cable and still reach the operator requirements.
- This means in theory again we can budget for -4 dB loss for example in the transmission line (could be less or more).
- It leaves us -6 dB in loss for the antenna.
- This is equivalent to the antenna average gain of -6 dB which is usually possible for the antenna designer to do.
What can Taoglas do to help?
Designing an optimized RF device depends on many parameters, both electrical and mechanical. Fortunately, Taoglas can utilize our experienced engineers, unparalleled range of antennas, and real industry experience to come out with a solid reliable process to enable a customer’s product to succeed.
Antenna type, layout, and design
Below are some simple rules to follow for the mechanical dimensions of a product which can pass the strictest operator TRP/TIS requirements. I am sure you are asking yourself — why did I used mobile phones that clearly violate these guidelines? Firstly they may not have targeted the above figures for device efficiency but if you look closely, most mobile phones do adhere to the guidelines below. Certain operators negotiate directly with mobile phone companies on lower TRP/TIS standards on their device on a case by case basis. These options are unlikely to be available to M2M devices.
| (A) | Ground planes < 65 mm long For a ground plane with a length of less than 65 mm (and 40 mm wide) the only solution is a complete custom antenna. The type of antenna material and design will vary from device to device and the process should begin at the start of the product design process. |
| (B) | Ground planes > 65 mm long |
| (i) On-board Antenna Solutions — minimum width needs to be 40 mm. |
PA-25a ceramic antenna
- Cleared area needs to be all the way across the short side of the board.
- From module side to antenna it requires 10 mm clearance to metal.
- Other sides must be completely free of metal.

Figure 1:PA-25a ceramic antenna.
Custom metal PIFA antenna
- Can work directly on ground plane on center edge of PCB minimum height of elements 10 mm, length 60 mm, and width 25 mm.
- Clearance to other metal components ideally 20 mm or greater in all directions.

Figure 2: Custom metal PIFA antenna.
| (ii) Off-board Antenna Solutions — Ground plane width of the device needs to be greater than 20 mm. | |
| A proven example is 80 mm x 40 mm of ground plane and 20 mm of clearance from antenna to metal, but in theory the ground plane of the device can be smaller. |
Flexible circuit antenna — FXP14
- Can be mounted to the inner plastic housing of the device.
- Minimum clearance of 20 mm from metal in all directions.
- Mount at right angles (perpendicular) to any main-board.
- Cable should be shorter than 150 mm, but not less than 80 mm.
- Place antenna away from noise/activity sources.

Figure 3: Flexible circuit antenna — FXP14.
PIFA on housing
- Dimensions approximately 60 mm x 20 mm x 10 mm.
- 20 mm clearance to metal.
- Spring contact can be used for connection.

Figure 4: PIFA on housing.
Rigid PCB FR4 antenna – PC.30
- Can be mounted to the inner plastic housing of the device.
- Minimum clearance of 20 mm from metal in all directions.
- Mount at right angles (perpendicular) to any main-board.
- Cable should be shorter than 150 mm, but not less than 80 mm.
- Place antenna away from noise/activity sources.

Figure 5: Rigid PCB FR4 antenna — PC.30.
PTCRB
For cellular wireless products sold in the USA, Canada, and other regions, it is necessary to apply for PTCRB approval from the CTIA wireless association.
A designated lab will test your product to establish if it meets the requirements.
PTCRB itself does not set minimum pass/fail standards for TRP/TIS, but there is a strict RSE standard - higher than the traditional FCC test standard. So you can actually pass RSE and get PTCRB even with compromised device performance (if TRP and TIS are not considered).
Individual operators may specify their own TRP/TIS test standards and even more tests before they will accept your device on their network. Taoglas can assist wireless device designers in meeting these approvals first time around.
Disclaimer: RF design is inherently difficult. Taoglas provides this article as a reference only and cannot be held responsible for errors or omissions in this information or for the performance of devices that use this above information. Users are advised to discuss with a Taoglas representative for a formal solution proposal before proceeding on any design.
מיאון אחריות: דעות, אמונות ונקודות מבט המובעות על ידי מחברים שונים ו/או משתתפי פורום באתר אינטרנט זה לא בהכרח משקפות את הדעות, האמונות ונקודות המבט של חברת DigiKey או את המדיניות הרשמית של חברת DigiKey.