Building Scalable Embedded Systems with Zephyr RTOS and NXP Semiconductors Platforms

מאת ‎Etiido Uko

באדיבות ‎DigiKey's North American Editors

Embedded systems have always involved tradeoffs, and engineers have had to choose between performance and power, flexibility and determinism, or speed to market and long-term maintainability. For the most part, these tradeoffs were manageable. Hardware was constrained, requirements were narrow, and a microcontroller might do little more than read a sensor or handle a simple user interface, often using bare-metal firmware written directly around a single control loop.

That is no longer the case. Modern embedded systems are being built to do far more. IoT devices, industrial automation controllers, and edge computing nodes are now required to support wireless connectivity, security stacks, over-the-air firmware updates, and multi-protocol communication simultaneously and reliably, often on resource-constrained microcontrollers with tight power and memory budgets. Bare-metal development does not scale well in that environment.

When multiple functions must operate concurrently, each with different timing requirements and priorities, a sequential control loop quickly becomes difficult to manage. Development teams end up spending weeks writing custom schedulers, porting drivers, and resolving low-level integration conflicts just to get the system working reliably.

An embedded real-time operating system addresses this by managing concurrent tasks, allocating processor time, and guaranteeing that time-critical operations execute predictably. However, task scheduling alone is not sufficient for modern embedded systems. System designers need networking stacks, security libraries, Bluetooth support, and broad hardware compatibility, all maintained and production-ready within a single framework. Zephyr RTOS provides exactly this.

A foundation for embedded firmware development

Zephyr is an open-source embedded real-time operating system (RTOS) hosted under the Linux Foundation. It supports platforms ranging from low-power Cortex-M microcontrollers to more capable edge-class processors, allowing the same software framework to scale across a wide range of embedded applications.

The system is built around a modular, Kconfig-driven architecture that allows developers to select only the subsystems their application requires, such as networking stacks, Bluetooth Low Energy (BLE), USB device support, cryptographic libraries, file systems, and power management features. Anything not selected is excluded at compile time, enabling the firmware to scale with the application rather than a fixed operating system footprint. This flexibility is critical in resource-constrained firmware development.

At the kernel level, Zephyr provides preemptive, priority-based scheduling with bounded interrupt latency and configurable tick resolution. This deterministic real-time behavior allows time-critical operations, such as motor control, sensor sampling, industrial control loops, and wireless communication tasks, to execute predictably even in multi-threaded environments.

The hardware abstraction model exposes peripherals like GPIO, SPI, I2C, and PWM through stable APIs, regardless of the underlying silicon. By using board support packages (BSPs) to map these interfaces to specific hardware, Zephyr allows developers to write portable firmware that avoids platform-specific register configurations, significantly reducing the effort needed to migrate or scale embedded systems designs.

Beyond the kernel, Zephyr includes production-ready subsystems for Bluetooth 5.x, IEEE 802.15.4, a native TCP/IP stack, MQTT, CoAP, TLS via Mbed TLS, and secure bootloading through MCUboot. These components are actively maintained, tested on real hardware, and widely used in commercial products, reducing the need for developers to independently assemble and validate the software stack (Figure 1).

Image of NXP Zephyr RTOS architecture diagramFigure 1: The Zephyr RTOS architecture diagram, showing the full software stack from the platform layer through the kernel, OS services, and application services to the application layer. (Image source: NXP Semiconductors)

Zephyr provides a strong software foundation for modern embedded development. However, realizing its full capabilities in a production design equally depends on the ecosystem of the hardware it runs on. A silicon vendor's BSPs, peripheral drivers, and toolchain alignment all determine how completely Zephyr's capabilities translate into working firmware. Where these are incomplete or immature, integration problems surface late in the development cycle, where they are most costly to resolve.

The importance of the hardware ecosystem in embedded systems

The gap between RTOS capability and hardware readiness is where the strength of the underlying silicon ecosystem becomes a critical engineering consideration. NXP Semiconductors closes this gap with industry-leading Zephyr support across its broad portfolio of microcontrollers and processors.

As one of the six founding members of the Zephyr Project, NXP Semiconductors helped shape its architecture and direction under the Linux Foundation from the very beginning. This foundational involvement is reflected in the depth, consistency, and wide range of NXP's Zephyr support today.

NXP currently offers more than 40 hardware platforms with Zephyr OS support, spanning low-power wireless MCUs, high-performance crossover processors, secure IoT endpoints, and automotive-grade controllers with CAN FD connectivity. Across all of these, Zephyr board support is maintained and aligned with each platform's capabilities, giving development teams access to a consistent software framework across the full range of NXP hardware.

NXP Semiconductors achieves this compatibility by contributing directly to Zephyr RTOS’s core subsystems, upstream driver development, and platform enablement within the mainline codebase, not as vendor-specific forks or out-of-tree patch sets. NXP Semiconductor hardware support stays current with every quarterly Zephyr release, covering new networking features, security subsystem improvements, and kernel updates. As a result, development teams do not have to wait for a separate vendor SDK update to access new Zephyr features, as support for these features is already upstream.

NXP's tooling completes this alignment. MCUXpresso IDE, LinkServer, and Visual Studio Code with the MCUXpresso extension all integrate with Zephyr's west-based build system, giving development teams a consistent environment from first bring-up through to production. J-Link debug probe support with SEGGER Ozone enables thread-aware debugging directly within Zephyr applications. The company also provides getting-started guides, lab guides, application notes, and training resources specifically for Zephyr development on its hardware.

For teams deploying Zephyr RTOS in production, NXP Semiconductors' combination of founding involvement, broad hardware support, active upstream contributions, and aligned tooling makes it a strong, coherent hardware foundation for reliable embedded systems.

From development to deployment: Zephyr and NXP in practice

The practical value of combining Zephyr RTOS with NXP Semiconductors hardware becomes most apparent during firmware development and implementation. Rather than manually assembling large portions of the software stack when building embedded systems, developers can begin prototyping on supported NXP evaluation platforms using pre-integrated development infrastructure aligned with Zephyr workflows.

For most projects, the natural starting point is an NXP FRDM or EVK development platform. The FRDM-MCXN947 (Figure 2), for example, ships with full Zephyr BSP support. Engineers can flash the board, run a working sample, and go straight to peripheral exploration with minimal setup. Peripheral configuration follows Zephyr's devicetree model, in which hardware settings are defined declaratively rather than via platform-specific register configurations.

Image of FRDM-MCXN947 evaluation board for the NXP MCX N947 dual-core Cortex-M33 MCUFigure 2: The FRDM-MCXN947 evaluation board for the NXP MCX N947 dual-core Cortex-M33 MCU, featuring an onboard MCU-Link debug probe and full Zephyr BSP support. (Image source: NXP Semiconductors)

Adding a peripheral, such as an SPI sensor or a CAN transceiver, becomes a matter of selecting the appropriate driver and updating a devicetree overlay rather than writing initialization code from scratch. Implementing networking and security follows the same pattern. BLE connectivity, encrypted transport via Mbed TLS, and OTA firmware updates through MCUboot are all available as existing Zephyr subsystems, configured through Kconfig.

The result of combining Zephyr RTOS with NXP Semiconductors hardware is a development workflow that gets embedded teams to application-ready firmware faster. This advantage is particularly valuable in applications where development timelines, reliability, and scalability are critical, including:

  • Industrial automation: Industrial controllers and fieldbus gateways require deterministic scheduling, robust CAN support, and long product lifecycles. The MIMXRT1176CVM8A's dual-core architecture, with its Cortex-M7 and Cortex-M4 cores, allows real-time control loops and communication tasks to be managed on separate cores with the RTOS scheduling both independently.
  • Low-power IoT devices: These devices benefit directly from Zephyr's modular networking and power management support. The FRDM-MCXW71, NXP Semiconductor's development platform for battery-powered IoT end nodes, integrates a Cortex-M33 application core with multiprotocol wireless connectivity, including BLE and Thread. Running Zephyr RTOS, it can use tickless idle and radio duty cycling to balance connectivity with battery life. The power management logic sits in the RTOS while the application handles sensor behavior.
  • Edge computing: The MIMXRT685SFVKB, which integrates a HiFi4 DSP and Ethos-U55 neural processing unit alongside its Cortex-M33 core, supports applications that combine real-time data acquisition with local inference (Figure 3). Running TensorFlow Lite Micro on Zephyr for this platform enables applications such as predictive maintenance without offloading processing to the cloud.

Image of NXP MIMXRT685SFVKB crossover MCUFigure 3: The MIMXRT685SFVKB crossover MCU combines an Arm Cortex-M33 core with a Cadence Xtensa HiFi4 DSP. (Image source: NXP Semiconductors)

While these are among the most common applications, the combination of the Zephyr RTOS and the NXP semiconductor ecosystem is well-suited to any embedded application that demands performance and reliability.

Conclusion

As embedded systems grow more demanding, the software and hardware foundations they run on are increasingly critical. Zephyr RTOS provides the modular, scalable software framework that modern embedded firmware development requires. NXP Semiconductors, as a founding member of the Zephyr Project with broad hardware support, upstream contribution, and aligned tooling, translates this framework into a deployable, production-ready platform.

DigiKey logo

מיאון אחריות: דעות, אמונות ונקודות מבט המובעות על ידי מחברים שונים ו/או משתתפי פורום באתר אינטרנט זה לא בהכרח משקפות את הדעות, האמונות ונקודות המבט של חברת DigiKey או את המדיניות הרשמית של חברת DigiKey.

אודות כותב זה

Image of Etiido Uko

Etiido Uko

Etiido Uko is a mechanical engineer and senior technical writer with over a decade of experience producing authoritative content on engineering, manufacturing, and emerging industrial technologies. His work sits at the intersection of technical depth and clear communication, helping engineers, product developers, and decision-makers understand complex systems and apply them in real-world contexts. His work spans content creation for industry leaders across multiple sectors, including Autodesk, Siemens, Xometry, Telus, and Coca-Cola. Known for his rigorous research standards and attention to technical accuracy, he combines engineering knowledge with strong editorial discipline. Beyond writing, Etiido maintains a strong interest in the evolution of engineering and technology.

אודות מוציא לאור זה

DigiKey's North American Editors