Temperature Sensors: The Basics
באדיבות ‎Electronic Products
2011-10-27
Temperature sensors are used in diverse applications such as food processing, HVAC environmental control, medical devices, chemical handling and automotive under the hood monitoring (e.g., coolant, air intake, cylinder head temperatures, etc.). Temperature sensors tend to measure heat to ensure that a process is either; staying within a certain range, providing safe use of that application, or meeting a mandatory condition when dealing with extreme heat, hazards, or inaccessible measuring points.
There are two main flavors: contact and noncontact temperature sensors. Contact sensors include thermocouples and thermistors that touch the object they are to measure, and noncontact sensors measure the thermal radiation a heat source releases to determine its temperature. The latter group measures temperature from a distance and often are used in hazardous environments.
Temperature sensor types
Thermocouples
A thermocouple (TC) is a pair of junctions that are formed from two different and dissimilar metals. One junction represents a reference temperature and the other junction is the temperature to be measured. They work when a temperature difference causes a voltage (See beck effect) that is temperature dependent, and that voltage is, in turn, converted into a temperature reading. TCs are used because they are inexpensive, rugged, and reliable, do not require a battery, and can be used over a wide temperature range. Thermocouples can achieve good performance up to 2,750°C and can even be used for short periods at temperatures up to 3,000°C and as low as –250°C.
Strengths and challenges of thermocouples include:
- They measure their own temperature.
- The temperature of the object must be inferred, and the user must be sure there is no heat flow between them.
- They are prone to temperature-reading mistakes after long use. Reasons? If insulation of the wires loses resistance because of moisture or thermal conditions, or if there are chemical, nuclear radiation, or mechanical interference in the environment.
- They are electrical conductors so they cannot contact another source of electricity.
- They do not measure at the junctions.
- These devices react rapidly when compared with resistance thermometers.
Thermistors, like thermocouples, are also inexpensive, readily available, easy to use, and adaptable temperature sensors. They are used, however, to take simple temperature measurements rather than for high temperature applications. They are made of semiconductor material with a resistivity that is especially sensitive to temperature. The resistance of a thermistor decreases with increasing temperature so that when temperature changes, the resistance change is predictable. They are widely used as inrush current limiters, temperature sensors, self-resetting overcurrent protectors, and self-regulating heating elements.
Thermistors differ from resistance temperature detectors (RTD) in that (1) the material used for RTDs is pure metal and (2) the temperature response of the two is different. Thermistors can be classified into two types; depending on the sign of k (this function refers to the Steinhart-Hart Thermistor Equation to convert thermistor resistance to temperature in degrees Kelvin). If k is positive, the resistance increases with increasing temperature, and the device is called a positive temperature coefficient (PTC) thermistor. If k is negative, the resistance decreases with increasing temperature, and the device is called a negative temperature coefficient (NTC) thermistor.
As an example of NTC thermistors, we will examine the GE Type MA series thermistor assemblies designed for intermittent or continual patient temperature monitoring. This application demands repeatability and fast response, especially when used with the care of infants and during general anesthesia.
The MA300 (Figure 1) makes routine continuous patient temperature monitoring feasible by using the convenience of the patient’s skin site as an indicator of body temperature. The stainless steel housing used is suitable for both reusable and disposable applications, while maintaining maximum patient comfort. Nominal resistance values of 2,252, 3,000, 5,000, and 10,000 Ω at 25°C are available

Figure 1: GE’s MA300 thermistor assembly is made of stainless steel with medical-grade PVC Teflon insulation. (Courtesy of GE.)
Resistance temperature detectors
Resistance temperature detectors (RTDs) are temperature sensors with a resistor that changes resistive value simultaneously with temperature changes. Accurate and known for repeatability and stability, RTDs can be used with a wide temperature range from -50°C to 500°C for thin film and -200°C to 850°C for the wire-wound variety.
Thin-film RTD elements have a thin layer of platinum on a substrate. A pattern is created that provides an electrical circuit that is trimmed to give a specific resistance. Lead wires are attached, and the assembly is coated to protect both the film and connections. In comparison, wire-wound elements are either coils of wire packaged in a ceramic or glass tube, or they can be wound around glass or ceramic material.
An RTD example is Honewell’s TD Series used for such applications as HVAC — room, duct and refrigerant temperature, motors for overload protection, and automotive — air or oil temperature. Within the TD Series, the TD4A liquid temperature sensor is a two- terminal threaded anodized aluminum housing. The environmentally sealed liquid temperature sensors are designed for simplicity of installation, such as in the side of a truck, but are not designed for total immersion. Typical response time (for one time constant) is four minutes in still air and 15 seconds in still water.

TD Series temperature sensors respond rapidly to temperature changes (Figure 2) and are accurate to ±0.7C° at 20C°—and are completely interchangeable without recalibration. They are RTD (resistance temperature detector) sensors, and provide 8 Ω/°C sensitivity with inherently near-linear outputs.
RTDs have a better accuracy than thermocouples as well as good interchangeability. They are also stable over the long term. With such high-temperature capabilities, they are used often in industrial settings. Stability is improved when RTDs are made of platinum, which is not affected by corrosion or oxidation.
Infrared sensors
Infrared sensors are used to measure surface temperatures ranging from -70 to 1,000°C. They convert thermal energy sent from an object in a wavelength range of 0.7 to 20 um into an electrical signal that converts the signal for display in units of temperature after compensating for any ambient temperature.
These sensors are used to measure temperature when:
- Thermocouples or probes cannot be used.
- If the target object is in motion (on rollers, moving machinery, conveyor belts).
- If the target object is in a vacuum.
- If there is a hazard such as high voltage.
- If distances are great.
- If temperatures are too high for contact sensors.
- When a very fast response is required.
A recently announced product, the Texas Instruments TMP006, (Figure 3) is an infrared thermopile sensor in a chip-scale package. It is contactless and uses a thermopile to absorb the infrared energy emitted from the object being measured and uses the corresponding change in thermopile voltage to determine the object temperature.

Infrared sensor voltage range is specified from –40° to 125°C to enable use in a wide range of applications. Low power consumption along with low operating voltage makes the part suitable for battery-powered applications. The low package height of the chip-scale format enables standard high volume assembly methods, and can be useful where limited spacing to the object being measured is available.
The use of either contact or noncontact sensors requires basic assumptions and inferences when used to measure temperature. So it is important to read the data sheets carefully and make sure you have an understanding of influencing factors so you will be confident that the actual temperature is the same as the indicated temperature.
מיאון אחריות: דעות, אמונות ונקודות מבט המובעות על ידי מחברים שונים ו/או משתתפי פורום באתר אינטרנט זה לא בהכרח משקפות את הדעות, האמונות ונקודות המבט של חברת DigiKey או את המדיניות הרשמית של חברת DigiKey.