Reducing Voltage Drop with Heavy-Duty Extension Cables
When using equipment with lengthy extension cords, typically 50 ft or longer, voltage drop becomes a concern as electricity traverses a greater distance. While this issue is often negligible for lower-wattage or lighter-duty appliances, it becomes more pronounced with heavier-duty equipment.
To mitigate voltage drop, AC Connectors has engineered heavy-duty cables with 12-gauge wire, typically used for 20 amps, and super-duty cables with 10-gauge wire, typically used for 30 amps. Despite their robust construction, these cables are designed for regular household usage, limiting the current to a maximum of 15 amps.
(Image source: AC Connectors)
It's important to note that the more wattage a piece of equipment draws, the greater the voltage drop over longer distances. This underscores the importance of using a higher wire gauge to minimize this drop. Our cords excel in applications such as power tools, yard work, and trickle charging for electric vehicles.
Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.
Visit TechForum