Webinar – Easy-To-Use Switch Mode Power Supply Matrix

Terms like intelligent power and the SMPS matrix sound like scientific lore, but to onsemi’s Switch Mode Power Supply (SMPS) developers and managers, these terms help to define state-of-the-art power supplies from low wattage to the kilowatt range in a wide array of voltages and customization levels. So, where does a designer start when choosing an SMPS?
Bob Card, onsemi’s Americas Marketing Manager for the Analog Mixed Signal Group (AMG), leads the tutorial by solving the problems associated with choosing the right power supply for specific applications and efficiency requirements. Using the SMPS matrix, Card will demonstrate the ease of locating the right supply based on parameters such as controller type, gate drivers, and even available MOSFETs.
The one-hour online webinar takes place on Wednesday, August 7, 2024, at 10 AM CDT. Even if you are unable to attend the live session, please be sure to register so we can send you a link to the recording when it is complete.
Register here: https://event.on24.com/wcc/r/4646000/B8BC94B3BD850C246E9C342D0E986085?partnerref=blog
Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.
Visit TechForum