• Preferred Supplier

Kingston Technology

Image of Kingston DataTraveler Duo USB Flash

DataTraveler Duo USB Flash Drive

Kingston® DataTraveler® Duo features dual USB connectors that work with both USB Type-A and USB Type-C®1 ports for maximum compatibility.

Image of Kingston IronKey Keypad 200 Series

Kingston IronKey Keypad 200 Series USB Flash Drive

The Kingston® IronKey™ Keypad 200 series are OS-independent hardware-encrypted USB Type-A and USB Type-C®1 drives with an alphanumeric keypad for easy-to-use PIN access.

Image of Kingston SATA Solid-State Drives

Kingston Industrial SSD - mSATA SSD TLC

Kingston Industrial SSDs incorporate advanced controllers that automatically perform wear-leveling, garbage collection and other NAND Flash management features. Kingston’s 2.5” SATA SSDs are a drop-in replacement for hard drives and deliver up to 20x greater performance as well as high reliability. Industrial SSDs incorporate next-generation 3D TLC NAND Flash for the best cost and reliability.

Tools and Support

סרטונים מוצגים

pSLC eMMC from Kingston PIO | DigiKey
pSLC eMMC from Kingston PIO | DigiKey
Unleashing the Power of Kingston’s DCM3000ME – The Ultimate Enterprise SSD
Unleashing the Power of Kingston’s DCM3000ME – The Ultimate Enterprise SSD
DigiKey at embedded world with Kingston Technology
DigiKey at embedded world with Kingston Technology
Clone an HDD to an SSD with Acronis True Image
Clone an HDD to an SSD with Acronis True Image
הצג הכול

אודות Kingston Technology

As the world’s largest independent manufacturer of memory product, Kingston Technology offers a wide variety of memory products (eMMC, eMCP, ePOP, DRAM components) to industrial and embedded OEM customers of all sizes globally. Kingston also offers a line of SATA and NVMe SSDs created specifically for system designers and builders.

"This distribution partnership with DigiKey greatly expands Kingston's presence in the design engineer community," said Sarah Shen, general manager of U.S. embedded business for Kingston. "As an established and trusted brand in the memory industry with over three decades of experience, we look forward to working with DigiKey."

Additional Content

KINGSTON ON SOCIAL MEDIA