What Are Power Line Filter Modules and Why Do You Need Them?

Line filters are components designed to suppress conducted EMI on power and signal lines. They prevent noise generated within a device from escaping into the power network, and just as importantly, block external interference from entering sensitive electronics. Without proper filtering, EMI can lead to data corruption, system malfunctions, premature component failure, or failure to meet global EMC standards.

TE Connectivity offers a broad portfolio of single‑phase, three‑phase (Delta) or three-phase (Wye), and DC line filters, engineered to handle a wide range of voltages, currents, and environmental conditions. These filtering solutions help ensure signal integrity and long-term reliability. The difference between Delta and Wye is the wires.  Delta has 3 wires – without neutral and Wye has 4 wires with the neutral line for common mode filters or single-phase loads.

Some examples of TE Connectivity Corcom’s inline power filters. (Image source: TE Connectivity Corcom)

Once you know the “phase”, you can then pick single, two, or three stage configuration on DigiKey’s Website. What is the difference between phase and state, you ask?  It all relates to whether you are focusing on the signal’s timing/distortion (phase) or the filter’s operating mode/behavior (state).

  • Phase refers to the time shift or delay different frequencies experience through the filter, affecting transient response and wave shape. Pick this if you are concerned with time-domain distortion.
  • State (often seen as "State Variable Filter") refers to the operational mode of the filter, such as simultaneously providing low-pass, band-pass, and high-pass outputs. Pick this one if you need functional versatility, such as classic analog sound quality.

TE Connectivity understands that not all applications are the same, and that is why their line filter offering covers a wide range of products from Corcom to Schaffner products. Schaffner was acquired by TE Connectivity in 2023 to broaden their footprint. This acquisition leveraged their combined strengths across the entire portfolio for their customers. (Source: Schaffner | Now part of TE Connectivity | TE Connectivity).

Commonly Power Line Filters are used in a variety of industries and applications, including:

  • Industrial automation and motor drives
  • Medical imaging and diagnostic equipment
  • Data centers and networking infrastructure
  • Aerospace and defense electronics
  • Renewable energy and power conversion systems

TE designs line filters that integrate seamlessly into modern electronic systems. Their solutions are developed with system‑level performance in mind, helping engineers reduce EMI at the source rather than relying on secondary fixes downstream.

Table 1 makes it easier to find your best fit solution, just click on any family/series to go right to DigiKey’s website. This represents just a snapshot of the more than 3,000 part number solutions offered by TE Connectivity. If there is something you need that is not on the list, please click this LINK to see the entire product offering.

Performance Category  Stage  Family / Series  Current Range  Notes 
Standard Performance Single Stage Filter FN332 1A-10A  
Standard Performance Single Stage Filter FN2450 1A-10A  
Standard Performance Single Stage Filter H style 3A-15A  
Standard Performance Single Stage Filter B style 1A-30A  
Standard Performance Single Stage Filter HT style 6A-15A  
Standard Performance Single Stage Filter FN2010 1A-60A  
Standard Performance Single Stage Filter K style 1A-60A earth line choke
Standard Performance Single Stage Filter FN2020 1A-60A  
Standard Performance Single Stage Filter SK style 3A-40A earth line choke
Standard Performance Single Stage Filter FN2030 (A, AZ, R, Z) 1A-30A  
Standard Performance Single Stage Filter FN350 8A-55A  
Standard Performance Single Stage Filter FN2410 / FN2412 8A-100A / 8A-42A  
High Performance Double Stage Filter FN343 1A-10A earth line choke
High Performance Double Stage Filter FN2415 6A-20A  
High Performance Double Stage Filter MV style 3A-20A  
High Performance Double Stage Filter HT/HQ style 15A / 3A-6A  
High Performance Double Stage Filter R style 1A-20A earth line choke
High Performance Double Stage Filter FN2060 (A & L) 1A-30A  
High Performance Double Stage Filter FN2070 1A-36A  
High Performance Double Stage Filter FC style / S style 6A-50A / 3A-60A  
High Performance Double Stage Filter EP/VP style 3A-20A  
High Performance Double Stage Filter FN2080 1A-16A  
High Performance Double Stage Filter Q style 3A-20A  
High Performance Double Stage Filter T style 3A-20A  
High Performance Double Stage Filter FN2090 1A-30A  
Very High Performance Triple Stage Filter FN700Z 6A-20A 2CM + 1DM choke
Very High Performance Triple Stage Filter FN352Z 6A-30A 1CM + 2DM choke
Lighting performance FB / FBL / FBH style 1A-20A  
Lighting performance MRI style (DC filter) 3A  

Table 1: Highlights of filters suitable for various performance needs. (Source: Kathy Hutton)

Summary

EMI control is essential in today’s noise-sensitive electronic environments. TE Connectivity’s line filters provide that proven, reliable way to protect system performance, ensure compliance and simplified design challenges. DigiKey helps you find the right filter to help you build cleaner, quieter, and more dependable electronics from Prototype to Production.

Additional Information

FN3297/FN3298 Series Three-Phase+N Filters

FN2640/FN2660 Single-Phase Low-Profile EMC/EMI Filters

FN222/FN223/FN224 Series DC-Busbar EMC/RFI Filter

FN3025/FN3026 Three-Phase Compact Lightweight Filters

FN2500 / FN2520 Single Phase EMC/EMI Filters

FN2410(H)/FN2412(H) Line Filters

FN3258 Series 3-Phase Filters

EMI/EMC Filtering Solutions for Medical Electronics

Have You Considered Everything in the Design of Your EMI Filter

אודות כותב זה

Image of Kathy Hutton

Kathy Hutton, Senior Supplier Business Development Manager at DigiKey, has been with DigiKey since 2003 and has responsibilities for interconnect, passive and electromechanical products. She is in daily communications with engineers/customers (both internal and external) to help drive sales with her extensive product knowledge. Kathy holds an Electrical/Automation Technical Degree and was part of the DigiKey Applications Engineering team prior to her role in Product Management. Outside of work, she is an avid fisherwoman, both competitively and just for some fun on the water.

More posts by Kathy Hutton
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum