Maker.io main logo

Laser Distance Measurements using Garmins LIDAR LITE v3HP

362

2018-10-03 | By John LeDuc

The idea of using light to measure distance is a bit mind-boggling, knowing that light travels at 186,000 miles a second, seems like it would be nearly impossible to measure distance accurately from one point to another however by combining a laser packaged with a photo sensor coupled with a very fast microcontroller, we can measure distance from one point to another down to a couple centimeters. One such product is the Garmin LIDAR-Lite v3HP (DigiKey Part No.1568-1867-ND) which is a High-speed Optical Distant Measurement Sensor with the following features:

  • Compact, lightweight, power-efficient ranging and proximity sensor with sturdy IPX7-rated housing for drone, robot or unmanned vehicle applications
  • Easy-to-use 40-meter laser-based sensor offers greater than 1 kHz measurement speed up to 10-meter distances — and improved accuracy at all distances
  • User configurability allows adjustment between accuracy, operating range and measurement time
  • Communicates via I2C and PW
  • Low power consumption; requires less than 85 milliamps during acquisition
  • Regulatory approvals: CLASS 1 LASER PRODUCT CLASSIFIED EN/IEC 60825-1 2014
  • This LIDAR is an ideal solution for use in drones, robots and or unmanned vehicles, or any device you can think of that may need an accurate distance measurement. It can even be used like radar to create topographic maps by a sweeping or a spinning motion and collecting distance points to display a picture.

    A project I used for a display at SparkFun’s AVC (DigiKey sponsored the event) and for displaying a project at Maker Faire New York, I combined some of our parts into a project, putting together the use of a SparkFun Red board edge (1568-1871-ND), the LIDAR (1568-1867-ND) a giant keyboard push button switch (1528-5306-ND), 3 large LED seven segment displays (1568-1912-ND) all housed into a DigiKey cardboard box.

    Looking at the figure below, when you press the large orange button, a program loaded into the UNO Red Board Edge (shown behind the clear plexiglass below the DigiKey logo), takes a measurement and displays the distance on the large LEDs (showing a measurement of 18 centimeters) For more information how this project was created click this link.

    Laser Distance Measurements using Garmins LIDAR LITE v3HP

    מק"ט יצרן # 08530
    DISPLAY LED 7-SEG 6.02" SGL RED
    SparkFun Electronics
    Add all DigiKey Parts to Cart
    Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.