Maker.io main logo

2019 Holiday Gift Guide

75

2019-12-02 | By ASHLEY

This year’s Holiday Gift Guide has you covered for everyone from the Electrician to the Maker in your life. The Gift Guide’s products are split into five categories to ease the process of finding just what you’re looking for this year.

The first set of products will please anyone on your list that is interested in robotics; but let’s be honest, who isn’t?

  • From SparkFun Electronics we have the Redboard Inventor’s Kit. This kit is perfect for someone looking to intermix programming and hardware. Detailed projects are included in the kit to cover five different sensor integrations and also familiarize the user with the C++ programming language and the Arduino Integrated Development Environment (IDE).
  • Next are two products featured together. The DigiKey edition of the :MOVE mini with bumper add-on and the :MOVE mini MK2. What’s so cool about these and why are we featuring two? The :MOVE minis are easy to program using either MakeCode's Graphical Block or JavaScript programming, and they are great for autonomous, Bluetooth, or radio control depending on the user’s preference. The DigiKey edition sports an awesome color scheme plus it includes the bumper which is typically purchased separately; while the MK2 is the original Kitronik color scheme, but with a few updates! The biggest update to the MK2 is the injection molded wheels with o-ring tires to provide better grip and mobility.
  • This Devastator Tank Mobile Robot Platform from DFRobot is spectacular for many reasons. This product comes with the chassis, assembly hardware, motors, wheels, and tracks, leaving the user to pick their choice of microcontroller. There is a recommended all-in-one board (Romeo BLE), but a Raspberry Pi or most Arduino-based boards also do the trick. This is great for users already experienced with a specific board where they may even have one on-hand already. Another cool thing about the Devastator? There are plenty of spaces on the aluminum chassis to add all kinds of sensors as well. Beginners to Engineers and everyone in between are sure to enjoy this kit.

The second set of products will actually please anyone on your list. No seriously, it’s all about lights and music. Who doesn’t love the blinkies and music?!

  • First up is a Bluetooth speaker from Klein Tools. This small speaker has many features that are ideal for a variety of environments. It has a 10 meter connectivity range, is drop protected up to 2 meters, has an IP45 rating (dust protection >1 mm, liquid protection water jets at 3 m), and has a 10 hour battery life. Another awesome feature is the variety of mounting options. There is a magnet on the back, a lanyard tie point, and a ¼-20 mount for standard tripods. While it is great in a semi-rugged environment, it is also a fitting gift for anyone that enjoys music on the go.
  • Next is another product combo. NeoPixels from Adafruit are an easy and fun way to add some flash and bling to any project. To feature this series we are showcasing a matrix and a strip, but there are plenty of other options within the series to fit any LED project need.
  • Last in this set is sort of a combination of the previous two products and then some. The Neotrellis M4 from Adafruit is an all-in-one NeoPixel and audio board powered by the SAMD51 microcontroller. This easy-to-use board can be programmed in the Arduino IDE or with Circuit Python in any text editor the user prefers. Like any Adafruit product, there is a Getting Started guide and multiple projects complete with full documentation and code examples.

The third set of products to go over will cover any fixer or tinkerer on your list.

  • Up first is the IFIXIT Pro Tech Toolkit from Pimoroni. If you’re a professional breaker like myself, you’ll need this kit in your tool arsenal. In the words of Pimoroni, it “contains all the poking, prying, gripping, lifting, ESD safety, and screw driving tools” you’ll need, whether you’re a pro or hobbyist.
  • Next, (I’m going out of order here but you’ll see why) are a couple of multimeters. Depending on preference or use, we have a manual ranging multimeter and an auto-ranging multimeter - both from B&K Precision. These both come with batteries, hangers, manuals, and test leads. The manual ranging also comes with a temperature probe. These sturdy, reliable and handy-to-have multimeters are a must for any level of designer or troubleshooter.
  • Last is the ultimate case from Serpac to house these tools and more for safekeeping. This particular case is 19.75” L x 15.53” W x 5.413” H and includes the foam inserts shown in the product photo. To top it off, this case is water and air tight with an IP67 rating.

This next set of products will cover any gamers on the list, from casual to hardcore.

  • The Arduboy from Seeed Technology is a compact (credit card sized), open platform game system powered by the ATmega32u4. It can be programmed using the Arduino IDE, Codebender, GCC, and AVRDude. Want to start playing and program later? There are plenty of published games that are free to play, or you can even download open source games to edit and make your own.
  • This is the latest version of the awesome desktop retro arcade machine from Pimoroni. The PiCade has new artwork, a dedicated power button, and comes with an 8 inch or 10 inch display! All you need to get started is the PiCade kit, a Raspberry Pi, USB-C power supply, and a micro SD card. When the company’s name stands for Pirate Monkey Robot Ninja, you KNOW their product has to be cool.
  • Last is another credit card sized gaming system from Seeed Technology - the Meowbit. The coolest feature about this product? You can program it with MakeCode arcade and Python, which allows implementation of hardware devices! Bridging the gap between the digital world of gaming and the physical world in a simple, user-friendly way.

The fifth and final set of products will cover a variety of people. Check out these products and you’ll understand why.

  • The Raspberry Pi 4 Model B is a versatile and powerful single-board computer. Creators will love the 64-bit quad-core processor, the dual micro HDMI ports that support up to 4K resolution, and all of the other amazing features on this board because honestly, we could go on and on.
  • Next is a product that goes hand-in-hand with the Raspberry Pi - a 7” touchscreen display. This TFT display is an 800 x 480 pixel, RGB (red, green, blue) graphic color touchscreen to help enhance Raspberry Pi projects so the user can make them interactive. Just think of all the awesome applications this could have!
  • Last in this set is the MeArm by Kitronic. This easy-to-assemble robot arm is controlled by the micro:bit (sold separately) - meaning it’s also easy to program! Users can choose from MakeCode, JavaScript, or Python. They’ve included example programming that can be found on the GitHub online repository to help users get moving quickly. Just assemble, download the code, power it up, and commence robotic arm wars! Or whatever other logical thing you’d do with such a cool robot…

Now that you definitely have some gift ideas (at least for yourself), go ahead and navigate through these categories to see what other COOL items you may stumble upon. The DigiKey website is full of all types of unique products you may never have thought we would carry. Best part? In-stock parts are always available for same day shipping when orders are placed by 8PM CT. Happy gifting!

מק"ט יצרן # CK_5624DK_01
:MOVE MINI W_BUMPER DK EDITION
Kitronik Ltd.
מק"ט יצרן # 5652
MOVE:MINI MK2
Kitronik Ltd.
מק"ט יצרן # DFR0305
ROMEO BLE ATMEGA328P/CC2540
DFRobot
מק"ט יצרן # ROB0128
DEVASTATOR TANK MOBILE ROBOT
DFRobot
מק"ט יצרן # 2547
ADDRESS LED MATRIX SERIAL RGB
Adafruit Industries LLC
TACTILE ON/OFF SWITCH WITH LEADS
מק"ט יצרן # 1092
TACTILE ON/OFF SWITCH WITH LEADS
Adafruit Industries LLC
מק"ט יצרן # 4020
ADAFRUIT NEOTRELLIS M4 WITH ENCL
Adafruit Industries LLC
מק"ט יצרן # 2706B
DMM W/TEMP MANUAL RANGING TOOL
B&K Precision
מק"ט יצרן # 2705B
DMM AUTO RANGING TOOL
B&K Precision
מק"ט יצרן # SE710F,BK
CASE PLAS 19.750"L X 15.530"W
Serpac
מק"ט יצרן # PIM469
PICADE - 10-INCH DISPLAY
Pimoroni Ltd
₪ 1,092.34
הצגת עוד Details
מק"ט יצרן # 102991182
KITTENBOT MEOWBIT CARDSIZED GRAP
Seeed Technology Co., Ltd
מק"ט יצרן # SC1227
GRAPHIC DISPLAY TFT RGB 7"
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.