Maker.io main logo

Creating Project Enclosures

3,001

2023-08-08 | By bekathwia

Creating the perfect enclosure is an important step in finishing any electronics project. It keeps your circuit safe while improving the function and look of your project! Here are a few different ways to make your own.

Image of Episode 11 Writeup - Creating Project Enclosures

Let's start with the most accessible enclosures made from materials you find around the house. Plastic takeout containers make great prototype enclosures. Just cut holes for wires and external interface components and mount everything inside using hot glue or double-sided tape.

Image of Episode 11 Writeup - Creating Project Enclosures

Recycled cardboard can provide a simple enclosure too. You can cut it into custom shapes and sizes to accurately fit your project's size.

Image of Episode 11 Writeup - Creating Project Enclosures

Foam core board is also an inexpensive material that can be easily cut and shaped. Foam core enclosures are lightweight yet sturdy, making them a better long-term choice than cardboard.

Image of Episode 11 Writeup - Creating Project Enclosures

For working with all three of these materials, I recommend a sturdy utility knife and a cutting mat, as well as a metal ruler for making straight cuts. Be very careful to keep your fingers out of the path of the blade.

Image of Episode 11 Writeup - Creating Project Enclosures

You might find that making a disposable prototype enclosure helps you visualize your project and iterate on your user interface without a lot of investment or waste. Then, you can head into the process of making a more sophisticated enclosure with a more certain idea of what will work.

Image of Episode 11 Writeup - Creating Project Enclosures

For a more polished and less DIY appearance, consider ready-made electronics project enclosures. These can provide a cleaner and more professional look, and often already have mounting spots for your circuit board. Waterproof enclosures are also available.

Image of Episode 11 Writeup - Creating Project Enclosures

But your search shouldn’t stop at boxes designed for electronics. You can also get clear plastic boxes designed for memorabilia display like hockey pucks and baseballs in a variety of sizes, and they work quite well.

Image of Episode 11 Writeup - Creating Project Enclosures

I am particularly fond of using shadowboxes as electronic enclosures because they offer a nice-looking display while being easy to add your components. You can use the glass along with some printer paper to diffuse some LEDs or leave it out to provide access to touch buttons and knobs.

Image of Episode 11 Writeup - Creating Project Enclosures

When drilling into plastic, I recommend using a step drill to avoid cracking it. These cone-shaped drill bits also work well on metal project boxes.

Image of Episode 11 Writeup - Creating Project Enclosures

Laser-cutting is a popular option for making enclosures, often from thin plywood, sheet acrylic, or even cardboard. There are a handful of laserable box generators online that make it easy to create an appropriately sized box based on your project dimensions.

Image of Episode 11 Writeup - Creating Project Enclosures

For a totally bespoke enclosure, 3D printing your own enclosure is an excellent option.

Image of Episode 11 Writeup - Creating Project Enclosures

First, use calipers to measure your project’s dimensions. You need accurate information to create the perfect fit. Record the length, width, and height of your circuit board, as well as the clearance needed and positioning for any components that need to protrude to the outside of the enclosure.

Image of Episode 11 Writeup - Creating Project Enclosures

Make a sketch of your object and use it to record the relevant dimensions. Even if it’s just a rough diagram, it will help you find a project box that will fit.

Image of Episode 11 Writeup - Creating Project Enclosures

Next, use a free 3D modeling program like Tinkercad or Fusion 360 to design your enclosure. Make sure to include necessary mounting points and openings for switches, connectors, and LEDs. Be sure to include a little extra space, called tolerance, since in real life the parts need to sit next to each other and can’t overlap.

You’ll find some exquisite examples of custom enclosure design online. Sometimes they have space for specific fastening hardware like nuts and bolts or heat-set inserts.

The basic strategy is to make a hollow box with holes in the right places for your components, but 3D design is a big topic, and there’s much more to learn! Here are some resources if you’d like to explore this more:

Image of Episode 11 Writeup - Creating Project Enclosures

Once you have your enclosure in 3D, you can print it out yourself or send off the file to be printed for you. The digital design will become a physical copy. Then you can put your components inside and determine if any revisions are needed. It’s normal to make several iterations and make improvements along the way.

If you want my recommendation for getting into 3D printing, it’s to get a basic FDM machine and some PLA filament, then branch out to different materials from there. Set it up in a space with ventilation– even just an open window.

Beyond 3D printing, you could also consider CNC milling for your enclosure as well. I’ve seen bespoke wooden and metal enclosures made this way that turned out super well.

So, there you have it! You can build a DIY enclosure for your electronics projects in a bunch of different ways, depending on what skills, tools, and materials you have available.

Check out the rest of this series for more information on getting started with electronics design!

מק"ט יצרן # 17610
LONG TRIGGER HOT GLUE GUN
Aven Tools
מק"ט יצרן # 3C301-NB
CALIPER 6" ELECT DGTL STEEL
TPI (Test Products Int)
מק"ט יצרן # 44302
FLICKBLADE UTILITY KNIFE
Klein Tools, Inc.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.