Maker.io main logo

Meet the Compute Module 5: What’s New and Improved?

2,610

2025-02-05 | By Travis Foss

Single Board Computers Raspberry Pi SBC

TL;DR: The Compute Module 5 introduces major upgrades, including 500MB/s eMMC bandwidth (4× faster), RAM options up to 16GB, and an expanded 64GB eMMC configuration, while retiring older 1GB and 8GB models. It replaces the former 2 lane MIPI interface with dual USB 3.0 ports for higher speed peripherals and maintains the CM4 style dual 100 pin form factor for compatibility with carrier boards. An updated ecosystem — including the CM5 Development Kit, a feature-rich IO Board (dual HDMI 2.0, dual 4 lane MIPI DSI/CSI 2, M.2 PCIe slot, GbE with PoE), and a protective IO Case — enables faster prototyping and more capable embedded designs.

Meet the Compute Module 5: What’s New and Improved?

Raspberry Pi recently unveiled the exciting Compute Module 5, a remarkable step forward in technology. This new module features impressive enhancements over the Compute Module 4, including a peak eMMC bandwidth of up to 500 MBps, an astounding four times faster than its predecessors! To match this speed, the Compute Module 5 series introduces a 16GB RAM option, empowering users to push boundaries like never before. Plus, with the addition of a 64GB eMMC option, the possibilities for larger applications are limitless. While embracing innovation, the decision was made to retire the 1GB RAM and 8GB eMMC options, making way for a brighter future. Let’s explore the specifications of these groundbreaking modules and discover how they can ignite creativity and inspire new solutions.

Meet the Compute Module 5: What’s New and Improved?

Meet the Compute Module 5: What’s New and Improved?

CM5

Here is a brief comparison of the specifications between the CM4 and CM5 models.

Meet the Compute Module 5: What’s New and Improved?

The CM5 includes several changes to its features compared to previous models. Notably, it no longer supports Composite Video Output, RUN_PG, or the 2-lane MIPI Interface. Instead, it offers two USB 3.0 ports, which have replaced the 2-lane MIPI interface, providing enhanced connectivity options.

Raspberry Pi is excited to introduce a range of new accessories designed to enhance your experience with the innovative new modules, ensuring you can fully harness their powerful features.

Development Kit

The first of these new accessories is the Compute Module 5 Development Kit.

Meet the Compute Module 5: What’s New and Improved?

Meet the Compute Module 5: What’s New and Improved?

This Kit includes the following:

  • 1 – CM5104032 Compute Module 5
  • 1 – Compute Module 5 IO Board Case
  • 1 – Compute Module 5 IO Board
  • 1 – Compute module 5 Passive Cooler
  • 1 – Raspberry Pi 27W USB Type-C PD Power Supply
  • 1 – Cm5 Antenna Kit
  • 2 – standard HDMI cable
  • 1 – USB-A to USB-C Cable

The CM5 development kit is available in various country configurations. At launch, there are versions for the EU, UK, and US.

IO Board

The next new accessory is the Raspberry Pi Compute Module 5 IO Board. This new board is designed to facilitate the development and integration of the Raspberry Pi Compute Module 5 into various projects, providing essential interfaces and connectivity options for project development.

Meet the Compute Module 5: What’s New and Improved?

Meet the Compute Module 5: What’s New and Improved?

Features of this board include:

  • Standard 40-pin GPIO connector
  • 2 – full-sized HDMI 2.0 connectors
  • 2 – 4-lane MIPI DSI/CSI-2 FPC connectors (22-pin, 0.5 mm pitch cable)
  • 2 – USB 3.0 connectors
  • Gigabit Ethernet Jack with PoE support (requires a separate Raspberry Pi PoE HAT)
  • M.2 M-key PCIe socket (for 2230, 2242, 2260, and 2280 modules)
  • MicroSD card socket (for use with Lite modules)
  • RTC battery socket
  • 4-pin fan connector
  • External power via a USB-C power supply (sold separately)

IO Case

The next accessory to enhance your setup is the Compute Module 5 IO Case, a simple but functional enclosure designed to protect your hardware while providing easy access to all the essential input and output connections.

Meet the Compute Module 5: What’s New and Improved?

Meet the Compute Module 5: What’s New and Improved?

This sleek metal case is designed to perfectly house the Compute Module 5 IO Board. But that’s not all – it comes equipped with an integrated fan that seamlessly connects to the 4-pin fan connector on the IO Board. Say goodbye to overheating and hello to enhanced thermal performance!

Passive Cooler

The final addition to the CM5 accessory lineup is the Compute Module 5 Passive Cooler, designed to enhance your computing experience by keeping things perfectly cool and efficient.

Meet the Compute Module 5: What’s New and Improved?

Meet the Compute Module 5: What’s New and Improved?

This aluminum heatsink is designed to optimize heat transfer from key components, including the CPU, memory, and wireless module (if applicable), as well as eMMC (if present). It's important to note that the increased performance of the CM5 model generally results in higher operating temperatures compared to the CM4. As such, utilizing this heatsink, complete with thermal pads, can significantly enhance cooling efficiency and maintain optimal performance.

As you embark on your next Raspberry Pi project, consider integrating the CM5 to elevate your work to new heights. Don't miss out on the opportunity to transform your project!

מק"ט יצרן # SC1967
RASPBERRY PI CM5IO BOARD
Raspberry Pi
מק"ט יצרן # SC1966
RASPBERRY PI CM5 IO CASE
Raspberry Pi
מק"ט יצרן # SC1752
RASPBERRY PI CM5 PASSIVE COOLER
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.