Maker.io main logo

Reversing the Polarity on LiPo Battery JST Connectors

660

2025-10-31 | By PTSolns

Batteries Connectors

The 2-Pin JST-PH 2.0 connector is found on many LiPo batteries used in hobby drones, RC cars and toys, and of course, electrical boards and modules. These are handy little connectors, but there is one problem - the polarity convention. About half of the vendors connect the negative (black wire) on the left and the positive (red wire) on the right sides. The other half does it the other way around. This can be an issue if the board or electronics you want to plug the LiPo battery into have the reversed polarity convention. Plugging in the LiPo terminals backwards can cause damage to onboard components on many boards that do not have reversed polarity protection. It is easy to reverse the polarity on these JST connectors.

TL;DR

Check out our video on how to reverse the polarity of JST connectors commonly used on LiPo batteries.

Two Polarity Convention

JST connectors themselves have no indication which terminal should be designated as the negative and which as the positive. This decision is left for the manufacturer who inserts the crimped wires into the connector. For example, one particular manufacturer of a LiPo battery may assemble the battery terminal wires, most often red for positive and black for negative, using the black-red convention. Yet a different manufacturer assembles them with the opposite convention, red-black. The two conventions are shown in Fig. 1.

This is a problem.

Image of Reversing the Polarity on LiPo Battery JST Connectors [Fig. 1 - Polarity convention for JST connectors. Left: black-red, Right: red-black.]

When inserting a LiPo battery into a board via the JST connector, polarity often matters. There are many custom or specialized boards that do not have reversed polarity protection, and inserting the positive and negative terminals may cause damage to onboard components.

NOTE: We've even heard of poorly made unbranded LiPo batteries where the black wire was NOT the negative terminal, and the red wire was NOT the positive terminal. The manufacturer had mistakenly attached the wires backward. The best practice is to confirm the polarity with a multimeter.

The Method

The crimped wire has a small metal hook that latches under a flap on the JST connector, as shown in Fig. 2. The goal is to lift the flap up and away from the hook just barely enough so that the hook is free to slide underneath and out of the connector. Bending the flap too much, too aggressively, or even too many times will fatigue the joint where the flap attaches to the main body of the JST connector.

Image of Reversing the Polarity on LiPo Battery JST Connectors [Fig. 2 - Flaps and hooks on JST connector.]

We recommend using a small flathead screwdriver to lift the flap up. Using the flathead, there are two methods to lift the flap.

  1. Come in from the side (Fig. 3), or
  2. Come in from the top (Fig. 4).

Both methods work, but we slightly prefer the coming-in-from-the-top method. This tends to leave fewer marks on the plastic body of the JST connector. This is also the method we show in our video.

Image of Reversing the Polarity on LiPo Battery JST Connectors [Fig. 3 - Method 1, come in from the side.]

Image of Reversing the Polarity on LiPo Battery JST Connectors [Fig. 3 - Method 2, come in from the top.]

If doing Method 1, then we suggest using a rotating movement of the screwdriver so that the flap is naturally lifted up by the side of the flat head that is furthest away from the joint of the flap to the body.

If doing Method 2, we suggest first applying a small inward force so that the wire moves into the JST connector as deeply as possible (without bending, crushing, etc.). The crimped wire tends to have about a 1mm jiggle when it is inside the connector. So extend that jiggle so that the wire is deeply inserted. This causes a small gap between the hook and the flap, which is just enough for the flathead screwdriver to get into. This part really is best to view in the video!

The next part is more or less a user preference. We prefer to hold the wire that is to be removed between the middle finger and the thumb. Gently pulling these towards the hand while using the index finger to press up against the JST connector causes a slight tension between the wire and the connector. When the flap is lifted just enough, the wire will pull out.

And that's really it; just be careful not to allow the battery contacts to touch and short the battery! One last thing to remember is when reinserting the wires into the JST connector, to make sure the wire is rotated such that the hook on the crimp is up (so that the flap can re-latch onto it). If one pushes the wire with enough force in the wrong orientation, it will go into the connector, but it will be incorrect.

For good measure, we use the flathead screwdriver to gently press down on the flaps after reinserting the wires just to make sure the flaps are latching well. A quick inspection of the JST connector is done to make sure no damage was done and the integrity of the connector remains.

Conclusion

Reversing the polarity of a 2-pin JST-PH connector is a simple but delicate process that can prevent costly damage to your electronics. The key is patience and precision — lift the flap just enough to release the crimp, swap the wires, and reinsert them in the correct orientation. Always verify polarity with a multimeter before plugging a LiPo battery into any board, especially those without reverse-polarity protection. With careful handling, your JST connector polarity can be safely reversed, and the connector can be used on boards and modules that have either polarity convention.

Resources

PTSolns supplier center: https://www.digikey.com/en/supplier-centers/ptsolns-pylon-technology-solutions

PTSolns Documentation Repository: https://docs.ptsolns.com

מק"ט יצרן # PTS-00134-001
25-IN-1 PRECISION S2 SCREWDRIVER
PTSolns
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.