Maker.io main logo

Arduino FFT Audio Spectrum Analyzer on 8x32 Color Matrix WS2812B

550

2024-04-17 | By Mirko Pavleski

License: General Public License Audio Arduino

The spectrum analyzer displays the amplitude of signals as a function of frequency, allowing engineers and technicians to visualize and analyze signal characteristics. In particular, the audio analyzer performs a visual presentation of an acoustic signal in the frequency domain, where the frequency of the signal is displayed on the x-axis, while the amplitude of a certain frequency is displayed on the y-axis. In several of my previous videos ( I have presented several different types of such devices, but this time the FHT Arduino library is used for the first time. This library is several times faster than the commonly used FFT library, but at the expense of speed certain loss of resolution and precision appear at the two ends of the audio range.

 

 

However, in the specific case we do not have to develop a measuring instrument but a simple gadget, we do not need extreme precision, we just have to turn on a handful of LEDs in musical rhythm. By the way, the project has been submitted to the Arduino Project Hub by the user with the nickname januks  and is actually a rework of Shaajeb's excellent Spectrum analyzer project. I made minimal modifications to the hardware and code based on my ideas and requirements.

ytr

 

The device is really simple to build and consists of only a few components:

- Arduino Nano MCU board

- 8x64 color LED Matrix with WS2812B addressable LEDs

- Two (three) touch buttons

- three resistors

- and one capacitor

Now let's see how the device works in real conditions considering that it is very simple, the device works immediately without any previous settings. One button is used to adjust the LED light intensity in 7 steps. With the other button, we move through 6 different mods with specific color sets, and we can also add more, with very small modifications to the code.

rse

Next, let's test the frequency range that this analyzer covers. For this purpose we will use a simple online tone generator. As you can see, the device covers the entire hearing range, from 20 Hertz to 20 kilohertz. Such a large-range device is excellent when used for visual FFT analysis, but has one practical drawback when it comes to presenting musical materials.

zxdf

Namely, a large percentage (perhaps 90%) of this music signal is in the range of up to 10Khz, and only a small part belongs to higher frequencies. This would practically mean that for the entire time that the music signal is being emitted, the far right part of the analyzer would be inactive. Let's see how it looks in practice (Here is an example with a speech signal, so we will try it with musical material as well). Since, as I mentioned at the beginning, this is a visual decorative addition and not a precise measuring instrument, it is desirable to reduce the bandwidth by half, actually to 10 Kilohertz. For this case, I made some modification in the code, but it is also desirable to set a simple Low-pass filter on the input. Let's test the range with an online tone generator at the input. The range is up to 10Khz.

ghkhj

Now, in this case the matrix is completely filled and visually it looks much better. As for the external appearance of the device, I tried to make a simple, but still functional version made of PVC board and glass with a thickness of 4 mm. And finally, a short conclusion. This is an extremely simple project intended for beginners, but still visually very effective and can serve as a gadget on your desktop, or as an addition to an audio device. It can also be used as a simple school FFT spectrum analyzer instrument intended for educational purposes.

bhjkhj

 

מק"ט יצרן # A000005
ARDUINO NANO ATMEGA328 EVAL BRD
Arduino
מק"ט יצרן # 2294
ADDRESS LED MATRIX SERIAL RGB
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.