Maker.io main logo

Arduino Two Wheel Self-Balancing Robot

467

2025-03-10 | By Mirko Pavleski

License: General Public License Arduino

A self-balancing robot is a device that can keep itself from falling to the ground. Its function is to maintain balance using the motor’s axis movement of the wheels and body. There are several types of self-balancing robots, and in this particular case I will present you a way to make a Two-Wheeled Balancing Robot. Actually, I made this robot together with one of my students and it is a high school graduation project. This is the simplest type of balancing robot and only requires a few components to build.

First, let's explain the components used and their functions.

- MPU6050 Accelerometer and Gyroscope sensor with Micro Electro Mechanical System(MEMS) technology, which is used to detect the angle of tilt or inclination along the X, Y, and Z axes.

- The information from this sensor is transmitted to a microcontroller, and in our case, it is an Arduino Uno board. This board is the brain of the robot, processes the sensor data, and determines the actions needed to keep the robot upright.

- Processed data from the Arduino is sent to the motor driver board, which in our case is the L298N 5AD type. A motor driver circuit controls the direction and speed of the motors.

- This robot uses two DC motors, each connected to a wheel. These motors adjust the speed of the wheels to correct the robot’s tilt.

- and power source, specifically two lithium batteries connected in series which provide energy to the motors and electronics. All components are mounted on a suitable supporting structure made of 5mm thick PVC board.

mjk

Now, let's briefly explain the working principle: the accelerometer gives a measure of the robot’s orientation relative to gravity, and the gyroscope detects the rate of tilt. The Arduino uses a PID (Proportional, Integral, Derivative) controller to process the data from the sensors.

cvxg

The PID controller calculates the necessary speed and direction adjustments needed to maintain the robot’s balance. If the robot tilts forward, the motors spin faster to move the robot forward and prevent a fall. If it tilts backward, the motors move the robot backward to regain balance. As the robot detects an imbalance, it compensates by adjusting the wheel speed, shifting its center of mass, or moving forward or backward to maintain its position.

A few words about the Arduino code. The method of installing the code has been described many times before, so now I will only focus on the modifications that need to be made individually for each case due to the different characteristics of the components used, as well as the method of their placement.

Now comes the fun part, which is customizing the code specifically for our built device. Depending on the layout of the components, the center of gravity of the robot changes, and also each MPU6050 board has minimal differences that need to be compensated for in part of the code. If we look at the code in more detail, we will see that there is a place where the Gyro offset is set.

gh

hjk

In this part of the code, errors are corrected during the manufacturing of the MPU6050 chip. For each individual chip, these values ​​are different. Their value is determined using Arduino code made specifically for this purpose and you can download it at the end of this text.

Next, we need to move on to setting the Accelerometer. In the "double setpoint' line, we need to put a value that corresponds to our device.

jhk

To obtain this value, we need to hold the robot in an ideal vertical position, perpendicular to the surface, and read the required value on the serial monitor. In my case, it is about 182

Finally, we need to experimentally determine the values ​​of Kp, Kd, and Ki, needed for PID control.

fcgf

For this purpose, we set all three values ​​to zero. Now we put some value for Kp and perform testing. Too little Kp will make the robot fall over. Too much Kp will make the robot go back and forth wildly. A good Kp will make the robot go slightly back and forth. Next, we need to set Kd. A good Kd value will lessen the oscillation until the robot is almost steady and will keep the robot standing. Lastly, set the Ki. The correct Ki value will shorten the time it takes for the robot to stabilize. I want to emphasize that the surface needs to be rough enough to increase the friction between it and the wheels.

And finally, a short conclusion. This is a relatively simple, visually effective balancing robot project that only requires 3 components to make. However, its setup, although it can be time-consuming, is still a lot of fun trying to get the robot to stand steadily on its "own feet". Just to mention we created this project together with my students as a final high school exam.

bhnjb

Copy Code
#include "I2Cdev.h"
#include <PID_v1.h> //From https://github.com/br3ttb/Arduino-PID-Library/blob/master/PID_v1.h
#include "MPU6050_6Axis_MotionApps20.h" //https://github.com/jrowberg/i2cdevlib/tree/master/Arduino/MPU6050
MPU6050 mpu;
// MPU control/status vars
bool dmpReady = false;  // set true if DMP init was successful
uint8_t mpuIntStatus;   // holds actual interrupt status byte from MPU
uint8_t devStatus;      // return status after each device operation (0 = success, !0 = error)
uint16_t packetSize;    // expected DMP packet size (default is 42 bytes)
uint16_t fifoCount;     // count of all bytes currently in FIFO
uint8_t fifoBuffer[64]; // FIFO storage buffer
// orientation/motion vars
Quaternion q;           // [w, x, y, z]         quaternion container
VectorFloat gravity;    // [x, y, z]            gravity vector
float ypr[3];           // [yaw, pitch, roll]   yaw/pitch/roll container and gravity vector
/*********Tune these 4 values for your BOT*********/
double setpoint= 182; //set the value when the bot is perpendicular to ground using serial monitor. 
//Read the project documentation on circuitdigest.com to learn how to set these values
double Kp = 15; //21 Set this first
double Kd = 0.9; //0.8 Set this secound
double Ki = 140; //140 Finally set this 
/******End of values setting*********/
double input, output;
PID pid(&input, &output, &setpoint, Kp, Ki, Kd, DIRECT);
volatile bool mpuInterrupt = false;     // indicates whether MPU interrupt pin has gone high
void dmpDataReady()
{
    mpuInterrupt = true;
}
void setup() {
  Serial.begin(115200);
  // initialize device
    Serial.println(F("Initializing I2C devices..."));
    mpu.initialize();
     // verify connection
    Serial.println(F("Testing device connections..."));
    Serial.println(mpu.testConnection() ? F("MPU6050 connection successful") : F("MPU6050 connection failed"));
    // load and configure the DMP
    devStatus = mpu.dmpInitialize();
    // supply your own gyro offsets here, scaled for min sensitivity
    mpu.setXGyroOffset(-479);
    mpu.setYGyroOffset(84);
    mpu.setZGyroOffset(15);
    mpu.setZAccelOffset(1638); 
      // make sure it worked (returns 0 if so)
    if (devStatus == 0)
    {
        // turn on the DMP, now that it's ready
        Serial.println(F("Enabling DMP..."));
        mpu.setDMPEnabled(true);
        // enable Arduino interrupt detection
        Serial.println(F("Enabling interrupt detection (Arduino external interrupt 0)..."));
        attachInterrupt(0, dmpDataReady, RISING);
        mpuIntStatus = mpu.getIntStatus();
        // set our DMP Ready flag so the main loop() function knows it's okay to use it
        Serial.println(F("DMP ready! Waiting for first interrupt..."));
        dmpReady = true;
        // get expected DMP packet size for later comparison
        packetSize = mpu.dmpGetFIFOPacketSize();
        //setup PID
        pid.SetMode(AUTOMATIC);
        pid.SetSampleTime(10);
        pid.SetOutputLimits(-255, 255);
    }
    else
    {
        // ERROR!
        // 1 = initial memory load failed
        // 2 = DMP configuration updates failed
        // (if it's going to break, usually the code will be 1)
        Serial.print(F("DMP Initialization failed (code "));
        Serial.print(devStatus);
        Serial.println(F(")"));
    }
//Initialise the Motor outpu pins
    pinMode (6, OUTPUT);
    pinMode (9, OUTPUT);
    pinMode (10, OUTPUT);
    pinMode (11, OUTPUT);
//By default turn off both the motors
    analogWrite(6,LOW);
    analogWrite(9,LOW);
    analogWrite(10,LOW);
    analogWrite(11,LOW);
}
void loop() {
    // if programming failed, don't try to do anything
    if (!dmpReady) return;
    // wait for MPU interrupt or extra packet(s) available
    while (!mpuInterrupt && fifoCount < packetSize)
    {
        //no mpu data - performing PID calculations and output to motors     
        pid.Compute();
        //Print the value of Input and Output on serial monitor to check how it is working.
        Serial.print(input); Serial.print(" =>"); Serial.println(output);
        if (input>150 && input<200){//If the Bot is falling 
        if (output>0) //Falling towards front 
        Forward(); //Rotate the wheels forward 
        else if (output<0) //Falling towards back
        Reverse(); //Rotate the wheels backward 
        }
        else //If Bot not falling
        Stop(); //Hold the wheels still
    }
    // reset interrupt flag and get INT_STATUS byte
    mpuInterrupt = false;
    mpuIntStatus = mpu.getIntStatus();
    // get current FIFO count
    fifoCount = mpu.getFIFOCount();
    // check for overflow (this should never happen unless our code is too inefficient)
    if ((mpuIntStatus & 0x10) || fifoCount == 1024)
    {
        // reset so we can continue cleanly
        mpu.resetFIFO();
        Serial.println(F("FIFO overflow!"));
    // otherwise, check for DMP data ready interrupt (this should happen frequently)
    }
    else if (mpuIntStatus & 0x02)
    {
        // wait for correct available data length, should be a VERY short wait
        while (fifoCount < packetSize) fifoCount = mpu.getFIFOCount();
        // read a packet from FIFO
        mpu.getFIFOBytes(fifoBuffer, packetSize);
        // track FIFO count here in case there is > 1 packet available
        // (this lets us immediately read more without waiting for an interrupt)
        fifoCount -= packetSize;
        mpu.dmpGetQuaternion(&q, fifoBuffer); //get value for q
        mpu.dmpGetGravity(&gravity, &q); //get value for gravity
        mpu.dmpGetYawPitchRoll(ypr, &q, &gravity); //get value for ypr
        input = ypr[1] * 180/M_PI + 180;
   }
}
void Forward() //Code to rotate the wheel forward 
{
    analogWrite(6,output);
    analogWrite(9,0);
    analogWrite(10,output);
    analogWrite(11,0);
    Serial.print("F"); //Debugging information 
}
void Reverse() //Code to rotate the wheel Backward  
{
    analogWrite(6,0);
    analogWrite(9,output*-1);
    analogWrite(10,0);
    analogWrite(11,output*-1);
    Serial.print("R");
}
void Stop() //Code to stop both the wheels
{
    analogWrite(6,0);
    analogWrite(9,0);
    analogWrite(10,0);
    analogWrite(11,0);
    Serial.print("S");
}

מק"ט יצרן # SEN0142
6 DOF SENSOR - MPU6050
DFRobot
מק"ט יצרן # DRI0002
EVAL BOARD FOR L298
DFRobot
מק"ט יצרן # 13302
GEARMOTOR 140 RPM 4.5V QTY 2
SparkFun Electronics
מק"ט יצרן # 13259
WHEEL - 65MM (RUBBER TIRE, PAIR)
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.