Maker.io main logo

Artemis Global Tracker Hookup Guide

86

2022-02-16 | By SparkFun Electronics

License: General Public License Wireless

Courtesy of SparkFun

Guide by QCPETE, EL DUDERINO

Introduction

The SparkFun Artemis Global Tracker provides a powerful tracking system combining remote short ‎messaging via the Iridium satellite network with GPS tracking and environmental sensing all ‎powered by the SparkFun Artemis module. The Global Tracker design focuses on truly remote ‎tracking, data collection and transmission so whether you're looking to transmit environmental data ‎from the top of a mountain, send data from a traveling balloon, control and monitor remote ‎equipment or maybe communicate in an emergency when other networks are not available; the ‎Artemis Global Tracker may be just the right tool for your remote data project.

SparkFun Artemis Global Tracker

 

The Artemis Global Tracker features an Iridium 9603N satellite transceiver, u-blox ZOE-M8Q GNSS ‎module and MS8607 pressure, humidity, and temperature sensor. We designed the Artemis Global ‎Tracker with the idea of creating a robust data tracking module that works anywhere in the world, ‎including the polar regions, far beyond the reach of Wi-Fi and GSM networks.‎

Required Materials

The Artemis Global Tracker (or AGT as we'll sometimes refer to it in this guide) requires a few ‎external components to get up and running properly. First and foremost is a power supply. The ‎AGT receives power via either USB-C, single-cell LiPo battery or an external solar panel or battery ‎pack (max 6V). Take a look at the products below for power supply options for the AGT:‎

USB-C

LiPo Battery

Solar Panel

Note: The Artemis Global Tracker uses a JST connector for both the LiPo and Solar Panel / Battery ‎Pack power inputs. The panels listed above all terminate in a standard barrel jack, so users need to ‎modify the termination or use an adapter like this Barrel Jack to JST Adapter.‎

Antenna

The AGT also requires an external antenna for the 9603N and M8Q modules. The AGT routes both ‎modules' antenna pins to a shared SMA connector so to keep things simple, we recommend ‎a passive antenna tuned for Iridium/GPS/GLONASS bands like the antenna shown below:‎

External Capacitors

Users powering the Artemis Global Tracker with a solar panel or lower-current power configurations ‎need to attach a pair of external 10F capacitors like the ones below to provide the extra current for ‎‎9603N SBD transmissions:‎

  • Super Capacitor - 10F/2.5V‎

Satellite Network Line Rental

The Iridium modem requires a monthly rental service to exchange information with the Iridium ‎satellite network. Set up an account with Rock7 here. You only pay for months in which you wish to ‎use the modem. No annual contract is required. Line rental costs £12GBP (about $15USD) per ‎month and includes access to the RockBLOCK management system for managing your devices. ‎The billing system is built-in and allows you to pay for only what you use. Airtime for Iridium ‎modems must be purchased from Rock Seven via the admin portal once the units are registered. ‎You cannot use the devices with another Iridium airtime provider by default. If you would like to use ‎it with another provider, you will need to pay an unlock fee of $60USD per modem.‎

Recommended Reading

Users who have never used the Artemis module or other Artemis boards may want to read through ‎the following tutorials before getting started with the Artemis Global Tracker:‎

  • Three Quick Tips About Using U.FL: Quick tips regarding how to connect, protect, and ‎disconnect U.FL connectors.‎

  • Using SparkFun Edge Board with Ambiq Apollo3 SDK: We will demonstrate how to ‎get started with your SparkFun Edge Board by setting up the toolchain on your computer, ‎examining an example program, and using the serial uploader tool to flash the chip.‎

  • Designing with the SparkFun Artemis: Let's chat about layout and design considerations ‎when using the Artemis module.‎

  • Artemis Development with the Arduino IDE: This is an in-depth guide on developing in ‎the Arduino IDE for the Artemis module and any Artemis microcontroller development board. Inside, ‎users will find setup instructions and simple examples from blinking an LED and taking ADC ‎measurements; to more complex features like BLE and I2C.‎

  • Installing Board Definitions in the Arduino IDE: How do I install a custom Arduino ‎board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the ‎Arduino Board Manager. We will also go over manually installing third-party cores, such as the ‎board definitions required for many of the SparkFun development boards.‎

Hardware Overview

Let's take a look at the Artemis Global Tracker and all the hardware on it. There is a lot to cover ‎here so buckle up.‎

Major AGT Components

The Artemis Global Tracker combines the SparkFun Artemis module, Iridium 9603N Satellite ‎Transceiver, ZOE-M8Q GNSS module and MS8607 PHT sensor to provide location and ‎environmental data to a powerful, low-power processor system capable of transmitting collected ‎data from anywhere on the planet using the Iridium Satellite network. First up we'll cover these ‎major components in more detail.‎

major_1

Artemis Microprocessor

As the name suggests, the SparkFun Artemis Module rests at the core of the Artemis Global ‎Tracker. The Artemis Module is built on the Apollo3 MCU platform and is a Cortex-M4F based ‎module with BLE 5.0 that runs at 48MHz clock frequency (up to 96MHz burst mode) and low-power ‎consumption as low as 6µA per MHz. The Artemis also features plenty of storage space with up to ‎‎1MB of Flash memory and up to 384KB RAM, BLE 5 RF sensitivity of -93dBm (typical) and TX peak ‎output power of 4.0dBm. For a complete overview of the Artemis module, please review ‎the Artemis Integration Guide and Graphical Datasheet.‎

The Artemis works on multiple development platforms; the SparkFun Apollo3 Arduino Core, Python, ‎as well as Ambiq's Apollo3 SDK allowing users to choose which development environment works ‎best for their application. Note, the examples for the Artemis Global Tracker are written for the ‎Arduino IDE.‎

Iridium 9603N Satellite Transceiver

The AGT uses an Iridium 9603N Satellite Transceiver to take advantage of the Iridium Satellite ‎transmission network to send and receive small data packets in truly remote areas with no Wi-Fi and ‎GSM network coverage. With a clear view of the sky, the Iridium can send short messages ‎anywhere in the world, including polar regions outside the range of traditional wireless networks like ‎Wi-Fi and GSM networks. Refer to the datasheet for more information on the 9603N.‎

Note: The Iridium modem requires a monthly rental service to exchange information with the Iridium ‎satellite network. You only pay for months in which you wish to use the modem. No annual contract ‎is required. Line rental costs £12GBP (about $17USD) per month and includes access to the ‎RockBLOCK management system for managing your devices. The billing system is built-in and ‎allows you to pay for only what you use. Airtime for Iridium modems must be purchased from ‎Ground Control (formerly known as Rock Seven) via the admin portal once the units are registered. ‎You cannot use the devices with another Iridium airtime provider by default. If you would like to use ‎it with another provider, you will need to pay an unlock fee of $60USD per modem.‎

The 9603N is a small form-factor satellite transceiver that uses Iridium's satellite network in Low-‎Earth Orbit which reduces latency greatly as compared to networks using geostationary satellites. ‎The 9603N design focuses on creating a robust transceiver capable of working in inhospitable ‎environments with an operating temperature range of -40°C to 85°C and up to 75% humidity.‎

The module draws relatively low current during idle, transmission and receive. Short-Burst-Data ‎transfers require the most current for short periods (8ms) but the design accommodates for that by ‎powering the 9603N with a pair of 1F supercapacitors and charge/current regulation circuit covered ‎in more detail below. The table below shows the typical and max values for each of those ‎operations (all values operating at 5V):‎

Table1_2

The AGT ties the 9603N's Shutdown Pin to Artemis pin D17 to allow software control of power to ‎the module. This software control is important to take note of when transmitting data using an ‎antenna attached to the SMA connector as the 9603N shares an antenna connection with the ZOE-‎M8Q. The AGT includes a switching circuit to select which module uses the antenna as both ‎modules cannot use the antenna at the same time. This circuit defaults to use the ZOE-M8Q ‎antenna line when the device is powered so make sure to power the GNSS module down prior to ‎transmitting data with the 9603N.‎

ZOE-M8Q GNSS Module

The ZOE-M8Q GNSS module from u-blox adds positional data to the Artemis Global Tracker. The ‎ZOE-M8Q is an ultra-small GNSS module that works with all major GNSS constellations (GPS, ‎GLONASS, Galileo and BeiDou). For a complete overview of the ZOE-M8Q refer to the datasheet. ‎The module also supports up to four circular geofencing areas so you can trigger alarm messages ‎sent over the Iridium network when your device either enters or exits one of those areas.‎

The AGT uses the ZOE-M8Q's I2C bus to communicate between the module and the Artemis ‎controller. With a passive antenna, the ZOE-M8Q achieves up to 2.5m accuracy with GPS lock. ‎From a cold start, the module has a Time-To-First Fix of 29s with GPS and a hot start fix time ‎of 1s on all constellations. The table below outlines the ZOE-M8Q's specifications:‎

Table2_3

Power to the ZOE-M8Q is controlled by a P-Channel MOSFET tied to Artemis pin D26. This allows ‎users to turn the module off and on when positioning data is not needed. The board also includes ‎a 1mAh backup battery and charging circuit for the ZOE-M8Q to allow the module to operate in ‎Hardware Backup Mode for up to 12 hours to keep the clock running and allow a hot or warm start ‎later. The backup battery recharges only with USB power connected (to help minimise the 3.3V ‎current draw during sleep).‎

As a reminder, the ZOE-M8Q shares the antenna connection with the 9603N module. Both modules ‎cannot use the antenna at the same time, so the board includes a switching circuit to select which ‎module uses the antenna.‎

MS8607 PHT Sensor

The Artemis Global Tracker includes the MS8607 Pressure, Humidity, and Temperature sensor ‎from TE Connectivity for an integrated environmental monitoring system at your remote station as ‎well an effective altimeter for balloon applications. For a complete overview of the MS8607, refer to ‎the datasheet.‎

The MS8607 offers a wide operating range with excellent precision for pressure, temperature, and ‎humidity. The table below outlines these parameters.‎

Table3_4

Power

The Artemis Global Tracker includes three power input options in USB-C, single-cell LiPo battery or ‎a solar panel (or battery pack), LiPo charging circuit and a dedicated supercapacitor power and ‎charging circuit for the 9603N.‎

power_5

Primary Power Inputs

Low-forward-voltage diodes isolate the three power inputs from each other so that users can have ‎all three power sources present without harming anything on the AGT. If USB voltage is present ‎‎(along with other power supplies), the AGT prefers to draw power from USB. If just Solar ‎Cell/Battery Pack and LiPo are connected, the AGT defaults to drawing power from the Solar ‎Cell/Battery Pack input, making the LiPo redundant.‎

Table4_6

LiPo Battery Charge Circuit

The AGT includes a charging circuit for an attached single-cell LiPo battery using one of our ‎favorite LiPo management controllers, the MCP73831 from Microchip. The charge circuit ‎configuration sets the charge rate to 500mA. The LiPo charging circuit only receives power via ‎VUSB; USB power is required to charge an attached LiPo battery.‎

Supercapacitors and Charge Circuit

The AGT provides power to the 9603N through a pair of supercapacitors charged by an LTC3225 ‎supercapacitor charger regulated by an ADM4210 in-rush current limit circuit. The charge circuit ‎defaults to source enough current (150mA) to power the 9603N during normal operation and the ‎supercapacitors provide the extra 1.3A required during the Short Burst Data (SBD) transfers ‎‎(8.3ms).‎

The charge circuit is configurable to switch to a lower max current (60mA) for low-current power ‎configurations like solar. While in the low max current configuration users need to add a pair of 10F ‎capacitors to provide the extra current required by the 9603N module during normal operation and ‎SBD transfers.‎

The AGT ties the LTC3225's Shutdown Input pin to Artemis pin D27 which allows users to put the ‎charger into Shutdown Mode to help reduce power consumption when the supercapacitor charge ‎circuit is not needed. Set D27 LOW to put the LTC3225 into Shutdown Mode and reduce current ‎consumption by the charge circuit to approximately 1µA. Users looking for more detailed ‎information on the LTC3225 should refer to the datasheet.‎

Bus Voltage

The AGT includes a voltage monitoring circuit to keep track of the bus voltage (from the USB, LiPo ‎or external cells). The board uses Artemis pin AD13 for voltage measurement via a simple two ‎resistor divider dividing the bus voltage by three. Power to the resistor divider is switched by an N-‎channel MOSFET so the power draw can be minimized during sleep.‎

GPIO PTHs

The AGT breaks out an assortment of helpful GPIO pins from the Artemis module to PTH headers ‎to interface with external devices. The board routes the following: SPI, I2C, Reset, and eleven multi-‎purpose GPIO pins to PTH headers:‎

GPIO_7

SPI/I2C Bus and Reset PTHs

  • SDA

  • SCL

  • RST

  • CIPO

  • COPI

GPIO PTHs

  • AD11~‎

  • AD12~‎

  • AD29~

  • AD31~‎

  • AD32~

  • AD35~ (SPI CS1)

  • D4~ (SPI CS2)‎

  • D15

  • D37*

  • D42~‎

  • D43~‎

  • Pins marked with a "~" are PWM-capable

  • I2C pins (SDA and SCL) are shared with ZOE-M8Q and MS8607 @3.3V

  • ‎*D37 is a low-Impedance pin. Useful for controlling MOSFETs to power external devices

For detailed information on alternate functionality and GPIO multiplexing options, refer to ‎the Designing with the SparkFun Artemis tutorial and Artemis/Apollo3 Pin Function Map.‎

LEDs

The AGT has seven status LEDs highlighted in the photo below:‎

leds_8

  • ‎9603N PWR: Illuminates when the 9603N is powered on

  • CHARGING: Illuminates when the supercapacitor charge circuit is active

  • POWER: Illuminates when 3.3V is present

  • GNSS: Illuminates when ZOE-M8Q is powered on

  • D19: General status LED tied to Artemis D19

  • RX0: UART0 RX data indicator LED

  • TX0: UART0 TX data indicator LED

Solder Jumpers

The Artemis Global Tracker has four solder jumpers labeled PWR LED, Supercaps Charge ‎Current, 3.3V EN and MEAS.‎

solder_9

The PWR_LED jumper allows users to disable the Power LED to help reduce power consumption ‎for low-power applications. This jumper is CLOSED by default. Sever the trace between the two ‎pads to open the jumper and disable the Power LED.‎

The Supercaps Charge Current Jumper adjusts the maximum current for the LTC3225 ‎Supercapacitor charger by tying the PROG pin to Ground through one of two different valued ‎resistors (12kΩ (default) and 30.1kΩ). By default, it sets the charge current to 150mA, opening the ‎jumper sets the charge current to 60mA. When in this configuration additional capacitors are ‎required to provide the extra power drawn by the 9603N during transmission cycles.‎

The 3.3V EN Jumper controls the Enable Pin on the 3.3V regulator to VIN. The jumper is CLOSED ‎by default and ties the Enable Pin to VIN. Opening the jumper leaves the Enable Pin tied only to the ‎PTH labeled EN on the AGT allowing users to use that PTH pin to turn the regulator on and off.‎

The MEAS Jumper allows users to measure the current draw of the AGT. By default, the jumper is ‎CLOSED and nets all three power inputs to VIN.‎

Board Dimensions

The Artemis Global Tracker measures 2.5in x 2.0in (63.5mm x 50.8mm) with four mounting holes ‎that fit a 4-40 screw.‎

dimensions_10

Hardware Assembly

The Artemis Global Tracker comes basically ready-to-use out of the box for most applications. The ‎only assembly required for basic use is to connect an antenna to the SMA connector and attach ‎your power supply (USB, solar panel and/or battery). Users powering the AGT with a solar panel or ‎other low-current supply most likely need to solder additional supercapacitors to the provided PTH ‎connections.‎

Basic Assembly (USB/LiPo Battery)‎

Simple assembly of the AGT only requires a power source and antenna connection. On initial setup ‎you'll want to connect it to a computer via USB to program the board. With your preferred code ‎running on the AGT, connect the antenna to the SMA connector and then power it with either a ‎USB power supply, LiPo battery or solar panel/battery pack connected to the properly labeled ‎connection (USB or JST connector). Reminder, the LiPo charging circuit only operates with voltage ‎from USB.‎

basic_11

Additional Supercapacitor Assembly

Solar powered or other low-current applications may require users to adjust the Charge Current ‎jumper to set the charge rate from 150mA to 60mA. The reduced current provides enough for the ‎‎9603N's 39mA average current draw during receive, but larger supercapacitors are needed to ‎supply the average current pulled during a complete receive/transmit cycle.‎

Before soldering to the board, remove the 9603N from the AGT by unscrewing the mounting ‎screws, carefully unplug the u.Fl cable and then remove the 9603N from the board making sure to ‎pull directly upwards. After removing the 9603N, turn the board over and solder a pair of additional ‎‎10F capacitors like these to the labeled pads on the back of the board taking care to match the ‎polarity:‎

assembly_12

assembly_13‎ ‎ ‎

Iridium and Artemis Software Setup

The Artemis Global Tracker requires a couple of software setup steps users need to complete ‎before they start working with the device. You must create an account for Rock7 Operations to set ‎up line rental and message credits for the 9603N. Users wanting to use the AGT with the Arduino ‎IDE may need to install the SparkFun Apollo3 Arduino core to upload code to the Artemis Module.‎

Rock7 Operations

Head over to Rock7's Operations webpage to create an account to use the 9603N on the Iridium ‎Satellite Network. You must create an account and link the 9603N to it as well as set up a line rental ‎and purchase message credits with Rock7 to send data over the network. The website has easy-to-‎follow instructions to get the 9603N registered and operating on the network.‎

Artemis Arduino Guides

Users needing to install the SparkFun Apollo3 Arduino Core should read through the tutorial below:‎

guides_14

Artemis Development with the Arduino IDE

This is an in-depth guide on developing in the Arduino IDE for the Artemis module and any Artemis ‎microcontroller development board.

Inside, users will find setup instructions and simple examples ‎from blinking an LED and taking ADC measurements; to more complex features like BLE and I2C.‎

Important! The Artemis Global Tracker examples currently work only on version 2.1.0 of the ‎SparkFun Apollo3 Arduino core. Make sure to install that version of the Arduino core when using ‎the Artemis Global Tracker. You can select the version when using the Boards Manager tool in the ‎Arduino IDE or users who prefer to manually manage the board definitions can find version ‎‎2.1.0 here. We are currently working on an update to the Arduino core to resolve this issue. You ‎can keep track of the development process on the Apollo3 Arduino core GitHub Repository. We will ‎update this guide once this issue is resolved.‎

The Artemis Global Tracker uses the Artemis ATP board definitions. The Artemis Arduino Core ‎install includes this board definition but in case you are interested in learning more about the ‎Artemis ATP, head on over to the Hookup Guide:‎

guides_15

Hookup Guide for the SparkFun RedBoard Artemis ATP

Get started with the RedBoard Artemis ATP - all the functionality of the SparkFun Artemis module ‎wrapped in the Mega Arduino Footprint.‎

Artemis Global Tracker Arduino Examples

The AGT ships with a comprehensive Global Tracker example pre-loaded on the board for users to ‎get started quickly with the Artemis Global Tracker Configuration Tool so if you want to skip ahead ‎and use the Configuration Tool, jump ahead to the next section.‎

Arduino Examples

Note: These examples assume the latest version of the Arduino IDE is used. If this is your first time ‎using Arduino, please review our tutorials on Installing the Arduino IDE and Installing an Arduino ‎Library.‎

We've written twenty examples for users to familiarize themselves with all of the hardware present ‎on the Artemis Global Tracker using the Arduino IDE. The examples build on each other to quickly ‎test functionality of different circuits on the AGT and demonstrate how to use the PHT sensor, ‎ZOE-M8Q and 9603N individually with some highlighting features of these components as well as ‎three examples showing how to create a tracking device using the AGT. Download the examples ‎either from the GitHub repository or you can download a ZIP of the GitHub repo by clicking the ‎button below:‎

ARTEMIS GLOBAL TRACKER GITHUB REPOSITORY (ZIP)‎

Open the examples either from the folder they downloaded to or you can put them in ‎your "Arduino Sketchbook" folder to open them in the Arduino IDE. If you're not certain where ‎your Sketchbook folder is, open the "Preferences" menu in Arduino and look for the filepath under ‎the selection titled "Sketchbook location".‎

Required Arduino Libraries

The Artemis Global Tracker examples use three SparkFun libraries users need to install prior to ‎working with them:‎

Install the libraries through the Arduino Library Manager tool by searching ‎for "IridiumSBDi2c", "SparkFun u-blox GNSS Arduino Library" and "SparkFun PHT MS8607 ‎Arduino Library". Users who prefer to manually install the libraries can download the ZIP of each ‎library repository by clicking the buttons below:‎

SPARKFUN IRIDIUM SBD I2C ARDUINO LIBRARY (ZIP)

SPARKFUN U-BLOX GNSS ARDUINO LIBRARY (ZIP)‎

SPARKFUN PHT MS8607 ARDUINO LIBRARY (ZIP)‎

Arduino Examples

Reminder: The Artemis Global Tracker Arduino Examples only work on v2.1.0 of the SparkFun ‎Apollo3 Arduino Core. Make sure you are using that version when uploading the examples. We will ‎update this note once the current version of the Apollo3 Arduino Core is compatible with these ‎examples.‎

With the Artemis Arduino Core and necessary libraries installed we can move on to using the ‎examples. This tutorial covers six of the Arduino examples we find most helpful to demonstrate how ‎to use the major components on the AGT and then how to use them all in conjunction to create a ‎global tracking device.‎

Users looking to write their own code for the AGT should take note of the following pin definitions ‎and functions:‎

Copy Code
// D4 can be used as an SPI chip select or as a general purpose IO pin
#define spiCS1              4  

// Input for the ZOE-M8Qs PIO14 (geofence) pin
#define geofencePin         10 

// Bus voltage divided by 3 (Analog in)
#define busVoltagePin       13 

// Iridium 9603N ON/OFF (sleep) pin: pull high to enable the 9603N
#define iridiumSleep        17 

// Input for the Iridium 9603N Network Available
#define iridiumNA           18 

// White LED
#define LED                 19 

// ADM4210 ON: pull high to enable power for the Iridium 9603N
#define iridiumPwrEN        22 

// GNSS Enable: pull low to enable power for the GNSS (via Q2)
#define gnssEN              26 

// LTC3225 super capacitor charger: pull high to enable the super capacitor charger
#define superCapChgEN       27 

// Input for the LTC3225 super capacitor charger PGOOD signal
#define superCapPGOOD       28 

// Bus voltage monitor enable: pull high to enable bus voltage monitoring (via Q4 and Q3)
#define busVoltageMonEN     34 

// D35 can be used as an SPI chip select or as a general purpose IO pin
#define spiCS2              35 

// Input for the Iridium 9603N Ring Indicator
#define iridiumRI           41     

void gnssON(void) // Enable power for the GNSS
{
  am_hal_gpio_pincfg_t pinCfg = g_AM_HAL_GPIO_OUTPUT; // Begin by making the gnssEN pin an open-drain output
  pinCfg.eGPOutcfg = AM_HAL_GPIO_PIN_OUTCFG_OPENDRAIN;
  pin_config(PinName(gnssEN), pinCfg);
  delay(1);

  digitalWrite(gnssEN, LOW); // Enable GNSS power (HIGH = disable; LOW = enable)
}

void gnssOFF(void) // Disable power for the GNSS
{
  am_hal_gpio_pincfg_t pinCfg = g_AM_HAL_GPIO_OUTPUT; // Begin by making the gnssEN pin an open-drain output
  pinCfg.eGPOutcfg = AM_HAL_GPIO_PIN_OUTCFG_OPENDRAIN;
  pin_config(PinName(gnssEN), pinCfg);
  delay(1);

  digitalWrite(gnssEN, HIGH); // Disable GNSS power (HIGH = disable; LOW = enable)
}

void setup()
{
  // Configure the I/O pins
  pinMode(LED, OUTPUT);

  pinMode(iridiumPwrEN, OUTPUT); // Configure the Iridium Power Pin (connected to the ADM4210 ON pin)
  digitalWrite(iridiumPwrEN, LOW); // Disable Iridium Power
  pinMode(superCapChgEN, OUTPUT); // Configure the super capacitor charger enable pin (connected to LTC3225 !SHDN)
  digitalWrite(superCapChgEN, LOW); // Disable the super capacitor charger
  gnssOFF(); // Disable power for the GNSS

  pinMode(busVoltageMonEN, OUTPUT); // Make the Bus Voltage Monitor Enable an output
  digitalWrite(busVoltageMonEN, HIGH); // Set it high to enable the measurement
  //digitalWrite(busVoltageMonEN, LOW); // Set it low to disable the measurement (busV should be ~zero)

  analogReadResolution(14); //Set resolution to 14 bit

Example 3 - PHT

The first example we'll take a look at is Example 3 - PHT. This example demonstrates how to ‎interact with the MS8607 PHT Sensor to retrieve pressure, humidity, and temperature data from the ‎sensor. The code performs all of the AGT pin definitions and custom functions listed above and ‎initializes the MS8607 on the I2C bus:‎

Copy Code
if (barometricSensor.begin(agtWire) == false)
  {
    Serial.println("MS8607 sensor did not respond. Trying again...");
    if (barometricSensor.begin(agtWire) == false)
    {
      Serial.println("MS8607 sensor did not respond. Please check wiring.");
      while(1)
        ;
    }
  }

After initializing the sensor, the code polls for temperature (in °C), pressure (in hPa or mbar) and ‎humidity (in %RH) data from the sensor and prints it out over serial every 500ms. Open the serial ‎monitor with the baud set to 115200 to watch the environmental data print out.‎

Users who prefer to use an external PHT sensor should refer to Example 4 - External PHT for a ‎demonstration of that application.‎

Example 5 - GNSS

Example 5 shows how to use the ZOE-M8Q to get GNSS positioning data. Upload the example and ‎open the serial terminal with the baud set to 115200 and input set to Newline. The setup initializes ‎the Wire port and sets the clock speed to 100kHz for optimal performance:‎

Copy Code
agtWire.begin();
agtWire.setClock(100000);

Before initializing the ZOE-M8Q, the code waits for a user input to confirm the serial monitor ‎settings are correct. After user input, the code turns the ZOE-M8Q on, waits one second for the ‎module to power up, initializes it on the I2C bus, and sets it to output only UBX data:‎

Copy Code
Serial.println(F("Please check that the Serial Monitor is set to 115200 Baud"));
Serial.println(F("and that the line ending is set to Newline."));
Serial.println(F("Then click Send to start the example."));
Serial.println();
while(Serial.available() == 0)
;

gnssON(); // Enable power for the GNSS
delay(1000); // Let the ZOE power up

if (myGNSS.begin(agtWire) == false) //Connect to the u-blox module using pads 8 & 9
{
    Serial.println(F("u-blox GNSS not detected at default I2C address. Please check wiring. Freezing."));
    while (1)
        ;
}    

//myGNSS.factoryDefault(); delay(5000); // Uncomment this line to reset the ZOE-M8Q to the factory defaults

//myGNSS.enableDebugging(); // Uncomment this line to enable helpful debug messages on Serial

myGNSS.setI2COutput(COM_TYPE_UBX);

The main loop checks for the GNSS fix and prints out what type of fix the module has (Dead ‎Reckoning, 2D, 3D or GNSS+Dead Reckoning). Once the ZOE-M8Q has a GNSS fix the code pulls ‎and prints out latitude, longitude, and altitude data from the module.‎

The two commented out lines allow the user to reset the ZOE-M8Q to factory defaults and enable ‎serial debugging. Sending the factory default command can help recover the ZOE-M8Q in case it ‎gets stuck in an unresponsive state. Enabling serial debugging tells the ZOE-M8Q to send all ‎debug data over serial for troubleshooting.‎

Example 6 - Geofence

Example 6 builds on the previous example to set up four geofence areas for the ZOE-M8Q to ‎monitor. The code sets everything up just like the previous GNSS example. When the module finds ‎a 3D fix, the code prints the longitude and latitude, creates settings for the four geofence areas, ‎clears any existing geofences stored and then sets four geofence areas of 5m, 10m, 15m, and 20m:‎

Copy Code
uint32_t radius = 500; // Set the radius to 5m (radius is in m * 10^-2 i.e. cm)
byte confidence = 2; // Set the confidence level: 0=none, 1=68%, 2=95%, 3=99.7%, 4=99.99%
byte pinPolarity = 0; // Set the PIO pin polarity: 0 = low means inside, 1 = low means outside (or unknown)
byte pin = 14; // ZOE-M8Q PIO14 is connected to the geofencePin

Serial.print(F("Clearing any existing geofences. clearGeofences returned: "));
Serial.println(myGNSS.clearGeofences());

Serial.print(F("addGeofence for geofence 1 returned: "));
Serial.println(myGNSS.addGeofence(latitude, longitude, radius, confidence, pinPolarity, pin));

radius = 1000; // 10m
Serial.print(F("addGeofence for geofence 2 returned: "));
Serial.println(myGNSS.addGeofence(latitude, longitude, radius, confidence, pinPolarity, pin));

radius = 1500; // 15m
Serial.print(F("addGeofence for geofence 3 returned: "));
Serial.println(myGNSS.addGeofence(latitude, longitude, radius, confidence, pinPolarity, pin));

radius = 2000; // 20m
Serial.print(F("addGeofence for geofence 4 returned: "));
Serial.println(myGNSS.addGeofence(latitude, longitude, radius, confidence, pinPolarity, pin));

The main loop monitors the state of the four geofences and prints out both the combined and ‎individual status of the geofences every second:‎ 

Copy Code
geofenceState currentGeofenceState; // Create storage for the geofence state

boolean result = myGNSS.getGeofenceState(currentGeofenceState);

Serial.print(F("getGeofenceState returned: ")); // Print the combined state
Serial.print(result); // Get the geofence state

if (!result) // If getGeofenceState did not return true
{
Serial.println(F(".")); // Tidy up
return; // and go round the loop again
}

// Print the Geofencing status
// 0 - Geofencing not available or not reliable; 1 - Geofencing active
Serial.print(F(". status is: "));
Serial.print(currentGeofenceState.status);

// Print the numFences
Serial.print(F(". numFences is: "));
Serial.print(currentGeofenceState.numFences);

// Print the combined state
// Combined (logical OR) state of all geofences: 0 - Unknown; 1 - Inside; 2 - Outside
Serial.print(F(". combState is: "));
Serial.print(currentGeofenceState.combState);

// Print the state of each geofence
// 0 - Unknown; 1 - Inside; 2 - Outside
Serial.print(F(". The individual states are: "));
for(int i = 0; i < currentGeofenceState.numFences; i++)
{
if (i > 0) Serial.print(F(","));
Serial.print(currentGeofenceState.states[i]);
}

byte fenceStatus = digitalRead(geofencePin); // Read the geofence pin
digitalWrite(LED, !fenceStatus); // Set the LED (inverted)
Serial.print(F(". Geofence pin (PIO14) is: ")); // Print the pin state
Serial.print(fenceStatus);
Serial.println(F("."));

delay(1000);

The on-board LED is configured to illuminate when the AGT is inside the combined geofence areas ‎and will go out when the AGT is outside them to provide a visual indicator for quickly identifying the ‎geofence area limits.‎

Example 10 - Basic Send

Reminder: The 9603N needs to be linked to an active account and line rental on Rock7 ‎Operations with sufficient message credits for the example to work properly.‎

Example 10 demonstrates how to perform a basic data transmission using the 9603N to send the ‎classic "Hello, world!" over the Iridium satellite network. The code declares the IridiumSBD object ‎with the sleep (ON/OFF) and RI (Ring Indicator) pins and creates two functions to set up and ‎control Artemis Serial1 to communicate with the 9603N modem:‎

Copy Code
IridiumSBD modem(Serial1, iridiumSleep, iridiumRI);

void IridiumSBD::beginSerialPort() // Start the serial port connected to the satellite modem
{
  diagprint(F("custom IridiumSBD::beginSerialPort\r\n"));

  // Configure the standard ATP pins for UART1 TX and RX - endSerialPort may have disabled the RX pin

  am_hal_gpio_pincfg_t pinConfigTx = g_AM_BSP_GPIO_COM_UART_TX;
  pinConfigTx.uFuncSel = AM_HAL_PIN_24_UART1TX;
  pin_config(D24, pinConfigTx);

  am_hal_gpio_pincfg_t pinConfigRx = g_AM_BSP_GPIO_COM_UART_RX;
  pinConfigRx.uFuncSel = AM_HAL_PIN_25_UART1RX;
  pinConfigRx.ePullup = AM_HAL_GPIO_PIN_PULLUP_WEAK; // Put a weak pull-up on the Rx pin
  pin_config(D25, pinConfigRx);

  Serial1.begin(19200);
}    

void IridiumSBD::endSerialPort()
{
  diagprint(F("custom IridiumSBD::endSerialPort\r\n"));

  // Disable the Serial1 RX pin to avoid the code hang
  am_hal_gpio_pinconfig(PinName(D25), g_AM_HAL_GPIO_DISABLE);
}

After uploading the code, open the serial monitor with the baud set to 115200. The code waits for ‎the user to open the serial monitor and press send before continuing with the rest of the sketch. ‎After the input, the code enables the supercapacitor charger, begins the charge cycle, and then ‎attempts to initialize the 9603N once the charge cycle is complete. Serial prints accompany all these ‎functions for users to follow along with.‎

Assuming the 9603N initialized correctly, the code checks the signal quality, prints out a value ‎between 0 and 5 (5 being the strongest signal quality) and then attempts to send a text message of ‎‎"Hello, world!" over the network. This may take several minutes, if the message was sent ‎successfully, the code prints "Hey, it worked!" otherwise, the code prints "Try again with a better ‎view of the sky.".‎

Regardless of success or failure of sending the text message, the code finishes by clearing the ‎Mobile Originated message buffer, puts the 9603N to sleep and then disables power to the 9603N ‎and supercapacitor charge circuit. Note, this code is not a loop and if it fails, you'll need to reset the ‎AGT before attempting again.‎

Example 16 - Global Tracker

The last example this tutorial combines everything together to provide a comprehensive global ‎tracker capable of receiving a host of settings updates either via USB-C or wirelessly using Iridium ‎SBD messages. This means users can monitor and configure the device depending on the ‎application's needs while the AGT is in the field.‎

The example gets a 3D fix from the ZOE-M8Q, environmental readings from the MS8607, ‎measures the bus voltage, and transmits the data at a set interval via Iridium SBD messages. The ‎code also stores many settings in EEPROM (Flash) to be configured either via the USB port or an ‎Iridium binary message sent from Rock7 Operations. ‎

On top of all that, the example includes the capability for users to add up to eight custom functions ‎for additional sensor or other devices in use with the AGT. For those curious about the message ‎format, please review this page in the GitHub repository.‎

The code defaults to send a text message every five minutes of the following data fields:

  • DATETIME: GNSS date and time in YYYYMMDDHHMMSS format

  • LAT: GNSS latitude in degrees

  • LON: GNSS longitude in degrees

  • ALT: GNSS altitude above mean sea level in meters

This example works in tandem with the Artemis Global Tracker Configuration Tool we cover in the ‎next section.‎

Artemis Global Tracker Configuration Tool

The Artemis Global Tracker Configuration Tool lets users quickly update a host of settings on the ‎AGT while running the Global Tracker Arduino Example either locally using a USB-C connection or ‎remotely via Iridium messages.‎

Artemis Global Tracker Configuration Tool

The AGT Configuration tool provides a helpful GUI (Graphical User Interface) for users to pick and ‎choose what information the AGT sends in its update messages, message format, and various alarm ‎messages. The AGT ships with Example 16 - Global Tracker running on the board to let you use ‎the Configuration Tool out of the box. Note, the AGT must be running this example for the ‎Configuration Tool to function. Users looking to modify the example to add their own functions ‎should note the example allows for adding up to eight custom functions to interact with using the ‎Configuration Tool.‎

tool_16

The Configuration Tool is available both as a Python script and Windows executable (.exe). Users ‎familiar with Python and able to install PyQt5 along with all other required modules can ‎run AGTCT.py otherwise users can run the tool as an executable on Windows 64-bit systems. Both ‎versions of the tool are hosted on the GitHub repository in the "Tools" folder and function ‎identically on the front-end user interface.‎

Configuration Tool Options

The Configuration Tool offers a lot of options to customize the data sent by the AGT. Users can ‎customize everything from data sent in messages, various alarm messages ranging from ‎environmental readings, Geofence positions to battery voltage and even custom functions users ‎can write into the Global Tracker Example. Users curious about the message format can read about ‎it on this page in the GitHub repository.‎

Local Configuration Tool Updates

For local updates, start off by plugging the AGT to your computer with a USB-C cable and take note ‎of the COM port the device enumerates on. Open the Configuration Tool, select your port and click ‎the "Open Port" button. (If you do not see the correct port, click the Refresh button, and retry.) You ‎should see a welcome message in the Serial Monitor window with the firmware version after ‎opening the port.‎

Remote Configuration Tool Updates

Remote configuration using Iridium messages follows nearly the same steps as local configuration. ‎Before selecting the settings in the Configuration Tool, go ahead and log into your Rock7 ‎Operations account. Next, open the Configuration Tool (if it is not open already) and go through the ‎steps to create the configuration files as you would normally do but without opening a port. Once ‎you are ready, click the "Calculate Config" button and you should see a long hex string in the ‎‎"Configuration Message" window. Select the entire message and copy it.‎

With the message copied, go to your Rock7 Operations and click on the "Send a message" tab. ‎Make sure to select "Mode Hex" and then paste the configuration message into the "Hex String" ‎window. Select the RockBLOCK serial number for the tracker(s) you want to update and click "Send ‎Message". This saves the settings and stores them for the next time the AGT sends a message.‎

Artemis Global Tracker Mapping Tools

We also have a suite of Mapping Tools hosted on the GitHub Repository to allow users to track up ‎to eight AGT devices using Google Maps Static API. For more information on these tools and how ‎to use them, refer to this page in the GitHub repository.‎

Troubleshooting

This tutorial covered a lot so in this section we'll revisit a few troubleshooting tips for the Artemis ‎Global Tracker included in this guide.‎

Arduino Examples

The Arduino Examples provide the quickest way to troubleshoot most common problems with the ‎AGT. We've done our best to have dedicated examples to most circuits on the board to test ‎everything from the bus voltage to low power mode along with testing the PHT sensor, ZOE-M8Q ‎and 9603N. We recommend any users experiencing issues with their AGT start with these ‎examples to help narrow down and potentially resolve the issue.‎

Compile Errors

If you experience any compilation or upload errors in Arduino, make sure you are using ‎version 2.1.0 of the Apollo3 Arduino core. Once the latest version of that core has no issues with ‎the AGT Arduino Examples we'll update this section.‎

Insufficient Power for 9603N SBD Transmission

As a reminder, power configurations using a solar panel or other low-current power supply need to ‎have an additional pair of 10F capacitors soldered to the indicated PTH pads. Solar panels cannot ‎typically provide sufficient current to run the supercapacitor charge circuit at 150mA and we ‎recommend adjusting the Charge Current jumper to set the charge current to 60mA.‎

Iridium Line Rental and Credits

In order to send and receive messages on the Rock7 network users must set up an account ‎on Rock7, purchase a line rental and credits from Rock7.‎

Example 10 Message Lost

You may find when running Example 10 (or other messaging examples if you skip Example 10) the ‎message does not arrive at the endpoints/delivery group on first try. We found this message can ‎get "lost" on first use with a new modem. If you do not receive the message on the endpoint, try ‎running the example again and it should send the message. Note, you should not be charged any ‎credits for the first "lost" message.‎

Antenna Signal

One of the most common causes of issues with both the ZOE-M8Q GNSS transceiver and 9603N ‎modem is antenna signal. If either of these components have issues with receiving or sending data, ‎make sure the antenna has a clear view of the sky away from large objects like buildings or large ‎trees.‎

Also, remember to only power the 9603N or ZOE-M8Q individually to prevent conflicts using the ‎shared antenna. While the AGT includes a protection circuit to prevent both devices from using the ‎antenna at the same time, the circuit prioritizes the ZOE-M8Q antenna over the 9603N so if both ‎are powered on, only the ZOE-M8Q will have an antenna connection.‎

General Troubleshooting and Technical Assistance

Not working as expected and need help? ‎

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.

CREATE NEW FORUM ACCOUNT        LOG INTO SPARKFUN FORUMS

Resources and Going Further

If you made it this far, congratulations! Your Artemis Global Tracker should be fully configured and ‎ready to transmit data from anywhere on Earth. For more information about the AGT or the ‎components on it, please refer to the resources below:‎

Artemis Global Tracker Documentation

Artemis Module Documentation

Iridium 9603N Transceiver Documentation

u-blox M8Q Documentation

MS8607 PHT Sensor Documentation

מק"ט יצרן # 18712
ARTEMIS GLOBAL TRACKER ZOE-M8Q
SparkFun Electronics
₪ 1,636.52
הצגת עוד Details
מק"ט יצרן # 15426
CBL USB2.0 A PLUG TO C PLG 0.98'
SparkFun Electronics
מק"ט יצרן # 15425
CBL USB2.0 A PLUG TO C PLG 2.62'
SparkFun Electronics
מק"ט יצרן # 14743
CABLE A PLUG TO C PLUG 3.28'
SparkFun Electronics
מק"ט יצרן # 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
מק"ט יצרן # 13782
MONOCRYSTALIN SOLAR CELL 3.5W 7V
SparkFun Electronics
מק"ט יצרן # 13781
MONOCRYSTALLINE SOLAR CELL 2W 7V
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.