Maker.io main logo

Assembling Keybow

2024-03-21 | By Pimoroni

License: See Original Project Raspberry Pi SBC

Courtesy of Pimoroni

Guide by Pimoroni

In this tutorial, you'll learn how to assemble your Keybow mini mechanical ‎keyboard. Assembly should take 15 to 20 minutes, and the only tool you'll ‎need is a Phillips screwdriver. We'll fit the Raspberry Pi Zero WH to the acrylic ‎baseplate first, then fit the Keybow PCB, and last of all fit the switches and ‎key caps.‎

Attaching the Raspberry Pi Zero WH to the baseplate

We'll begin by attaching the rubber feet to the thicker acrylic plate.‎

Peel the protective film off the two acrylic pieces very carefully. The thinner ‎piece is especially fragile, so be really careful when peeling the film off this ‎one. Take the thicker piece and turn it so that you can read the Keybow text. ‎Stick the four rubber, self-adhesive feet to the acrylic where the four outlined ‎circles are.‎

attach_1

Next, we'll attach the Raspberry Pi Zero WH to the acrylic baseplate.‎

Remove the Zero WH from its antistatic bag. Flip the baseplate over, so that ‎the rubber feet are now sitting on the surface on which you're working, and ‎the outline of the Zero WH is at the top left corner. Sit the Zero WH on this ‎space, with the GPIO pins towards the top of the acrylic baseplate (the solder ‎joints underneath the Zero WH's header should sit neatly in the cutout at the ‎top). Use two of the M2.5 metal screws and two nuts to attach the Zero WH ‎using the bottom pair of mounting holes (the ones further away from the ‎Zero WH's GPIO pins.)‎

mount_2

The thinner acrylic piece is a shim layer that levels up the metal standoffs ‎that attach the Keybow PCB to the baseplate and Zero WH, so that they all ‎sit at the same height. We'll fit it now, using one of the standoffs.‎

Slot the shim layer next to the Zero WH on the baseplate; it'll only fit one way. ‎Take one of the metal standoffs and one of the metal M2.5 screws. Push the ‎screw through the hole at the bottom right corner of the baseplate and shim ‎layer, from below, then screw the female end of the metal standoff onto the ‎screw.‎

Take care not to overtighten any of the metal screws, as you'll risk cracking ‎the acrylic.‎

Lastly, screw the remaining nut all the way onto the male thread on the top ‎of the standoff that you just fitted. This will sit in the mounting hole on the ‎Keybow PCB that doesn't have a threaded metal post and keep that corner ‎level.‎

level_3

Don't fit any of the other standoffs to the acrylic baseplate yet!‎

Attaching the Keybow PCB

The three other mounting holes on the Keybow PCB have threaded metal ‎posts. We'll be screwing the male-threaded ends of the metal standoffs into ‎these metal posts. Peel off the little amber pieces of protective film off the ‎posts and screw in the standoffs.‎

attach_4

You can now push your Keybow PCB's female GPIO header down onto the ‎male GPIO pins on the Zero WH. Make sure that all the pins are lined up ‎correctly. There will be a little gap left between the headers, but don't worry ‎because they'll still be making good electrical contact.‎

Use the remaining three metal M2.5 screws to attach the standoffs to the ‎acrylic baseplate, again taking care not to overtighten them and crack the ‎acrylic.‎

baseplate_5

Mounting the switches and key caps

The switches push tightly into the PCB switch plate, and then the whole plate ‎with switches mounted pushes down onto the Keybow PCB, with the pins on ‎the switches being gripped in the hot-swap sockets.‎

It's important that you orient the switches the right way round when pushing ‎them into the plate. If you look carefully at the switches, you'll see they have ‎a little cavity underneath on one edge. If you turn the switch plate so that the ‎black and gold side is facing upwards, and the KEYBOW text is at the right-‎hand side, then the cavities on the switches should all be at the top.‎

Push each switch into the plate, so that they sit flush. They're quite a tight fit, ‎but they should click in when they're properly fitted.‎

switch_6

Next, we'll mount the key caps. It doesn't matter which way round they go, as ‎they're completely symmetrical. Push them all the way down onto the stems ‎on the switches.‎

flip_7

Flip the switch plate with switches and key caps mounted and take a look at ‎all of the pins on the switches. Sometimes, they can get bent slightly in ‎transit, but they all need to be straight to fit correctly into the hot-swap ‎sockets. You can gently bend them back into position if you need to.‎

turn_8

Turn your Keybow PCB assembly and switch plate so that the KEYBOW logos ‎are both at the same side. Align the two pieces with each other, and gently ‎sit the switch plate and switches in the correct location with the pins on the ‎switches in the sockets on the PCB. Once you're happy that they're all ‎correctly aligned, then push the switches down into the sockets. It's best to ‎hold the whole thing at both sides and apply even pressure, so that they all ‎go in straight. The bottoms of all of the switches should sit flush with the ‎Keybow PCB.‎

Next steps

The next step is to set up the Keybow software and customise your key ‎mappings. We'll cover all of that in the Setting up the Keybow OS tutorial.‎

That's all folks!

מק"ט יצרן # PIM450
KEYBOW MINI MACRO PAD KIT - CLIC
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.