Maker.io main logo

Bitcoin / Multi Crypto Coin Price Ticker with 24 candlechart

83

2023-01-08 | By M5Stack

License: General Public License Arduino

* Thanks for the source code and project information provided by @frittna

Story

2

 

MULTI CRYPTO COIN PRICE TICKER with 24 candle stick chart for M5Stack Core

##SD-CARD Version with configuration text file##

receiving WiFi data from Binance API/Websocket_v3

This will show a 24-candle chart, the min/max price and the volume as line, date and time are from time.nist.gov timeserver. For M5-Stack MCU, coded in ArduinoIDE 1.8.13 - last modified Nov.20.2021 15:20 CET - Version 1.0.53fix - using spiffs SDconfig (https://github.com/frittna/Crypto_Coin_Ticker)

LAST (small) EDITS:

-added cycling function (ButtonA ButtonC together) which steps through your currencies after a certain time (default:off; when on - default:15sec for each)

-added Timezone for Singapore (UTC 8)

-code merged to one version, so there is no need to have different versions anymore

-autodetect the built in SHT room sensor and adds a 12pixel high sensor panel when the M5Stack is in its vertical BTC stand (original grey holder)

-temperature unit C or F and offset can be set by SD-Config and is not hard-coded anymore (because the M5-Stack is heating up itself it will never be accurate and has only limited expressiveness.)

> do not forget to update your sdconfig.cfg on SD-card too <

 

 

##Using the App:

  • This version needs a SD-Card (at least on first load) with your WiFi credentials, favorite coinpairs, timezone and language (eng/ger/esp) etc. in a textfile - see instructions
  • ButtonA: switches through your favorite coinpairs (as many you want) e.g: BTC/USDT or LINK/BNB etc. which are available on Binance.com's spot maket.
  • ButtonB: changes the LCD-Brightness in 4 levels
  • ButtonC: 9 changeable Timeframes from 1 Minute to 1 Month
  • turn OFF the device pressing the red button once OR by holding ButtonC for over 1 second if USB is connected
  • Press buttonC, then, within 2 sec press buttonA to switch down, or buttonB to switch up through the timeframes: 1min->15mins->1hour->...or vice versa
  • available timeframes are 1minute, 3m, 5m, 15m, 1h, 4h, 1d, 1w, 1Month
  • if you hold ButtonC at Startup: it will start with alternative SSID2/WiFi-password2 instead (e.g your mobile phone's hotspot)
  • press ButtonA and ButtonC together to enable/disable automatic cycling through all currencies after a set time (default: off, when turned on default: 15sec)

 

 

 

##Further description:

  • The top info panel shows WiFi-strength, battery level, colored indicators for "busy", Sleep Timer on, price moving and if it is charging from usb (can have delay up to 30s)
  • right now: English, German, Spanish (for day and month names)
  • Sleep Timer: when holding ButtonB longer than 1, 5 seconds it will start a user defined timer to power OFF the device (45min default)
  • If WiFi is failing more than 2 minutes, it reduces the reconnect interval and brightness level - after 10 minutes -> shutdown device
  • SDMenu Loader compatible, if SD-Updater (menu.bin) is installed in your SD-card hold buttonA while booting up to start MenuLoader to load your apps (ver. 0.5.2 tested only)
  • It is prepared for the use of a Neopixel RGB-LED bar (I use the built-in one in the Battery-Bottom Module for M5Stack/Fire with RGB 10 LEDs)
  • All settings will remain stored in internal memory after a reset so you can eject the SD-Card after setting up you favorites.
  • If you want to clear all stored settings from internal memory hold ButtonB at start-up
  • If M5-Stack is in the BTC stand (the original grey vertical stand) the internal SHT room sensor is found and shows temp and humidity in degree F or C.

--> SEE CODE OR READMEs FOR INSTRUCTION IF YOU'RE NOT SURE <--

 

3

 

4

3

4

5

6

7

8

10

 

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.