Maker.io main logo

Building the scroll:bit Bear Badge Kit

2022-08-25 | By Pimoroni

License: See Original Project

Coutesy of Pimoroni

Guide by Pimoroni

This tutorial will show you how to put your scroll:bit kit (also known as the ‎Bear Badge Kit) together. The materials in the kit include three versions of ‎the bear's t-shirt, so you can pick your favourite colour and save the others ‎for later.‎

With this kit you'll be able to complete a number of projects that we've ‎written for the scroll:bit, including a name badge and a fortune-telling bear!‎

It should take less than 15 minutes to assemble the kit.‎

We have included simplified instructions in with the kit, on the first of the ‎printed cards. If you prefer video instructions, take a look at our YouTube ‎channel.‎

cards_1

Prepare the Acrylic Pieces

The acrylic pieces come with a protective plastic film on them that you'll have ‎to peel off before you assemble the kit. You'll need to do this for the bear's ‎body, two arms, and whichever colour t-shirt you choose.‎

acrylic_2

Stacking the Pieces

The arms can be placed either way up, giving your bear an arms-up "yay!" ‎effect, or an arms-down bodybuilder bear. The choice is yours!‎

stack_3

Whichever way you decide the arms should go, make sure the holes on the ‎arms line up with the four holes on the bear's body. Just lie the arms down ‎on top for now.‎

arm_4

The next thing you'll need is the scroll:bit, which you'll find in the silver anti-‎static bag. It has four holes that line up with the ones on the body and the ‎arms. Add the scroll:bit to the stack, and then choose a coloured t-shirt.‎

next_5

Again, line up the four holes in the t-shirt with the holes on the stack of ‎pieces. This completes the stack, and now we just need to bolt it together.‎

line_6

Bolting the Stack Together

There are a few different bits in the bolt pack, but you'll you want the long ‎black bolts for this kit (the bolt pack is also used for other things, so you'll ‎have some left over). Find the matching black hexagonal nuts; you'll need ‎four bolts and four nuts.‎

Note that the white bolts in the pack are too short to assemble the whole bear ‎stack, although you could use them for a bear without a t-shirt!‎

bolts_7

Starting from the front, push the first bolt through all the pieces. The bolt ‎goes through the t-shirt, then through the scroll:bit, then through the arm, ‎then through the body.‎

start_8

start_9

Repeat this for the other three bolts. If the other arm falls off while you are ‎doing one side, just tuck it back in between the body and the scroll:bit once ‎you've finished the other side.‎

repeat_10

This is what the finished bear looks like. We're ready now to add the micro:bit ‎and accessories.‎

finish_11

Adding the Accessories

To finish your Bear Badge, we need to add the micro:bit, lanyard, and battery ‎pack.‎

The micro:bit pushes into a slot on the scroll:bit. It's right at the front and I'm ‎pointing at it in the picture below. When you push the micro:bit into the slot, ‎make sure it's lined up correctly so as not to damage anything.‎

accessories_12

The micro:bit should be facing you (the side with the two buttons and LED ‎matrix), and the shiny gold connectors at the bottom push down into the slot ‎on the scroll:bit. It's quite a tight fit, so you'll need to press firmly.‎

press_13

If you want to carry the bear around, clip the lanyard to the oval hole at the ‎top. You can also clip it to either ear if you want your bear a jaunty angle!‎

carry_14

To connect the battery pack, look for the white socket on top of the micro:bit ‎‎(it's on the back). It has a little notch on the side of the socket nearest the ‎bear's body, and if you look at the white connector on the battery pack cable, ‎you'll see a ridge. Line this ridge on the connector up with the notch on the ‎socket and push it in.‎

connect_15

You can tape or Blu Tack the battery pack to the back of the bear, if you like, ‎to keep it from flapping around.‎

tape_16

You're done! Remember you can change the t-shirt colour and arm position.‎

done_17

To buy the Bear Badge Kit head to our shop or, to see a video version of this ‎tutorial, head to our youtube channel.‎

Next steps

Now that you've built your bear badge, you can start coding it! Follow the ‎activities on the cards in your kit to learn how to install the scroll:bit software, ‎and how to turn your bear into a name badge or fortune-teller.‎

That's all folks!‎

מק"ט יצרן # PIM362
SCROLL:BIT MICRO:BIT KIT
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.