Maker.io main logo

Character LCD with Raspberry Pi or BeagleBone Black

145

2016-01-04 | By Adafruit Industries

License: See Original Project BeagleBone Raspberry Pi SBC

Courtesy of Adafruit

Guide by Tony DiCola

Overview

Looking for a simple way to add a text display to your Raspberry Pi or BeagleBone Black project? Consider using a character LCD with the Python character LCD library! These classic displays can show a few lines of text, are inexpensive, and easily readable during the day or night with a bright backlight. You can follow this guide to learn how to connect a character LCD to a Raspberry Pi or BeagleBone Black and control the display from your own Python code!

Before you get started it will help to familiarize yourself with the character LCD guide. You will also want to make sure your Raspberry Pi is running the latest Raspbian operating system, and your BeagleBone Black is running the latest Debian or Debian-based distribution like Ubuntu.

If you haven't used a Raspberry Pi or BeagleBone Black, be sure to follow the Learn Raspberry Pi series or BeagleBone Black SSH guide to understand the basic usage of each board and how to connect to a command terminal.

When you're ready to get started, grab a character LCD, contrast adjustment potentiometer (included with Adafruit character LCDs), and a Raspberry Pi or BeagleBone Black. Continue to the next page to learn how to wire the display to your board.

Wiring

Follow the steps below to wire a character LCD to your development board. Be careful to connect each wire to the correct pins as there are quite a few wires necessary to use the character LCD.

Note: The wiring below is for an RGB backlight display. If you're using a monochrome backlight display you can use the wiring as-is and ignore the green and blue backlight wires. The red backlight wire will be used to control the monochrome display's backlight.

If you would like to permanently turn on the LCD backlight, connect the red, green, blue backlight wires to ground instead of to your development board.

Raspberry Pi

Wire your character LCD to the Raspberry Pi as follows:

  • Connect Pi 5V power to the power rail of the breadboard. From the power rail connect one outer lead of the potentiometer, LCD pin 2 (VDD), and LCD pin 15 (LED ).
  • Connect Pi ground to the ground rail of the breadboard. From the ground rail connect the other outer lead of the potentiometer, LCD pin 1 (VSS), and LCD pin 5 (R/W).
  • Connect the middle lead of the potentiometer to LCD pin 3 (V0/contrast).
  • Connect Pi pin 27 (or 21 on older revision Pi's) to LCD pin 4 (RS).
  • Connect Pi pin 22 to LCD pin 6 (E/clock enable).
  • Connect Pi pin 25 to LCD pin 11 (DB4).
  • Connect Pi pin 24 to LCD pin 12 (DB5).
  • Connect Pi pin 23 to LCD pin 13 (DB6).
  • Connect Pi pin 18 to LCD pin 14 (DB7).
  • Connect Pi pin 4 to LCD pin 16 (-R/red).
  • Connect Pi pin 17 to LCD pin 17 (-G/green).
  • Connect Pi pin 7 / CE1 to LCD pin 18 (-B/blue).

BeagleBone Black

Wire your BeagleBone Black to the LCD as follows. If you aren't familiar with how to identify pins on the board, be sure to read the BeagleBone Black GPIO guide.

  • Connect BeagleBone Black 5V power pin P9_7 to the power rail of the breadboard. From the power rail connect one outer lead of the potentiometer, LCD pin 2 (VDD), and LCD pin 15 (LED ).
  • Connect BeagleBone Black ground pin P8_2 to the ground rail of the breadboard. From the ground rail connect the other outer lead of the potentiometer, LCD pin 1 (VSS), and LCD pin 5 (R/W).
  • Connect the middle lead of the potentiometer to LCD pin 3 (V0/contrast).
  • Connect BeagleBone Black pin P8_8 to LCD pin 4 (RS).
  • Connect BeagleBone Black pin P8_10 to LCD pin 6 (E/clock enable).
  • Connect BeagleBone Black pin P8_18 to LCD pin 11 (DB4).
  • Connect BeagleBone Black pin P8_16 to LCD pin 12 (DB5).
  • Connect BeagleBone Black pin P8_14 to LCD pin 13 (DB6).
  • Connect BeagleBone Black pin P8_12 to LCD pin 14 (DB7).
  • Connect BeagleBone Black pin P8_7 to LCD pin 16 (-R/red).
  • Connect BeagleBone Black pin P8_9 to LCD pin 17 (-G/green).
  • Connect BeagleBone Black pin P8_11 to LCD pin 18 (-B/blue).

BeagleBone Black with PWM

The above wiring will use digital IO to control the colors of the backlight display. This means the backlight can only show 7 different colors (all the combinations of the 3 backlight LEDs). However because the BeagleBone Black supports PWM (pulse-width modulation) control of some hardware pins, it's possible to use PWM pins to control the backlight LEDs and display a range of almost all colors.

To use PWM control of the backlight LEDs, wire your BeagleBone Black to the LCD as follows. Note that this wiring is exactly the same as the non-PWM wiring, except the 3 backlight LED pins (red, green, blue) are moved to different pins.

  • Connect BeagleBone Black 5V power pin P9_7 to the power rail of the breadboard. From the power rail connect one outer lead of the potentiometer, LCD pin 2 (VDD), and LCD pin 15 (LED ).
  • Connect BeagleBone Black ground pin P8_2 to the ground rail of the breadboard. From the ground rail connect the other outer lead of the potentiometer, LCD pin 1 (VSS), and LCD pin 5 (R/W).
  • Connect the middle lead of the potentiometer to LCD pin 3 (V0/contrast).
  • Connect BeagleBone Black pin P8_8 to LCD pin 4 (RS).
  • Connect BeagleBone Black pin P8_10 to LCD pin 6 (E/clock enable).
  • Connect BeagleBone Black pin P8_18 to LCD pin 11 (DB4).
  • Connect BeagleBone Black pin P8_16 to LCD pin 12 (DB5).
  • Connect BeagleBone Black pin P8_14 to LCD pin 13 (DB6).
  • Connect BeagleBone Black pin P8_12 to LCD pin 14 (DB7).
  • Connect BeagleBone Black pin P9_16 to LCD pin 16 (-R/red).
  • Connect BeagleBone Black pin P9_14 to LCD pin 17 (-G/green).
  • Connect BeagleBone Black pin P8_13 to LCD pin 18 (-B/blue).

Usage

Dependencies

Before installing the character LCD library you'll need to make sure a few dependencies are installed by following the steps below. Make sure your development board has access to the internet so the software can be downloaded.

Raspberry Pi

On the Raspberry Pi execute the following commands in a terminal/SSH session on the Pi:

Copy Code
sudo apt-get update
sudo apt-get install build-essential python-dev python-smbus python-pip git
sudo pip install RPi.GPIO

You can ignore any warnings about dependencies already being installed.

BeagleBone Black

On the BeagleBone Black execute the following commands in a terminal/SSH session on the device:

Copy Code
sudo apt-get update
sudo apt-get install build-essential python-dev python-smbus python-pip git
sudo pip install Adafruit_BBIO

You can ignore any warnings about dependencies already being installed.

Installation

Once the dependencies above have been installed you can install the character LCD module by executing the following commands on the device:

Copy Code
cd ~
git clone https://github.com/adafruit/Adafruit_Python_CharLCD.git
cd Adafruit_Python_CharLCD
sudo python setup.py install

These commands will clone the GitHub repository with the library source and then execute the setup.py script to install the library.

Usage

Once the library is installed you can find a few examples of its usage in the examples subdirectory. If you're using a monochrome backlight LCD (i.e. single color, like a white on blue LCD) the char_lcd.py script will demonstrate the basic usage.

If you're using a Raspberry Pi and have wired it according to this guide, you can immediately run the example. However if you're using a BeagleBone Black or changed the wiring, first open char_lcd.py in a text editor (like nano) and uncomment/comment the lines towards the top that set the LCD pins.

Note: If you're using a BeagleBone Black wired for hardware PWM of the backlight, skip down the page to the section on using hardware PWM.

To run the example execute:

Copy Code
cd examples
python char_lcd.py

You should see the LCD backlight turn on and messages printed to the display. For example below is what you will see with a 20x4 blue backlight LCD:

To demonstrate the usage of the library I'll walk through the source code of the char_lcd.py example below. 

Copy Code
import math
import time
     
import Adafruit_CharLCD as LCD

The first part of the script are commands to import modules that will be used. In particular the Adafruit_CharLCD module is imported under the name LCD. Later in the script you can see how classes from the char LCD module are used to interact with the LCD. 

Copy Code
# Raspberry Pi pin configuration:
lcd_rs        = 27  # Note this might need to be changed to 21 for older revision Pi's.
lcd_en        = 22
lcd_d4        = 25
lcd_d5        = 24
lcd_d6        = 23
lcd_d7        = 18
lcd_backlight = 4
     
# BeagleBone Black configuration:
# lcd_rs        = 'P8_8'
# lcd_en        = 'P8_10'
# lcd_d4        = 'P8_18'
# lcd_d5        = 'P8_16'
# lcd_d6        = 'P8_14'
# lcd_d7        = 'P8_12'
# lcd_backlight = 'P8_7'

The next part of the script configures which pins are connected to the LCD. You can see the Raspberry Pi configuration is uncommented by default, and below it the BeagleBone Black configuration is commented. You can use any digital GPIO pins in the configuration. 

Copy Code
# Define LCD column and row size for 16x2 LCD.
lcd_columns = 16
lcd_rows    = 2
     
# Alternatively specify a 20x4 LCD.
# lcd_columns = 20
# lcd_rows    = 4

This section of the script configures the size of the LCD. By default the code assumes a 16 column, 2 row LCD however you can adjust the configuration to a 20x4 or other size display supported by the HD44780.

Copy Code
# Initialize the LCD using the pins above.
lcd = LCD.Adafruit_CharLCD(lcd_rs, lcd_en, lcd_d4, lcd_d5, lcd_d6, lcd_d7, 
                           lcd_columns, lcd_rows, lcd_backlight)

Next an instance of the Adafruit_CharLCD class is created based on the configuration specified earlier in the script. 

Copy Code
# Print a two line message
lcd.message('Hello\nworld!')
     
# Wait 5 seconds
time.sleep(5.0)
     
# Demo showing the cursor.
lcd.clear()
lcd.show_cursor(True)
lcd.message('Show cursor')
     
time.sleep(5.0)
     
# Demo showing the blinking cursor.
lcd.clear()
lcd.blink(True)
lcd.message('Blink cursor')
     
time.sleep(5.0)
     
# Stop blinking and showing cursor.
lcd.show_cursor(False)
lcd.blink(False)

The next lines demonstrate basic usage of the LCD display class. The message function can be used to write a string of text to the display (including support for line breaks). The clear function clears the display, and the show_cursor and blink functions specify if the cursor is shown and should blink.

Although not shown above, there are other functions you might find useful on the LCD class. To see details on all functions you can have Python print help text for the class by executing (ignore the >>> prompt, it's only shown for reference as the Python interpreter):

Copy Code
python
>>> import Adafruit_CharLCD as LCD
>>> help(LCD.Adafruit_CharLCD)

You should see a description of each function on the LCD class, including some functions not shown in the example:

  • autoscroll(autoscroll) - Autoscroll will 'right justify' text from the cursor if set True, otherwise it will 'left justify' the text.
  • enable_display(enable) - Enable or disable the display. Set enable to True to enable.
  • home() - Move the cursor back to its home (first line and first column).
  • set_backlight(backlight) - Enable or disable the backlight. If PWM is not enabled (default), a non-zero backlight value will turn on the backlight and a zero value will turn it off. If PWM is enabled, backlight can be any value from 0.0 to 1.0, with 1.0 being full intensity backlight.
  • set_cursor(col, row) - Move the cursor to an explicit column and row position.

Finally, the last portion of the char_lcd.py script:

Copy Code
# Demo scrolling message right/left.
lcd.clear()
message = 'Scroll'
lcd.message(message)
for i in range(lcd_columns-len(message)):
    time.sleep(0.5)
    lcd.move_right()
for i in range(lcd_columns-len(message)):
    time.sleep(0.5)
    lcd.move_left()
     
# Demo turning backlight off and on.
lcd.clear()
lcd.message('Flash backlight\nin 5 seconds...')
time.sleep(5.0)
# Turn backlight off.
lcd.set_backlight(0)
time.sleep(2.0)
# Change message.
lcd.clear()
lcd.message('Goodbye!')
# Turn backlight on.
lcd.set_backlight(1)

You can see how the move_right and move_left functions are used to scroll the display, and further down how the set_backlight function turns off and on the backlight.

That's all there is to using the Adafruit_CharLCD class!

RGB Character LCD

If you're using an RGB backlight LCD the char_lcd_rgb.py script will demonstrate the usage.

If you're using a Raspberry Pi and have wired it according to this guide, you can immediately run the script. However if you're using a BeagleBone Black or have changed the wiring, edit the script with a text editor and uncomment/change the lines at the top that define the LCD pins.

To execute the RGB backlight example run this command from inside the examples directory:

Copy Code
sudo python char_lcd_rgb.py

You should see the LCD turn on and display different backlight colors. For example:

If you open the file char_lcd_rgb.py in a text editor (such as nano) I'll describe the important differences between it and the previous char_lcd.py example below.

Copy Code
# Example Raspberry Pi configuration:
lcd_rs = 27  # Change this to pin 21 on older revision Raspberry Pi's
lcd_en = 22
lcd_d4 = 25
lcd_d5 = 24
lcd_d6 = 23
lcd_d7 = 18
lcd_red   = 4
lcd_green = 17
lcd_blue  = 7  # Pin 7 is CE1
     
# Example BeagleBone Black configuration:
# lcd_rs = 'P8_8'
# lcd_en = 'P8_10'
# lcd_d4 = 'P8_18'
# lcd_d5 = 'P8_16'
# lcd_d6 = 'P8_14'
# lcd_d7 = 'P8_12'
# lcd_red   = 'P8_7'
# lcd_green = 'P8_9'
# lcd_blue  = 'P8_11'

The first important difference is the configuration of LCD pins. Notice there are now explicit pins defined for the red, green, and blue backlight LEDs.

Copy Code
# Initialize the LCD using the pins 
lcd = LCD.Adafruit_RGBCharLCD(lcd_rs, lcd_en, lcd_d4, lcd_d5, lcd_d6, lcd_d7,
                              lcd_columns, lcd_rows, lcd_red, lcd_green, lcd_blue)

The next line creates an instance of the Adafruit_RGBCharLCD class using the pin configuration defined earlier.

The Adafruit_RGBCharLCD class inherits from the Adafruit_CharLCD class so it has all the same functionality as demonstrated in the char_lcd.py example. In addition to the basic character LCD functionality the RGB character LCD class adds some functions to set the RGB color of the backlight. 

Copy Code
# Show some basic colors.
lcd.set_color(1.0, 0.0, 0.0)
lcd.clear()
lcd.message('RED')
time.sleep(3.0)
     
lcd.set_color(0.0, 1.0, 0.0)
lcd.clear()
lcd.message('GREEN')
time.sleep(3.0)
     
lcd.set_color(0.0, 0.0, 1.0)
lcd.clear()
lcd.message('BLUE')
time.sleep(3.0)
     
lcd.set_color(1.0, 1.0, 0.0)
lcd.clear()
lcd.message('YELLOW')
time.sleep(3.0)
     
lcd.set_color(0.0, 1.0, 1.0)
lcd.clear()
lcd.message('CYAN')
time.sleep(3.0)
     
lcd.set_color(1.0, 0.0, 1.0)
lcd.clear()
lcd.message('MAGENTA')
time.sleep(3.0)
     
lcd.set_color(1.0, 1.0, 1.0)
lcd.clear()
lcd.message('WHITE')
time.sleep(3.0)

The code above demonstrates each basic color by calling the set_color function and passing in which red, green, and blue LEDs to enable. For example the first call to set_color(1.0, 0.0, 0.0) will turn on the red LED and turn off the green and blue LED so the backlight will have a red color.

Notice how later lines combine multiple LEDs to get different colors, like calling set_color(1.0, 0.0, 1.0) to combine red and blue LEDs for a magenta/violet color.

RGB Character LCD with PWM

If you're using a RGB character LCD you can use PWM (pulse-width modulation) for fine control of the backlight color. By turning the different backlight red, green, and blue LEDs on and off very quickly with PWM, it's possible to precisely control the color of the backlight.

Note that PWM control works best when there's hardware support for PWM on your development board. The BeagleBone Black has support for up to 8 hardware controlled PWM pins and works great with the RGB character LCDs. However, the Raspberry Pi only has one hardware PWM pin and can be a little more troublesome to use PWM.

The RPi.GPIO library which is used by the character LCD library supports a software implementation of PWM on the Raspberry Pi. This lets you PWM control the RGB backlight even though the Pi doesn't have 3 hardware PWM pins. In my testing software PWM worked reasonably well with the RGB character LCD backlight. You might notice slightly incorrect colors, but otherwise software PWM is worth a shot to finely adjust the backlight color on the Raspberry Pi.

The char_lcd_rgb_pwm.py file demonstrates usage of PWM backlight control. If you're using a Raspberry Pi and have it wired to the LCD as described in this guide, you can immediately run the script. However if you have a BeagleBone Black or have changed the wiring, edit the file char_lcd_rgb_pwm.py in a text editor and comment/uncomment the lines at the top which define the LCD pins.

If you're using the BeagleBone Black make sure you've followed the wiring for hardware PWM. Specifically, the red, green, and blue backlight pins need to be connected to the P9_16, P9_14, and P8_13 pins respectively.

To run the example, make sure you're in the examples folder and run:

Copy Code
sudo python char_lcd_rgb_pwm.py

You should see the backlight turned on to different colors for a short period of time, and then a continuous gradient of colors displayed with a message showing the red, green, and blue color displayed on the LCD. For example:

You can press Ctrl-C to top the script.

The code for PWM control is very similar to non-PWM control from char_lcd_rgb.py, however there are a few important differences. The first difference is how the Adafruit_RGBCharLCD class is intialized. Notice the enable_pwm=True flag is passed to the constructor/init function:

Copy Code
# Initialize the LCD using the pins 
lcd = LCD.Adafruit_RGBCharLCD(lcd_rs, lcd_en, lcd_d4, lcd_d5, lcd_d6, lcd_d7,
                              lcd_columns, lcd_rows, lcd_red, lcd_green, lcd_blue, 
                              enable_pwm=True)

MCP230xx IO Expander

One problem with using a character LCD is that you give up a lot of GPIO pins to talk to the LCD. Four pins are used to send data, two pins are used for write and clock signals, and another pin or three are used for the backlight for a total of ~6-9 total pins! On a platform like the Raspberry Pi model A/B with only a dozen or so GPIO pins you can quickly run out of pins for other parts of your project. However with chips like the MCP23008 or MCP23017 you can easily add extra GPIO pins to your development board through an I2C interface!

If you aren't familiar with the MCP230xx series of chips, there's a great guide that describes their usage with a Raspberry Pi. Note that you don't need to install the library or code from the guide, it's only provided for reference.

Wiring

To use an MCP230xx chip with a character LCD you will need to wire the MCP chip to your board's I2C pins, and then wire the LCD to the MCP chip. Below are examples of wiring an MCP23017 to the Raspberry Pi or BeagleBone Black.

If you'd like to use an MCP23008 instead of the MCP23017 the wiring is similar, however consult the MCP23008 datasheet to see which pins are for power, ground, I2C, and GPIO.

Raspberry Pi

Wire your MCP23017 and LCD as follows:

  • Connect Pi 3.3V power to the power rail of the breadboard, and connect the MCP VDD and RESET to 3V power. Be careful to connect the 3.3 volt and not 5 volt power to these pins!
  • Connect Pi ground to the ground rail of the breadboard, and connect the MCP VSS and address pins, one outer lead of the potentiometer, the LCD ground, and the LCD R/W pin to the ground rail.
  • Connect Pi 5V power to the other outer lead of the potentiometer, LCD power, and LCD backlight pins. Note that 5 volt and not 3.3 volt power is used to power the LCD!
  • Connect the middle pin of the potentiometer to the LCD contrast/V0 pin.
  • Connect Pi I2C SCL to MCP I2C SCL.
  • Connect Pi I2C SDA to MCP I2C SDA.
  • Connect MCP GPIOA0 to LCD RS.
  • Connect MCP GPIOA1 to LCD EN/clock enable.
  • Connect MCP GPIOA2 to LCD DB4.
  • Connect MCP GPIOA3 to LCD DB5.
  • Connect MCP GPIOA4 to LCD DB6.
  • Connect MCP GPIOA5 to LCD DB7.
  • Connect MCP GPIOA6 to LCD -R/red backlight.
  • Connect MCP GPIOA7 to LCD -G/green backlight.
  • Connect MCP GPIOB0 to LCD -B/blue backlight.

Make sure you've enabled I2C on the Raspberry Pi if you haven't done so already.

BeagleBone Black

Wire your MCP23017 and LCD as follows:

  • Connect BeagleBone Black 3.3V power pin P9_3 to the power rail of the breadboard, and connect the MCP VDD and RESET to 3V power. Be careful to connect the 3.3 volt and not 5 volt power to these pins!
  • Connect BeagleBone Black ground pin P9_1 to the ground rail of the breadboard, and connect the MCP VSS and address pins, one outer lead of the potentiometer, the LCD ground, and the LCD R/W pin to the ground rail.
  • Connect BeagleBone Black 5V power pin P9_7 to the other outer lead of the potentiometer, LCD power, and LCD backlight pins. Note that 5 volt and not 3.3 volt power is used to power the LCD!
  • Connect the middle pin of the potentiometer to the LCD contrast/V0 pin.
  • Connect BeagleBone Black I2C SCL pin P9_19 to MCP I2C SCL.
  • Connect BeagleBone Black I2C SDA pin P9_20 to MCP I2C SDA.
  • Connect MCP GPIOA0 to LCD RS.
  • Connect MCP GPIOA1 to LCD EN/clock enable.
  • Connect MCP GPIOA2 to LCD DB4.
  • Connect MCP GPIOA3 to LCD DB5.
  • Connect MCP GPIOA4 to LCD DB6.
  • Connect MCP GPIOA5 to LCD DB7.
  • Connect MCP GPIOA6 to LCD -R/red backlight.
  • Connect MCP GPIOA7 to LCD -G/green backlight.
  • Connect MCP GPIOB0 to LCD -B/blue backlight.

Note that the BeagleBone Black has two I2C interfaces and this wiring will use the/dev/i2c-1 interface. Make sure there aren't any device tree overlays loaded which use these I2C pins for other purposes. The default BeagleBone Black device tree configuration with no overlays loaded will expose the necessary I2C interface for the wiring above. 

Usage

The char_lcd_mcp.py file in the library's examples folder demonstrates the usage of a character LCD (non-RGB version) with an MCP23017 IO extender. Run the script by executing this command inside the examples directory: 

Copy Code
sudo python char_lcd_mcp.py

You should see a simple demo of the LCD displaying text, cursors, and scrolling just like the char_lcd.py demo described on the previous page.

If you open char_lcd_mcp.py in a text editor you can see how to use the character LCD library with the MCP chip. Below is an overview of the file: 

Copy Code
import math
import time
     
import Adafruit_CharLCD as LCD
import Adafruit_GPIO.MCP230xx as MCP

First the required modules are imported. Notice the addition of the Adafruit_GPIO.MCP230xx module (imported under the name MCP). This MCP230xx class will be used to talk to the MCP chip and interface with the LCD. 

Copy Code
# Define MCP pins connected to the LCD.
lcd_rs        = 0
lcd_en        = 1
lcd_d4        = 2
lcd_d5        = 3
lcd_d6        = 4
lcd_d7        = 5
lcd_backlight = 6
# Optionally if the backlight is not controllable then set:
# lcd_backlight = None
     
# Define LCD column and row size for 16x2 LCD.
lcd_columns = 16
lcd_rows    = 2
     
# Alternatively specify a 20x4 LCD.
# lcd_columns = 20
# lcd_rows    = 4

Next the LCD pins are defined in the script. Note that these pin numbers are the MCP chip GPIO pin numbers, and NOT Raspberry Pi/BeagleBone Black pin numbers!

Copy Code
# Initialize MCP23017 device using its default 0x20 I2C address.
gpio = MCP.MCP23017()
     
# Alternatively you can initialize the MCP device on another I2C address or bus.
# gpio = MCP.MCP23017(0x24, busnum=1)

Next an instance of the MCP23017 class is created. By default this class will use the I2C address 0x20 (default for MCP chips) and appropriate I2C bus for the running development board. However if you need to override the address or bus number you can see in the commented line how these are passed as parameters.

Also note if you're using an MCP23008 chip you can instead create an instance of the MCP23008 class. This class is exactly the same as the MCP23017 class, but only supports 8 GPIO pins. 

Copy Code
# Initialize the LCD using the pins 
lcd = LCD.Adafruit_CharLCD(lcd_rs, lcd_en, lcd_d4, lcd_d5, lcd_d6, lcd_d7, 
                           lcd_columns, lcd_rows, lcd_backlight, gpio=gpio)

Now the Adafruit_CharLCD class instance is created. The big difference with this line and previous examples is that the MCP23017 class (created with the name 'gpio') is passed in as the gpio parameter. By passing in an explicit gpio parameter, the char LCD class will use that GPIO class for talking to the LCD instead of the default development board GPIO pins.

The rest of the example code is exactly the same as the non-MCP character LCD example. You only need to change the setup and initialization of the character LCD class to use the MCP IO extender with an LCD!

Note you can also use an RGB character LCD with an MCP IO extender, however the MCP IO extender does NOT support PWM control of the backlight!

Raspberry Pi Char LCD Plate

The character LCD plate is a great way to add a simple character LCD and buttons to your Raspberry Pi project. Because the character LCD plate is based on the MCP23017 IO expander, the character LCD library easily supports the character LCD plate!

If you aren't familiar with the character LCD plate, make sure to first read the guide on its usage.

To use this character LCD library with the plate, make sure the library is installed by following the steps on the usage page. Then connect the LCD plate to your Raspberry Pi and execute the char_lcd_plate.py script in the library's examples folder:

Copy Code
sudo python char_lcd_plate.py

Note that the example assumes an RGB character LCD is attached to the plate, however it will still run with a monochrome LCD (you just might see the backlight turn on and off in different ways as colors as displayed).

When you run the example you should see the backlight run through different colors, and then the display will tell you to press buttons. If you press different buttons on the LCD plate you should see the button name and a different color displayed. Try pressing buttons to see how the script reacts!

Examine the code for the char_lcd_plate.py script to see how to use the character LCD plate code. The usage of the LCD plate is very similar to RGB or monochrome LCD usage, with a few key differences.

The first difference is that you create and instance of the Adafruit_CharLCDPlate class. You don't need to pass any parameters in to this class' constructor/init function because it is preconfigured for the LCD plate.

Copy Code
# Initialize the LCD using the pins 
lcd = LCD.Adafruit_CharLCDPlate()

The second difference is that the Adafruit_CharLCDPlate adds a function to test if a button is pressed. Notice how the is_pressed function is called for each button, and if it returns True then the button press is detected.

For example to check if the select button is pressed you can call is_presssed(LCD.SELECT), or to check if the right button is pressed you can call is_pressed(LCD.RIGHT).

Copy Code
# Make list of button value, text, and backlight color.
buttons = ( (LCD.SELECT, 'Select', (1,1,1)),
            (LCD.LEFT,   'Left'  , (1,0,0)),
            (LCD.UP,     'Up'    , (0,0,1)),
            (LCD.DOWN,   'Down'  , (0,1,0)),
            (LCD.RIGHT,  'Right' , (1,0,1)) )
     
print 'Press Ctrl-C to quit.'
while True:
    # Loop through each button and check if it is pressed.
    for button in buttons:
    	if lcd.is_pressed(button[0]):
    		# Button is pressed, change the message and backlight.
    		lcd.clear()
    		lcd.message(button[1])
    		lcd.set_color(button[2][0], button[2][1], button[2][2])

One final thing to note, just like using an MCP230xx IO extender the character LCD plate does not support PWM control of the backlight LEDs!

That's all there is to using the character LCD plate with the character LCD Python library!

מק"ט יצרן # MCP23008-E/P
IC XPNDR 1.7MHZ I2C 18DIP
Microchip Technology
מק"ט יצרן # MCP23017-E/SP
IC XPNDR 1.7MHZ I2C 28SDIP
Microchip Technology
מק"ט יצרן # 1110
LCD/KEYPAD RGB NEG 16X2 RASP PI
Adafruit Industries LLC
מק"ט יצרן # 1109
LCD/KEYPAD RGB POS 16X2 RASP PI
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.