Maker.io main logo

Circuit Playground Quick Draw

39

2017-02-07 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by Carter Nelson

You know the scene. Old West town. Two gunslingers face each other on a dusty street. Tumble weed rolls by. Everyone is eying the town clock. Tick. Tick. 'Cause when it strikes high noon, the gunslingers.........DRAW!

Pew! Pew! Who was the Quickest Draw?

Well put your guns away pardnah. Let's just use these two buttons we got here on our Circuit Playground. This here is a two person show down game to see who can press their button the quickest.

Required Parts

This project uses the sensors already included on the Circuit Playground. The only additional items needed are batteries for power and a holder for the batteries.

Circuit Playground Quick Draw

Before Starting

 If you are new to the Circuit Playground, you may want to first read these overview guides.

This project will use the Arduino IDE. Make sure you have added the board support for the Circuit Playground as well as installed the Circuit Playground library. MUST DO BOTH. This is covered in the guides linked above.

The Town Clock

In the classic gunslinger show down portrayed in numerous movies, the town clock was often used as the 'go' or 'draw' signal for the two gunslingers. High noon or some other on-the-hour time was used so that the minute hand was the main 'go' indicator. As soon as it pointed straight up, it was time to draw.

For our Circuit Playground Quick Draw game, we'll use the NeoPixels instead. They will initially be all off. The two players should then be at the ready. Then, after a random period of time, we will turn on all of the NeoPixels. This is the 'go' signal at which point the two players press their buttons as quick as they can. The winner is whoever pressed their button the quickest.

Random Isn't Random

We can create the random period of time needed for the countdown using the random() function available in the Arduino library. However, it may not behave like you think it behaves. Let's take a look.

Try running the simple sketch below.

Copy Code
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Random Demo
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)

#include <Adafruit_CircuitPlayground.h>

#define SHORTEST_DELAY 1000 // milliseconds
#define LONGEST_DELAY 10000 // "

///////////////////////////////////////////////////////////////////////////////
void setup() {
Serial.begin(9600);

CircuitPlayground.begin();
}

///////////////////////////////////////////////////////////////////////////////
void loop() {
// Wait for button press
while (!CircuitPlayground.leftButton() &&
!CircuitPlayground.rightButton()) {
// Do nothing, just waiting for a button press...
}

// Print a random number
Serial.println(random(SHORTEST_DELAY, LONGEST_DELAY));

// Debounce delay
delay(500);
}

With this code loaded and running on the Circuit Playground, open the Serial Monitor.

Tools -> Serial Monitor

and then press either button. Each time, a random number from SHORTEST_DELAY to LONGEST_DELAY will be printed out. Let me guess, you got the same sequence I did as shown below.

Circuit Playground Quick Draw

And if you reset the Circuit Playground and try this again, you will get the same sequence again. So what's going on?

In turns out that the random() function implemented in the Arduino library is only a pseudo-random function. This simply means it isn't fully random (pseudo = false). It just produces a random like sequence of numbers, and the same sequence every time.

To get around this, we need to initialize the random function with a random value. This is called seeding the function and the value is called the seed. But where can we come up with a random seed value? One way is to use some of the (hopefully) unconnected pads on the Circuit Playground and read in their analog values. Since the pads are not connected, the value returned by a call to analogRead() will contain noise. Noise is random, and that's what we want.

Here's a new version of the code that includes a call to randomSeed() in the setup(). This seed is generated by reading all four of the available analog inputs.

Copy Code
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Random Demo with Seed
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)

#include <Adafruit_CircuitPlayground.h>

#define SHORTEST_DELAY 1000 // milliseconds
#define LONGEST_DELAY 10000 // "

///////////////////////////////////////////////////////////////////////////////
void setup() {
Serial.begin(9600);

CircuitPlayground.begin();

// Seed the random function with noise
int seed = 0;

seed = analogRead(12);
seed = analogRead(7);
seed = analogRead(9);
seed = analogRead(10);

randomSeed(seed);
}

///////////////////////////////////////////////////////////////////////////////
void loop() {
// Wait for button press
while (!CircuitPlayground.leftButton() &&
!CircuitPlayground.rightButton()) {
// Do nothing, just waiting for a button press...
}

// Print a random number
Serial.println(random(SHORTEST_DELAY, LONGEST_DELAY));

// Debounce delay
delay(500);
}

Load this code, open the Serial Monitor, and try again by pressing the buttons. Hopefully you get a different sequence this time, and it's different than the one I got.

Circuit Playground Quick Draw

While this isn't perfect, it will work for our needs. This is what we will use to generate the random amount of time needed for our countdown timer.

Game Design

Game Logic

Once we have our random countdown time figured out, the game logic is very simple:

  1. Turn off all of the NeoPixels.
  2. Wait the determined countdown time.
  3. If a player presses a button during this time, they drew too soon (misdraw).
  4. Once countdown time has elapsed, turn on all of the NeoPixels.
  5. Look for the first (quickest) button press.
  6. Whichever button was pressed first is the Quick Draw winner.

Player Buttons

This is pretty straight forward. We've got two players, we've got two buttons. So we can assign them as shown in the figure below.

Circuit Playground Quick Draw

Countdown NeoPixels

This could be anything, but to keep it simple we'll just turn on all the NeoPixels to white when the countdown completes.

DRAW!

When all of the lights come on (all white), press your button as fast as you can.

Circuit Playground Quick Draw

Player NeoPixels

We can use the NeoPixels on the left to indicate Player 1's outcome, and the NeoPixels on the right to indicate Player 2's outcome. There are two possible outcomes: a misdraw if a player draws too soon, or a game with a winning outcome.

PLAYER 1 MISDRAW!

If all of the lights on the Player 1 side turn red, Player 1 misdrew (pressed the button too soon).

Circuit Playground Quick Draw

PLAYER 2 MISDRAW!

If all of the lights on the Player 2 side turn red, Player 2 misdrew (pressed the button too soon).

Circuit Playground Quick Draw

PLAYER 1 WON!

If all of the lights on the Player 1 side turn green, Player 1 was the quickest.

Circuit Playground Quick Draw

PLAYER 2 WON!

If all of the lights on the Player 2 side turn green, Player 2 was the quickest.

Circuit Playground Quick Draw

The Countdown

We could just use the delay() function to wait the random amount of time determined for the countdown. Something like this:

 

Copy Code
  // Wait a random period of time
unsigned long countTime = random(SHORTEST_DELAY, LONGEST_DELAY);
delay(countTime);

 

However, we need to monitor the buttons during the countdown to make sure one of the players did not cheat (misdraw). We can do this by using a while() loop instead of delay() for the countdown and polling the buttons inside the loop. That would look something like the following, note that there is now no use of delay().

 

Copy Code
  // Wait a random period of time
unsigned long countTime = random(SHORTEST_DELAY, LONGEST_DELAY);
unsigned long startTime = millis();
while (millis() - startTime < countTime) {
// Check if player draws too soon.
if (CircuitPlayground.leftButton()) showOutcome(1, false);
if (CircuitPlayground.rightButton()) showOutcome(2, false);
}

 

But what's the showOutcome() function? Well, we'll talk about that next.

Show Outcome

The showOutcome() function will be created to, as the name implies, show the outcome of the game. The first parameter will be the player who's button was pressed. The second parameter is a boolean to indicate if the button press was a winning press (true) or a misdraw (false).

By generalizing the outcome code, to be able to show the proper NeoPixels for either player and for either outcome, we make our code more compact. Otherwise we would need to duplicate a lot of code in more than one place. It also makes it easier to change the behavior of the code in the future.

The complete code for the showOutcome() function will be shown at the end. Here, we'll go through it in pieces. First, we need to declare it:

 

Copy Code
void showOutcome(int player, bool winner) {

 

We aren't going to return anything, so the return parameter is void. We take in two parameters: the player who's button was pressed as an int, and whether this was a winning game or not as a bool.

Next, we create a couple of variables to be used locally within the function.

 

Copy Code
  int p1, p2;
uint32_t color;

Then we turn off all of the NeoPixels, just to insure a known state.

Copy Code
  // Turn them all off
CircuitPlayground.clearPixels();

Then we set the pixel color depending on the game outcome, green for a winning game, red for a misdraw.

Copy Code
  // Set pixel color
if (winner) {
color = 0x00FF00;
} else {
color = 0xFF0000;
}

Then we set the range of NeoPixels to be lit up based on which payer pressed their button.

Copy Code
  // Set pixel range for player
switch (player) {
case 1:
p1 = 0;
p2 = 4;
break;
case 2:
p1 = 5;
p2 = 9;
break;
default:
p1 = 0;
p2 = 9;
}

Now we have a color for the NeoPixels, and which ones to turn on, so do that.

Copy Code
  // Show which player won/lost
for (int p=p1; p<=p2; p ) {
CircuitPlayground.setPixelColor(p, color);
}

And why not play a little tune. A happy one if this was a winning game, a more error sounding one if it was a misdraw.

Copy Code
  // Play a little tune
if (winner) {
CircuitPlayground.playTone(800, 200);
CircuitPlayground.playTone(900, 200);
CircuitPlayground.playTone(1400, 200);
CircuitPlayground.playTone(1100, 200);
} else {
CircuitPlayground.playTone(200, 1000);
}

And we are done with the game, so we'll just sit here forever until the reset button is pressed to start a new game.

Copy Code
  // Sit here forever
while (true) {};

And don't forget the closing curly bracket to finish off the showOutcome() function.

Copy Code
}

OK. Let's put it all together.

Code Listing

Here's the complete code listing for the Quick Draw game.

Copy Code
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Quick Draw
//
// Who's faster?
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)

#include <Adafruit_CircuitPlayground.h>

#define SHORTEST_DELAY 1000 // milliseconds
#define LONGEST_DELAY 10000 // "

///////////////////////////////////////////////////////////////////////////////
void showOutcome(int player, bool winner) {
int p1, p2;
uint32_t color;

// Turn them all off
CircuitPlayground.clearPixels();

// Set pixel color
if (winner) {
color = 0x00FF00;
} else {
color = 0xFF0000;
}

// Set pixel range for player
switch (player) {
case 1:
p1 = 0;
p2 = 4;
break;
case 2:
p1 = 5;
p2 = 9;
break;
default:
p1 = 0;
p2 = 9;
}

// Show which player won/lost
for (int p=p1; p<=p2; p ) {
CircuitPlayground.setPixelColor(p, color);
}

// Play a little tune
if (winner) {
CircuitPlayground.playTone(800, 200);
CircuitPlayground.playTone(900, 200);
CircuitPlayground.playTone(1400, 200);
CircuitPlayground.playTone(1100, 200);
} else {
CircuitPlayground.playTone(200, 1000);
}

// Sit here forever
while (true) {};
}

///////////////////////////////////////////////////////////////////////////////
void setup() {
// Initialized the Circuit Playground
CircuitPlayground.begin();

// Turn off all the NeoPixels
CircuitPlayground.clearPixels();

// Seed the random function with noise
int seed = 0;

seed = analogRead(12);
seed = analogRead(7);
seed = analogRead(9);
seed = analogRead(10);

randomSeed(seed);

// Wait a random period of time
unsigned long countTime = random(SHORTEST_DELAY, LONGEST_DELAY);
unsigned long startTime = millis();
while (millis() - startTime < countTime) {
// Check if player draws too soon.
if (CircuitPlayground.leftButton()) showOutcome(1, false);
if (CircuitPlayground.rightButton()) showOutcome(2, false);
}

// Turn on all the NeoPixels
for (int p=0; p<10; p ) {
CircuitPlayground.setPixelColor(p, 0xFFFFFF);
}
}

///////////////////////////////////////////////////////////////////////////////
void loop() {
if (CircuitPlayground.leftButton()) showOutcome(1, true);
if (CircuitPlayground.rightButton()) showOutcome(2, true);
}

Questions and Code Challenges

The following are some questions related to this project along with some suggested code challenges. The idea is to provoke thought, test your understanding, and get you coding!

While the sketch provided in this guide works, there is room for improvement and additional features. Have fun playing with the provided code to see what you can do with it.

Questions

  • Does it matter which order the functions leftButton() and rightButton() are called in?
  • Can you think of a way to cheat the countdown timer? (hint: seed)

Code Challenges

  • Put the code that does the random seeding into a function called initRandom().
  • Change the color of the NeoPixels for the countdown.
  • Come up with a different way to start a new game, instead of using reset button.
מק"ט יצרן # 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
מק"ט יצרן # 727
BATTERY HOLDER AAA 3 CELL LEADS
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.