Maker.io main logo

CircuitPython BLE Multi-Temperature Monitoring

87

2020-05-19 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by John Park

Overview

Are you doing a lot of slow cooking or smoking in the BBQ? Or perhaps you've got sourdough proofing on the counter and another in the oven? If so, you may find yourself looking to monitor a number of temperatures all at once.

 

sensor_1

Wireless Bluetooth Low Energy (BLE) temperature sensors are a great way to do just that, and now we can use the iBBQ protocol to display multiple temperature probe values simultaneously on the CLUE's display!

These affordable and easy-to-use temperature probes are designed to work with an app - but with a little CircuitPython, we can even read these probes into a microcontroller board for transfer over Wi-Fi, long term data storage, or analysis.

Parts

In addition to the CLUE, you'll also need a BLE BBQ thermometer that utilizes the iBBQ protocol. Here are a few:

  • InkBird
  • Easy BBQ from PyleUSA
  • NutriChef
  • Evoland

 

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront desktop software downloads. Simply copy and edit files on the CIRCUITPY flash drive to iterate.

The following instructions will show you how to install CircuitPython. If you've already installed CircuitPython but are looking to update it or reinstall it, the same steps work for that as well!

Set up CircuitPython Quick Start!

Follow this quick step-by-step for super-fast Python power :)

Download the latest version of CircuitPython for CLUE from circuitpython.org

Click the link above to download the latest version of CircuitPython for the CLUE.

Download and save it to your desktop (or wherever is handy).

pdf_2

Plug your CLUE into your computer using a known-good USB cable.

A lot of people end up using charge-only USB cables and it is very frustrating! So, make sure you have a USB cable you know is good for data sync.

Double-click the Reset button on the top (magenta arrow) on your board, and you will see the NeoPixel RGB LED (green arrow) turn green. If it turns red, check the USB cable, try another USB port, etc. Note: The little red LED next to the USB connector will pulse red. That's ok!

If double-clicking doesn't work the first time, try again. Sometimes it can take a few tries to get the rhythm right!

clue_3

You will see a new disk drive appear called CLUEBOOT.

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.

clueboot_4

clueboot_5

The LED will flash. Then, the CLUEBOOT drive will disappear and a new disk drive called CIRCUITPY will appear.

If this is the first time you're installing CircuitPython or you're doing a completely fresh install after erasing the filesystem, you will have two files - boot_out.txt, and code.py, and one folder - lib on your CIRCUITPY drive.

If CircuitPython was already installed, the files present before reloading CircuitPython should still be present on your CIRCUITPY drive. Loading CircuitPython will not create new files if there was already a CircuitPython filesystem present.

That's it, you're done! :)

drive_6

CLUE CircuitPython Libraries

The CLUE is packed full of features like a display and a ton of sensors. Now that you have CircuitPython installed on your CLUE, you'll need to install a base set of CircuitPython libraries to use the features of the board with CircuitPython.

Follow these steps to get the necessary libraries installed.

Installing CircuitPython Libraries on your CLUE

If you do not already have a lib folder on your CIRCUITPY drive, create one now.

Then, download the CircuitPython library bundle that matches your version of CircuitPython from CircuitPython.org.

Download the latest library bundle from circuitpython.org

The bundle downloads as a .zip file. Extract the file. Open the resulting folder.

downloads_7

Open the lib folder found within.

lib_8

Once inside, you'll find a lengthy list of folders and .mpy files. To install a CircuitPython library, you drag the file or folder from the bundle lib folder to the lib folder on your CIRCUITPY drive.

listfolders_8

Copy the following folders and files from the bundle lib folder to the lib folder on your CIRCUITPY drive:

  • adafruit_apds9960
  • adafruit_bmp280.mpy
  • adafruit_bus_device
  • adafruit_clue.mpy
  • adafruit_display_shapes
  • adafruit_display_text
  • adafruit_lis3mdl.mpy
  • adafruit_lsm6ds.mpy
  • adafruit_register
  • adafruit_sht31d.mpy
  • adafruit_slideshow.mpy
  • neopixel.mpy

Your lib folder should look like the image below. These libraries will let you run the demos in the CLUE guide.

libraries_9

Coding the BBQLUE

coding_10

Setup

Once you've set up the board, click Download: Project Zip below in the code section. Expand the .zip file and then drag the font folder to your CLUE's CIRCUITPY drive via USB.

Your CLUE's CIRCUITPY drive should look like this.

CIRCUITPY_11

Here's how the CLUE will work:

  • On start, show a home screen logo with the word "BBQLUE" in a circle with a square at one corner
  • Begin scanning for a BLE device advertising the ibbq service
  • When such a device is found, connect to it, switch the temperatures screen layout with "BBQLUE" at the top and the probe temperatures listed in color coding
  • Watch the A button for presses to switch between Fahrenheit and Celsius
  • If connection is lost, swap back to home screen logo and begin scanning again

Code

Copy the code from the code-block below and paste it into the Mu editor and save it to your CLUE as code.py (or copy code.py from the zip file and place on the CIRCUITPY drive).

Download: Project Zip or clue_bbq.py

Copy Code
# Adafruit BBQ display works with ibbq protocol-based BLE temperature probes

import time

import displayio
import _bleio
import adafruit_ble
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble_ibbq import IBBQService
from adafruit_clue import clue
from adafruit_display_shapes.circle import Circle
from adafruit_display_text import label
from adafruit_bitmap_font import bitmap_font

clue.display.brightness = 1.0
homescreen_screen = displayio.Group(max_size=3)
temperatures_screen = displayio.Group(max_size=2)

# define custom colors
GREEN = 0x00D929
BLUE = 0x0000FF
RED = 0xFF0000
ORANGE = 0xFF6A00
YELLOW = 0xFFFF00
PURPLE = 0xE400FF
BLACK = 0x000000
WHITE = 0xFFFFFF
BURNT = 0xBB4E00

unit_mode = False # set the temperature unit_mode. True = centigrade, False = farenheit

# Setup homescreen
color_bitmap = displayio.Bitmap(120, 120, 1)
color_palette = displayio.Palette(1)
color_palette[0] = BURNT
bg_sprite = displayio.TileGrid(color_bitmap, x=120, y=0, pixel_shader=color_palette)
homescreen_screen.append(bg_sprite)

clue_color = [GREEN, BLUE, RED, ORANGE, YELLOW, PURPLE]

outer_circle = Circle(120, 120, 119, fill=BLACK, outline=BURNT)
homescreen_screen.append(outer_circle)


title_font = bitmap_font.load_font("/font/GothamBlack-50.bdf")
title_font.load_glyphs("BQLUE".encode("utf-8"))
title_label = label.Label(title_font, text="BBQLUE", color=clue.ORANGE, max_glyphs=15)
title_label.x = 12
title_label.y = 120
homescreen_screen.append(title_label)

clue.display.show(homescreen_screen)

# Setup temperatures screen
temp_font = bitmap_font.load_font("/font/GothamBlack-25.bdf")
temp_font.load_glyphs("0123456789FC.-<".encode("utf-8"))

my_labels_config = [
(0, "", GREEN, 2, 100),
(1, "", BLUE, 2, 150),
(2, "", RED, 2, 200),
(3, "", ORANGE, 135, 100),
(4, "", YELLOW, 135, 150),
(5, "", PURPLE, 135, 200),
]

my_labels = {} # dictionary of configured my_labels

text_group = displayio.Group(max_size=8, scale=1)

for label_config in my_labels_config:
(name, text, color, x, y) = label_config # unpack a tuple into five var names
templabel = label.Label(temp_font, text=text, color=color, max_glyphs=15)
templabel.x = x
templabel.y = y
my_labels[name] = templabel
text_group.append(templabel)

temperatures_screen.append(text_group)

temp_title_label = label.Label(
title_font, text="BBQLUE", color=clue.ORANGE, max_glyphs=15
)
temp_title_label.x = 12
temp_title_label.y = 30
temperatures_screen.append(temp_title_label)

# PyLint can't find BLERadio for some reason so special case it here.
ble = adafruit_ble.BLERadio() # pylint: disable=no-member

ibbq_connection = None

while True:
# re-display homescreen here
clue.display.show(homescreen_screen)

print("Scanning...")
for adv in ble.start_scan(ProvideServicesAdvertisement, timeout=5):
clue.pixel.fill((50, 50, 0))
if IBBQService in adv.services:
print("found an IBBq advertisement")
ibbq_connection = ble.connect(adv)
print("Connected")
break

# Stop scanning whether or not we are connected.
ble.stop_scan()

try:
if ibbq_connection and ibbq_connection.connected:
clue.pixel.fill((0, 0, 50))
ibbq_service = ibbq_connection[IBBQService]
ibbq_service.init()
while ibbq_connection.connected:

if clue.button_a: # hold a to swap between C and F
print("unit_mode swapped")
unit_mode = not unit_mode
clue.red_led = True
clue.play_tone(1200, 0.1)
clue.red_led = False
time.sleep(0.1) # debounce

temps = ibbq_service.temperatures
batt = ibbq_service.battery_level
if temps is not None:
probe_count = len(temps) # check how many probes there are
for i in range(probe_count):
if temps[i] != 0 and temps[i] < 1000: # unplugged probes
if unit_mode:
clue.pixel.fill((50, 0, 0))
temp = temps[i]
my_labels[i].text = "{} C".format(temp)
clue.pixel.fill((0, 0, 0))
print("Probe", i + 1, "Temperature:", temp, "C")
else: # F
clue.pixel.fill((50, 0, 0))
temp = temps[i] * 9 / 5 + 32
my_labels[i].text = "{} F".format(temp)
clue.pixel.fill((0, 0, 0))
print("Probe", i + 1, "Temperature:", temp, "F")
else:
print(
"Probe", i + 1, "is unplugged",
)
my_labels[i].text = " ---"
clue.display.show(temperatures_screen)

except _bleio.ConnectionError:
continue

Code Explainer

Let's now look at how the code works.

Libraries

First, we'll import the necessary libraries, including those needed for displayio, BLE, adafruit_clue, shapes, text, fonts, and the iBBQ service.

Download: file

Copy Code
import time

import displayio
import _bleio
import adafruit_ble
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble_ibbq import IBBQService
from adafruit_clue import clue
from adafruit_display_shapes.circle import Circle
from adafruit_display_text import label
from adafruit_bitmap_font import bitmap_font

Display Groups

We'll set up two different displayio Groups, you can think of these as two distinct screens that we and switch between. One for the homescreen logo, the other for the temperature readouts.

Download: file

Copy Code
clue.display.brightness = 1.0
homescreen_screen = displayio.Group(max_size=3)
temperatures_screen = displayio.Group(max_size=2)

Variables

We'll use a few different colors throughout the code, so here we'll create a set of variables that give us nice names to use for specific color hex values.

We'll also create a variable called unit_mode to switch between Celsius and Fahrenheit.

Download: file

Copy Code
GREEN = 0x00D929
BLUE = 0x0000FF
RED = 0xFF0000
ORANGE = 0xFF6A00
YELLOW = 0xFFFF00
PURPLE = 0xE400FF
BLACK = 0x000000
WHITE = 0xFFFFFF
BURNT = 0xBB4E00

unit_mode = False # set the temperature unit_mode. True = celsius, False = fahrenheit

Homescreen

Here we will set up the homescreen. This will consist of a 120x120 pixel square in the upper right corner called bg_sprite, in the BURNT umber color.

The displayio system is a hierarchy of objects with a displayio.Group at the top of the hierarchy. In this case, we append the bg_sprite object to the homescreen_screen group.

We next create a black circle with a BURNT outline named outer_circle and append it, too, too the homescreen_screen group.

To add the BBQLUE title, we load a bitmap font, preload the glyphs (characters) we'll need, and create a label object named title_label. The label is positioned on x and y at the center of the screen, and then it is appended to the homescreen_screen group.

Finally, we show all of this on the CLUE display with the clue.display.show(homescreen_screen) command.

Download: file

Copy Code
color_bitmap = displayio.Bitmap(120, 120, 1)
color_palette = displayio.Palette(1)
color_palette[0] = BURNT
bg_sprite = displayio.TileGrid(color_bitmap, x=120, y=0, pixel_shader=color_palette)
homescreen_screen.append(bg_sprite)

clue_color = [GREEN, BLUE, RED, ORANGE, YELLOW, PURPLE]

outer_circle = Circle(120, 120, 119, fill=BLACK, outline=BURNT)
homescreen_screen.append(outer_circle)


title_font = bitmap_font.load_font("/font/GothamBlack-50.bdf")
title_font.load_glyphs("BQLUE".encode('utf-8'))
title_label = label.Label(title_font, text="BBQLUE", color=clue.ORANGE, max_glyphs=15)
title_label.x = 12
title_label.y = 120
homescreen_screen.append(title_label)

clue.display.show(homescreen_screen)

Temperature Screen

The temperature_screen is created in much the same way as the homescreen_screen. However, there will be no bitmap shapes, only text.

Since we want a different position and color for each label correlated to a temperature probe, we create a list of tuples called my_labels_config to contain these values. Each tuple (set of multiple values) in the list represents one of the temperature probes.

By creating the my_labels dictionary, we can unpack the list of tuples into nicely named objects such as "name", "text", "color", and so on, instead of referring to them as indexed numbers.

We'll append each of these label objects to a text group with their corresponding colors and positions, and then append the text group to the temperatures_screen.

We won't show this screen yet, however. We'll wait until we've received data from a sensor.

Download: file

Copy Code
temp_font = bitmap_font.load_font("/font/GothamBlack-25.bdf")
temp_font.load_glyphs("0123456789FC.-<".encode('utf-8'))

my_labels_config = [(0, "", GREEN, 2, 100),
(1, "", BLUE, 2, 150),
(2, "", RED, 2, 200),
(3, "", ORANGE, 135, 100),
(4, "", YELLOW, 135, 150),
(5, "", PURPLE, 135, 200)
]

my_labels = {} # dictionary of configured my_labels

text_group = displayio.Group(max_size=8, scale=1)

for label_config in my_labels_config:
(name, text, color, x, y) = label_config # unpack a tuple into five var names
templabel = label.Label(temp_font, text=text, color=color, max_glyphs=15)
templabel.x = x
templabel.y = y
my_labels[name] = templabel
text_group.append(templabel)

temperatures_screen.append(text_group)

temp_title_label = label.Label(title_font, text="BBQLUE", color=clue.ORANGE, max_glyphs=15)
temp_title_label.x = 12
temp_title_label.y = 30
temperatures_screen.append(temp_title_label)

BLE Prep

The radio is instantiated, and a variable called ibbq_connection is created to hold the status of connections to a device advertising the ibbq service.

Download: file

Copy Code
ble = adafruit_ble.BLERadio()  # pylint: disable=no-member

ibbq_connection = None

Main Loop

Here's the main loop of the code that repeats over and over now that things are set up.

The homescreen_screen is redrawn (this will be useful later when a connection is dropped).

Then, any BLE advertisements that are found are checked to see if they are advertising the ibbq service. If found, we connect!

Download: file

Copy Code
while True:
# re-display homescreen here
clue.display.show(homescreen_screen)

print("Scanning...")
for adv in ble.start_scan(ProvideServicesAdvertisement, timeout=5):
clue.pixel.fill((50, 50, 0))
if IBBQService in adv.services:
print("found an IBBq advertisement")
ibbq_connection = ble.connect(adv)
print("Connected")
break

# Stop scanning whether or not we are connected.
ble.stop_scan()

Connected

Once the CLUE is connected to a device with the ibbq service available, the service is initialized so it will send data.

Download: file

Copy Code
try:
if ibbq_connection and ibbq_connection.connected:
clue.pixel.fill((0, 0, 50))
ibbq_service = ibbq_connection[IBBQService]
ibbq_service.init()
while ibbq_connection.connected:

Button Unit Swap

In order to switch between Fahrenheit and Celsius, we set up the clue.button_a. It will flip the unit_mode between True and False each time it is pressed, as well as play a small beep on the built-in buzzer so the user knows the press has been registered.

Download: file

Copy Code
if clue.button_a:  # hold a to swap between C and F
print("unit_mode swapped")
unit_mode = not unit_mode
clue.red_led = True
clue.play_tone(1200, 0.1)
clue.red_led = False
time.sleep(0.1) # debounce

Temperature Display

To read and display the temperature data coming from each probe, first a variable called temps is set to the values of the ibbq_service.temperatures attribute that has been received from the BLE temperature device.

If the temps value is not None (at first when the devices connect this value is empty, so we ignore that until real data comes through) we then iterate through each probe value that has been received.

If the value isn't 0 and is less than 1000, it means there is a temperature probe plugged into that port.

Depending on the unit_mode we will then display the Celsius value directly, or first calculate the Fahrenheit value with the formula <value> * 9 / 5 +32.

This value is displayed in the proper label color and position on screen, and then this is repeated for each subsequent probe.

If the value is 0 or greater than 1000, then there is not a probe plugged in and we'll display three dashes "---".

Once the labels are updated we re-draw the screen with the clue.display.show(temperatures_screen) command.

Download: file

Copy Code
temps = ibbq_service.temperatures
batt = ibbq_service.battery_level
if temps != None:
probe_count = len(temps) # check how many probes there are
for i in range(probe_count):
if temps[i] is not 0 and temps[i] < 1000: # unplugged probes
if unit_mode:
clue.pixel.fill((50, 0, 0))
temp = temps[i]
my_labels[i].text = "{} C".format(temp)
clue.pixel.fill((0, 0, 0))
print("Probe", i + 1, "Temperature:", temp, "C")
else: # F
clue.pixel.fill((50, 0, 0))
temp = temps[i] * 9 / 5 + 32
my_labels[i].text = "{} F".format(temp)
clue.pixel.fill((0, 0, 0))
print("Probe", i + 1, "Temperature:", temp, "F")
else:
print(
"Probe", i + 1, "is unplugged",
)
my_labels[i].text = " ---"
clue.display.show(temperatures_screen)

Connection Lost

If the connection is lost, we go back to the top and draw the homescreen_screen will be attempting to find a new connection!

Download: file

Copy Code
except _bleio.ConnectionError:
continue

Using the BBQLUE

Here's how to use the BBQLUE.

Startup

When you power on the CLUE, you'll see the BBQLUE logo show up after it is done preloading the graphics and font glyphs.

It then begins searching for an iBBQ protocol BLE device being advertised.

bbqlue_12

Probes

Plug in as many of the temperature probes as needed into the main unit (if your unit features multiple probes, some may only have one).

probes_13

To keep the probe color coding consistent with the text color on the CLUE, use this order:

  • probe 1 = green
  • probe 2 = blue
  • probe 3 = red
  • probe 4 = orange
  • probe 5 = yellow
  • probe 6 = purple

Turn on the BBQ thermometer main unit and it will begin broadcasting BLE advertisements of its iBBQ service availability.

Temperature Probe Display

The BBQLUE will then switch to the second display group and begin to display the advertised attribute values for the temperature probes.

For any probes that aren't plugged in, the value will be out of range and display as three dashes "---".

display_14

Unit Swap

By default, the temperatures are displayed in degrees Fahrenheit. Press the A button on the CLUE at any time to swap to Celsius. When you hear the beep, the button press has registered, and you may let go.

swap_15

Now, you can insert the temperature probes in your items that are cooking and remotely monitor the temperatures!

monitor_16

monitor_17

monitor_18

Kitchen Science Experiment

Which pot of water contains a secret ingredient NaCl? In this experiment, we can find out by using the CLUE temperature sensor display.

 

Boiling Point Elevation

Water boils at 212° Fahrenheit (100° Celsius). Or does it?!

When we say water boils at 212° F, we are talking about "typical" drinking water that comes from a tap, filter, or bottle. However, there's a common ingredient you can add to your drinking water to significantly raise its boiling point -- salt.

By dissolving enough salt in the water, you will observe a phenomenon called "boiling point elevation". You are essentially making the solution use an increased amount of heat energy to make the phase transition from liquid to gas begin.

How it Works

It takes heat energy to transition water from its liquid phase state to gas. When salt (a.k.a., sodium chloride or NaCl) is dissolved in water it splits into sodium and chlorine ions.

Water molecules (a.k.a., dihydrogen monoxide or H20) are a bit like magnets for each other. They have a negative side and a positive side. Breaking these bonds between molecules with heat causes the water to phase change from liquid to gas.

However, the dissolved salt has just provided some extra strength to these bonds. The sodium ions are positively charged and align with the negative oxygen side of the water molecules. The chlorine ions are negatively charged, thus align with the positively charged hydrogen side of the water molecules.

These convenient alignments strengthen the interactions between the water molecules, thus requiring more heat energy to boil.

Let's put this theory into practice and see how much we can raise the boiling point.

Experiment Materials

Here's what we'll need to run the experiment:

  • Two small pots (I used 1-1/4 Qt. pots)
  • Clothes pins
  • Rubber bands
  • Measuring cups
  • Salt
  • Water
  • Stove

materials_19

materials_20

materials_21

materials_22

Probe Prep

First, we'll create a rig to hold the probes with the metal tips near the center of the pot without touching. (We need to measure the water temperature, not the temperature of the pot.)

Wrap a rubber band a few times around the probe end and slip it over one leg of the clothespin.

Clip the clothespin to the side of the pot.

prep26

prep27

prep28

prep29

Water

Pour a quart of water into each pot. I used filtered tap water.

water_24

water_23

 

Add Salt to Pot B

Pot A will be the control pot, with regular water in it.

To pot B, add 1/2 C. of table salt. Stir to dissolve.

salt_24

salt_25

Turn on the Heat

With the pots positioned on two equal sized burners, turn up the heat to high. If you are using a gas range, make sure there is no danger of the probe, clothespin, or wire being in direct contact with the open flame.

You will see the temperatures rise on both pots on the CLUE's display. Note how the pot B is slower to raise its temperature due to the added thermal mass of the salt.

When the water is at a full boil on pot A, the temperature will read right about 212° F (100° C) and stay at that temperature. It can go no higher!

However, pot B with all of that salt will continue on well beyond -- mine went all the way up to 217.4° F (103° C)!

heat_30

heat_31

heat_32

meastemp_26

meastemp_27

You have now solved the mystery of the hotter than usual boiling water!

Further Experiments

What happens if you increase or decrease the ratio of salt to water? Do other solutes behave similarly or differently?

מק"ט יצרן # UR050-003
CBL USB2.0 A PLUG-MCR B PLUG 3'
Eaton Tripp Lite
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.