Maker.io main logo

Companion Robot Backpack

99

2023-10-01 | By bekathwia

License: None

 

Today I’m making a backpack for my friend Jayy’s companion robots.‎

jayy_1

Jorvon Moss, aka Odd_Jayy, is a maker of robots and gadgets, including his shoulder-mounted ‎companion robots. Check out his work on maker.io, or follow him on Instagram at @odd_jayy.‎

Supplies

Here are all the supplies you'll need if you want to make this project yourself:‎

  • Heavyweight fabric, I used both cotton canvas 10oz and ballistic nylon
  • ‎1" nylon webbing‎‎
  • ‎1" buckles (2)
  • D-rings (2)
  • Swivel clasps (2)
  • Paracord‎
  • Cord locks
  • Zipper (optional)‎
  • Grommet kit
  • Fabric scissors
  • Sewing machine‎
  • Thread
  • Sewing needle
  • Sewing pins and/or clips
  • Thread snips (optional but handy)
  • Thin upholstery foam (for strap)
  • Printer with paper (for pattern)
  • ‎3D printer‎
  • PETG filament

This project is sponsored by DigiKey, where you can find a surprisingly large variety of scissors, ‎in addition to all your robot-building supplies.‎

Making the First Prototype

pieces_2

peices_3

sewing_4

I whipped up a first prototype designed around a round drawstring compartment for the robot. I ‎printed out the pattern and cut out the pieces from black canvas– it’s heavy-weight enough to ‎simulate the final bag, but easier to work with, and less expensive than the sturdy nylon I planned ‎to use for the final bag.‎

bag_5

cord_6

feed_7

I used paracord to make the drawstring and fed it through the hem using a big safety pin. I had a ‎few of these spring-loaded closures hanging around, called cord locks, so I used them for the ‎drawstring adjuster. This particular size is a pain to get two sections of normal-size paracord ‎through, but by the end of this project, I developed a technique that works reliably well.‎

box_8

tri_9

I used a piece of cardboard to stiffen the bottom of the bot compartment and folded the tabs ‎under it to attempt to make a bot support bracket. I didn’t think the cardboard one would hold up, ‎but I wanted to test out the geometry of everything.‎

cardboard_10

Of course, it got smushed the instant Jayy tried this one on with any weight up top. After ‎completing the first test fit, we decided the bot needed to sit further forward on the shoulder than ‎in this initial design, so I needed to make the bot compartment its own separate piece. ‎

bag_11

adjust_12

adjust_13

Adjusting the Design

hold_14

model_15

form_16

I 3D modeled a platform in Tinkercad for the bot to sit on affixed with zip ties, using PETG ‎filament, which is less brittle than PLA. ‎

fabric_17

base_18

sewing_19

The fabric top of the robot compartment remains the same as before, but I needed to do its ‎machine stitching before attaching it to the rigid base.‎

attaching

This drawstring cord lock still gave me a lot of trouble this time, but I promise I’m getting closer to ‎the ultimate tip for this situation.‎

attach_21

attach_22

Then I sewed the drawstring bag to the 3D-printed base around the edge by hand. Since I wasn’t ‎sure where exactly the robot's waist was, and wanted it to be flexible for future robot versions, I ‎added some nylon straps for cinching down any extra fabric.‎

straps_23

straps_24

straps_25

The rest of the bag came together similarly to the first prototype– I made the strap with a ‎sandwich of nylon and upholstery foam, two layers this time, and used 1-inch webbing for the ‎straps, with compatible 1-inch buckles and D-rings and all that. The thing that’s new in this ‎version is the use of grommets, which I’m using to make the link between the platform and the ‎strap, as well as for the backpack compartment closure.‎

bag_26

The idea to make the platform perforated for attaching the robot was the real breakthrough in the ‎stability of this design. Jay reports that this backpack holds up his robot companion securely and ‎comfortably.‎

platform_27

platform_28

platform_29

So, I made a second basket assembly with rounder 3D printed edges since it’s easy to swap the ‎whole basket out on the backpack base. I used orange canvas for this one and hand sewed the ‎fabric to the base. The base is held to the strap with two more pieces of paracord.‎

hold_30

hold_31

Paracord Tip

tip_32

And finally, here’s my tip for getting the two ends of the paracord through the cord lock device– ‎you can tightly wrap the cords together with thread, then push them through together. It’s the ‎same sort of technique some folks use to remove a ring that’s stuck on a swollen finger. Or, you ‎can just buy bigger cord locks... But I was determined to use the ones I already had.‎

Backpack

This was such a fun collaboration and a really satisfying design challenge. I love working with my ‎friends, Jayy is just the best, and the result is better than either of us imagined.‎

Recommended Reading

Shadow's LED Dog Vest

EL Wire Hoodie

Waxed Canvas Tool Roll

Getting Started with LilyPad

Stick Person Costume with Neon LED Strips

Prototype Wearable LED Dance Harness

Asi, a 3D Printed Wearable Robot Friend

Zipper Switch

מק"ט יצרן # G208
SHEARS OFFSET HANDLE
Klein Tools, Inc.
מק"ט יצרן # 372S-Y35.NP
PROCUT SCISSORS, STRAIGHT, 3.5"
Ideal-tek S.A.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.