Maker.io main logo

Cosplay Floating LED Fireball with Motion Sensing

65

2022-03-29 | By Adafruit Industries

License: See Original Project Wearables Circuit Playground

Courtesy of Adafruit

Guide by Erin St Blaine

Overview

Complete your cosplay with this Magical Item: a floating fireball that flares up at your ‎command. Whether you're portraying Kael'thas Sunstrider from WoW or trading flaming ‎shots with Super Mario and Luigi, this fireball will push your outfit over the top.‎

 

This is a very easy project, with no soldering required. The Circuit Playground board makes ‎motion-sensing programmable lights a snap. Customize your colors and your animation speed ‎with Microsoft MakeCode's drag-and-drop code editor. You'll be stopped for so many photos ‎that you'll never make it to that panel discussion at DragonCon.‎

This project was inspired by late-night browsing on Etsy, where a lot of creative makers have ‎similar products. What makes this one special is the ability to customize your own light colors ‎and flame colors, as well as the motion-sensitive flare up!‎

flare_1

Materials

You'll Also Need

  • Cellophane gift wrap in your desired colors - get it at the craft or stationary store

  • A heat gun or hair dryer

  • A 3d Printer (or you can order the part online)

  • Glue dots - I used these from Scotch

3D Printing‎

These rings were designed in TinkerCad. TinkerCad is an easy-to-use 3d design program ‎which is great for beginners, or for anyone who wants to quickly model simple shapes.‎

If you don't have access to a 3d printer, you can order them from Shapeways here:‎

If you are printing your own, download the files below. I've included all three sizes in ‎the .zip file, so select and print the one that fits you best.‎

fireball_holders.zip

holder_2

Print Settings

I printed in clear PLA, with a raft and supports. I had the most success when I printed the ‎widget lying down on its side.‎

My clear PLA didn't really come out clear -- it looks really white and shows up more than ‎I'd like. A flesh-colored filament would probably look better if your character is bare-‎handed. If your character wears gloves, print in a color to match the gloves. ‎

Customizing the Size

If none of these sizes is quite right for you, it's easy to edit the files in TinkerCad to get a ‎perfect fit. ‎

Do not shortcut and simply resize the whole .stl file before printing -- the top end is sized ‎to screw into the Circuit Playground case and if you resize the whole thing, it will no longer ‎screw in tightly.‎

Edit in Tinkercad

Select the size ‎that's closest ‎to the one you ‎want. Click ‎the "ungroup" ‎button in the ‎upper ‎right ‎corner.‎

select_3

Click on the rings to select them. Click the white box in the corner and you'll see measurements ‎appear. Hold the shift key while you drag with ‎your mouse to resize without changing the aspect ‎ratio. ‎

click_4

This looks better, but now we're mis-aligned. This is easy to fix. Drag a box around the rings and the stem to select them both. Click the "align" ‎tool in the upper right, then click the dot in the bottom center to align the rings with the stem.‎

this_5

Once you're happy with sizing and alignment, select the rings and stem and click the "group" button to attach them back together.‎

once_6

Select your resized widget and click the "export" button. Choose "selected shape" and "stl" to download your updated file for printing.‎

select_7

If you want a longer or shorter stem, you can use the same method. Just be careful not to ‎resize the screw tip.‎

Code with MakeCode

code_8

Microsoft's MakeCode editor is a great way to get your Circuit Playground Express to do things ‎without having to muck about in actual code. It's a fun drag-and-drop editor that's easy to use ‎and sneakily teaches you how to write code while you're making pretty things that light up.‎

This sample code makes a flickering flame effect with red, orange, and yellow. When "shake" ‎is triggered, the lights flare up to a bright yellow, then slowly dim back down to the flicker.

‎You can download the completed code and get up and running right away, or you can follow ‎along and create your own code, adding your own customizations as you go.‎

Complete Fireball MakeCode

Code Walkthrough

Let's take a look at each of the different blocks to see what's happening. Head ‎to makecode.com to get started.‎

On Start

Click the Circuit Playground Express and then New Project. You'll see your workspace, ‎with a Circuit Playground on the left, some tabs in the middle and your workspace on the ‎right. Click the LOOPS tab and find on_start. Drag it into your workspace.‎

Whatever you put into the on_start loop will run once, when you first boot up ‎your Circuit Playground Express.‎

I've created two variables: bright and on. The bright variable will be used to ‎determine how bright our lights are, and the on variable will be used with an ‎on/off switch hooked up to the two onboard buttons.‎

Brightness will be a changing number between 0 and 255. Our on/off switch ‎will be a toggle, so I've set it to true (found under the LOGIC tab).‎

whatever_9

Flame Function

A function is a container for a block of code. I've made a function for our flickering animation, ‎since this is the most complicated part of the code. Putting it inside a function will keep it ‎together and out of the way of the rest of the code. The FUNCTIONS tab is under ADVANCED. ‎I called my function flame.‎

There's a lot going on here. The power lies in the hue, sat, val block that's ‎embedded in the set pixel color block. Both can be found under the LIGHTS tab. ‎

Using the hue, sat, val block in conjunction with a pick random block allows us to ‎choose specific color ranges and have them flicker at random. ‎

using_10

Forever Loop

Whatever we put in the forever loop will run over and over, forever. This is sort of the main ‎control area of the code.‎

Since most of the heavy lifting was done in our flame function, we can keep our forever loop ‎pretty simple.‎

This if/else block is found under the LOGIC tab. If our fireball is turned on (if on = ‎true), the flame function will play. If it's turned off (if on = false), all the lights will ‎turn to black (off). ‎

Check your emulator on the left. You should see the lights on the face of the ‎Circuit Playground start to flicker in your chosen colors.‎

check_11

Changing Your Fireball Colors

Change your colors in the flame function block by changing the numbers in the hue area. For ‎example, if you want greens and yellows, make the three hue blocks read 60-70, 70-80, ‎and 80-90. You can also change the saturation (sat) and make the colors paler or more vibrant. ‎The value (val) numbers will change the brightness of the lights. I have mine on full brightness ‎‎(255).‎

Experiment here until you get colors you like. The changes will show up on the emulator on the ‎left side of the screen.

‎You can also change the speed of the flicker by increasing or decreasing the pause time.‎

On/Off Switch

Under the INPUT tab, we can find this block. I've set up a simple toggle using ‎our on variable. ‎

Try it out on the emulator to be sure it works.‎

try_12

For this project, the buttons will be a little bit hard to reach. I don't want to have to futz ‎around and hit the wrong button when I'm trying to quickly turn my fireball on or off. So, I did ‎a copy/paste with this block and changed the button A dropdown to button B. With both ‎blocks present, I can press either button and the lights will toggle on or off.‎

This is a little user-experience nicety that only takes a second to code but will save you endless ‎futzing time when you're at an event.‎

On Shake - the Flare-up Feature

Finally, we want to make the fireball flare up when you activate the motion sensor on the ‎Circuit Playground.‎

This block is also in the INPUT tab. The first part of the code makes the initial ‎flash, setting all pixels to bright yellow.‎

Then, the second half of the code makes the yellow fade out until it goes dark, ‎at which time the flame function will kick back in.‎

You can add a pause block inside your repeat block to slow the fade down. But I ‎like it at this speed. It feels nice and responsive.‎

you_13

Give your code a name (I called mine Fireball) and save it. Click the Download button and a file ‎will download to your computer. Plug your Circuit Playground Express into your USB port and ‎click the reset button. You should see all the lights on the face of your Circuit Playground ‎Express turn green, and a drive will appear on your computer called CPLAYBOOT. If you see a ‎drive called CIRCUITPY, press the reset button a second time to get to CPLAYBOOT.‎

Drag the downloaded file onto this drive to program the Circuit Playground Express.‎

Once you've got your lights hooked up, shake the Circuit Playground to see the lights flare up!‎

If you're having trouble with the download process, head over to the Circuit Playground ‎Express guide for some more detailed instructions and troubleshooting ideas.‎

Make the Flames

Open your ornament case. Cut off the hanger bit with a pair of flush cutters.‎

open_14

Drill or melt a 1/4" hole into the center of the dome. If you're drilling, start ‎with a smaller drill bit and work your way up through 2-3 sizes to ‎minimize the risk of breaking the acrylic. If you're melting, use a soldering ‎iron with a tip you don't care about and push it right through the plastic. ‎Make sure your window is open, so you don't breathe the fumes.‎

drill_15

We'll use glue dots to stick all the pieces together. These things are great. ‎They're not messy, and they have a really strong hold after just a few ‎minutes. ‎

If you mess up and need to get them off, 99% alcohol will help release the ‎stick.‎

if_16

Open up your Circuit Playground case. Find the case bottom (the one with ‎the screw hole in the middle). Stick 3-4 glue dots on the outside of the ‎case around the perimeter.‎

open_17

Press the case into the ornament half, aligning the screw hole with the ‎hole you drilled.‎

press_18

Cut pieces of colored cellophane wrap to around 12" square. I like the look ‎of rougher edges rather than tidy corners here, but don't worry about the ‎shape too much. You'll have time to finesse it later.‎

Put a few glue dots in the center of your first piece of cellophane.‎

cut_19

Wrap the cellophane layer around your ball, sticking the glue dots to the ‎plastic firmly.‎

Put the top on your ball, then wrap the cellophane around the whole ball ‎and secure it loosely with a rubber band.‎

cwrap_20

Gently heat the cellophane with a heat gun or hair dryer. It will shrink to fit ‎the ball. Don't heat it too much or you may melt holes in it.‎

gently_21

Repeat with your second layer of cellophane. I like to put the lighter / ‎more transparent layer on the outside since it gives such a lovely depth of ‎color. ‎

Gently melt the tops and corners of the cellophane layers. You can trim off ‎any too-long bits with scissors. It's also fun to cut little flaps in the top and ‎then melt the edges a bit, to give a nice random flame look.‎

gently_21a

Gently open the top of the cellophane and pull out the top half of the ball. ‎Put a glue dot on your battery and plug the battery into the Circuit ‎Playground. Place the Circuit Playground inside the bottom of the case ‎and slip the case top in to click it in place. ‎

Stick the battery someplace out of the way, along the edge of the ball.‎

gently_22

If you like, add a little more crumpled cellophane over the Circuit Playground to further ‎diffuse the light for those looking down on the fireball.‎

if_23

Melt a small hole in the cellophane aligned with the screw hole in the ‎bottom of the fireball. Melting works better than cutting here. If you cut ‎the cellophane it's likely to tear, but a melted hole will stay put.‎

melt_24

Screw the 3d printed widget into the screw hole in the Circuit Playground ‎case.‎

screw_25

Slip your fingers through the rings so the fireball hovers above your hand. ‎Shake it around to be sure everything is secure, and watch the lights flare ‎up!‎

Reach in and press either of the Circuit Playground buttons to turn the ‎lights off.‎

screw_26

Battery Life

Turning the lights off with the buttons will lengthen your battery life, but the buttons do NOT ‎cut power to the Circuit Playground. To turn the fireball fully off, you'll need to unplug the ‎battery. If you just leave the lights in the "off" mode, your battery will slowly drain -- no ‎Bueno! ‎

It might not hurt to get a couple extra batteries, and always have your charger on hand.

battery_27

מק"ט יצרן # 3333
CIRCUIT PLAYGROUND EXPRESS
Adafruit Industries LLC
מק"ט יצרן # 3915
CASE PLASTIC TRANSPARENT
Adafruit Industries LLC
מק"ט יצרן # 1865
EDGE-LAUNCH SMA CONNECTOR FOR 1.
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.