Maker.io main logo

Creating Your First Tilemap Game with CircuitPython

48

2020-09-16 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by Tim C

Overview

This project will show you how to create your first tile map game with CircuitPython. We will learn how to make and modify indexed bmp graphics for the game. ugame is used for device agnostic control handling. See how to use spreadsheet applications to create and edit game maps.

tilemap_1

Everything will come together in a sample game with two levels. Once you reach the end of the guide you'll have all the tools you need to customize the sample game or create one of your very own!

The guide is meant to be used with any of these devices: PyGamer, PyBadge, PyBadge LC, Edge Badge, or Pew Pew M4.

Parts

CircuitPython Setup

CircuitPython Setup for the PyBadge and PyGamer

First, to make sure you're running the most recent version of CircuitPython for the PyBadge or PyGamer:

Click to read on installing CircuitPython on the PyBadge devices

Or

Click to read installing CircuitPython on the PyGamer

If you have an Edge Badge the process is the same as PyBadge but use the button below to download the firmware file.

If you have a Pew Pew M4 the process is very similar as the others, but there is no button for the reset pin. Short the R (reset) and - (GND) pins with a wire twice in quick succession to access the BOOT drive. Use the button below to download the firmware file.

Download Edge Badge firmware

Or

Download Pew Pew M4 firmware

CircuitPython Libraries

You'll need a few CircuitPython libraries in the lib folder on the CIRCUITPY drive of your device for the code to work. Head to https://circuitpython.org/libraries to download the latest library bundle matching the major version of CircuitPython now on your board (5 for CircuitPython 5.x, etc.). The procedure is available in the Grand Central M4 Express guide.

Once you've downloaded the libraries bundle, add these library directories to the lib folder on the CIRCUITPY drive:

  • adafruit_display_text
  • adafruit_imageload

Download Circuit Python Library bundle

Tilegame Assets

Included with this project is a directory called tilegame_assets. You must copy this directory onto the CIRCUITPY drive. This contains the artwork, maps, and other modules needed for the game.

With everything in place, your drive should have these files on it:

files_2

It's okay if your device has other files as well, but it must have these ones at a minimum.

Project Files

To get all the code and files for this project, click Download: Project Zip in the code box below. Unzip them and place a copy of them on the CIRCUITPY drive of your device in the directories noted above.

Download: Project Zip or code.py | View on Github

Copy Code
import time
import random
import gc
import board
import displayio
import adafruit_imageload
import ugame
import terminalio
from adafruit_display_text import label
from tilegame_assets.tiles import TILES
from tilegame_assets.states import (
STATE_PLAYING,
STATE_MAPWIN,
STATE_WAITING,
STATE_LOST_SPARKY,
STATE_MINERVA,
)
from tilegame_assets.fun_facts import FACTS
from tilegame_assets.text_helper import wrap_nicely

# pylint: disable=bad-continuation

# Direction constants for comparison
UP = 0
DOWN = 1
RIGHT = 2
LEFT = 3

# how long to wait between rendering frames
FPS_DELAY = 1 / 60

# how many tiles can fit on thes screen. Tiles are 16x16 pixels
SCREEN_HEIGHT_TILES = 8
SCREEN_WIDTH_TILES = 10

# list of maps in order they should be played
MAPS = ["map0.csv", "map1.csv"]

GAME_STATE = {
# hold the map state as it came out of the csv. Only holds non-entities.
"ORIGINAL_MAP": {},
# hold the current map state as it changes. Only holds non-entities.
"CURRENT_MAP": {},
# Dictionary with touple keys that map to lists of entity objects.
# Each one has the index of the sprite in the ENTITY_SPRITES list
# and the tile type string
"ENTITY_SPRITES_DICT": {},
# hold the location of the player in tile coordinates
"PLAYER_LOC": (0, 0),
# list of items the player has in inventory
"INVENTORY": [],
# how many hearts there are in this map level
"TOTAL_HEARTS": 0,
# sprite object to draw for the player
"PLAYER_SPRITE": None,
# size of the map
"MAP_WIDTH": 0,
"MAP_HEIGHT": 0,
# which map level within MAPS we are currently playing
"MAP_INDEX": 0,
# current state of the state machine
"STATE": STATE_PLAYING,
}

# dictionary with tuple keys that map to tile type values
# e.x. {(0,0): "left_wall", (1,1): "floor"}
CAMERA_VIEW = {}

# how far offset the camera is from the GAME_STATE['CURRENT_MAP']
# used to determine where things are at in the camera view vs. the MAP
CAMERA_OFFSET_X = 0
CAMERA_OFFSET_Y = 0

# list of sprite objects, one for each entity
ENTITY_SPRITES = []

# list of entities that need to be on the screen currently based on the camera view
NEED_TO_DRAW_ENTITIES = []


def get_tile(coords):
"""
:param coords: (x, y) tuple
:return: tile name of the tile at the given coords from GAME_STATE['CURRENT_MAP']
"""
return GAME_STATE["CURRENT_MAP"][coords[0], coords[1]]


def get_tile_obj(coords):
"""
:param coords: (x, y) tuple
:return: tile object with stats and behavior for the tile at the given coords.
"""
return TILES[GAME_STATE["CURRENT_MAP"][coords[0], coords[1]]]


#
def is_tile_moveable(tile_coords):
"""
Check the can_walk property of the tile at the given coordinates
:param tile_coords: (x, y) tuple
:return: True if the player can walk on this tile. False otherwise.
"""
return TILES[GAME_STATE["CURRENT_MAP"][tile_coords[0], tile_coords[1]]]["can_walk"]


print("after funcs {}".format(gc.mem_free()))

# display object variable
display = board.DISPLAY

# Load the sprite sheet (bitmap)
sprite_sheet, palette = adafruit_imageload.load(
"tilegame_assets/sprite_sheet.bmp",
bitmap=displayio.Bitmap,
palette=displayio.Palette,
)

# make green be transparent so entities can be drawn on top of map tiles
palette.make_transparent(0)

# Create the castle TileGrid
castle = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=10,
height=8,
tile_width=16,
tile_height=16,
)

# Create a Group to hold the sprite and castle
group = displayio.Group(max_size=33)

# Add castle to the group
group.append(castle)


def load_map(file_name):
# pylint: disable=global-statement,too-many-statements,too-many-nested-blocks,too-many-branches
global ENTITY_SPRITES, CAMERA_VIEW

# empty the sprites from the group
for cur_s in ENTITY_SPRITES:
group.remove(cur_s)
# remove player sprite
try:
group.remove(GAME_STATE["PLAYER_SPRITE"])
except ValueError:
pass

# reset map and other game state objects
GAME_STATE["ORIGINAL_MAP"] = {}
GAME_STATE["CURRENT_MAP"] = {}
ENTITY_SPRITES = []
GAME_STATE["ENTITY_SPRITES_DICT"] = {}
CAMERA_VIEW = {}
GAME_STATE["INVENTORY"] = []
GAME_STATE["TOTAL_HEARTS"] = 0

# Open and read raw string from the map csv file
f = open("tilegame_assets/{}".format(file_name), "r")
map_csv_str = f.read()
f.close()

# split the raw string into lines
map_csv_lines = map_csv_str.replace("\r", "").split("\n")

# set the WIDTH and HEIGHT variables.
# this assumes the map is rectangular.
GAME_STATE["MAP_HEIGHT"] = len(map_csv_lines)
GAME_STATE["MAP_WIDTH"] = len(map_csv_lines[0].split(","))

# loop over each line storing index in y variable
for y, line in enumerate(map_csv_lines):
# ignore empty line
if line != "":
# loop over each tile type separated by commas, storing index in x variable
for x, tile_name in enumerate(line.split(",")):
print("%s '%s'" % (len(tile_name), str(tile_name)))

# if the tile exists in our main dictionary
if tile_name in TILES.keys():

# if the tile is an entity
if (
"entity" in TILES[tile_name].keys()
and TILES[tile_name]["entity"]
):
# set the map tiles to floor
GAME_STATE["ORIGINAL_MAP"][x, y] = "floor"
GAME_STATE["CURRENT_MAP"][x, y] = "floor"

if tile_name == "heart":
GAME_STATE["TOTAL_HEARTS"] += 1

# if it's the player
if tile_name == "player":
# Create the sprite TileGrid
GAME_STATE["PLAYER_SPRITE"] = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=1,
height=1,
tile_width=16,
tile_height=16,
default_tile=TILES[tile_name]["sprite_index"],
)

# set the position of sprite on screen
GAME_STATE["PLAYER_SPRITE"].x = x * 16
GAME_STATE["PLAYER_SPRITE"].y = y * 16

# set position in x,y tile coords for reference later
GAME_STATE["PLAYER_LOC"] = (x, y)

# add sprite to the group
group.append(GAME_STATE["PLAYER_SPRITE"])
else: # not the player
# Create the sprite TileGrid
entity_srite = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=1,
height=1,
tile_width=16,
tile_height=16,
default_tile=TILES[tile_name]["sprite_index"],
)
# set the position of sprite on screen
# default to off the edge
entity_srite.x = -16
entity_srite.y = -16

# add the sprite object to ENTITY_SPRITES list
ENTITY_SPRITES.append(entity_srite)
# print("setting GAME_STATE['ENTITY_SPRITES_DICT'][%s,%s]" % (x,y))

# create an entity obj
_entity_obj = {
"entity_sprite_index": len(ENTITY_SPRITES) - 1,
"map_tile_name": tile_name,
}

# if there are no entities at this location yet
if (x, y) not in GAME_STATE["ENTITY_SPRITES_DICT"]:
# create a list and add it to the dictionary at the x,y location
GAME_STATE["ENTITY_SPRITES_DICT"][x, y] = [_entity_obj]
else:
# append the entity to the existing list in the dictionary
GAME_STATE["ENTITY_SPRITES_DICT"][x, y].append(
_entity_obj
)

else: # tile is not entity
# set the tile_name into MAP dictionaries
GAME_STATE["ORIGINAL_MAP"][x, y] = tile_name
GAME_STATE["CURRENT_MAP"][x, y] = tile_name

else: # tile type wasn't found in dict
print("tile: %s not found in TILES dict" % tile_name)
# add all entity sprites to the group
print("appending {} sprites".format(len(ENTITY_SPRITES)))
for entity in ENTITY_SPRITES:
group.append(entity)


print("loading map")
load_map(MAPS[GAME_STATE["MAP_INDEX"]])

# Add the Group to the Display
display.show(group)

# variables to store previous value of button state
prev_up = False
prev_down = False
prev_left = False
prev_right = False


# helper function returns true if player is allowed to move given direction
# based on can_walk property of the tiles next to the player
def can_player_move(direction):
try:
if direction == UP:
tile_above_coords = (
GAME_STATE["PLAYER_LOC"][0],
GAME_STATE["PLAYER_LOC"][1] - 1,
)

return TILES[
GAME_STATE["CURRENT_MAP"][tile_above_coords[0], tile_above_coords[1]]
]["can_walk"]

if direction == DOWN:
tile_below_coords = (
GAME_STATE["PLAYER_LOC"][0],
GAME_STATE["PLAYER_LOC"][1] + 1,
)
return TILES[
GAME_STATE["CURRENT_MAP"][tile_below_coords[0], tile_below_coords[1]]
]["can_walk"]

if direction == LEFT:
tile_left_of_coords = (
GAME_STATE["PLAYER_LOC"][0] - 1,
GAME_STATE["PLAYER_LOC"][1],
)
return TILES[
GAME_STATE["CURRENT_MAP"][
tile_left_of_coords[0], tile_left_of_coords[1]
]
]["can_walk"]

if direction == RIGHT:
tile_right_of_coords = (
GAME_STATE["PLAYER_LOC"][0] + 1,
GAME_STATE["PLAYER_LOC"][1],
)
return TILES[
GAME_STATE["CURRENT_MAP"][
tile_right_of_coords[0], tile_right_of_coords[1]
]
]["can_walk"]
except KeyError:
return False

return None


# set the appropriate tiles into the CAMERA_VIEW dictionary
# based on given starting coords and size
def set_camera_view(startX, startY, width, height):
# pylint: disable=global-statement
global CAMERA_OFFSET_X
global CAMERA_OFFSET_Y
# set the offset variables for use in other parts of the code
CAMERA_OFFSET_X = startX
CAMERA_OFFSET_Y = startY

# loop over the rows and indexes in the desired size section
for y_index, y in enumerate(range(startY, startY + height)):
# loop over columns and indexes in the desired size section
for x_index, x in enumerate(range(startX, startX + width)):
# print("setting camera_view[%s,%s]" % (x_index,y_index))
try:
# set the tile at the current coordinate of the MAP into the CAMERA_VIEW
CAMERA_VIEW[x_index, y_index] = GAME_STATE["CURRENT_MAP"][x, y]
except KeyError:
# if coordinate is out of bounds set it to floor by default
CAMERA_VIEW[x_index, y_index] = "floor"


# draw the current CAMERA_VIEW dictionary and the GAME_STATE['ENTITY_SPRITES_DICT']
def draw_camera_view():
# list that will hold all entities that have been drawn based on their MAP location
# any entities not in this list should get moved off the screen
drew_entities = []
# print(CAMERA_VIEW)
# pylint: disable=too-many-nested-blocks

# loop over y tile coordinates
for y in range(0, SCREEN_HEIGHT_TILES):
# loop over x tile coordinates
for x in range(0, SCREEN_WIDTH_TILES):
# tile name at this location
tile_name = CAMERA_VIEW[x, y]

# if tile exists in the main dictionary
if tile_name in TILES.keys():
# if there are entity(s) at this location
if (x + CAMERA_OFFSET_X, y + CAMERA_OFFSET_Y) in GAME_STATE[
"ENTITY_SPRITES_DICT"
]:
# default background for entities is floor
castle[x, y] = TILES["floor"]["sprite_index"]

# if it's not the player
if tile_name != "player":
# loop over all entities at this location
for entity_obj_at_tile in GAME_STATE["ENTITY_SPRITES_DICT"][
x + CAMERA_OFFSET_X, y + CAMERA_OFFSET_Y
]:
# set appropriate x,y screen coordinates
# based on tile coordinates
ENTITY_SPRITES[
int(entity_obj_at_tile["entity_sprite_index"])
].x = (x * 16)
ENTITY_SPRITES[
int(entity_obj_at_tile["entity_sprite_index"])
].y = (y * 16)

# add the index of the entity sprite to the draw_entities
# list so we know not to hide it later.
drew_entities.append(
entity_obj_at_tile["entity_sprite_index"]
)

else: # no entities at this location
# set the sprite index of this tile into the CASTLE dictionary
castle[x, y] = TILES[tile_name]["sprite_index"]

else: # tile type not found in main dictionary
# default to floor tile
castle[x, y] = TILES["floor"]["sprite_index"]

# if the player is at this x,y tile coordinate accounting for camera offset
if GAME_STATE["PLAYER_LOC"] == ((x + CAMERA_OFFSET_X, y + CAMERA_OFFSET_Y)):
# set player sprite screen coordinates
GAME_STATE["PLAYER_SPRITE"].x = x * 16
GAME_STATE["PLAYER_SPRITE"].y = y * 16

# loop over all entity sprites
for index in range(0, len(ENTITY_SPRITES)):
# if the sprite wasn't drawn then it's outside the camera view
if index not in drew_entities:
# hide the sprite by moving it off screen
ENTITY_SPRITES[index].x = int(-16)
ENTITY_SPRITES[index].y = int(-16)


# variable to store timestamp of last drawn frame
last_update_time = 0

# variables to store movement offset values
x_offset = 0
y_offset = 0


def show_splash(new_text, color, vertical_offset=18):
text_area.text = ""
text_area.text = new_text
text_area.y = round(text_area.text.count("\n") * vertical_offset / 2)
text_area.color = color
group.append(splash)


# game message background bmp file
with open(
"tilegame_assets/game_message_background.bmp", "rb"
) as game_message_background:
# Make the splash context
splash = displayio.Group(max_size=4)

odb = displayio.OnDiskBitmap(game_message_background)

bg_grid = displayio.TileGrid(odb, pixel_shader=displayio.ColorConverter())

splash.append(bg_grid)

# Text for the message
text_group = displayio.Group(max_size=8, scale=1, x=14, y=18)
text_area = label.Label(terminalio.FONT, text=" " * 180, color=0xD39AE5)
text_group.append(text_area)
splash.append(text_group)

# main loop
while True:
# set the current button values into variables
cur_btn_vals = ugame.buttons.get_pressed()
cur_up = cur_btn_vals & ugame.K_UP
cur_down = cur_btn_vals & ugame.K_DOWN
cur_right = cur_btn_vals & ugame.K_RIGHT
cur_left = cur_btn_vals & ugame.K_LEFT
cur_a = cur_btn_vals & ugame.K_O or cur_btn_vals & ugame.K_X

if GAME_STATE["STATE"] == STATE_WAITING:
print(cur_a)
if cur_a:
GAME_STATE["STATE"] = STATE_PLAYING
group.remove(splash)

if GAME_STATE["STATE"] == STATE_PLAYING:
# check for up button press / release
if not cur_up and prev_up:
if can_player_move(UP):
x_offset = 0
y_offset = -1

# check for down button press / release
if not cur_down and prev_down:
if can_player_move(DOWN):
x_offset = 0
y_offset = 1

# check for right button press / release
if not cur_right and prev_right:
if can_player_move(RIGHT):
x_offset = 1
y_offset = 0

# check for left button press / release
if not cur_left and prev_left:
if can_player_move(LEFT):
x_offset = -1
y_offset = 0

# if any offset is not zero then we need to process player movement
if x_offset != 0 or y_offset != 0:
# variable to store if player is allowed to move
can_move = False

# coordinates the player is moving to
moving_to_coords = (
GAME_STATE["PLAYER_LOC"][0] + x_offset,
GAME_STATE["PLAYER_LOC"][1] + y_offset,
)

# tile name of the spot player is moving to
moving_to_tile_name = GAME_STATE["CURRENT_MAP"][
moving_to_coords[0], moving_to_coords[1]
]

# if there are entity(s) at spot the player is moving to
if moving_to_coords in GAME_STATE["ENTITY_SPRITES_DICT"]:
print("found entity(s) where we are moving to")

# loop over all entities at the location player is moving to
for entity_obj in GAME_STATE["ENTITY_SPRITES_DICT"][
moving_to_coords
]:
print("checking entity %s" % entity_obj["map_tile_name"])
# if the entity has a before_move behavior function
if "before_move" in TILES[entity_obj["map_tile_name"]].keys():
print(
"calling before_move %s, %s, %s"
% (
moving_to_coords,
GAME_STATE["PLAYER_LOC"],
entity_obj,
)
)
# call the before_move behavior function act upon it's result
if TILES[entity_obj["map_tile_name"]]["before_move"](
moving_to_coords,
GAME_STATE["PLAYER_LOC"],
entity_obj,
GAME_STATE,
):
# all the movement if it returned true
can_move = True
else:
# break and don't allow movement if it returned false
break
else: # entity does not have a before_move function
# allow movement
can_move = True
if can_move:
# set the player loc variable to the new coords
GAME_STATE["PLAYER_LOC"] = moving_to_coords

else: # no entities at the location player is moving to
# set player loc variable to new coords
GAME_STATE["PLAYER_LOC"] = moving_to_coords

# reset movement offset variables
y_offset = 0
x_offset = 0

# set previous button values for next iteration
prev_up = cur_up
prev_down = cur_down
prev_right = cur_right
prev_left = cur_left

# current time
now = time.monotonic()

# if it has been long enough based on FPS delay
if now > last_update_time + FPS_DELAY:
# Set camera to 10x8 centered on the player
# Clamped to (0, MAP_WIDTH) and (0, MAP_HEIGHT)
set_camera_view(
max(
min(
GAME_STATE["PLAYER_LOC"][0] - 4,
GAME_STATE["MAP_WIDTH"] - SCREEN_WIDTH_TILES,
),
0,
),
max(
min(
GAME_STATE["PLAYER_LOC"][1] - 3,
GAME_STATE["MAP_HEIGHT"] - SCREEN_HEIGHT_TILES,
),
0,
),
10,
8,
)
# draw the camera
draw_camera_view()
# if player beat this map
if GAME_STATE["STATE"] == STATE_MAPWIN:
GAME_STATE["MAP_INDEX"] += 1
# if player has beaten all maps
if GAME_STATE["MAP_INDEX"] >= len(MAPS):
GAME_STATE["MAP_INDEX"] = 0
GAME_STATE["STATE"] = STATE_WAITING
load_map(MAPS[GAME_STATE["MAP_INDEX"]])
show_splash(
"You Win \n =D \nCongratulations. \nStart Over?", 0x29C1CF
)
else:
# prompt to start next
GAME_STATE["STATE"] = STATE_WAITING
load_map(MAPS[GAME_STATE["MAP_INDEX"]])
show_splash(
"You beat this level\n =D \nCongratulations. \nStart Next?",
0x29C1CF,
)
# game over from sparky
elif GAME_STATE["STATE"] == STATE_LOST_SPARKY:
GAME_STATE["MAP_INDEX"] = 0
GAME_STATE["STATE"] = STATE_WAITING
game_over_text = (
"Be careful not to \ntouch Sparky unless \n"
"you've collected \nenough Mho's.\nStarting Over"
)
load_map(MAPS[GAME_STATE["MAP_INDEX"]])
show_splash(game_over_text, 0x25AFBB)

# talking to minerva
elif GAME_STATE["STATE"] == STATE_MINERVA:
GAME_STATE["STATE"] = STATE_WAITING
random_fact = random.choice(FACTS)
minerva_txt = wrap_nicely("Minerva: {}".format(random_fact), 23)
show_splash(minerva_txt, 0xD39AE5, 10)

# store the last update time
last_update_time = now

Rendering and Movement

Basic Rendering Code

If you are brand new to CircuitPython or displayio based programs, or even if it's just been a while, you should start by going over the Multiple Tilegrids page in the displayio guide. After you've done that then come back here.

To start, let’s look at this example:

Download: Project Zip or basic_rendering.py | View on Github

Copy Code
import board
import displayio
import adafruit_imageload

display = board.DISPLAY

# Load the sprite sheet (bitmap)
sprite_sheet, palette = adafruit_imageload.load(
"tilegame_assets/castle_sprite_sheet.bmp",
bitmap=displayio.Bitmap,
palette=displayio.Palette,
)

# Create the sprite TileGrid
sprite = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=1,
height=1,
tile_width=16,
tile_height=16,
default_tile=0,
)

# Create the castle TileGrid
castle = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=10,
height=8,
tile_width=16,
tile_height=16,
)

# Create a Group to hold the sprite and add it
sprite_group = displayio.Group()
sprite_group.append(sprite)

# Create a Group to hold the castle and add it
castle_group = displayio.Group(scale=1)
castle_group.append(castle)

# Create a Group to hold the sprite and castle
group = displayio.Group()

# Add the sprite and castle to the group
group.append(castle_group)
group.append(sprite_group)

# Castle tile assignments
# corners
castle[0, 0] = 3 # upper left
castle[9, 0] = 5 # upper right
castle[0, 7] = 9 # lower left
castle[9, 7] = 11 # lower right
# top / bottom walls
for x in range(1, 9):
castle[x, 0] = 4 # top
castle[x, 7] = 10 # bottom
# left/ right walls
for y in range(1, 7):
castle[0, y] = 6 # left
castle[9, y] = 8 # right
# floor
for x in range(1, 9):
for y in range(1, 7):
castle[x, y] = 7 # floor

# put the sprite somewhere in the castle
sprite.x = 16 * 4
sprite.y = 16 * 3

# Add the Group to the Display
display.show(group)
while True:
pass

In this code we have two Groups, one for the castle and one for the sprite or player icon, Blinka. These groups each get a TileGrid created and added to them. The castle TileGrid is sized 10x8 and divides evenly into the 160x128 pixel screen with each tile being 16x16 pixels. It holds the tiles that make up the portion of the map visible currently. The sprite TileGrid is only 1x1 but does still use the same 16x16 pixel size. It holds the Blinka image for the player.

If you do you do not understand the basics of how this layout works take a look back at the Multiple Tilegrids page in the displayio guide. We will build on these concepts to create the rest of the game map. The first thing we'll do is add a movement system so we can make Blinka move around using the d-pad or joystick.

Tilegrids_3

Basic Movement Code

In the code above, we have a variable player_loc that stores the coordinates of the player in tile coordinates. It's set to {"x":4, "y":3} by default. These correspond to the indexes of the tiles starting from the top left corner at {"x":0, "y":0}.

code_4

To handle player movement, we will use a library called ugame. This helper module abstracts away the differences between different boards and leaves us with common signals to use for D-pad and other buttons.

The code above already contains the import for it, here is what it looks like:

Download: file

Copy Code
import ugame

After it's been imported we can access the current button states with ugame.buttons.get_pressed() it will return a number which holds each button state accessible by anding with the button constants like this:

Download: file

Copy Code
ugame.buttons.get_pressed() & ugame.K_UP # True if up btn is pressed.
ugame.buttons.get_pressed() & ugame.K_DOWN # True if down btn is pressed.
ugame.buttons.get_pressed() & ugame.K_RIGHT # True if right btn is pressed.
ugame.buttons.get_pressed() & ugame.K_LEFT # True if left btn is pressed.

We'll use these values in the main loop along with the prev_btn_vals to decide when we need to change the player_loc. Inside the main loop we update the sprite.x and sprite.y values to match the player_loc. This will make Blinka move around when the player presses D-pad buttons or uses the joystick.

Update the code from above to use this main loop.

Download: file

Copy Code
# Variable to old previous button state
prev_btn_vals = ugame.buttons.get_pressed()
while True:
cur_btn_vals = ugame.buttons.get_pressed() # update button sate
# if up button was pressed
if not prev_btn_vals & ugame.K_UP and cur_btn_vals & ugame.K_UP:
player_loc["y"] = max(1, player_loc["y"]-1)
# if down button was pressed
if not prev_btn_vals & ugame.K_DOWN and cur_btn_vals & ugame.K_DOWN:
player_loc["y"] = min(6, player_loc["y"]+1)
# if right button was pressed
if not prev_btn_vals & ugame.K_RIGHT and cur_btn_vals & ugame.K_RIGHT:
player_loc["x"] = min(8, player_loc["x"]+1)
# if left button was pressed
if not prev_btn_vals & ugame.K_LEFT and cur_btn_vals & ugame.K_LEFT:
player_loc["x"] = max(1, player_loc["x"]-1)

# update the the player sprite position
sprite.x = 16 * player_loc["x"]
sprite.y = 16 * player_loc["y"]

# update the previous values
prev_btn_vals = cur_btn_vals

Now we can use the D-pad or joystick to move Blinka around!

Blinka_5

Next, we will change the graphics to get rid of the white square around Blinka.

Indexed BMP Graphics

There are many image editing programs that can be used to create and modify bmp assets for use with CircuitPython. If you have access to and are familiar with Adobe Photoshop you can use that. If you are into making games and/or pixel art specifically, there is Aespire which offers many great features that make it very easy to work with pixel art indexed bmp files. It's not free, but it is a nice utility for making and editing graphics.

For this guide, we'll use a free alternative: The GNU Image Manipulation Program or GIMP. This works on Linux, Mac, and Windows PCs, and it's free to use and open sourced. We will use this to edit the image so that we can make the white background appear as transparent in the game. If you don't already have GIMP installed, use the link above and follow the installation instructions for your OS.

We'll starting from this bmp file:

castle_sprite_sheet.bmp

Open this file in GIMP by using File -> Open or Ctrl+O then navigate to the directory where you've download the bmp file or project zip.

At real size 100% zoom the image will likely appear very small in GIMP. It's very helpful to zoom in with Ctrl+MouseWheel or the plus and minus buttons.

GIMP_6

Transparency within Indexed BMPs

The bmp file format does not directly support transparency. Instead we are able to add code in CircuitPython that declares certain colors to appear as transparent instead of showing normally. You can think of it sort of like a green screen effect.

In the existing image, white is the color in the background, but we don't want to set white as transparent because Blinka and the Robot's eyes contain white, so they would look wrong. Sometimes bright pink is used as the background color in sprite sheets for this purpose. But we have the heart graphic already using pink though, so we don't want to use pink either. We'll use green instead to follow with the green screen analogy. But really it could be any color that is not already used in the graphic.

Converting to RGB Mode

Before we can modify the image, we need to change it back to RGB color mode. Right now, the image is in indexed color mode which means it only has access to a small set of colors.

Here are the currently available colors for this image:

colors_7

Since the green we want to use is not one of these colors it won't work, by default GIMP would choose the closest available color. But instead we want to add green to the available colors and use it. So, we need to switch back to RGB color mode for now.

To do that click Image -> Mode -> RGB

RGB_8

Filling in the Background

Now you can set your foreground color and use the paint bucket tool to fill in the background parts of the sprite image with pure green #00FF00.

green_9

In the image above, I've added small paint bucket icons in the two spots I clicked with the paint bucket tool to fill in the background green.

Converting back to Indexed Color Mode

Once the background is filled in we need to switch the image back to indexed color mode so that CircuitPython can use it.

Click: Image -> Mode -> Indexed

index_10

Leave the default settings in the Convert Image to Index Colors configuration dialog. It should look like this.

Click the Convert button.

convert_11

Re-arrange the Color Index

In the CircuitPython code we will need to specify a color index that is going to be shown as transparent. We can see the colors and their indexes inside of gimp in the Rearrange Colormap window. To access it:

Click: Color -> Map -> Rearrange Colormap

colormap_12

window_13

In my case, the newly added pure green transparency placeholder is at index 14. It may be different for you, if so that's no problem.

We could make note of this index and use it in the CircuitPython code. But then if we ever change the image, we would need to make sure to go change the code if the index changed again due to us adding or removing colors.

Instead let's move the transparency placeholder to index 0. Then we can always make index 0 transparent in the code and as long as we always follow this rule when preparing bmp files, we can use the same code everywhere and it will work.

So, click and drag your placeholder color over to the very first position in the list. The index still shows the wrong number but that is okay for now.

list_14

Once your transparency placeholder is in the first position, click the Ok button.

At this point you are ready to export your image as a bmp file.

But I know it is weird the indexes were wrong on the previous screen... If you like to double check on things you can click Color -> Map -> Rearrange Colormap again to open up a new window and see that the indexes are updated to the proper numbers. It would look like this now:

map_15

Saving the Image as a BMP File

Now the image is ready to be exported out of gimp as a bitmap file that is ready to show with CircuitPython displayio.

Click: File -> Export As..

or Press: Ctrl+Shift+E

You can choose any name for your file, but it must end with .bmp because this will be the format that gimp saves the file with. I am going to use the name castle_sprite_sheet_edited.bmp. You can choose a different name if you like, if you do make sure to edit the rest of the sample code to use your own bmp filename.

At a minimum, you need to export one copy to your CIRCUITPY drive, but you can also save a copy to your local file system if you like. For this example, we are going to save it into the tilegame_assets directory.

copy_16

Once you've got the filename and location selected click on the Export button at the bottom.

Leave the default values in the export dialog.

Click the Export button.

export_17

Now we can change the sprite image loading code to use the new image and set the color at index 0 to be transparent.

Download: file

Copy Code
sprite_sheet, palette = adafruit_imageload.load("tilegame_assets/castle_sprite_sheet_edited.bmp",
bitmap=displayio.Bitmap,
palette=displayio.Palette)

# Make the color at index 0 show as transparent
palette.make_transparent(0)

sprite_18

Download: Project Zip or basic_movement_transparent_sprite.py | View on Github

Copy Code
import board
import displayio
import adafruit_imageload
import ugame

display = board.DISPLAY
player_loc = {"x": 4, "y": 3}

# Load the sprite sheet (bitmap)
sprite_sheet, palette = adafruit_imageload.load(
"tilegame_assets/castle_sprite_sheet_edited.bmp",
bitmap=displayio.Bitmap,
palette=displayio.Palette,
)
# make the color at 0 index transparent.
palette.make_transparent(0)

# Create the sprite TileGrid
sprite = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=1,
height=1,
tile_width=16,
tile_height=16,
default_tile=0,
)

# Create the castle TileGrid
castle = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=10,
height=8,
tile_width=16,
tile_height=16,
)

# Create a Group to hold the sprite and add it
sprite_group = displayio.Group()
sprite_group.append(sprite)

# Create a Group to hold the castle and add it
castle_group = displayio.Group(scale=1)
castle_group.append(castle)

# Create a Group to hold the sprite and castle
group = displayio.Group()

# Add the sprite and castle to the group
group.append(castle_group)
group.append(sprite_group)

# Castle tile assignments
# corners
castle[0, 0] = 3 # upper left
castle[9, 0] = 5 # upper right
castle[0, 7] = 9 # lower left
castle[9, 7] = 11 # lower right
# top / bottom walls
for x in range(1, 9):
castle[x, 0] = 4 # top
castle[x, 7] = 10 # bottom
# left/ right walls
for y in range(1, 7):
castle[0, y] = 6 # left
castle[9, y] = 8 # right
# floor
for x in range(1, 9):
for y in range(1, 7):
castle[x, y] = 7 # floor

# put the sprite somewhere in the castle
sprite.x = 16 * player_loc["x"]
sprite.y = 16 * player_loc["y"]

# Add the Group to the Display
display.show(group)

prev_btn_vals = ugame.buttons.get_pressed()

while True:
cur_btn_vals = ugame.buttons.get_pressed()
if not prev_btn_vals & ugame.K_UP and cur_btn_vals & ugame.K_UP:
player_loc["y"] = max(1, player_loc["y"] - 1)
if not prev_btn_vals & ugame.K_DOWN and cur_btn_vals & ugame.K_DOWN:
player_loc["y"] = min(6, player_loc["y"] + 1)

if not prev_btn_vals & ugame.K_RIGHT and cur_btn_vals & ugame.K_RIGHT:
player_loc["x"] = min(8, player_loc["x"] + 1)
if not prev_btn_vals & ugame.K_LEFT and cur_btn_vals & ugame.K_LEFT:
player_loc["x"] = max(1, player_loc["x"] - 1)

# update the the player sprite position
sprite.x = 16 * player_loc["x"]
sprite.y = 16 * player_loc["y"]

# update the previous values
prev_btn_vals = cur_btn_vals

Game Code Structure

State Machine

At the highest level inside the main loop, the game program uses a state machine to behave the correct way at any given time, based on what the player has done so far. If you don't know what a state machine is, or just want a refresher there is a nice guide here: https://learn.adafruit.com/circuitpython-101-state-machines

GAME_STATE Object

The state machine in this game uses numbers to track the state and we give each number a descriptive variable name to use in the code.

The current state that the state machine is in gets stored in GAME_STATE["STATE"]. All of the possible states are in tilegame_assets\states.py:

Download: Project Zip or states.py | View on Github

Copy Code
# State machine constants

# playing the game: draw the map, listen for D-pad buttons to move player
STATE_PLAYING = 0

# player beat this map level
STATE_MAPWIN = 1

# waiting for player to press A button to continue
STATE_WAITING = 2

# player lost by touching sparky
STATE_LOST_SPARKY = 3

# minerva shows a fun fact
STATE_MINERVA = 4

The "STATE" item within the GAME_STATE dictionary is the only one that refers to the state machine logic.

The rest of the items in the GAME_STATE dictionary store information about the current game and map.

Here are the starting values:

Download: file

Copy Code
GAME_STATE = {
# hold the map state as it came out of the csv. Only holds non-entities.
"ORIGINAL_MAP": {},
# hold the current map state as it changes. Only holds non-entities.
"CURRENT_MAP": {},
# Dictionary with touple keys that map to lists of entity objects.
# Each one has the index of the sprite in the ENTITY_SPRITES list
# and the tile type string
"ENTITY_SPRITES_DICT": {},
# hold the location of the player in tile coordinates
"PLAYER_LOC": (0, 0),
# list of items the player has in inventory
"INVENTORY": [],
# how many hearts there are in this map level
"TOTAL_HEARTS": 0,
# sprite object to draw for the player
"PLAYER_SPRITE": None,
# size of the map
"MAP_WIDTH": 0,
"MAP_HEIGHT": 0,
# which map level within MAPS we are currently playing
"MAP_INDEX": 0,
# current state of the state machine
"STATE": STATE_PLAYING,
}

Their values will change as the map gets loaded and the player moves around and does things within the game.

CSV Maps and Tile Types

Map File

The game will load the maps from CSV (Comma Separated Value) files. We can edit these with any spreadsheet program. Here is an example of a map:

spreadsheet_19

Any blank cells will get treated as empty tiles that can't be walked on. Every cell that isn't empty must have an entry in the main TILES dictionary which is located inside of tilegame_assets\tiles.py.

Loading the Map

To load the CSV map, we start by loop over each row. split(',') breaks the row down into a list which we will also loop over. On each item within the row, we look it up in the TILES dictionary. Non-entities get added to the ORIGINAL_MAP and CURRENT_MAP game state objects.

The enumerate() function is used on the loops to easily track x and y coordinates so we know where to add tiles to the map objects.

Entities also get added to the ENTITY_SPRITES_DICT game state object. Their sprites are loaded and added to the sprite_group so they'll be drawn on the screen. In the map objects a "floor" tile is placed at the location of the entity. The entity will be drawn on top of the floor.

Here is the code that loads the map:

Download: file

Copy Code
def load_map(file_name):
# pylint: disable=global-statement,too-many-statements,too-many-nested-blocks,too-many-branches
global ENTITY_SPRITES, CAMERA_VIEW

# empty the sprites from the group
for cur_s in ENTITY_SPRITES:
group.remove(cur_s)
# remove player sprite
try:
group.remove(GAME_STATE["PLAYER_SPRITE"])
except ValueError:
pass

# reset map and other game state objects
GAME_STATE["ORIGINAL_MAP"] = {}
GAME_STATE["CURRENT_MAP"] = {}
ENTITY_SPRITES = []
GAME_STATE["ENTITY_SPRITES_DICT"] = {}
CAMERA_VIEW = {}
GAME_STATE["INVENTORY"] = []
GAME_STATE["TOTAL_HEARTS"] = 0

# Open and read raw string from the map csv file
f = open("tilegame_assets/{}".format(file_name), "r")
map_csv_str = f.read()
f.close()

# split the raw string into lines
map_csv_lines = map_csv_str.replace("\r", "").split("\n")

# set the WIDTH and HEIGHT variables.
# this assumes the map is rectangular.
GAME_STATE["MAP_HEIGHT"] = len(map_csv_lines)
GAME_STATE["MAP_WIDTH"] = len(map_csv_lines[0].split(","))

# loop over each line storing index in y variable
for y, line in enumerate(map_csv_lines):
# ignore empty line
if line != "":
# loop over each tile type separated by commas, storing index in x variable
for x, tile_name in enumerate(line.split(",")):
print("%s '%s'" % (len(tile_name), str(tile_name)))

# if the tile exists in our main dictionary
if tile_name in TILES.keys():

# if the tile is an entity
if (
"entity" in TILES[tile_name].keys()
and TILES[tile_name]["entity"]
):
# set the map tiles to floor
GAME_STATE["ORIGINAL_MAP"][x, y] = "floor"
GAME_STATE["CURRENT_MAP"][x, y] = "floor"

if tile_name == "heart":
GAME_STATE["TOTAL_HEARTS"] += 1

# if it's the player
if tile_name == "player":
# Create the sprite TileGrid
GAME_STATE["PLAYER_SPRITE"] = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=1,
height=1,
tile_width=16,
tile_height=16,
default_tile=TILES[tile_name]["sprite_index"],
)

# set the position of sprite on screen
GAME_STATE["PLAYER_SPRITE"].x = x * 16
GAME_STATE["PLAYER_SPRITE"].y = y * 16

# set position in x,y tile coords for reference later
GAME_STATE["PLAYER_LOC"] = (x, y)

# add sprite to the group
group.append(GAME_STATE["PLAYER_SPRITE"])
else: # not the player
# Create the sprite TileGrid
entity_srite = displayio.TileGrid(
sprite_sheet,
pixel_shader=palette,
width=1,
height=1,
tile_width=16,
tile_height=16,
default_tile=TILES[tile_name]["sprite_index"],
)
# set the position of sprite on screen
# default to off the edge
entity_srite.x = -16
entity_srite.y = -16

# add the sprite object to ENTITY_SPRITES list
ENTITY_SPRITES.append(entity_srite)
# print("setting GAME_STATE['ENTITY_SPRITES_DICT'][%s,%s]" % (x,y))

# create an entity obj
_entity_obj = {
"entity_sprite_index": len(ENTITY_SPRITES) - 1,
"map_tile_name": tile_name,
}

# if there are no entities at this location yet
if (x, y) not in GAME_STATE["ENTITY_SPRITES_DICT"]:
# create a list and add it to the dictionary at the x,y location
GAME_STATE["ENTITY_SPRITES_DICT"][x, y] = [_entity_obj]
else:
# append the entity to the existing list in the dictionary
GAME_STATE["ENTITY_SPRITES_DICT"][x, y].append(
_entity_obj
)

else: # tile is not entity
# set the tile_name into MAP dictionaries
GAME_STATE["ORIGINAL_MAP"][x, y] = tile_name
GAME_STATE["CURRENT_MAP"][x, y] = tile_name

else: # tile type wasn't found in dict
print("tile: %s not found in TILES dict" % tile_name)
# add all entity sprites to the group
print("appending {} sprites".format(len(ENTITY_SPRITES)))
for entity in ENTITY_SPRITES:
group.append(entity)

Tile Types

These entries define the look and behavior of the tiles. Here is an example of a tile type entry:

Download: file

Copy Code
# ... behavior functions declared above...
TILES = {
# ... many tile type entries ...
"mho": {
"sprite_index": 2,
"can_walk": True,
"entity": True,
"before_move": take_item
},
# ... more entries ...
}

The keys within the TILES dictionary match up with the values from the map CSV file. One of the mho tiles is located at cell D3. There may be tile keys that aren't present in a particular map, they will have no effect when playing that map level in the game.

These entries define the look and behavior of tiles using the following properties:

  • sprite_index - The index within the sprite sheet to show for this tile.
  • can_walk - Whether the player is allowed to walk on this tile.
  • entity - Whether this tile represents an entity. If so it will get drawn on top of a floor tile and theoretically it could move around the map. The player is an entity as well as Mho, Heart, Minerva, and Robot. However, the player is the only entity in the example game that moves.
  • before_move - (Optional) If set to a function the function will get called when the player tries to walk on this tile. If the function returns True the player will be allowed to walk on the tile if the function returns False the player will not be allowed to walk on it.

Behavior Functions

These functions must be declared before the main TILES dictionary because tiles that want special behaviors will get them by setting the before_move property in their tile type entry to a behavior function. These are also declared inside the file: tilegame_assets\tiles.py. The existing behavior functions are:

  • take_item- if the item is still here then adding it to the player's inventory and remove it from this tile. In the example game both "mho" and "heart" tile types use this function.
  • sparky_walk - if the player has a "Mho" in their inventory it gets consumed and the Sparky is removed from this tile. If they player has no "Mho" they let the smoke out and must restart this level.
  • minerva_walk - change the game state to STATE_MINERVA in this state Minerva will show the player a fun fact and prompt them to press a button to continue. This function always returns False so the player is never allowed to actually move on to this tile. The fun facts are stored as a list inside the file: tilegame_assets\fun_facts.py. If you add your own facts to this list Minerva will show them to the player sometimes.
  • robot_walk - if the player has gathered all of the hearts from this map then they are allowed to move to the robot, and they win this level. Game state is changed to STATE_MAPWIN. If they have not gathered all available hearts, then they are not allowed to move to this tile.

You can declare your own tile types and behavior functions in this file to customize your game!

tiles_20

tiles.py

Download: Project Zip or tiles.py | View on Github

Copy Code
from tilegame_assets.states import (
STATE_MAPWIN,
STATE_LOST_SPARKY,
STATE_MINERVA,
)
# pylint: disable=unused-argument


# Minerva before_move. Set game state to STATE_MINERVA
def minerva_walk(to_coords, from_coords, entity_obj, GAME_STATE):
GAME_STATE["STATE"] = STATE_MINERVA
return False


# Sparky before_move. If user does not have a Mho in inventory they lose.
# If user does have Mho subtract one from inventory and consume Sparky.
def sparky_walk(to_coords, from_coords, entity_obj, GAME_STATE):
if GAME_STATE["INVENTORY"].count("mho") > 0:
GAME_STATE["INVENTORY"].remove("mho")
GAME_STATE["ENTITY_SPRITES_DICT"][to_coords].remove(entity_obj)
if len(GAME_STATE["ENTITY_SPRITES_DICT"][to_coords]) == 0:
del GAME_STATE["ENTITY_SPRITES_DICT"][to_coords]
if (-1, -1) in GAME_STATE["ENTITY_SPRITES_DICT"]:
GAME_STATE["ENTITY_SPRITES_DICT"][-1, -1].append(entity_obj)
else:
GAME_STATE["ENTITY_SPRITES_DICT"][-1, -1] = [entity_obj]
return True
else:
GAME_STATE["STATE"] = STATE_LOST_SPARKY
return True


# Robot before_move. If user has all Hearts they win the map.
def robot_walk(to_coords, from_coords, entity_obj, GAME_STATE):
if GAME_STATE["INVENTORY"].count("heart") == GAME_STATE["TOTAL_HEARTS"]:
GAME_STATE["STATE"] = STATE_MAPWIN
return True

return False


# Remove the item from this location and add it to player inventory.
def take_item(to_coords, from_coords, entity_obj, GAME_STATE):
print(entity_obj)
GAME_STATE["INVENTORY"].append(entity_obj["map_tile_name"])
GAME_STATE["ENTITY_SPRITES_DICT"][to_coords].remove(entity_obj)
if len(GAME_STATE["ENTITY_SPRITES_DICT"][to_coords]) == 0:
del GAME_STATE["ENTITY_SPRITES_DICT"][to_coords]

if (-1, -1) in GAME_STATE["ENTITY_SPRITES_DICT"]:
GAME_STATE["ENTITY_SPRITES_DICT"][-1, -1].append(entity_obj)
else:
GAME_STATE["ENTITY_SPRITES_DICT"][-1, -1] = [entity_obj]

return True


# main dictionary that maps tile type strings to objects.
# each one stores the sprite_sheet index and any necessary
# behavioral stats like can_walk or before_move
TILES = {
# empty strings default to floor and no walk.
"": {"sprite_index": 10, "can_walk": False},
"floor": {"sprite_index": 10, "can_walk": True},
"top_wall": {"sprite_index": 7, "can_walk": False},
"top_right_wall": {"sprite_index": 8, "can_walk": False},
"top_left_wall": {"sprite_index": 6, "can_walk": False},
"bottom_right_wall": {"sprite_index": 14, "can_walk": False},
"bottom_left_wall": {"sprite_index": 12, "can_walk": False},
"right_wall": {"sprite_index": 11, "can_walk": False},
"left_wall": {"sprite_index": 9, "can_walk": False},
"bottom_wall": {"sprite_index": 13, "can_walk": False},
"robot": {
"sprite_index": 1,
"can_walk": True,
"entity": True,
"before_move": robot_walk,
},
"heart": {
"sprite_index": 5,
"can_walk": True,
"entity": True,
"before_move": take_item,
},
"mho": {
"sprite_index": 2,
"can_walk": True,
"entity": True,
"before_move": take_item,
},
"sparky": {
"sprite_index": 4,
"can_walk": True,
"entity": True,
"before_move": sparky_walk,
},
"minerva": {
"sprite_index": 3,
"can_walk": True,
"entity": True,
"before_move": minerva_walk,
},
"player": {"sprite_index": 0, "entity": True,},
}

Camera View

In order to allow the map to be larger than the screen or shaped differently than a plain rectangle we use a CAMERA_VIEW dictionary. Just like the full map dictionary, the keys are (x,y) coordinate tuples and the values are tile type strings. But unlike the full map dictionary the CAMERA_VIEW is always the exact same size and shape 10x8 tiles in this game, which matches up with the screen size on the PyGamer and PyBadge devices.

There are two functions related to camera management: set_camera_view() and draw_camera_view().

set_camera_view() will build the CAMERA_VIEW dictionary based on the current game state. It accepts parameters for x, y starting point within the map as well as width and height. The example game will always use 10, 8 for the size so it fits perfectly on the 160x128 pixel screen. If you wanted to adapt the game code to work with a different sized screen you could change these values.

draw_camera_view() will draw the current contents of the CAMERA_VIEW dictionary onto the screen. It will also check for the existence of and draw any entities that are within the coordinates of the CAMERA_VIEW.

view_21

In this game, the camera will always stay centered on the player because we reference the player location in the x, and y value parameters when set_camera_view() is called.

Here are the set_camera_view() and draw_camera_view() function definitions:

Download: file

Copy Code
# set the appropriate tiles into the CAMERA_VIEW dictionary
# based on given starting coords and size
def set_camera_view(startX, startY, width, height):
global CAMERA_OFFSET_X
global CAMERA_OFFSET_Y
# set the offset variables for use in other parts of the code
CAMERA_OFFSET_X = startX
CAMERA_OFFSET_Y = startY

# loop over the rows and indexes in the desired size section
for y_index, y in enumerate(range(startY, startY + height)):
# loop over columns and indexes in the desired size section
for x_index, x in enumerate(range(startX, startX + width)):
# print("setting camera_view[%s,%s]" % (x_index,y_index))
try:
# set the tile at the current coordinate of the MAP into the CAMERA_VIEW
CAMERA_VIEW[x_index, y_index] = GAME_STATE["CURRENT_MAP"][x, y]
except KeyError:
# if coordinate is out of bounds set it to floor by default
CAMERA_VIEW[x_index, y_index] = "floor"


# draw the current CAMERA_VIEW dictionary and the GAME_STATE['ENTITY_SPRITES_DICT']
def draw_camera_view():
# list that will hold all entities that have been drawn based on their MAP location
# any entities not in this list should get moved off the screen
drew_entities = []
# print(CAMERA_VIEW)

# loop over y tile coordinates
for y in range(0, SCREEN_HEIGHT_TILES):
# loop over x tile coordinates
for x in range(0, SCREEN_WIDTH_TILES):
# tile name at this location
tile_name = CAMERA_VIEW[x, y]

# if tile exists in the main dictionary
if tile_name in TILES.keys():
# if there are entity(s) at this location
if (x + CAMERA_OFFSET_X, y + CAMERA_OFFSET_Y) in GAME_STATE[
"ENTITY_SPRITES_DICT"
]:
# default background for entities is floor
castle[x, y] = TILES["floor"]["sprite_index"]

# if it's not the player
if tile_name != "player":
# loop over all entities at this location
for entity_obj_at_tile in GAME_STATE["ENTITY_SPRITES_DICT"][
x + CAMERA_OFFSET_X, y + CAMERA_OFFSET_Y
]:
# set appropriate x,y screen coordinates
# based on tile coordinates
ENTITY_SPRITES[
int(entity_obj_at_tile["entity_sprite_index"])
].x = (x * 16)
ENTITY_SPRITES[
int(entity_obj_at_tile["entity_sprite_index"])
].y = (y * 16)

# add the index of the entity sprite to the draw_entities
# list so we know not to hide it later.
drew_entities.append(
entity_obj_at_tile["entity_sprite_index"]
)

else: # no entities at this location
# set the sprite index of this tile into the CASTLE dictionary
castle[x, y] = TILES[tile_name]["sprite_index"]

else: # tile type not found in main dictionary
# default to floor tile
castle[x, y] = TILES["floor"]["sprite_index"]

# if the player is at this x,y tile coordinate accounting for camera offset
if GAME_STATE["PLAYER_LOC"] == ((x + CAMERA_OFFSET_X, y + CAMERA_OFFSET_Y)):
# set player sprite screen coordinates
GAME_STATE["PLAYER_SPRITE"].x = x * 16
GAME_STATE["PLAYER_SPRITE"].y = y * 16

# loop over all entity sprites
for index in range(0, len(ENTITY_SPRITES)):
# if the sprite wasn't drawn then it's outside the camera view
if index not in drew_entities:
# hide the sprite by moving it off screen
ENTITY_SPRITES[index].x = int(-16)
ENTITY_SPRITES[index].y = int(-16)

In this game, the camera will always stay mostly centered on the player, because we reference the player location in the x and y value parameters when set_camera_view() is called. The max and min functions are used to minimize the amount of "outside the map" area that we show.

Here is the code inside the main loop that calls set_camera_view() and draw_camera_view():

Download: file

Copy Code
# inside main game loop:
set_camera_view(
max(min(GAME_STATE['PLAYER_LOC'][0]-4,GAME_STATE['MAP_WIDTH']-SCREEN_WIDTH_TILES),0),
max(min(GAME_STATE['PLAYER_LOC'][1]-3,GAME_STATE['MAP_HEIGHT']-SCREEN_HEIGHT_TILES),0),
10,
8
)
# draw the camera
draw_camera_view()
מק"ט יצרן # 4242
PYGAMER FOR MAKECODE ARCADE, CIR
Adafruit Industries LLC
מק"ט יצרן # 4200
ADAFRUIT PYBADGE FEATHER
Adafruit Industries LLC
מק"ט יצרן # 3939
ADAFRUIT PYBADGE LC (LOW COST)
Adafruit Industries LLC
מק"ט יצרן # 4400
EDGEBADGE MCU TENSORFLOW LITE
Adafruit Industries LLC
מק"ט יצרן # 4277
PYGAMER STARTER KIT
Adafruit Industries LLC
מק"ט יצרן # 4238
CASE ACRYLIC BLK
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.