Maker.io main logo

DigiKey Custom 3D Printed Death Racer RC Combat Tanks

260

2023-07-25 | By Travis Foss

License: See Original Project 3D Print Accessories 3D Printing

When DigiKey decided to exhibit at the FIRST Robotics 2023 World Championship in Houston, ‎TX, we decided to showcase something that highlights the 3D printers, printer filaments, and ‎printer accessories we carry. After thinking of different ideas, we decided to print two of the so-‎called “Death Racers” that have taken the spotlight at recent RepRap 3D printing festivals. If ‎you aren’t familiar with what a Death Racer is, it is a 3D-printed tank with a plastic rider atop ‎and a boom that extends from the back of the machine. There is also a game format that ‎surrounds these machines where the drivers of them use the boom to knock the head off the ‎riders of the other competitors. There is a switch that turns off the motor ESCs (Electronic Speed ‎Controllers) and causes the robot to shut down when the head is knocked off. The premise is ‎similar to Rock ‘Em Sock ‘Em Robots. The competitions typically have 20 to 30 machines ‎competing at a time and are quite a sight to see.‎

 

Although we had not planned to attend any of the RepRap festivals, I thought this could be a ‎fun project to show off the capabilities of the Lulzbot Printers and various 3D printing Filaments ‎that we carry in addition to a number of the electronics that one can integrate into these ‎Machines.‎

To get the files to print the robot, I subscribed to Michael Babbeley’s Patreon. I was able to download all of the original ‎Death Racer STL’s and fusion files to build the original version of these machines. Around that ‎time, I came across Edge Of 3D’s YouTube channel, and he had just released his own modified ‎body for the Death Racers, which looks more similar to a Formula One car. I downloaded those ‎files and began the printing marathon that ensued. ‎

The treads were the first thing to print for the Death Racers. Each track requires 30 of the track ‎STLs. We used Polymaker’s Polyflex filament in Black and True Red for the tracks, as they ‎closely match DigiKey’s colors. A tip if you are printing TPU filament onto a PEI-coated print ‎bed - use some adhesive on the print bed. I found out the hard way that if not used, the TPU will ‎bond with the PEI film, and when removing the print, it will damage the bed. After putting a ‎hole in the flexible bed, I discovered that adhesive is needed to create a barrier between the bed ‎and the filament. The adhesive we used for the flexible filaments was Magigoo Flex formula ‎adhesive. It worked wonderfully for this application and, as the bed cools, the Magigoo allows ‎the part to release, making removal very easy. And afterward, only water is needed to remove the ‎excess adhesive from the bed.‎

fresh_1

Freshly printed TPU Treads

After printing the treads, the drive gears for the wheels were printed using Polymaker Polylite ‎PETG. It's recommended to print these with eight wall perimeters and eight top and bottom ‎layers. After printing the drive gears, the body and rider parts were printed with 3D fuel PLA in ‎Midnight Black and Fire Engine Red. One nice thing about building two opposite-colored Death ‎Racers is that we could print one of every part in red and one set in black. If you are not building ‎multiples, I recommend planning which pieces will be which color before starting printing. There ‎are quite a few parts to print, so it can get overwhelming to figure out which part to print in ‎which color. A nice feature included in the Patreon files is that the rider pieces are separated into ‎two color files, one for color A and one for color B, which helps immensely as several pieces ‎make up the rider.‎

drive2

Drive hubs

another_3

Another Drive Hub

more_4

More Drive hubs

While printing the parts, we made a few modifications to get the parts to fit or look correct. The ‎first were the heads of the riders. I gave one rider a Deadpool-style head since the color scheme ‎matched our design. The idea for the second rider came to me after speaking with some of my ‎Coworkers. My supervisor had used a 3D scan of his head for another project, so he seemed like ‎a perfect candidate for the rider of the second racer. While the Deadpool head required some ‎post-processing and painting, the head of the other rider was printed in a skin-tone PLA and is ‎one of the cleanest prints of the entire build. I didn’t have to do any post-processing on the ‎second print. The next modified part was the boom mount for the back servo on the Death Racer. ‎The original file called for an aluminum servo horn with a specific shape; however, while our ‎servo came with a similarly shaped horn, it was slightly larger than the one in the original design. ‎The downloaded files also include a Fusion 360 file of all the parts so they can be modified ‎easily. For instance, I used Fusion 360 to modify the boom mount to perfectly fit our servo's ‎horn.‎

deadpool_5

Unfinished Deadpool head

right_6

The right part is the original Servo horn piece. Left is a test print of the newly modified piece to ‎make sure it fits over the new servo horn.‎

After finishing printing all the parts, assembly began. I recommend keeping a deburring tool ‎handy for this step. Our prints had a slight elephant’s foot, but the deburring tool works great to ‎remove this. The deburring tool is also convenient for holes where the fit is just a little too tight. ‎With just a couple turns of the deburring tool, the parts fit together nicely!‎

The modded files from Edge of 3D are designed to use heat-set inserts. To install the inserts, it ‎works best to set the temp of the soldering iron slightly higher than the printing temp of the ‎filament. This makes inserting the heat set insert easy as it slides into the designed hole quickly ‎and gives a good bond between the filament and the insert. While installing the first handful of ‎inserts, I found that I had set the temperature to low. The inserts would melt into the model; ‎however, once light pressure was applied while tightening the screws, the inserts broke free. ‎Also, note that you should use blue thread lock on any metal-to-metal connection. I used it on ‎every metal-to-metal connection point except for one - the motor shaft adapter that holds the ‎drive gear to the motor! While driving the robots during the FIRST Robotics event, these screws ‎backed out, resulting in the loss of power to one track on each of the robots. I guess I can mark ‎that down as a lesson learned.‎

head_7

Heat Set inserts in the motor mount

During the assembly, two carbon fiber rods are added between the track frames and the body to ‎increase strength. When these were purchased, they were about 50mm too long, so they needed ‎to be cut down. To keep the rods from splintering, I wrapped both in blue painter’s tape at the ‎length I needed, which resulted in a clean cut. With the rods cut, they are sandwiched between ‎the drive frame and tracks within the designated grooves in the models.‎

tape_8

With most of the assembly complete, it came to the point I needed to hook up the electronics. I ‎decided to add a few extras to the racers, mainly to add lights on the front bumper. In the nose ‎of the car, a Seeed Xiao RP2040 board and two SparkFun RGB LEDs were installed. The LEDs ‎used are addressable, so the Xiao board was programmed in the Arduino IDE using the Adafruit ‎Neopixel library to create a few different flashing patterns. The Xiao board and LEDs are ‎soldered to a Solderful Breadboard hidden inside the cavity in the nose of the racer, and power ‎is controlled via a switch installed on the rider’s console.‎

After getting the LED’s up and running, the next thing to set up was the remote receiver and all ‎the connections to it set up. The below picture is how I connected the motors, servos, and the ‎power to the xiao board. Channel 1 of the ESC connects to the left track, and channel 2 is the ‎right track. Next is the servo that controls the boom, which connects to channel 4. Channels 5 ‎and 6 are the servos that control the left and right hands of the rider. Last, the power and ground ‎wires from the xiao board connect to the B/VCC port. I used Deans connectors for the ESC ‎power input wires, which is the same connector that's installed on the 2S lipo battery packs we ‎used. I also ran the connection through the switch connected to the head and back to the ESC, so ‎it powers down when switched off.‎

rc_9

RC Receiver wiring

After the electronics were together, there were a few settings on the controller to control the ‎robot in a tank-drive manner. In the menu on the controller, the Elevon setting must be switched ‎on, which mixes the right stick motion to control channels 1 and 2 into a tank drive style control. ‎The left stick’s side-to-side motion controls the bludger servo and doesn’t require any additional ‎changes. The last change that was needed was to mix the arm servos with the channels 1 and 2 ‎control to match the motion of the right stick so that the rider appears to be controlling the racer. ‎To accomplish this, navigate into the controller’s menu and select mixes. Set channel 5 to mix ‎with channel 1 on mix 1, and channel 6 to mix with channel 2 on mix 2. This causes the arms to ‎move forward when the drive stick on the remote is pressed forward and backward when it was ‎pulled back. Since the controller is limited to only 3 mixes, the last mix is to mix channel 5 with ‎channel 3 on mix 3, which causes the arm to move on turns.

 

With the electronics complete and installed, it was time for the final assembly and the first test ‎drive. The body was placed on top of the drivetrain and fastened with 10 M3 screws. However, ‎once I had the racers together, I noticed one of the tracks had some extra resistance when ‎driving. Upon investigation, it was discovered that the drive wheel was slightly contacting the ‎drive frame, but with a bit of sanding and trimming the rubbing was eliminated, and the racers ‎were fully operational.‎

racer_10

Partially assembled Racer

racer_11

Partially assembled Racer

robots_12

robots_13

The robots turned out great!!‎

robots_14

Finished Robots

 

While I haven’t had much drive time with these racers, this is an excellent project for anyone that ‎wants to improve their 3d printing skills. It will challenge you to get your 3d printer printing at its ‎best. If you are looking to improve your skills, I recommend looking into this one.‎

https://twitter.com/i/status/1648796061501124608

(embed tweet: <blockquote class="twitter-tweet"><p lang="en" dir="ltr">FIRST Championship 2023 is officially under way and we’re loving the enthusiasm 👏. <br><br>Good luck to all teams! <a href="https://twitter.com/FRCTeams?ref_src=twsrc%5Etfw">@FRCTeams</a> <a href="https://twitter.com/FIRSTweets?ref_src=twsrc%5Etfw">@FIRSTweets</a> <br><br>Be sure to come say hi at booth #1108 in the <a href="https://twitter.com/hashtag/Robotics?src=hash&amp;ref_src=twsrc%5Etfw">#Robotics</a> Center 👋 <a href="https://twitter.com/hashtag/FIRSTChamps?src=hash&amp;ref_src=twsrc%5Etfw">#FIRSTChamps</a><br><br>P.s. peep the <a href="https://twitter.com/hashtag/3dprinted?src=hash&amp;ref_src=twsrc%5Etfw">#3dprinted</a> RC car feat <a href="https://twitter.com/Kwalseth?ref_src=twsrc%5Etfw">@Kwalseth</a> 👀 <a href="https://t.co/UsQ2Ape8mP">pic.twitter.com/UsQ2Ape8mP</a></p>&mdash; DigiKey (@digikey) <a href="https://twitter.com/digikey/status/1648796061501124608?ref_src=twsrc%5Etfw">April 19, 2023</a></blockquote> <script async src="https://platform.twitter.com/widgets.js" charset="utf-8"></script>)

If you want to add headlights similar to what I did with these racers, here is the code I used for the Xiao microcontroller.  

Copy Code
‎#include <Adafruit_NeoPixel.h>‎
‎#ifdef __AVR__‎
‎ #include <avr/power.h> // Required for 16 MHz Adafruit Trinket‎
‎#endif‎

‎// Which pin on the Arduino is connected to the NeoPixels?‎
‎// On a Trinket or Gemma we suggest changing this to 1:‎
‎#define LED_PIN 7‎

‎// How many NeoPixels are attached to the Arduino?‎
‎#define LED_COUNT 2‎

‎#define Power 27‎

‎// Declare our NeoPixel strip object:‎
Adafruit_NeoPixel strip(LED_COUNT, LED_PIN, NEO_GRB + NEO_KHZ800);‎
‎// Argument 1 = Number of pixels in NeoPixel strip
‎// Argument 2 = Arduino pin number (most are valid)‎
‎// Argument 3 = Pixel type flags, add together as needed:‎
‎// NEO_KHZ800 800 KHz bitstream (most NeoPixel products w/WS2812 LEDs)‎
‎// NEO_KHZ400 400 KHz (classic 'v1' (not v2) FLORA pixels, WS2811 drivers)‎
‎// NEO_GRB Pixels are wired for GRB bitstream (most NeoPixel products)‎
‎// NEO_RGB Pixels are wired for RGB bitstream (v1 FLORA pixels, not v2)‎
‎// NEO_RGBW Pixels are wired for RGBW bitstream (NeoPixel RGBW products)‎

‎// setup() function -- runs once at startup --------------------------------‎

void setup() {‎
‎ // These lines are specifically to support the Adafruit Trinket 5V 16 MHz.‎
‎ // Any other board, you can remove this part (but no harm leaving it):‎
‎#if defined(__AVR_ATtiny85__) && (F_CPU == 16000000)‎
‎ clock_prescale_set(clock_div_1);‎
‎#endif‎
‎ // END of Trinket-specific code.‎

‎ pinMode(Power,OUTPUT);‎
‎ digitalWrite(Power, HIGH);‎

‎ strip.begin(); // INITIALIZE NeoPixel strip object (REQUIRED)‎
‎ strip.show(); // Turn OFF all pixels ASAP
‎ strip.setBrightness(200); // Set BRIGHTNESS to about 1/5 (max = 255)‎
‎}‎

‎// loop() function -- runs repeatedly as long as board is on ---------------‎

void loop() {‎
‎ // Fill along the length of the strip in various colors...‎
‎ colorWipe(strip.Color(255, 0, 0), 100); // Red
‎ colorWipe(strip.Color( 0, 255, 0), 100); // Green
‎ colorWipe(strip.Color( 0, 0, 255), 100); // Blue

‎ // Do a theater marquee effect in various colors...‎
‎ // theaterChase(strip.Color(127, 127, 127), 150); // White, half brightness‎
‎ theaterChase(strip.Color(127, 0, 0), 100); // Red, half brightness
‎ theaterChase(strip.Color( 0, 0, 127), 100); // Blue, half brightness

‎ rainbow(10); // Flowing rainbow cycle along the whole strip
‎ theaterChaseRainbow(50); // Rainbow-enhanced theaterChase variant
redFadeIn(5);‎
redFadeOut(2);‎
policeLights(25);‎
redFadeIn(10);‎
redFadeOut(10);‎
‎}‎

‎// Some functions of our own for creating animated effects -----------------‎

‎// Fill strip pixels one after another with a color. Strip is NOT cleared‎
‎// first; anything there will be covered pixel by pixel. Pass in color‎
‎// (as a single 'packed' 32-bit value, which you can get by calling
‎// strip.Color(red, green, blue) as shown in the loop() function above),‎
‎// and a delay time (in milliseconds) between pixels.‎
void colorWipe(uint32_t color, int wait) {‎
‎ for(int i=0; i<strip.numPixels(); i++) { // For each pixel in strip...‎
‎ strip.setPixelColor(i, color); // Set pixel's color (in RAM)‎
‎ strip.show(); // Update strip to match
‎ delay(wait); // Pause for a moment
‎ }‎
‎}‎

‎// Theater-marquee-style chasing lights. Pass in a color (32-bit value,‎
‎// a la strip.Color(r,g,b) as mentioned above), and a delay time (in ms)‎
‎// between frames.‎
void theaterChase(uint32_t color, int wait) {‎
‎ for(int a=0; a<10; a++) { // Repeat 10 times...‎
‎ for(int b=0; b<3; b++) { // 'b' counts from 0 to 2...‎
‎ strip.clear(); // Set all pixels in RAM to 0 (off)‎
‎ // 'c' counts up from 'b' to end of strip in steps of 3...‎
‎ for(int c=b; c<strip.numPixels(); c += 3) {‎
‎ strip.setPixelColor(c, color); // Set pixel 'c' to value 'color'‎
‎ }‎
‎ strip.show(); // Update strip with new contents
‎ delay(wait); // Pause for a moment
‎ }‎
‎ }‎
‎}‎

‎// Rainbow cycle along whole strip. Pass delay time (in ms) between frames.‎
void rainbow(int wait) {‎
‎ // Hue of first pixel runs 5 complete loops through the color wheel.‎
‎ // Color wheel has a range of 65536 but it's OK if we roll over, so‎
‎ // just count from 0 to 5*65536. Adding 256 to firstPixelHue each time‎
‎ // means we'll make 5*65536/256 = 1280 passes through this loop:‎
‎ for(long firstPixelHue = 0; firstPixelHue < 5*65536; firstPixelHue += 256) {‎
‎ // strip.rainbow() can take a single argument (first pixel hue) or‎
‎ // optionally a few extras: number of rainbow repetitions (default 1),‎
‎ // saturation and value (brightness) (both 0-255, similar to the‎
‎ // ColorHSV() function, default 255), and a true/false flag for whether‎
‎ // to apply gamma correction to provide 'truer' colors (default true).‎
‎ strip.rainbow(firstPixelHue);‎
‎ // Above line is equivalent to:‎
‎ // strip.rainbow(firstPixelHue, 1, 255, 255, true);‎
‎ strip.show(); // Update strip with new contents
‎ delay(wait); // Pause for a moment
‎ }‎
‎}‎

‎// Rainbow-enhanced theater marquee. Pass delay time (in ms) between frames.‎
void theaterChaseRainbow(int wait) {‎
‎ int firstPixelHue = 0; // First pixel starts at red (hue 0)‎
‎ for(int a=0; a<30; a++) { // Repeat 30 times...‎
‎ for(int b=0; b<3; b++) { // 'b' counts from 0 to 2...‎
‎ strip.clear(); // Set all pixels in RAM to 0 (off)‎
‎ // 'c' counts up from 'b' to end of strip in increments of 3...‎
‎ for(int c=b; c<strip.numPixels(); c += 3) {‎
‎ // hue of pixel 'c' is offset by an amount to make one full‎
‎ // revolution of the color wheel (range 65536) along the length
‎ // of the strip (strip.numPixels() steps):‎
‎ int hue = firstPixelHue + c * 65536L / strip.numPixels();‎
‎ uint32_t color = strip.gamma32(strip.ColorHSV(hue)); // hue -> RGB‎
‎ strip.setPixelColor(c, color); // Set pixel 'c' to value 'color'‎
‎ }‎
‎ strip.show(); // Update strip with new contents
‎ delay(wait); // Pause for a moment
‎ firstPixelHue += 65536 / 90; // One cycle of color wheel over 90 frames
‎ }‎
‎ }‎
‎}‎

void redFadeIn(int fadeInSpeed){‎

‎//for (int k=0; k<fadeInSpeed; k++){‎
‎ for (int j=0; j<256; j++){‎
‎ strip.fill(strip.Color(0,j,0));‎
‎ strip.show();‎
‎ delay(fadeInSpeed);‎
‎ }‎
‎//}‎
‎}‎

void redFadeOut(int fadeOutSpeed){‎

‎//for (int k=0; k<fadeOutSpeed; k++){‎
‎ for (int j=255; j>=0; j--){‎
‎ strip.fill(strip.Color(0,j,0));‎
‎ strip.show();‎
‎ delay(fadeOutSpeed);‎
‎ }‎
‎//}‎
‎}‎

void policeLights(int numFlashes){‎

‎ for (int j=0; j<numFlashes; j++){‎

‎ strip.fill(strip.Color(0,255,0));‎
‎ strip.show();‎
‎ delay(100);‎
‎ strip.fill(strip.Color(0,0,0));‎
‎ strip.show();‎
‎ delay(1);‎
‎ strip.fill(strip.Color(0,0,255));‎
‎ strip.show();‎
‎ delay(100);‎
‎ strip.fill(strip.Color(0,0,0));‎
‎ strip.show();‎
‎ delay(1);‎

‎ }‎
‎}‎
מק"ט יצרן # M30X170C
INSERT YELLOW 0.19"DIA X 0.17" H
Tri-Star Industries, Inc.
מק"ט יצרן # 1594MS100
MACH SCRW FLAT PHIL M3X0.5 100PK
Hammond Manufacturing
מק"ט יצרן # MPMS 003 0025 PH
MACH SCREW PAN PHILLIPS M3X0.5
BFirst Industrial
מק"ט יצרן # 30-00415
CABLE 2COND 18AWG BLK/RED 1M
Tensility International Corp
מק"ט יצרן # 5298
STANDARD SIZE ULTRA HIGH TORQUE
Adafruit Industries LLC
מק"ט יצרן # 8996
MAGNET 0.236"D X 0.118"THICK CYL
Radial Magnets, Inc.
מק"ט יצרן # 221-612
SPLICE LEVER 10AWG 2POS
WAGO Corporation
מק"ט יצרן # 11864
CONN PLUG/RCPT 2POS IN-LINE PAIR
SparkFun Electronics
מק"ט יצרן # 221-413
SPLICE LEVER 24-12AWG 3POS
WAGO Corporation
מק"ט יצרן # 12877
ADDRESS LED DISCR SERIAL RGB 5PC
SparkFun Electronics
מק"ט יצרן # 9-520183-2
CONN QC RCPT 18-22AWG 0.250
TE Connectivity AMP Connectors
מק"ט יצרן # SER0053
9G 300 CLUTCH SERVO
DFRobot
מק"ט יצרן # 4239
HEAT-SET INSERT FOR SOLDERING IR
Adafruit Industries LLC
מק"ט יצרן # 102010428
XIAO RP2040
Seeed Technology Co., Ltd
מק"ט יצרן # RM-PL0175
3D-FUEL, STANDARD PLA, MIDNIGHT
LulzBot
מק"ט יצרן # RM-PL0172
3D-FUEL, STANDARD PLA, FIRE ENGI
LulzBot
מק"ט יצרן # RM-TE0127
POLYMAKER POLYFLEX TPU95 FILAMEN
LulzBot
מק"ט יצרן # RM-TE0121
POLYMAKER POLYFLEX TPU95 FILAMEN
LulzBot
מק"ט יצרן # MF2019
MAGIGOO PRO FLEX - 50ML
Thought3D
מק"ט יצרן # RM-PE0031
POLYMAKER POLYLITE PETG FILAMENT
LulzBot
מק"ט יצרן # RM-PE0035
POLYMAKER POLYLITE PETG FILAMENT
LulzBot
מק"ט יצרן # KT-HB0021
SPARE TAZ SIDEKICK 747 MAGNETIC
LulzBot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.