Maker.io main logo

Digital Egg Drop Experiment with CLUE

378

2020-04-09 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by John Park

Overview

This classic physics experiment is a really fun one! You get to create a descent vehicle for an egg dropped from a great height that helps the egg land gently enough to avoid going SPLAT!

overview_1

Instead of testing design iterations on precious eggs, we can first prove out our vehicles using the CLUE board! It's packed with sensors and has a display and speaker for feedback -- we'll use those to study the impact g-force of our landing. Once we're satisfied with the data, we can swap out for the more fragile ovoid!

 

Here's an excellent video by Mark Rober explaining the physics behind the egg drop as well as showing five designs you can try out. Instead of testing on eggs each time, we will first determine the g forces sustained on impact with our CLUE board!

 

We really don't want you to break your CLUE board -- so be sure to test out your experiments in stages and ideally on softer surfaces before building up your confidence in your design to try it from full height over a harder surface!

experiment_2a

experiment_2

experiment_3

Parts

Materials & Tools

You'll want to try out some different materials and descent vehicle strategies.

  • Balloons
  • Cardboard
  • Plastic or paper drinking straws
  • Tape
  • Zip ties
  • Egg cartons
  • Rubber bands
  • Popcorn
  • Plastic or paper bags
  • Scissors
  • Hobby knife

One more bit of inspiration -- here's a MakeCode egg drop experiment setup running on the micro:bit:

 

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront desktop software downloads. Simply copy and edit files on the CIRCUITPY flash drive to iterate.

The following instructions will show you how to install CircuitPython. If you've already installed CircuitPython but are looking to update it or reinstall it, the same steps work for that as well!

Set up CircuitPython Quick Start!

Follow this quick step-by-step for super-fast Python power :)

Download the latest version of

CircuitPython for CLUE from circuitpython.org

Download_4

Click the link above to download the latest version of CircuitPython for the CLUE.

Download and save it to your desktop (or wherever is handy).

clue_5

Plug your CLUE into your computer using a known-good USB cable.

A lot of people end up using charge-only USB cables and it is very frustrating! So, make sure you have a USB cable you know is good for data sync.

Double-click the Reset button on the top (magenta arrow) on your board, and you will see the NeoPixel RGB LED (green arrow) turn green. If it turns red, check the USB cable, try another USB port, etc. Note: The little red LED next to the USB connector will pulse red. That's ok!

If double-clicking doesn't work the first time, try again. Sometimes it can take a few tries to get the rhythm right!

You will see a new disk drive appear called CLUEBOOT.

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.

diskdrive_6

diskdrive_7

The LED will flash. Then, the CLUEBOOT drive will disappear and a new disk drive called CIRCUITPY will appear.

If this is the first time you're installing CircuitPython or you're doing a completely fresh install after erasing the filesystem, you will have two files - boot_out.txt, and code.py, and one folder - lib on your CIRCUITPY drive.

If CircuitPython was already installed, the files present before reloading CircuitPython should still be present on your CIRCUITPY drive. Loading CircuitPython will not create new files if there was already a CircuitPython filesystem present.

That's it, you're done! :)

LED_8

CLUE CircuitPython Libraries

The CLUE is packed full of features like a display and a ton of sensors. Now that you have CircuitPython installed on your CLUE, you'll need to install a base set of CircuitPython libraries to use the features of the board with CircuitPython.

Follow these steps to get the necessary libraries installed.

Installing CircuitPython Libraries on your CLUE

If you do not already have a lib folder on your CIRCUITPY drive, create one now.

Then, download the CircuitPython library bundle that matches your version of CircuitPython from CircuitPython.org.

Download the latest library bundle from circuitpython.org

The bundle downloads as a .zip file. Extract the file. Open the resulting folder.

download_9

Open the lib folder found within.

lib_10

Once inside, you'll find a lengthy list of folders and .mpy files. To install a CircuitPython library, you drag the file or folder from the bundle lib folder to the lib folder on your CIRCUITPY drive.

drive_11

Copy the following folders and files from the bundle lib folder to the lib folder on your CIRCUITPY drive:

  • adafruit_apds9960
  • adafruit_bmp280.mpy
  • adafruit_bus_device
  • adafruit_clue.mpy
  • adafruit_display_shapes
  • adafruit_display_text
  • adafruit_lis3mdl.mpy
  • adafruit_lsm6ds.mpy
  • adafruit_register
  • adafruit_sht31d.mpy
  • adafruit_slideshow.mpy
  • neopixel.mpy

Your lib folder should look like the image on the left. These libraries will let you run the demos in the CLUE guide.

folderlib_13

Code the Egg Drop CLUE with CircuitPython

Libraries

We'll need to make sure we have these libraries installed. (Check out this link on installing libraries if needed.)

  • adafruit_bus_device
  • adafruit_display_text
  • adafruit_register
  • adafruit_lsm6ds

code_1

Text Editor

Adafruit recommends using the Mu editor for editing your CircuitPython code. You can get more info in this guide.

Alternatively, you can use any text editor that saves files.

Image Files and Code.py

This project uses a couple of .bmp image files -- you can get them by downloading the Project Zip link in the embed below. Unzip the downloaded zip archive and then drag the two image files to your CLUE board's CIRCIUTPY drive.

Copy the code shown below, paste it into Mu. Save the code from Mu to the CLUE's CIRCUITPY drive as code.py

Download: Project Zip or clue_egg_drop.py

Copy Code
import time
import math
import board
from digitalio import DigitalInOut, Direction, Pull
import pulseio
from adafruit_lsm6ds import LSM6DS33, AccelRange, AccelHPF, Rate
from adafruit_display_text import label
import displayio
import terminalio

button_a = DigitalInOut(board.BUTTON_A)
button_a.direction = Direction.INPUT
button_a.pull = Pull.UP

splash = displayio.Group(max_size=3)

# draw the bad egg!
begg_file = open("broken_egg.bmp", "rb")
begg_bmp = displayio.OnDiskBitmap(begg_file)
begg_sprite = displayio.TileGrid(begg_bmp,
pixel_shader=displayio.ColorConverter())
splash.append(begg_sprite)

# draw the good egg on top
gegg_file = open("good_egg.bmp", "rb")
gegg_bmp = displayio.OnDiskBitmap(gegg_file)
gegg_sprite = displayio.TileGrid(gegg_bmp,
pixel_shader=displayio.ColorConverter())
splash.append(gegg_sprite)

# Draw a label
text_group = displayio.Group(max_size=1, scale=2, x=10, y=220)
text = "Current & Max Acceleration"
text_area = label.Label(terminalio.FONT, text=text, color=0x0000FF)
text_group.append(text_area) # Subgroup for text scaling
splash.append(text_group)

# display everything so far
board.DISPLAY.show(splash)

# connect to the accelerometer
sensor = LSM6DS33(board.I2C())
# highest range for impacts!
sensor.accelerometer_range = AccelRange.RANGE_16G
# we'll read at about 1KHz
sensor.accelerometer_rate = Rate.RATE_1_66K_HZ
# Instead of raw accelerometer data, we'll read the *change* in acceleration (shock)
sensor.high_pass_filter = AccelHPF.SLOPE
sensor.high_pass_filter_enabled = True

# and make a lil buzzer
buzzer = pulseio.PWMOut(board.SPEAKER, variable_frequency=True)
buzzer.frequency = 1000

max_slope = 0
egg_ok = True
while True:
# This isn't the acceleration but the SLOPE (change!) in acceleration
x, y, z = sensor.acceleration
# take the vector length by squaring, adding, taking root
slope_g = math.sqrt(x*x + y*y + z*z) / 9.8 # take vector, convert to g
# we'll track the max delta g

if max_slope < slope_g:
max_slope = slope_g
print(slope_g)
text_area.text = "Max Slope %0.1fg" % (max_slope)
if max_slope >= 9 and egg_ok:
gegg_sprite.x = 300
time.sleep(0.1)
egg_ok = False
buzzer.duty_cycle = 2**15
time.sleep(2)
buzzer.duty_cycle = 0
continue


if button_a.value is False and egg_ok is False:
print("Reset")
time.sleep(0.1) # debounce
max_slope = 0
gegg_sprite.x = 0
egg_ok = True

How It Works

Library Import

First, the code imports libraries: time, math, board, digitalio (in this case for using the A button), pulseio for sounding the buzzer, the accelerometer adafruit_lsm6 library, and, so we can display text and graphics on screen, adafruit_display_text, displayio and terminalio.

Download: file

Copy Code
import time
import math
import board
from digitalio import DigitalInOut, Direction, Pull
import pulseio
from adafruit_lsm6ds import LSM6DS33, AccelRange, AccelHPF, Rate
from adafruit_display_text import label
import displayio
import terminalio

Button Setup

Next, we'll set up the button as an input with pull up resistor.

Download: file

Copy Code
button_a = DigitalInOut(board.BUTTON_A)
button_a.direction = Direction.INPUT
button_a.pull = Pull.UP

Display

To prepare the screen for bitmap display, we'll create a displayio.Group() called splash, and then create tiles for the two egg .bmp image files saved on the CLUE.

Download: file

Copy Code
splash = displayio.Group(max_size=3)

# draw the bad egg!
begg_file = open("broken_egg.bmp", "rb")
begg_bmp = displayio.OnDiskBitmap(begg_file)
begg_sprite = displayio.TileGrid(begg_bmp,
pixel_shader=displayio.ColorConverter())
splash.append(begg_sprite)

# draw the good egg on top
gegg_file = open("good_egg.bmp", "rb")
gegg_bmp = displayio.OnDiskBitmap(gegg_file)
gegg_sprite = displayio.TileGrid(gegg_bmp,
pixel_shader=displayio.ColorConverter())
splash.append(gegg_sprite)

Label

We'll also prepare the text display by creating a text group with the text "Current & Max Acceleration".

All of these elements will be drawn to the screen with the command board.DISPLAY.show(splash)

Download: file

Copy Code
# Draw a label
text_group = displayio.Group(max_size=1, scale=2, x=10, y=220)
text = "Current & Max Acceleration"
text_area = label.Label(terminalio.FONT, text=text, color=0x0000FF)
text_group.append(text_area) # Subgroup for text scaling
splash.append(text_group)

# display everything so far
board.DISPLAY.show(splash)

Accelerometer & Buzzer

The accelerometer object will be instantiated as sensor connected over the I2C bus to the LSM6DS33 package. The range is set to 16G so it can read large impacts (poor egg!) read at a rate of 1.66KHz.

To filter out noise, the accelerometer's high pass filter is enabled.

We'll also set up the buzzer using pulseio with a frequency of 1000Hz.

Download: file

Copy Code
# connect to the accelerometer
sensor = LSM6DS33(board.I2C())
# highest range for impacts!
sensor.accelerometer_range = AccelRange.RANGE_16G
# we'll read at about 1KHz
sensor.accelerometer_rate = Rate.RATE_1_66K_HZ
# Instead of raw accelerometer data, we'll read the *change* in acceleration (shock)
sensor.high_pass_filter = AccelHPF.SLOPE
sensor.high_pass_filter_enabled = True

# and make a lil buzzer
buzzer = pulseio.PWMOut(board.SPEAKER, variable_frequency=True)
buzzer.frequency = 1000

The max_slope variable is created with an initial value of 0 -- this is used to measure the slope change in acceleration.

The egg_ok variable is set to True and will be used to reset the board after a large impact beyond the maximum slope value of 9.

Download: file

Copy Code
max_slope = 0
egg_ok = True

Main Loop

In the main loop of the program the accelerometer is read, and a slope_g is determined by squaring, adding and taking the root of the accelerometer value.

When the egg drop CLUE is in freefall, we'll begin checking the max_slope value acceleration -- if it is greater than 9, the simulated egg has probably cracked!

In this case, we move the good egg sprite off screen by 300 pixels, revealing the bad egg image. The buzzer will also sound for two seconds.

Download: file

Copy Code
# This isn't the acceleration but the SLOPE (change!) in acceleration
x, y, z = sensor.acceleration
# take the vector length by squaring, adding, taking root
slope_g = math.sqrt(x*x + y*y + z*z) / 9.8 # take vector, convert to g
# we'll track the max delta g

if max_slope < slope_g:
max_slope = slope_g
print(slope_g)
text_area.text = "Max Slope %0.1fg" % (max_slope)
if max_slope >= 9 and egg_ok:
gegg_sprite.x = 300
time.sleep(0.1)
egg_ok = False
buzzer.duty_cycle = 2**15
time.sleep(2)
buzzer.duty_cycle = 0
continue

Button Reset

Now, we can check the button_a.value to see if it changes after the egg_ok variable has been set to False. Since the button is on a pull up resistor, it is normally True until pressed. When pressed, the button value will go to False and we can then reset the max_slope value, and return the good egg image, and reset the egg_ok to True!

Download: file

Copy Code
if button_a.value is False and egg_ok is False:
print("Reset")
time.sleep(0.1) # debounce
max_slope = 0
gegg_sprite.x = 0
egg_ok = True

At this point, we're ready for another try!

Next, we'll build a landing vehicle and take it for a spin (drop?)!

Build an Egg Landing Vehicle for Testing

setup_14

There are a nearly infinite number of different designs and approaches you can take to building an egg landing vehicle -- that's the whole point of this experiment after all!

Here's one approach that works very well -- a partial egg carton pod protected on all sides by impact absorbing balloons.

Power Pack

Place three AAA batteries into the battery holder and then screw the lid shut with the supplied screw.

Plug the JST cable into the CLUE.

Use double stick foam tape or poster putty to secure the CLUE to the battery holder.

Use the battery holder's integrated on/off switch to power the CLUE.

powerpack_16

powerpack_15

powerpack_17

powerpack_18

Balloon Lander

Blow up and knot the ends of six balloons to about 50% full size. We want there to be a nice amount of give so that the balloons deform on impact -- this will increase the amount of time it takes for the CLUE (and later the egg!) to stop moving, thus dissipating much of the kinetic energy.

Use zip ties or rubber bands to connect three of the balloons as shown. Repeat this step for the other balloons so you have two separate sets of three.

We want to be able to nestle our CLUE or egg in between the two sets of balloons.

Wrap rubber bands around the balloons so they are loosely hanging from the intersection points, then wrap them over the other set to join them with a flexible coupling.

Next, we'll build a pod for the CLUE that will be secured in this space between.

Balloon_20

Balloon_19

Balloon_21

Balloon_22

Balloon_23

Balloon_27

Carton Pod

To begin, cut off a four-egg end of a common egg carton.

An egg can sit perfectly in one of the egg holder spots, but the CLUE and battery pack will need to be strapped down with a rubber band to make sure they stay put.

To make it easier to view the impact data on the CLUE's screen, mark and cut a small window in the lid. This will also allow you to access the A button on the CLUE.

carton_28

carton_29

carton_30

carton_31

Place the carton pod into the flexible rubber-band coupled space between the two balloon sets as shown here. Use the rubber bands to make sure everything is secure.

secure_32

Drop Testing

I conducted a low-height drop to see how much impact force would be generated on the CLUE. (Note, this test was done before adding the carton pod.)

From this low height, with the balloons absorbing much of the impact, a 2.5 G force impact was recorded.

By comparison, with no balloons in place the impact from this height exceeds 10.5 Gs!

droptest_33

droptest_34

eggclue_35

eggclue_36

Full Test

For the full test, I moved to the second story balcony. This time, the balloon landing vehicle containing the CLUE would be dropped from a height of 16 feet onto concrete!

fulltest_35

fulltest_36

fulltest_37

Success!

Our CLUE survived the landing with an 8.0g impact!

Let's put our money where our mouths are and drop a real egg.

fulltest_37

New Cargo

Swap in an actual egg for the CLUE, then place the carton pod back into the balloon space.

Repeat the drop...

...it...

...impacts...

...and...

..survives!

newcargo_36

newcargo_37

newcargo_38

newcargo_39

What new vehicle types will you construct? Try using a cardboard box, such as a black Adafruit box, and some popcorn. Does that dampen the impact enough? Remember, we're shooting for less than a 9.0g impact.

Cardboard Lander

Here's another approach to landing the egg safely -- a cardboard box with shock absorbing rubber bands to secure the payload.

In this vehicle, when the box experiences the jerk force of hitting the ground, the egg/CLUE will slow down more gradually by converting the kinetic energy into heat as the rubber bands stretch. This can act as an effective shock absorber!

Materials

For this vehicle you'll need:

  • Medium sized cardboard box
  • Rubber bands
  • Bamboo skewer, or similar
  • Scissors or snips to cut the skewer

Build the Suspension Rig

Use the skewer or an awl, nail, or screwdriver to poke a hole at the center of the box walls -- the sides, front, and back will do.

Thread a rubber band (or series of them looped together) through the holes, front to back. Use a small cutoff section of the skewer to hold them in place as shown.

Repeat for the side-to-side connection.

rig_40

rig_41

rig_42

rig_43

comprig_44

Secure the Payload

Wrap the CLUE in the rubber band intersection as shown.

secure_45

secure_46

Testing

Now, test the new vehicle by dropping it -- you should get a very effective reduction in g-force.

 

rubberband_47

Note, a typical AAA battery pack may experience enough jerk force to momentarily jostle the spring-loaded batteries away from their contacts, thus causing a brown-out on the CLUE board. Here I'm using a LiPo battery to prevent this. You may be able to add tape to your battery pack to prevent this.

With safe, sub-9g results, it's time to graduate to a real egg! A couple more carefully applied rubber bands make for a good connection system.

realegg_48

 

מק"ט יצרן # 727
BATTERY HOLDER AAA 3 CELL LEADS
Adafruit Industries LLC
מק"ט יצרן # 44011
KNIFE PRECISION WITH #11 BLADE
Aven Tools
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.