Maker.io main logo

E-nose: MEMS AI Gas Detection with UNIHIKER K10

501

2025-04-24 | By DFRobot

License: Attribution Arduino ESP32

Introduction

This project showcases an AI-powered gas detection device based on the DFRobot UNIHIKER K10. The device utilizes four types of odor sensors (Odor, Smoke, VOC, and H2S) to collect real-time gas data from garlic and coffee beans. The data is then used to train an AI model on the Edge Impulse platform. After training, the model is deployed on the UNIHIKER K10, enabling intelligent differentiation between these two odors. With simple user interaction, the device can identify different odors, making it suitable for smart odor monitoring, environmental detection, and more applications.

The core functionality of the project is to control the display screen through the K10 hardware, providing real-time odor recognition results. A button triggers odor data collection and inference processing, streamlining the user experience.

Code Download Link: GitHub Repository

Operation Video: YouTube Link

image

System Components

Hardware Platform: The DFRobot UNIHIKER K10 is the main control platform, with Arduino IDE as the programming environment. The K10 features a built-in display screen and buttons, enabling it to display inference results and receive user input.

image

Gas Sensors: Four types of gas sensors — Odor, Smoke, VOC, and H2S — are responsible for capturing the odor data of garlic and coffee beans. By analyzing the changes in sensor data, the device can detect the unique characteristics of different odors.

image

Edge Impulse: The Edge Impulse platform is used to train the AI model using the collected odor data, creating a model for odor recognition.

Inference Engine: The inference engine, deployed on the UNIHIKER K10, is responsible for executing real-time AI inference, transforming the sensor input data into interpretable results.

Hardware List

DFR0992 DFRobot UNIHIKER K10

SEN0568 MEMS H2S

SEN0566 MEMS VOC

SEN0571 MEMS Odor

SEN0570 MEMS Smoke

DFR0553 DFRobot ADS1115 Bit ADC Module

Fan, connecting wires, and 3D-printed parts

Steps

1. Environment Setup

- Install Arduino IDE 1.8.19: Download Link

- Install the K10 board in Arduino IDE:

image

Tools -> Boards Manager

image

Search esp32 and install

image

done

image

- Install the DFRobot_ADS1115 library in Arduino IDE(Importing a .zip Library):https://docs.arduino.cc/software/ide-v1/tutorials/installing-libraries/

- Register for an account on the Edge Impulse platform: Edge Impulse Studio

- Install the Edge Impulse data-forwarder tool: Documentation Link

2. Hardware Connections

- Prepare the hardware components.

image

- Connecting gas Sensors: Connect the four gas sensors to the DFRobot ADS1115 using the VCC, GND, and ADC pins. The sensors should be connected to the analog input channels A0 to A3 on the ADS1115 (Connection order A0-A3: H2S, VOC, Odor, SMOKE). The K10 is connected to the ADS1115 module via the I2C interface.

- Assemble the Container: Place the object to be tested inside the container.

image

3. Data Collection and Labeling

- After powering on the device, the Arduino IDE code (data.ino) initializes the ADS1115 module. The DFRobot_ADS1115 library reads data from the sensors and converts it into voltage values.

- The code uses the drawLine() function to display real-time changes in sensor data on the K10 screen. This allows you to observe the trend of the data changes from the four sensors.

image

- Each time data is collected, the voltage readings from the sensors are stored in the sensorData array. To ensure real-time data updates, old data is overwritten when new data is stored, and a maximum of 8 data sets are retained. Every 100ms, the values from the four sensors are printed on the serial monitor.

- Open Windows PowerShell and run the Edge Impulse data-forwarder tool, enter:

$edge-impulse-data-forwarder --frequency 10

- Use the Edge Impulse platform's data acquisition tool to collect and label the serial data.

label:coffeebean、garlic

Sample length:800ms

Sensor: H2S, VOC, Odor, SMOKE

Training data is used to train your model, and testing data is used to test your model's accuracy after training. We recommend an approximate 80/20 train/test split ratio for your data for every class (or label) in your dataset, although especially large datasets may require less testing data.

image

4. Train model

- After collecting data for your project, you can now create your Impulse. A complete Impulse will consist of 3 main building blocks: input block, processing block, and a learning block. A project can contain multiple impulses, or Experiments, where each impulse contains either the same or a different combination of blocks. This allows you to view the accuracy and model prediction results for various learning and processing blocks using the same input training and testing datasets.

image

- The Flatten block performs statistical analysis of the signal. It is useful for slow-moving averages like temperature data, in combination with other blocks.

Flatten parameters

- Scale axes: Multiplies axes by this number

- Average: Calculates the average value for the window

- Minimum: Calculates the minimum value in the window

- Maximum: Calculates the maximum value in the window

- Root-mean square: Calculates the RMS value of the window

- Standard deviation: Calculates the standard deviation of the window

- Skewness: Calculates the skewness of the window

- Kurtosis: Calculates the kurtosis of the window

- Moving Average Number of Windows: Calculates the moving average by maintaining a rolling average of the last N windows. Note, that there is no zero padding; the block will accumulate averages up to N windows. (Ex. for the first window in a sample, the moving average will equal the average). The moving average resets for each sample during training and inference when run_classifier_init() is called. Note if you enable this, you probably don't want overlapping windows for training.

image

In most of our DSP blocks, you have the option to calculate feature importance. Edge Impulse Studio will then output a Feature Importance list that will help you determine which axes generated from your DSP block are most significant to analyze when you want to train a model.

image

After extracting meaningful features from the raw signal using signal processing, you can now train your model using a learning block.

image

Live classification lets you validate your model with data captured directly from any device or supported development board. This gives you a picture of how your model will perform with real-world data.

image

Impulses can be deployed as an Arduino library. This package includes all of your signal processing blocks, configuration, and learning blocks in a single package. You can include this package in your sketches to run the impulse locally. In this tutorial, you'll export an impulse and integrate the impulse in a sketch to classify sensor data.

image

5. Deployment

- Deploying the Trained TensorFlow Lite Model: The trained TensorFlow Lite model (using the enose2025_inferencing library) is deployed to the UNIHIKER K10 via the Arduino IDE development environment (Importing a .zip Library): Arduino IDE Library Installation Guide

- Upload the program (enose.ino). When the user presses the button, the system starts collecting sensor data and stores it in the features array. The run_classifier() function is called for inference, and the model predicts whether the current odor is garlic or coffee beans based on the input data.

- The corresponding odor icon (garlic or coffee beans) is displayed on the K10 screen based on the inference result's probability. Inference time and results are also printed via the serial monitor.

image

Instructions

- Step 1: Insert the odor probe into the sample jar containing garlic or coffee beans, and wait for the sensor readings to stabilize.

- Step 2: Press the A button on the K10. The screen will show “Loading” and begin collecting odor data.

- Step 3: After data collection is complete, the device will automatically perform inference and display the result (either garlic or coffee beans) on the screen.

- Step 4: After testing one object, use a fan to blow on the probe, remove residual odors, and prepare for the next round of testing.

- Note: When not in use, avoid leaving the probe in the jar for extended periods to prevent sensor contamination, which could affect subsequent tests.

Operation Video: YouTube Link

Code Analysis

The project's code is divided into several functional modules, mainly including the following parts:

1. Library Imports and Global Variables:

- DFRobot_ADS1115: Used for reading voltage values from the ADS1115 analog-to-digital converter, suitable for gas sensor data collection.

- unihiker_k10: Used for controlling the K10 display, providing drawing and display functions.

- enose2025_inferencing: Inference library for odor recognition.

2. Global Variables:

Includes settings for the screen direction, arrays for storing sensor data, and arrays for storing feature data.

3. Image Data and Feature Arrays:

- The image_data array stores images for the background, loading screen, and inference results to display the user interface.

- The features array stores the feature data collected from the sensors, which is used in the inference process.

4. Function Definitions:

- setup(): Initializes serial communication, the K10 display, sets the background image, and configures the button callback function.

- loop(): The main loop reads sensor data in real time and updates the display. Once the data reaches 8 sets, older data is removed, and only the latest 8 sets are kept.

- drawLine(): Draws real-time sensor data curves for easy observation of data trends.

- onButtonAPressed(): When the user presses the A button, the system begins collecting sensor data and calls the run_classifier() inference function. Based on the inference result, it displays the corresponding image.

5. Inference Result Handling:

Based on the inference result’s probability, the system determines whether the odor is garlic, or coffee beans and displays the corresponding image on the screen. It also prints inference time and any potential anomaly detection.

Conclusion

This AI-powered odor detection device, based on the K10 hardware, completes the full process from data collection to AI inference. By using four gas sensors to collect data on garlic and coffee beans, training the model on the Edge Impulse platform, and deploying the model on the K10 hardware, the system can perform odor recognition.

Reference

1.https://docs.edgeimpulse.com/docs

2.https://github.com/polamaxu/enose_K10

3.https://www.unihiker.com/wiki/K10

Related Tutorial:

  1. How to use TensorFlow Lite Micro on UNIHIKER K10 (ESP32 S3) with Arduino IDE

מק"ט יצרן # SEN0568
MEMS H2S GAS DETECTION SENSOR
DFRobot
מק"ט יצרן # SEN0566
MEMS VOC GAS DETECTION SENSOR
DFRobot
מק"ט יצרן # SEN0571
MEMS ODOR GAS DETECTION SENSOR
DFRobot
מק"ט יצרן # SEN0570
MEMS SMOKE DETECTION SENSOR
DFRobot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.