Maker.io main logo

ESP32 Analog Style VU Meter with GC9A01 Round Displays + Peak Meters

382

2025-03-18 | By Mirko Pavleski

License: General Public License Barrel Audio ESP32 Arduino

A typical VU meter measures audio signals and displays them with a visual indicator. The classic VU meter design uses a moving needle (actually a sensitive galvanometer) that points to a scale on a calibrated range.

df

The needle moves left or right depending on the strength of the audio signal. I recently acquired these small round TFT displays with a GC9A01 chip. Its basic purpose is to make smartwatches, but in fact its shape is ideally suited for making a retro-look VU meter. My attention was drawn to a project on thesolaruniverse blog, which describes in detail how to create meter gauges and dials on this display with Arduino Nano.

For the needs of this project, I made some modifications to the code but basically kept the beautiful retro design and colors. Now, instead of random values, the instrument shows the real values ​​of the voltage applied to the input pin of the microcontroller. For a more homogeneous movement of the needle, I now use a more powerful ESP32 microcontroller.

gh

Nowadays the price of ESP32 is very low, so for better separation of the channels, I decided to use a separate microcontroller for each channel. In this project, I also added a peak meter that signals the moment of exceeding the permitted level of the signal with an LED.

The device is very simple to make and consists of several components:

- ESP32 microcontroller - two pieces

- Two round displays with GC9A01 and 240x240 resolution

- envelope followers made with two small signal diodes and two capacitors

- and two LEDs with current limiting resistors

gyu

In particular, in this case, I use the simplest passive envelope follower consisting of a diode and a capacitor, because the whole device is mainly intended as a demo device for testing, and based on this idea, a precise, fully functional audio VU meter can be made later with certain software and hardware modifications.

And now let's see how this VU meter works in real conditions.

ml

Let me mention that a stereo potentiometer can be placed on the input in order to regulate the signal level, but for the sake of simplification I do it with the Windows mixer software.

And finally, a short conclusion: This small, simple, and interesting Arduino project can be made in a few hours, and has a beautiful retro look, so you can use it as an additional part of any audio device, or as a stand-alone unit. With minimal code modification, it can be used on many other devices (e.g. radio receivers) where signal strength measurement is required. The Vu meter is built in a suitable plastic box made of PVC material and lined with self-adhesive colored wallpaper.

Copy Code
// GCA901_Nano_voltage_meter
// 
// grid voltage variation monitor (230V - 250V AC)
// rolling averaged voltage (of 10 readings) is sent to display
// NOTE: here voltage generated with random function
//
// microcontroller: Arduino Nano
// display 240*240 circular SPI 3.3V TFT with GC9A01 controller
// 
// note: random function drives fluctuations of the parameter named 'volt'
// CG9A01    Arduino Nano
//  RST -------- NC
//  CST -------- 10
//  DC ---------  9
//  SDA -------- 11 - green wire
//  SCL -------- 13 - yellow wire
//  
// Floris Wouterlood
// September 1, 2023
// public domain

// made for a 240*240 pixel circular display
// all x-y-coordinates relative to center = x = 120 and y = 120
     
   #include "SPI.h"
   #include "Adafruit_GFX.h"
   #include "Adafruit_GC9A01A.h"

   #define TFT_DC 2
   #define TFT_CS 15
 
   Adafruit_GC9A01A tft (TFT_CS, TFT_DC);
 
   #define BLACK      0x0000                                                               // some extra colors
   #define BLUE       0x001F
   #define RED        0xF800
   #define GREEN      0x07E0
   #define CYAN       0x07FF
   #define MAGENTA    0xF81F
   #define YELLOW     0xFFE0
   #define WHITE      0xFFFF
   #define ORANGE     0xFBE0
   #define GREY       0x84B5
   #define BORDEAUX   0xA000
   #define AFRICA     0xAB21                // 0xce5f  //0xAB21                                                               // current dial color
    const int vlez = 34;
   #define DEG2RAD 0.0174532925 
   //int vlez;
   int sig = 0;
   int multiplier;
   int    frametime = 100; 
   int    x_pos;
   int    y_pos; 
   int    center_x = 120;                                                                  // center x of dial on 240*240 TFT display
   int    center_y = 120;                                                                  // center y of dial on 240*240 TFT display
   float  pivot_x, pivot_y,pivot_x_old, pivot_y_old;
   float  p1_x,p1_y,p2_x,p2_y,p3_x, p3_y, p4_x, p4_y, p5_x, p5_y; 
   float  p1_x_old,p1_y_old, p2_x_old, p2_y_old, p3_x_old, p3_y_old;
   float  p4_x_old, p4_y_old, p5_x_old, p5_y_old;
   float  angleOffset = 3.14;
   float  arc_x;
   float  arc_y;
   int    radius = 120;                                                                    // center y of circular scale                                                   
   float  angle_circle = 0;
   float  needleAngle = 0;
   int    iteration = 0;
   int    j;                                                            
   float  volt = 220;
   int    needle_multiplier = 1;
   float  needle_setter;             
 float currentNeedleValue = 230;  // Start with a base voltage or level
float needleSpeed = 10;         // Speed at which the needle returns to the left
   
                                                     // to start with
   
void setup() {

   //randomSeed (analogRead(0)); 
 pinMode(12, OUTPUT);
 
    
   pinMode(vlez, INPUT);
   tft.begin();    
   Serial.begin (9600); 
   Serial.println (""); 
   Serial.println (""); 
   tft.setRotation (0);  
   
   tft.fillScreen (BLACK);
   tft.drawCircle (center_x, center_y,120, BLACK);             
   pivot_x = center_x;
   pivot_y = center_y+50;

   p1_x_old = center_x; p1_y_old = center_y+50;
   p2_x_old = center_x; p2_y_old = center_y+50;
   p3_x_old = center_x; p3_y_old = center_y+50;
   p4_x_old = center_x; p4_y_old = center_y+50;
   p5_x_old = center_x; p5_y_old = center_y+30;
                                                                          
   create_dial ();
   needle_setter = volt;
   needleAngle = (((needle_setter)*DEG2RAD*1.8)-3.14);
   needle();  
   draw_pivot ();
}


void loop (){

  // Map the analog input (voltage) to the needle range
  float targetNeedleValue = map(analogRead(vlez), 0, 400, 230, 270);
  Serial.println(targetNeedleValue);
  sig = analogRead(vlez);
  if (sig > 280)  {digitalWrite(12, HIGH);} else {digitalWrite(12, LOW);}

  
  // If the target value is greater than the current needle position, move quickly
  if (targetNeedleValue > currentNeedleValue) {
    currentNeedleValue = targetNeedleValue;
  } 
  // If the target value is lower, move more slowly to simulate damping
  else if (targetNeedleValue < currentNeedleValue) {
    currentNeedleValue -= needleSpeed; // Decrease the value gradually
    if (currentNeedleValue < targetNeedleValue) {
      currentNeedleValue = targetNeedleValue;  // Ensure we don't overshoot
    }
  }

  // Update the needle position
  needle_setter = currentNeedleValue;
  needle();
  draw_pivot(); 

  delay(frametime);  // Control the update rate
} 


void needle (){                                                                            // dynamic needle management

   tft.drawLine (pivot_x, pivot_y, p1_x_old, p1_y_old, AFRICA);                            // remove old needle  
   tft.fillTriangle (p1_x_old, p1_y_old, p2_x_old, p2_y_old, p3_x_old, p3_y_old, AFRICA);  // remove old arrow head
   tft.fillTriangle (pivot_x, pivot_y, p4_x_old, p4_y_old, p5_x_old, p5_y_old, AFRICA);    // remove old arrow head
    
   needleAngle = (((needle_setter)*0.01745331*1.8)-3.14);
   p1_x = (pivot_x + ((radius)*cos(needleAngle)));                                         // needle tip
   p1_y = (pivot_y + ((radius)*sin(needleAngle))); 

   p2_x = (pivot_x + ((radius-15)*cos(needleAngle-0.05)));                                 // needle triange left
   p2_y = (pivot_y + ((radius-15)*sin(needleAngle-0.05))); 

   p3_x = (pivot_x + ((radius-15)*cos(needleAngle+0.05)));                                 // needle triange right
   p3_y = (pivot_y + ((radius-15)*sin(needleAngle+0.05))); 

   p4_x = (pivot_x + ((radius-90)*cos(angleOffset+(needleAngle-0.2))));                    // needle triange left
   p4_y = (pivot_y + ((radius-90)*sin(angleOffset+(needleAngle-0.2)))); 

   p5_x = (pivot_x + ((radius-90)*cos(angleOffset+(needleAngle+0.2))));                    // needle triange right
   p5_y = (pivot_y + ((radius-90)*sin(angleOffset+(needleAngle+0.2)))); 
  
   p1_x_old = p1_x; p1_y_old = p1_y;                                                       // remember previous needle position
   p2_x_old = p2_x; p2_y_old = p2_y;                                                                         
   p3_x_old = p3_x; p3_y_old = p3_y;                                                                      

   p4_x_old = p4_x; p4_y_old = p4_y;                                                       // remember previous needle counterweight position
   p5_x_old = p5_x; p5_y_old = p5_y;                                                                      

   tft.drawLine (pivot_x, pivot_y, p1_x, p1_y, BLACK);                                     // create needle 
   tft.fillTriangle (p1_x, p1_y, p2_x, p2_y, p3_x, p3_y, BLACK);                           // create needle tip pointer
  // tft.drawLine (center_x-80, center_y+70, center_x+80,center_y+70, BLACK);                // repair floor 
   tft.fillTriangle (pivot_x, pivot_y, p4_x, p4_y, p5_x, p5_y, BLACK);                     // create needle counterweight
}


void create_dial (){

   tft.fillCircle (center_x, center_y,120, AFRICA);                                        // general dial field
   tft.drawCircle (center_x, center_y,118,GREY);  
   tft.drawCircle (center_x, center_y,117,BLACK);
   tft.drawCircle (center_x, center_y,116,BLACK);  
   tft.drawCircle (center_x, center_y,115,GREY);

   for (j= 30; j<60    ; j+=5)
       {
        needleAngle = ((j*DEG2RAD*1.8)-3.14);
        arc_x = (pivot_x + ((radius+15)*cos(needleAngle)));                                // needle tip
        arc_y = (pivot_y + ((radius+15)*sin(needleAngle))); 
        tft.drawPixel  (arc_x,arc_y, BLACK);
        tft.fillCircle (arc_x,arc_y,2, BLACK);
        }

   for (j= 60; j<75    ; j+=5)
       {
        needleAngle = ((j*DEG2RAD*1.8)-3.14);
        arc_x = (pivot_x + ((radius+15)*cos(needleAngle)));                                // needle tip
        arc_y = (pivot_y + ((radius+15)*sin(needleAngle))); 
        tft.drawPixel  (arc_x,arc_y, RED);
        tft.fillCircle (arc_x,arc_y,2, RED);
        }        

   tft.setTextColor (BLACK,AFRICA);    
   tft.setTextSize (4);
   tft.setCursor (center_x+40, center_y+40);
   tft.print ("VU");  
      tft.setTextSize (4);
   tft.setCursor (center_x-60, center_y+40);
  tft.print ("R");   
                                                                                                                                                                           
  // tft.drawLine (center_x-80, center_y+70, center_x+80,center_y+70, WHITE);                // create floor   
}


void draw_pivot (){
 
   tft.fillCircle (pivot_x, pivot_y,8,RED);               
   tft.drawCircle (pivot_x, pivot_y,8,BLACK);            
   tft.drawCircle (pivot_x, pivot_y,3,BLACK);      
}
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.