Maker.io main logo

ESP32 Thing Plus (USB-C) Hookup Guide

1,848

2023-04-11 | By SparkFun Electronics

License: See Original Project Wifi Wireless

Courtesy of SparkFun

Guide by SANTAIMPERSONATOR, BRUDNERD

Introduction

Note: This guide is specific to the ESP32 Thing Plus (USB-C) board variant. For the variants with ‎the USB micro-B connector, please refer to the ESP32 Thing Plus hookup guide.‎

The SparkFun ESP32-WROOM Thing Plus (USB-C) enjoys all the features of our previous ESP32 ‎Thing Plus (Micro-B) boards, but with a few improvements. For this variant, we have included a SD ‎card slot, upgraded to a USB-C connector, integrated a RGB status LED and battery fuel gauge, ‎and provided two voltage regulators: offering separate 700mA current sources for the board and ‎Qwiic connector. The board still retains its standardized 28-pin Feather footprint, 2-pin JST battery ‎connector, and Qwiic connector like our other Thing Plus boards.‎

SparkFun Thing Plus - ESP32 WROOM (USB-C)‎

 

The ESP32-WROOM module on the board provides a rich set of peripherals, ranging from ‎capacitive touch sensors, SD card interface, Ethernet, high-speed SPI, UART, I2S, and I2C. ‎With Espressif's ESP32 comprehensive development platform and Bluetooth low-energy support ‎‎(i.e. BLE, BT4.0, Bluetooth Smart) these boards are jam packed with possibilities!‎

Note: The CH340C serial-to-UART bridge is used on this board. Therefore, a different driver ‎installation is required from previous versions of the ESP32 Thing Plus.‎

Not Yet Implemented: The Arduino core for the ESP32 microcontroller is still a work in progress. ‎There are a handful of peripherals and features that have yet to be implemented, including:‎

The peripherals are available (if, also, still in their infancy) in the IoT Development Framework for ‎the ESP32. If your application requires any of the features above, consider giving the ESP-IDF a ‎try! (Updated: June 2022.)‎

Required Materials

To get started, users will need a few items. Now some users may have a few of these items, feel ‎free to modify your cart accordingly.‎

  • SparkFun Thing Plus - ESP32 WROOM (USB-C)‎

  • USB 3.1 Cable A to C - 3 Foot - The USB interface serves two purposes: it powers the board ‎and allows users to upload programs. (*If your computer doesn't have a USB-A slot, then ‎choose an appropriate cable or adapter.)

  • Computer with an operating system (OS) that is compatible with all the software installation ‎requirements

HEADERS ‎

Headers & Accessories

Headers are great for development purposes, letting users swap parts with just a set of jumper ‎wires. If you would like to add headers to your board, check out some of the options for the Thing ‎Plus or Feather form factor boards below. For a full selection of our ‎available Headers or Soldering Tools, click on the associated links.‎

New to soldering? Check out our Through-Hole Soldering Tutorial for a quick introduction!‎

solder_1

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.‎

 

BATTERIES

Li-Po Battery

For mobile applications, users will want to pick up a single-cell LiPo battery from our catalog. Below, ‎are a few available options:‎

JUMPER MODIFICATION

Jumper Modification

To modify the jumpers, users will need soldering equipment and/or a knife.‎

New to jumper pads? Check out our Jumper Pads and PCB Traces Tutorial for a quick ‎introduction!‎

jumperpads_2

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a ‎solder jumper between pads to reroute connections, and repair a trace with the green wire method ‎if a trace is damaged.‎

Suggested Reading

As a more professionally oriented product, we will skip over the more fundamental tutorials ‎‎(i.e. Ohm's Law and What is Electricity?). However, below are a few tutorials that may help users ‎familiarize themselves with various aspects of the board.

  • How to Solder: Through-Hole Soldering: This tutorial covers everything you need to ‎know about through-hole soldering.‎

  • Serial Communication: Asynchronous serial communication concepts: packets, signal levels, ‎baud rates, UARTs and more!‎

  • Serial Peripheral Interface (SPI): SPI is commonly used to connect microcontrollers to ‎peripherals such as sensors, shift registers, and SD cards.‎

  • Pulse Width Modulation: An introduction to the concept of Pulse Width Modulation.‎

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software on ‎Windows, Mac, and Linux.‎

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.‎

  • Analog vs. Digital: This tutorial covers the concept of analog and digital signals, as they relate ‎to electronics.‎

  • How to Work with Jumper Pads and PCB Traces: Handling PCB jumper pads and ‎traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to ‎reroute connections, and repair a trace with the green wire method if a trace is damaged.‎

  • ESP32 Thing Plus Hookup Guide: Hookup guide for the ESP32 Thing Plus (Micro-B) using ‎the ESP32 WROOM's Wi-Fi/Bluetooth system-on-chip in Arduino.‎

  • How to Install CH340 Drivers: How to install CH340 drivers (if you need them) on Windows, ‎Mac OS X, and Linux.‎

  • Installing Board Definitions in the Arduino IDE: How do I install a custom Arduino ‎board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the ‎Arduino Board Manager. We will also go over manually installing third-party cores, such as the ‎board definitions required for many of the SparkFun development boards.‎

qwiic_3

One of the new, advanced features of the board is that it takes advantage of the Qwiic connect ‎system. We recommend familiarizing yourself with the Logic Levels and I2C tutorials. Click on the ‎banner above to learn more about Qwiic products.‎

 

 

Hardware Overview

Note: All mentions of GPIO in this section will refer to the I/O pins of the ESP32-WROOM module ‎as represented in the datasheets and pin numbers of the board definition in the ESP32 Arduino ‎core. They do not correspond with the net names for the Thing Plus Form Factor device in ‎the schematic. (The device in the schematic is primarily, used internally to facilitate the board ‎design process; just ignore the naming of the GPIO0 - GPIO6 nets.)‎

thing_plus_4

Board Dimensions

The board dimensions are illustrated in the drawing below. The listed measurements are in inches ‎and the two mounting holes are compatible with 4-40 standoff screws.‎

dimensions_5

Board dimensions (PDF) for the ESP32-WROOM Thing Plus, in inches.‎

USB-C Connector

The USB connector is provided to power and program the board. For most users, it will be the ‎primary programing interface for the ESP32.‎

connector_6

USB-C connector on the ESP32-WROOM Thing Plus.‎

CH340 Serial-to-UART

The CH340 allows the ESP32-WROOM to communicate with a computer/host device through the ‎board's USB-C connection. This allows the board to show up as a device on the serial (or COM) ‎port of the computer. Users will need to install the latest drivers for the computer to recognize the ‎board (see Software Overview section).‎

Power

The ESP32-WROOM Thing Plus only requires 3.3V to power the board. However, the simplest ‎method to power the board is through the USB-C connector. Alternatively, the 3V3, VBAT, ‎and VUSB pins can also be used to supply power to the board.‎

  • VUSB:‎

    • The maximum voltage for the LDOs and charge controller is 6V

    • The minimum voltage for the charge controller is 3.75V

  • VBAT:

    • Should not be connected to anything other than a single-cell LiPo battery‎

  • 3V3:‎

    • Requires a regulated 3.3V

    • Only powers the board and not the Qwiic connector‎

power_7

ESP32-WROOM Thing Plus power connections.

Below, is a general summary of the power circuitry on the board:‎

  • ‎3V3 - Provides a regulated 3.3V from the USB (5V) power and/or battery connections‎

    • Used to power the ESP32-WROOM module, µSD card slot, WS2812 RGB LED, ‎CH340C Serial-to-UART bridge, and power LED

      • The Qwiic connector is powered by its own voltage regulator, from the same ‎power source(s)

    • ‎The 3.3V XC6222 LDO regulator can source up to 700mA

      • ‎Output is controlled by the EN pin on the board

  • VUSB - The voltage from the USB-C connector, usually 5V

    • ‎Power source for the entire board

      • ‎Powers the 3.3V voltage regulators and the battery charging circuit for VBAT

    • Overides power from the battery through a P-channel MOSFET, when both are ‎connected

    • Utilizes a BAT20J protection diode for the USB-C connection.‎

  • VBAT - The voltage from the JST battery connector; meant for single cell LiPo batteries

    • Provides power to the 3.3V voltage regulators and MAX17048 battery fuel gauge

    • The MCP73831 linear charge management controller is powered from the USB (5V) ‎power supply

      • ‎The charge controller is configured for 500mA (max) rate of charge to a ‎connected battery

  • GND - The common ground or the 0V reference for the voltage supplies‎

  • Qwiic Connector - Provides a regulated 3.3V voltage from the USB (5V) power and/or ‎battery connections

    • ‎Operates independently from the 3V3 pin, with its own voltage regulator

    • The 3.3V XC6222 LDO regulator can source up to 700mA

      • ‎Output is controlled by GPIO 0 of the ESP32-WROOM‎

For more details, users can reference the schematic and the datasheets of the individual ‎components in the power circuitry.

Power Status LED

The red, PWR LED will light up once 3.3V is supplied to the board; however, for most users, it will ‎light up when 5V is supplied through the USB connection or when a LiPo battery is connected to ‎the JST connector.‎

indicator_8

ESP32-WROOM Thing Plus PWR status LED indicator.

Charging Circuit

The charging circuit utilizes the MCP73831 linear charge management controller and is powered ‎directly from the USB-C connector or VUSB. The controller is configured for a 500mA charge rate ‎and active charging is indicated by the yellow, CHG LED. If the charge controller is shutdown or ‎charging is complete, the CHG LED will turn off. For more information, please refer to ‎the MCP73831 datasheet and the Indicator LEDs section below.‎

Power Control

The power source for the XC6222 LDO voltage regulators is controlled by a P-channel MOSFET. ‎In addition, the 3.3V regulated output from the XC6222 LDOs are enabled by the control pin (CE).‎

circuits_9

Circuits for the 3.3V power on the ESP32-WROOM Thing Plus.‎

The P-channel MOSFET operates based on the voltages at the MOSFET's gate and source pins. ‎Depending on the power supplies connected to the board, the MOSFET will switch between the ‎battery and USB-C connection as power sources for the XC6222 voltage regulators.‎

table_10

The control pin (CE) of the XC6222 LDOs also provides an additional amount of control for the ‎board's power. By default, the regulated 3.3V output is enabled. To disable and shutdown the ‎output voltage from the XC6222, the control pin needs to be pulled low (i.e., shorted to ground ‎‎(GND)). For more information, please refer to the XC6222 datasheet.‎

  • The 3.3V power for the board (3V3) is controlled by the EN pin, which is broken out on the ‎board

  • The 3.3V power for the Qwiic connector is controlled by GPIO 0 of the ESP32-WROOM

pins_11

XC6222 control pins on the ESP32-WROOM Thing Plus.‎

Note: The BOOT button is also connected to GPIO 0. Therefore, pressing the BOOT button will ‎momentarily disable power to the Qwiic connector.‎

Current Consumption

According to the specifications, the ESP32-WROOM draws about 240 mA during RF transmissions. ‎With the Wi-Fi example in this tutorial, have measured it to average around 140 mA and peak at 300 ‎mA while actively transceiving. The table below, summarizes the approximate current draw of ‎the ESP32-WROOM Thing Plus (USB-C) for various operational conditions. The measurements in ‎the table below, were made with the Nordic Power Profiler Kit II.‎

table_12

It is possible for users to reach sub-mA power consumption levels with the deep sleep power ‎modes. Using the TimerWakeUp Deep Sleep example code, the LED jumpers cut, and powering the ‎board through the LiPo battery connection we measured a power consumption of 845 µA (990 µA ‎peak) @ 3.7V while the MCU was inactive.‎

measurement_13

The current measurement from VBAT at 3.7V during deep sleep.‎

ESP32-WROOM

This variant of the ESP32 Thing Plus is designed around the ESP32-WROOM module with 16MB ‎of flash memory. Espressif's ESP32-WROOM module is a versatile, WiFi BT BLE MCU module ‎that targets a wide variety of applications. At the core of this module is the ESP32-D0WDQ6 system ‎on a chip (SoC) which is designed to be both scalable and adaptive. Its laundry list of features ‎include:‎

  • Xtensa® Dual-Core 32-bit LX6 Microprocessor (up to 240MHz)‎

    • ‎448KB ROM and 520KB SRAM‎

    • ‎16MB of Embedded SPI Flash Storage

  • Cryptographic Hardware Accelerators

    • AES, SHA2, ECC, RSA-4096

  • ‎Integrated 802.11 b/g/n WiFi 2.4GHz Transceiver (up to 150Mbps)

  • Integrated dual-mode Bluetooth (Bluetooth v4.2 and BLE)

  • ‎26 GPIO (including strapping pins)‎

    • ‎8x Capacitive Touch Electrodes

  • Operating Voltage: 3.0 to 3.6V

    • Wi-Fi: 380mA (peak)

    • Light-Sleep: 800µA

    • Deep-Sleep: 10 - 150µA‎

Note: Users should be aware of the following nuances and details of this board

  • The ESP32-WROOM is only compatible with 2.4GHz WiFi networks; it will not work on the 5GHz ‎bands

  • For details on the boot mode configuration, please refer to section 3.3 Strapping Pins of the ‎ESP32-WROOM module datasheet

module_14

ESP32-WROOM module on the ESP32 Thing Plus (USB-C).

Note: The ESP32-WROOM module has various power modes:‎

  • Active - The chip radio is powered on. The chip can receive, transmit, or listen

  • Modem Sleep - The CPU is operational, and the clock is configurable. The Wi-Fi/Bluetooth ‎baseband and radio are disabled

  • Light Sleep - The CPU is paused. The RTC memory and RTC peripherals, as well as the ULP ‎coprocessor are running

  • Deep Sleep - Only the RTC memory and RTC peripherals are powered on. The ULP ‎coprocessor is functional

  • Hibernation - Only one RTC timer on the slow clock and certain RTC GPIOs are active

  • Off - Chip is powered off

For more information on the power management of the ESP32-WROOM module, please refer ‎to Section 3.7 and Tables: 8 and 17 of the ESP32 SoC Datasheet.‎

Debugging

For users interested in debugging their code, the JTAG pins are broken out on the board. However, ‎the debugging feature is only available through the ESP-IDF.‎

  • TMS: GPIO 14

  • TDI: GPIO 12

  • TCK: GPIO 13

  • TDO: GPIO 15‎

Note: Users should be aware that GPIO 13 is connected to the STAT LED with a pull-down resistor.‎

Firmware Download Mode

Users can manually force the board into the serial bootloader with the BOOT button. Please, refer to ‎the Boot Button section below for more information.‎

Peripherals and I/O

Note: Users should be aware of the following nuances of this board.‎

The ESP32-WROOM module has 26 multifunctional GPIO, of which, 21 I/O pins broken out into a ‎feather form factor layout on this board. All of the ESP32-WROOM Thing Plus (USB-C) pins have ‎a .1" pitch spacing for headers. With the pin multiplexing capabilities of the ESP32 SoC, various ‎pins can have several functionalities. For more technical specifications on the I/O pins, please refer ‎to the ESP32 SoC datasheet.‎

  • ‎13x 12-bit analog to digital converter (ADC) channels

  • ‎3x UARTs (only two are configured by default in the Arduino IDE, one UART is used for ‎bootloading/debug)

  • ‎3x SPI (only one is configured by default in the Arduino IDE)‎

  • ‎2x I2C (only one is configured by default in the Arduino IDE)‎

  • ‎2x I2S Audio

  • ‎2x digital-to-analog converter (DAC) channels

  • ‎16x 20-bit PWM outputs

  • ‎8x Capacitive Touch Inputs‎

graphical_15

Graphical datasheet for the ESP32-WROOM Thing Plus (USB-C).

Note: Users should be aware of the following limitations for the board in the Arduino IDE.‎

  • Not all of the features, listed above, are available in the Arduino IDE. For the full capabilities of ‎the ESP32, the Espressif IDF should be utilized

  • Only one I2C bus is defined

  • Only two UART interfaces are available

    • UART (USB): Serial

    • RX/TX Pins: Serial1‎

  • Only one SPI bus is defined.‎

For digital pins, users will need to declare the pinMode() (link) in the setup of ‎their sketch (programs written in the Arduino IDE) for the pins used.‎

Input

When configured properly, an input pin will be looking for a HIGH or LOW state. Input pins ‎are High Impedance and takes very little current to move the input pin from one state to another.‎

Output

When configured as an output the pin will be at a HIGH or LOW voltage. Output pins are Low ‎Impedance: This means that they can provide a relatively substantial amount of current to other ‎circuits.‎

Note: There are electrical limitations to the amount of current that the ESP32-WROOM module can ‎sink or source. For more details, check out the ESP32-WROOM module datasheet.‎

Additional Functions

There are several pins that have special functionality in addition to general digital I/O. These pins ‎and their additional functions are listed in the tabs below. For more technical specifications on ‎the I/O pins, you can refer to the schematic, ESP32-WROOM module datasheet, ESP32 SoC ‎datasheet, and documentation for the ESP32 Arduino core.‎

ANALOG INPUT

Analog Input Pins

The ESP32-WROOM module provides a 12-bit ADC input on thirteen of its I/O pins. This ‎functionality is accessed in the Arduino IDE using the analogRead(pin) function. (*The available ‎ADC pins are highlighted in the image below.)‎

input_16

Analog input pins on the ESP32-WROOM Thing Plus.‎

Note: By default, in the Arduino IDE, analogRead() returns a 10-bit value. To change the resolution ‎of the value returned by the analogRead() function, use the analogReadResolution(bits) function.

Note: To learn more about analog vs. digital signals, check out this great tutorial.‎

wave_17

Analog vs. Digital

This tutorial covers the concept of analog and digital signals, as they relate to electronics.

PWM/ANALOG OUTPUT

Pulse Width Modulation (PWM) and Analog (DAC) Output Pins

The ESP32-WROOM module supports up to sixteen channels of 20-bit PWM outputs on any of its ‎I/O pins. This is accessed in the Arduino IDE using the analogWrite(pin, value) function or ‎the LED Control API. (*Any I/O pin can be used for the PWM outputs; the available DAC pins, with ‎true analog outputs, are highlighted in the image below.)‎ ‎

output_18

Any I/O pin can be used for a PWM output, but these are the DAC pins on the ESP32-WROOM ‎Thing Plus.

Note: By default, in the Arduino IDE, analogWrite() accepts an 8-bit value. To change the ‎resolution of the PWM signal for the analogWrite() function, use ‎the analogWriteResolution(bits) function.‎

(*The PWM output is not a true analog signal. For a true analog output, please refer to the DAC ‎API for GPIO 25 and GPIO 26.)‎

Note: To learn more about pulse width modulation (PWM), check out this great tutorial.‎

pulse_19

Pulse Width Modulation

An introduction to the concept of Pulse Width Modulation.‎

SERIAL COMM.

Serial Communication Pins

The ESP32-WROOM module provides three UART ports. By default, the UART port for the USB ‎connection (Serial) and the labeled UART I/O pins on the board (Serial1) can be accessed ‎through the Arduino IDE using the serial communication class.‎ ‎

ports_20

Default UART ports on the ESP32-WROOM Thing Plus.‎

Note: By default, in the Arduino IDE, the SparkFun ESP32 Thing Plus C board definition ‎supports:‎

  • Serial - UART (USB)‎

  • Serial1 - Pins: RX/TX (GPIO 16/GPIO 17)‎

In order to utilize the serial communication on the strapping pins, users will need to create a custom ‎serial port object and declare which pins to access.‎

Note: To learn more about serial communication, check out this great tutorial.‎

serial_21

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!‎

Note: We have noticed that with the ESP32 Arduino core, Serial.available() does not operate ‎instantaneously. This is due to an interrupt triggered by the UART, to empty the FIFO when ‎the RX pin is inactive for two-byte periods:

  • At 9600 baud, hwAvailable takes [number of bytes received + 2] x 1 ms = 11 ms before ‎the UART indicates that data was received from: \r\nERROR\r\n

  • At 115200 baud, hwAvailable takes [number of bytes received + 2] x .087 ms = ~1 ‎ms before the UART indicates that data was received from: \r\nERROR\r\n.‎

For more information, please refer to this chatroom discussion.‎

SPI

SPI Communication

The ESP32-WROOM module provides three SPI buses. By default, in the Arduino IDE, the SPI ‎class is configured to utilize pins GPIO 18 (SCK), GPIO 19 (POCI), GPIO 23 (PICO). These pins ‎share the same SPI bus as the µSD card slot, which utilizes pin 5 (SS) for its chip select. In order ‎to utilize the other SPI ports or objects, users will need to create a custom SPI object and declare ‎which pins to access.‎

Note: To comply with the latest OSHW design practices, we have adopted the new SPI signal ‎nomenclature (SDO/SDI and PICO/POCI). The terms Master and Slave are now referred to as ‎Controller and Peripheral. The MOSI signal on a controller has been replaced with SDO or PICO. ‎Please refer to this announcement on the decision to deprecate the MOSI/MISO terminology and ‎transition to the SDO/SDI naming convention.‎ ‎

bus_22

Default SPI bus connections on the ESP32-WROOM Thing Plus.‎

table_23

Note: To learn more about the serial peripheral interface (SPI) protocol, check out this great tutorial.‎

 

spi_24

Serial Peripheral Interface (SPI)‎

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, ‎and SD cards.‎

I2C

I2C Communication Pins

The ESP32-WROOM module can support up to two I2C buses. By default, in the Arduino IDE, ‎the Wire class is configured to utilize pins GPIO 21 (SDA) and GPIO 22 (SCL). These pins share ‎the same I2C bus with the Qwiic connector and MAX17048 fuel gauge. In order to utilize the ‎other I2C ports, users will need to create a custom Wire object and declare which pins to access.‎ ‎

i2c_25

Default I2C bus connections for the ESP32-WROOM Thing Plus.‎

table_26

Note: To learn more about the inter-integrated circuit (I2C) protocol, check out this great tutorial.‎

controller_27

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.‎

Buttons

There are two buttons on ESP32-WROOM Thing Plus: an RST and BOOT button.‎

Reset Button

The RST (reset) button allows users to reset the program running on the ESP32-WROOM module ‎without unplugging the board.‎

button_28

RST button on the ESP32-WROOM Thing Plus.‎

Boot Button

The BOOT button can be used to force the board into the serial bootloader. Holding down ‎the BOOT button, while connecting the board to a computer through its USB-C connector or resetting ‎the board will cause it to enter the Firmware Download mode. The board will remain in this mode ‎until it power cycles (happens automatically after uploading new firmware) or the RST button is ‎pressed.‎

1. Hold the BOOT button down

2. Reset the MCU

o While unpowered, connect the board to a computer with through the USB-C ‎connection
o While powered, press the RST button

3. Release the BOOT button

4. After programming is completed, reboot the MCU

  • Press the RST button.‎

  • Power cycle the board.‎

boot_29

BOOT button on the ESP32-WROOM Thing Plus.‎

Note: The BOOT button is also connected to GPIO 0, which controls the voltage output to the Qwiic ‎connector. Therefore, pressing the BOOT button will momentarily disable power to the Qwiic ‎connector.‎

Indicator LEDs

There are four indicator LEDs on the ESP32-WROOM Thing Plus:‎

  • PWR: Power (Red)

  • CHG: Battery Charging (Yellow)

  • 13: GPIO 13 (Blue)

  • WS2812: GPIO 02 (RGB)‎

Power LED

The red, power (PWR) LED will light up once 3.3V is supplied to the board. For most users, it will ‎light up when 5V is supplied through the USB connection and/or when a LiPo battery is attached to ‎the JST connector.

 

status_30

ESP32-WROOM Thing Plus PWR status LED indicator.‎

Battery Charging LED

The yellow, battery charging (CHG) LED indicates the status of the MCP73831 charge management ‎controller. The LED will shut off when no battery is present, when the charge management ‎controller is in standby (after the battery charging has been completed), or when the charge ‎management controller is shutdown. The LED will illuminate when the charge management ‎controller is in the process of charging the battery. For more information, please refer to ‎the MCP73831 datasheet.‎

charge_31

The battery charging (CHG) LED indicator on the ESP32-WROOM Thing Plus.‎

table_32

STAT LED

The blue, status (STAT) LED is typically used as a test or status LED to make sure that a board is ‎working or for basic debugging. This indicator is connected to GPIO 13.‎

status_33

The status (STAT) LED indicator on the ESP32-WROOM Thing Plus.‎

WS2812 RGB LED

The WS2812 RGB LED is controlled with a 24-bit (GRB) data signal. This indicator is connected ‎to GPIO 02 and the digital output pin from the LED is available through a test point. For more ‎information, please refer to the WS2812C datasheet.‎

data_34

WS2812 LED indicator on the ESP32-WROOM Thing Plus.‎

Note: The latest ESP32 Arduino core, now provides a basic RGB LED driver for a WS2812 (or ‎NeoPixel) LED populated the board. For an example of how to utilize the RGB LED driver check out ‎the BlinkRGB example code, which can be accessed from the File drop down ‎menu (i.e File > Examples > ESP32 > GPIO > BlinkRGB).‎

‎µSD Slot‎

Note: To comply with the latest OSHW design practices, we have adopted the new SPI signal ‎nomenclature (SDO/SDI and PICO/POCI). The terms Master and Slave are now referred to as ‎Controller and Peripheral. Please refer to this announcement on the decision to transition to the ‎new naming convention.‎

The ESP32-WROOM Thing Plus (USB-C) includes an µSD card slot. This is great for data logging ‎applications or storing files. The µSD card slot is connected to the following dedicated GPIO:‎

  • GPIO 5: DATA 3/CS

  • N/A: DATA 2

  • N/A: DATA 1

  • GPIO 19: DATA 0/POCI (or Peripheral's SDO)

  • GPIO 18: CLK/SCK

  • GPIO 23: CMD/PICO (or Peripheral's SDI)‎

card_35

‎µSD card slot on the ESP32-WROOM Thing Plus.‎

Jumpers

There are two jumpers on the back of the board that can be used to easily modify the hardware ‎connections on the board.‎

  • SHLD - This jumper can be used to disconnect the USB shield from GND

  • PWR - This jumper can be used to remove power to the PWR LED

  • CHG LED - This jumper can be used to remove power to the CHG LED

    • Avoid cutting the box's silkscreen; there are traces under it:‎

traces_36

Traces around the CHG LED jumper.‎

jumper_37

The jumpers on the back of the ESP32-WROOM Thing Plus.‎

Never modified a jumper before? Check out our Jumper Pads and PCB Traces tutorial for a quick ‎introduction!‎

how_38

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a ‎solder jumper between pads to reroute connections, and repair a trace with the green wire method ‎if a trace is damaged.‎

Primary I2C Bus

The Qwiic connector and battery fuel gauge are attached to the primary I2C bus. The primary I2C ‎bus for this board utilizes the pin connections, detailed in the table below:‎

table_39

Battery Fuel Gauge

The MAX17048 fuel gauge measures the approximate charge or discharge rate, state of charge ‎‎(SOC) (based on ModelGauge algorithm), and voltage of a connected battery. Additionally, the chip ‎is powered directly from VBAT, when a LiPo battery is connected. For more information, please ‎refer to the MAX17048 datasheet.‎

max_40

The MAX17048 fuel gauge on the ESP32-WROOM Thing Plus.‎

table_41

Note: The Alert pin for the MAX17048 is not connected and cannot be utilized.‎

Qwiic Connector

A Qwiic connector is provided for users to seamlessly integrate with SparkFun's Qwiic Ecosystem.‎

qwiic_42

Qwiic connector and I2C pins on the ESP32-WROOM Thing Plus.‎

Power Control

In order to enable power for the Qwiic connector, users must toggle GPIO 0 high. This enables the ‎power output from the XC6222 LDO regulator to the Qwiic connector, which can source up ‎to 700mA at 3.3V . In order to conserve battery power or in low power applications, users can ‎toggle GPIO 0 low, to disable the power to the Qwiic connector.‎

Note: GPIO 0 is also connected to the BOOT button. Therefore, pressing the BOOT button will ‎momentarily disable power to the Qwiic connector.‎

What is Qwiic?‎

The Qwiic system is intended a quick, hassle-free cabling/connector system for I2C devices. Qwiic ‎is actually a play on words between "quick" and I2C or "iic".

 

 

Features of the Qwiic System

NO SOLDERING

Keep your soldering iron at bay.

Cables plug easily between boards making quick work of setting up a new prototype. We currently ‎offer three different lengths of Qwiic cables as well as a breadboard friendly cable to connect any ‎Qwiic enabled board to anything else. Initially you may need to solder headers onto the shield to ‎connect your platform to the Qwiic system but once that’s done it’s plug and go!‎

cables_43

Qwiic cables connected to Spectral Sensor Breakout

POLARIZED CONNECTOR

Minimize your mistakes.‎

How many times have you swapped the SDA and SCL wires on your breadboard hoping the sensor ‎will start working? The Qwiic connector is polarized so you know you’ll have it wired correctly, every ‎time, from the start.‎

The PCB connector is part number SM04B-SRSS (Datasheet) or equivalent. The mating connector ‎used on cables is part number SHR04V-S-B or equivalent. This is a common and low-cost ‎connector.‎

connector_44

‎1mm pitch, 4-pin JST connector

DAISY CHAIN

Expand with ease.‎

It’s time to leverage the power of the I2C bus! Most Qwiic boards will have two or more connectors ‎on them allowing multiple devices to be connected.‎

chain_45

Shown above: Qwiic Shield for Arduino on RedBoard, Spectral Sensor Breakout - NIR, Spectral Sensor Breakout - ‎Visible, and SparkFun GPS Breakout

Hardware Assembly

USB Programming

The USB connection is utilized for programming and serial communication. Users only need to plug ‎their ESP32-WROOM Thing Plus into a computer using a USB-C cable.‎

usb_46

The ESP32-WROOM Thing Plus with USB-C cable attached.‎

Battery

For remote IoT applications, a Li-Po battery can be connected. Additionally, users may be ‎interested in utilizing a solar panel and USB-C cable to recharge their battery.‎ ‎

connected_47

The ESP32-WROOM Thing Plus with a battery connected.‎

Note: DO NOT remove batteries by pulling on their wires. Instead, it is recommended that pair of ‎dikes (i.e., diagonal wire cutters), pliers, or tweezers be used to pull on the JST connector housing, ‎to avoid damaging the battery wiring.‎

disconnect_48

‎Using a pair of dikes to disconnect a battery.‎

Headers

The pins for the ESP32-WROOM Thing Plus are broken out to 0.1"-spaced pins on the outer ‎edges of the board. When selecting headers, be sure you are aware of the functionality you need. ‎If you have never soldered before or need a quick refresher, check out our How to Solder: ‎Through-Hole Soldering guide.‎

soldering_49

Soldering headers to the ESP32-WROOM Thing Plus.

The Feather Stackable Header Kit is a great option as it allows users to stack shields (w/ Feather ‎footprint) or it can be placed on the a breadboard; while, the pins are still accessible from the ‎female/male headers.‎

‎µSD Card Slot‎

The ESP32-WROOM Thing Plus (USB-C) includes a µSD card slot on the back of the board. The ‎card holder functions through a push/pull operation. (The card slot doesn't include a spring ‎retention mechanism; cards are held in place through friction.)‎

holder_50

Users can slide-in or pull-out a µSD card from the card holder. ‎

Qwiic Devices

The Qwiic system allows users to effortlessly prototype with a Qwiic compatible I2C device without ‎soldering. Users can attach any Qwiic compatible sensor or board, with just a Qwiic cable. (*The ‎example below, is for demonstration purposes and is not pertinent to the board functionality or this ‎tutorial.)‎

boards_51

The BME688 environmental and VL53L1X distance Qwiic sensor boards connected to the ESP32-‎WROOM Thing Plus.‎

Software Overview

CH340 Driver

Users will need to install the appropriate driver for their computer to recognize the serial-to-UART ‎chip on their board/adapter. Most of the latest operating systems will recognize CH340C chip on ‎the board and automatically install the required driver.‎

To manually install the CH340 driver on their computer, users can download it from the WCH ‎website. For more information, check out our How to Install CH340 Drivers Tutorial.

install_52

How to Install CH340 Drivers

How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.‎

Arduino IDE

Note: For first-time users, who have never programmed before and are looking to use the Arduino ‎IDE, we recommend beginning with the SparkFun Inventor's Kit (SIK), which includes a simpler ‎board like the Arduino Uno or SparkFun RedBoard and is designed to help users get started ‎programming with the Arduino IDE.‎

Most users may already be familiar with the Arduino IDE and its use. However, for those of you who ‎have never heard the name Arduino before, feel free to check out the Arduino website. To get ‎started with using the Arduino IDE, check out our tutorials below:‎

  • Installing an Arduino Library: How do I install a custom Arduino library? It's easy! This ‎tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries ‎not linked with the Arduino IDE, we will also go over manually installing an Arduino library.‎

  • What is an Arduino? What is this 'Arduino' thing anyway? This tutorial dives into what an ‎Arduino is and along with Arduino projects and widgets.‎

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software on ‎Windows, Mac, and Linux.‎

  • Installing Board Definitions in the Arduino IDE: How do I install a custom Arduino ‎board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the ‎Arduino Board Manager. We will also go over manually installing third-party cores, such as the ‎board definitions required for many of the SparkFun development boards.‎

Install Board Definition

Install the latest ESP32 board definitions in the Arduino IDE.‎

install_53

Installing Board Definitions in the Arduino IDE

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an ‎Arduino board definition using the Arduino Board Manager. We will also go over manually installing ‎third-party cores, such as the board definitions required for many of the SparkFun development ‎boards.‎

Note: For more instructions, users can follow this tutorial on Installing Additional Cores provided by ‎Arduino. Users will also need the .json file for the Espressif Arduino core:

https://raw.githubusercontent.com/espressif/arduino-esp32/gh-‎pages/package_esp32_index.json

When selecting a board to program in the Arduino IDE, users should select the SparkFun ESP32 ‎Thing Plus C from the Tools drop down menu (i.e., Tools > Board > ESP32 ‎Arduino > SparkFun ESP32 Thing Plus C). Alternatively, users can also select the ESP32 Dev ‎Module; however, they may lose some pin assignments (i.e., LED_BUILTIN).‎

select_55

Selecting the SparkFun ESP32 Thing Plus C from the Tools drop down menu in the Arduino IDE. ‎

Note: In the Arduino 2.0.x IDE users can also select the board from the Select Board drop down ‎menu and search for the SparkFun ESP32 Thing Plus C:‎

select_56

‎Selecting the SparkFun ESP32 Thing Plus C in the Arduino 2.0.x IDE.‎

Arduino Example: Blink

First-Time Users:‎

With the driver and ESP32 Arduino core installed, users are ready to program their board! When ‎selecting a board to program, users should select the SparkFun ESP32 Thing Plus C in the ‎Arduino IDE.‎

Once the ESP32 Thing Plus is connected to a computer with a USB cable, the board will be ‎assigned a unique port identifier. On Windows machines, this should appear as COM#, and on Macs ‎or Linux computers it should be /dev/tty.usbserial-####### in the Arduino IDE. Before code can ‎be uploaded, users will need to select the port that the board has been assigned to.‎

Loading Blink

To make sure the toolchain and board are properly set up, let us try to upload a simple sketch! ‎The STAT LED attached to GPIO 13 is perfect for a simple test. Copy and paste the example sketch ‎below into a fresh Arduino sketch:‎

Copy Code
int ledPin = 13;

void setup()
{
    pinMode(ledPin, OUTPUT);
    Serial.begin(115200);
}

void loop()
{
    Serial.println("Hello, world!");
    digitalWrite(ledPin, HIGH);
    delay(500);
    digitalWrite(ledPin, LOW);
    delay(500);
}

With everything setup correctly, upload the code! Once the upload is complete, open the serial ‎monitor and set the baud rate to 115200. Users should see a Hello, world! print statement begin ‎to fly by.‎

If the blue LED remains dimly lit, it's probably still sitting in the bootloader. After uploading a sketch, ‎users may need to tap the RST button to get their ESP32 Thing Plus to begin running the sketch.

com_57

Users may also notice that when the ESP32 boots up it prints out a long sequence of debug ‎messages. These are emitted every time the chip resets -- always at 115200 baud.‎

Arduino Example: Wi-Fi

Note: Users should be utilizing the 2.4GHz band of their wireless router. The current ESP32 ‎modules aren't compatible with 5GHz Wi-Fi signals; users will need to wait for the ESP32-C5 for ‎that feature. To get notifications on our latest products, sign-up for our newsletter!‎

The ESP32 Arduino core includes a handful of Wi-Fi examples, which demonstrate everything from ‎scanning for nearby networks. These Wi-Fi examples are available under ‎the File > Examples > Wi-Fi drop-down menu in the Arduino IDE.‎

Below, is a more advanced example utilizing the Wi-Fi Arduino library. It demonstrates how to ‎connect to a nearby Wi-Fi network and poll a remote domain (http://example.com/) as a client.‎

Copy Code
#include <WiFi.h>

// WiFi network name and password:
const char * networkName = "YOUR_NETWORK_HERE";
const char * networkPswd = "YOUR_PASSWORD_HERE";

// Internet domain to request from:
const char * hostDomain = "example.com";
const int hostPort = 80;

const int BUTTON_PIN = 0;
const int LED_PIN = 13;

void setup()
{
  // Initilize hardware:
  Serial.begin(115200);
  pinMode(BUTTON_PIN, INPUT_PULLUP);
  pinMode(LED_PIN, OUTPUT);

  // Connect to the WiFi network (see function below loop)
  connectToWiFi(networkName, networkPswd);

  digitalWrite(LED_PIN, LOW); // LED off
  Serial.print("Press button 0 to connect to ");
  Serial.println(hostDomain);
}

void loop()
{
  if (digitalRead(BUTTON_PIN) == LOW)
  { // Check if button has been pressed
    while (digitalRead(BUTTON_PIN) == LOW)
      ; // Wait for button to be released

    digitalWrite(LED_PIN, HIGH); // Turn on LED
    requestURL(hostDomain, hostPort); // Connect to server
    digitalWrite(LED_PIN, LOW); // Turn off LED
  }
}

void connectToWiFi(const char * ssid, const char * pwd)
{
  int ledState = 0;

  printLine();
  Serial.println("Connecting to WiFi network: " + String(ssid));

  WiFi.begin(ssid, pwd);

  while (WiFi.status() != WL_CONNECTED) 
  {
    // Blink LED while we're connecting:
    digitalWrite(LED_PIN, ledState);
    ledState = (ledState + 1) % 2; // Flip ledState
    delay(500);
    Serial.print(".");
  }

  Serial.println();
  Serial.println("WiFi connected!");
  Serial.print("IP address: ");
  Serial.println(WiFi.localIP());
}

void requestURL(const char * host, uint8_t port)
{
  printLine();
  Serial.println("Connecting to domain: " + String(host));

  // Use WiFiClient class to create TCP connections
  WiFiClient client;
  if (!client.connect(host, port))
  {
    Serial.println("connection failed");
    return;
  }
  Serial.println("Connected!");
  printLine();

  // This will send the request to the server
  client.print((String)"GET / HTTP/1.1\r\n" +
               "Host: " + String(host) + "\r\n" +
               "Connection: close\r\n\r\n");
  unsigned long timeout = millis();
  while (client.available() == 0) 
  {
    if (millis() - timeout > 5000) 
    {
      Serial.println(">>> Client Timeout !");
      client.stop();
      return;
    }
  }

  // Read all the lines of the reply from server and print them to Serial
  while (client.available()) 
  {
    String line = client.readStringUntil('\r');
    Serial.print(line);
  }

  Serial.println();
  Serial.println("closing connection");
  client.stop();
}

void printLine()
{
  Serial.println();
  for (int i=0; i<30; i++)
    Serial.print("-");
  Serial.println();
}

Make sure to fill in the networkName and networkPswd variables, at the beginning of the sketch, with ‎the name (or SSID) and password of your Wi-Fi network! Once that is done, upload the sketch to ‎the board and open the Serial Monitor of the Arduino IDE.‎

example_58

Example of the report out in the Serial Monitor.‎

After the ESP32 connects to the Wi-Fi network, it will wait for the user to press the BOOT button. ‎Tapping the button will cause the ESP32 to make an HTTP request to example.com. The board ‎should return a string of HTTP headers and HTML code, as shown above.‎

Arduino Example: BLE

Note: This example requires a compatible BLE app on a smart phone. We recommend the BLE ‎Scanner for iPhone or Android. Also, don't forget to enable the Bluetooth connection on the phone.‎

The ESP32 Arduino core also includes several Bluetooth examples that range from acting as a ‎simple BLE device to functioning as a Bluetooth server. This example will demonstrate how users ‎can send messages from their phone to ESP32 Thing Plus; and then display the message in the ‎serial monitor. Users will need to install the BLE Scanner app (iPhone or Android) on their smart ‎phone and enable the Bluetooth connection.‎

The example code is built into the Arduino IDE for the ESP32 Arduino core (users need to select ‎and ESP32 board definition first). Once an ESP32 board has been selected, the built-in BLE ‎examples will become available; select the BLE_write example from the Files > Examples > ESP32 ‎BLE Arduino > BLE_write drop down menu. Compile and upload the example code. Make sure ‎the correct port has been selected for the board.‎

Copy Code
/*
    Based on Neil Kolban example for IDF: https://github.com/nkolban/esp32-snippets/blob/master/cpp_utils/tests/BLE%20Tests/SampleWrite.cpp
    Ported to Arduino ESP32 by Evandro Copercini
*/

#include <BLEDevice.h>
#include <BLEUtils.h>
#include <BLEServer.h>

// See the following for generating UUIDs:
// https://www.uuidgenerator.net/

#define SERVICE_UUID        "4fafc201-1fb5-459e-8fcc-c5c9c331914b"
#define CHARACTERISTIC_UUID "beb5483e-36e1-4688-b7f5-ea07361b26a8"


class MyCallbacks: public BLECharacteristicCallbacks {
    void onWrite(BLECharacteristic *pCharacteristic) {
      std::string value = pCharacteristic->getValue();

      if (value.length() > 0) {
        Serial.println("*********");
        Serial.print("New value: ");
        for (int i = 0; i < value.length(); i++)
          Serial.print(value[i]);

        Serial.println();
        Serial.println("*********");
      }
    }
};

void setup() {
  Serial.begin(115200);

  Serial.println("1- Download and install an BLE scanner app in your phone");
  Serial.println("2- Scan for BLE devices in the app");
  Serial.println("3- Connect to MyESP32");
  Serial.println("4- Go to CUSTOM CHARACTERISTIC in CUSTOM SERVICE and write something");
  Serial.println("5- See the magic =)");

  BLEDevice::init("MyESP32");
  BLEServer *pServer = BLEDevice::createServer();

  BLEService *pService = pServer->createService(SERVICE_UUID);

  BLECharacteristic *pCharacteristic = pService->createCharacteristic(
                                         CHARACTERISTIC_UUID,
                                         BLECharacteristic::PROPERTY_READ |
                                         BLECharacteristic::PROPERTY_WRITE
                                       );

  pCharacteristic->setCallbacks(new MyCallbacks());

  pCharacteristic->setValue("Hello World");
  pService->start();

  BLEAdvertising *pAdvertising = pServer->getAdvertising();
  pAdvertising->start();
}

void loop() {
  // put your main code here, to run repeatedly:
  delay(2000);
}

Once the upload completes, open the serial monitor set the baud rate to 115200 bps.‎

com_59

Then open the BLE Scanner app on a smart phone. User should see several BLE devices ‎displayed; scroll through and connect to MyESP32.‎

open_60

Once connected, users will be taken to the following page. Select CUSTOM SERVICE to set ‎communication capability required for this example.‎

page_61

The next page, select the Write, Read option.‎

select_62

Finally, select the Write Value option to send a message to the board.‎

write_63

Make sure to select the Text option in the dialog box. Then, write a message in the text box and ‎click the Write button.‎

button_64

Now take look at the serial monitor, users should see New value: followed by the entry from the ‎text box.‎

com_65

This is just a quick walk through of one of the provided examples. We recommend looking through ‎the rest of the BLE examples and playing with the code. For more information on Bluetooth ‎technology and how it works, check out our Bluetooth Basics Tutorial.‎

Arduino Example: Test Sketches

For additional examples, users can check out the Test Sketches that we used to verify the ‎functionality of the board during our development phase. These can be downloaded from ‎the GitHub repository for the board hardware:‎

CLICK TO DOWNLOAD THE REPOSITORY

Troubleshooting Tips

Not working as expected and need help?‎

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.‎

SPARKFUN TECHNICAL ASSISTANCE PAGE

If you can't find what you need there, you'll need a Forum Account to search product forums and ‎post questions.‎

Upload Issues

If users are have issues during the uploading process, they can try to manually force the board into ‎the serial bootloader with the BOOT button. Holding down the BOOT button, while connecting the ‎board to a computer through its USB-C connector or resetting the board will cause the MCU to ‎enter the Firmware Download mode and its serial bootloader. The board will remain in this mode ‎until it power cycles (happens automatically after uploading new firmware) or the RST button is ‎pressed.‎

‎1.‎ Hold the BOOT button down

‎‎2.‎ Reset the MCU

‎o While unpowered, connect the board to a computer with through the USB-C ‎connection

‎o While powered, press the RST button

‎‎3.‎ Release the BOOT button

‎‎4.‎ After programming is completed, reboot the MCU

o Press the RST button

o Power cycle the board.‎

boot_66

BOOT button on the ESP32-WROOM Thing Plus.‎

COM Port Not Shown

If the board doesn't appear on a COM port, double check the correct driver has been installed. ‎Unlike previous versions of the ESP32 Thing Plus, this variant requires the CH340 driver to be ‎installed. For more information, check out our How to Install CH340 Drivers Tutorial.‎

install_67

How to Install CH340 Drivers

How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.‎

Users can also check their USB cable; some cables are power only. Try testing the cable with a ‎smart phone or tablet to see if it appears as a device on the computer. If the phone/tablet doesn't ‎appear, then the USB cable is power only.‎

Serial Stream Difficulties

We have noticed that with the ESP32 Arduino core, Serial.available() does not operate ‎instantaneously. This is due to an interrupt triggered by the UART, to empty the FIFO when ‎the RX pin is inactive for two-byte periods:‎

  • At 9600 baud, hwAvailable takes [number‎ of bytes received + 2] x 1 ms = 11 ms before the UART indicates that data was received ‎from: \r\nERROR\r\n

  • At 115200 baud, hwAvailable takes [number of bytes received + 2] x .087 ms = ~1 ‎ms before the UART indicates that data was received from: \r\nERROR\r\n

For more information, please refer to this chatroom discussion‎.

‎µSD Card‎

Make sure that the µSD card is compatible with the Arduino library being used for it. For example, ‎the default SD Arduino library is only compatible with FAT16 or FAT32 file systems; therefore, the ‎card capacity is limited to 16GB or 32GB and smaller. Another consideration is that the library was ‎also written to only handle short 8.3 names for files.‎

Qwiic Connector Power

For users having issues with the power to their Qwiic devices, don't forget that GPIO 0 controls the ‎power output from the XC6222 LDO regulator to the Qwiic connector. Users must toggle GPIO ‎‎0 high to enable power for the Qwiic connector. In order to conserve battery power or in low power ‎applications, users can toggle GPIO 0 low, to disable the power to the Qwiic connector.‎

Note: GPIO 0 is also connected to the BOOT button. Therefore, pressing the BOOT button will ‎momentarily disable power to the Qwiic connector.‎

Current Consumption

For ultra-low power projects, these are the current consumption of the individual components, as ‎specified in their datasheet:‎

  • XC6222 LDO Regulator:

    • Supply Current: 100 - 220 µA

  • MCP73831 Charger Controller:

    • Supply Current:

      • ‎510 - 1500 µA (Charging)

      • ‎53 - 200 µA (Charge complete; no battery)‎

    • Constant-Voltage Mode

      • Line/Load regulation: 100 - 50 mA

    • ‎Fast Charge Constant-Current Mode

      • Fast Charge Current: 450 - 550 mA‎

    • Battery Detection Current: 6 µA

    • Leakage Current: up to 2µA

    • Status Indicator:

      • Sink Current: 25 mA

  • MAX17048 Fuel Gauge:‎

    • Supply Current:‎

      • Sleep: 0.5 - 2 µA

      • Hibernate: 3 - 5 µA

      • Active: 23 - 40 µA‎

    • I2C: 0.2 - 0.4 µA

  • CH340C Serial-to-UART Bridge:

    • ‎Supply Current: 4 - 12 mA

      • ‎USB Suspended: 0.04 - 0.15 mA

  • ESP32 SoC:

    • ‎Rec Supply current: 500 mA

    • Active: 95 - 240 mA‎

      • w/ RF Transceiver:

        • ‎TX: up to 380 mA

        • RX: Up to 118 mA

    • Sleep Modes:‎

      • Modem: 20 - 68 mA

      • Light: .8 mA

      • Deep: 10 - 150 µA

      • Hibernation: 5 µA

      • Off: 1µA

  • WS2812 RGB LED:‎

    • Supply Current: 1µA (@5V)‎

    • LEDs: 5mA each (@5V)‎

Resources and Going Further

For more resources related to the ESP32 Thing Plus, check out the links listed here:‎

Espressif also provides great resources for their ESP32 module:‎

מק"ט יצרן # 14743
CABLE A PLUG TO C PLUG 3.28'
SparkFun Electronics
מק"ט יצרן # 15081
QWIIC CABLE KIT
SparkFun Electronics
מק"ט יצרן # 19096
QWIIC BME688 ENVIRONMENTAL SENSR
SparkFun Electronics
מק"ט יצרן # 14722
QWIIC 4M DISTANCE SENSOR VL53L1X
SparkFun Electronics
מק"ט יצרן # 15631
ARDUINO UNO INVENTOR KIT V4.1
SparkFun Electronics
מק"ט יצרן # A000073
ARDUINO UNO SMD R3 ATMEGA328
Arduino
מק"ט יצרן # 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
מק"ט יצרן # 14681
SPARKFUN BEGINNER TOOL KIT
SparkFun Electronics
מק"ט יצרן # 14321
PHOTON HEADER - 12 PIN FEMALE
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.