Maker.io main logo

Generate Renewable Energy with Wind Turbines

177

2023-03-30 | By Lulzbot

License: See Original Project 3D Printing

Courtesy of Lulzbot

Guide by Lulzbot

DESCRIPTION

Renewable energy sources are on the rise globally as we work to combat climate change and ‎man-made pollution across our planet. Through this lesson, we look at how Wind Turbines ‎generate electricity as students are challenged to create their own renewable energy sources!‎

INTRODUCTION

LESSON OVERVIEW:‎

Through this lesson, students will learn about the importance of renewable energy sources as ‎we cover the impact nonrenewable sources have on the Earth’s ecosystems. Students will learn ‎how wind turbines create electricity using generators, as well as how the airfoils of a wind ‎turbine’s blade functions.‎

Through the utilization of an engineering design process, students will brainstorm different ‎wind turbine designs based upon the specifications and constraints of the challenge. Students ‎will then apply prototyping techniques to design and build their very own wind turbine!‎

Once built, students will be able to test and evaluate the performance of their wind turbine as ‎we continue to make connections to the real-world. We will also discuss the importance of ‎redesign as we reflect upon the performance of our solutions and work to make improvements ‎using what we’ve learned.‎

There are countless ways to adapt and modify this lesson to suit the needs of elementary, ‎middle, or high school learners based upon prior experiences and abilities. There are also ‎endless adaptations that can be based upon available resources, time, and focus of your ‎course’s objectives.‎‎ ‎

prototypes_1

A HAWT and VAWT Turbine prototypes printed on a LulzBot Mini 2

UTILIZING AN ENGINEERING DESIGN PROCESS:‎

An Engineering Design Process, or design loop, is a method used by scientists, designers, and ‎engineers to develop solutions to our everyday problems. Through a design loop, students will ‎develop skills in problem solving as they brainstorm solutions and work to create a prototype ‎through hands-on activities.‎

Design loops come in many shapes and sizes, but none are ever truly ending. The “last” step of ‎any design loop is redesign, or reflection, where we look at what we’ve learned in our ‎developed prototype to improve upon its design. Not being afraid of failure is a powerful ‎concept that leads to greater success and implementation of redesign.‎

steps_2

LESSON OBJECTIVES:‎

  • Students will be able to identify the differences between renewable and nonrenewable ‎energy sources
  • Students will be able to identify how electricity can be created
  • Students will understand how wind turbines work
  • Students will utilize an engineering design process to develop their own solutions to a real-‎world problem
  • Students will utilize computer aided design (CAD) software to create a 3D, model that can be ‎produced on a 3D printer
  • Students will understand how 3D printers work and how they are used in industrial settings‎
  • Students will be able to safely apply prototyping techniques to construct designed solutions to ‎real-world problems

MATERIALS:‎

This is a list of materials each student will need to complete this lesson:‎

  • Computer or tablet with Internet access
  • Computer Aided Design (CAD) software
  • 3D Printer and Filament
  • DC Motor‎
  • Voltmeter (or multimeter) per student or per group
  • Paper, pencils
  • Click here for sample models shown throughout this lesson‎

MODIFICATIONS:‎

In addition to this lesson plan, see our One Page Brief [PDF] that can be used to guide students ‎through the lesson. These are additional examples as to how this lesson could be modified:‎

  • Additional tools and materials to construct prototypes such as cardboard, popsicle sticks, ‎Styrofoam, or hot glue to combine with 3D printed parts‎‎
  • LED bulbs can be attached to the motor as they will illuminate with generated electricity from ‎turbine
  • If DC motors used are 5v, a 5v USB adapter can be connected so the motors (generators) will ‎charge mobile devices (if enough electricity can be produced based on performance of the ‎turbine)
  • Incorporating a microcontroller, like a Micro:Bit or Arduino, to interact with wind turbine ‎prototypes could add elements for computer science

CONSIDERATIONS:‎

Based upon the age of your students, introduce the concepts of electricity, energy, renewable ‎and nonrenewable resources using terms and concepts familiar to their prior experiences and ‎needs.‎

When working with DC motors, choosing motors with wires already attached removes the need ‎for soldering and makes the motors easier to work with for younger students. Consider applying ‎tape or hot glue to the wires so they do not break off during prototyping.‎

Proper safety procedures should be introduced to students when working in any makerspace or ‎lab environment. When students are around machines such as 3D printers, or using tools to cut ‎or glue materials, students must be informed of potential hazards and taught how to use these ‎resources safely. For reference, see the safety resources offered by ITEEA.‎ ‎

wind_3

‎Example wind turbine made with a combination of materials in addition to 3D printed parts

Printed on a LulzBot Mini 2‎

ASSESSMENTS:‎

Opportunities for formative assessments will take place through observations and discussions ‎between students as they interact with the content in this lesson. For summative assessment, ‎we recommend utilizing a rubric to assess how a student was able to apply the engineering ‎design process to solve an open-ended problem. Example Rubric - PDF

IDENTIFY THE PROBLEM

WHERE DOES ELECTRICITY COME FROM?‎

In today’s world, we rely heavily on electricity. We need it for our homes, for our hospitals, to ‎cook or to travel, even non-electronic things were made and delivered to us using electricity. ‎But do we know what electricity is?‎

Electricity is phenomenon that exists in nature, but can also be created, stored, and used. This ‎generated form of electricity is comprised of atoms that contain a positive or negative charge. ‎These charged atoms are moving, or flowing, and we use this energy to power all of our ‎electronic devices!‎

To create electricity for our homes, we have used power plants. A power plant typically uses ‎fuels like coal or natural gas (fossil Fuels), or nuclear energy to create heat. This heat is then ‎used to boil water to make steam. Through a series of pipes, steam is directed to a turbine or ‎fan which is connected to a generator. Generators use magnetism to create electricity which is ‎then sent to your homes through our power grids.‎

Power plants like these are considered to be nonrenewable energy sources because the fuel ‎cannot be reused after being converted into heat to create steam. This process of burning fuel ‎also creates a byproduct of harmful greenhouse gases that pollute our ecosystems.‎

WHAT IS RENEWABLE ENERGY

Now that we’ve learned how typically power plants burn fossil fuels like coal or natural gas to ‎create heat, lets discuss a cleaner way to make electricity! Renewable energy are methods of ‎creating electricity with fuel, or energy that can be reused. Renewable resources include ‎natural energy forms like wind, water, or solar, as well as geothermal, biofuels, or even ‎biomass waste. Unlike nonrenewable energy, renewable energy does not directly create ‎greenhouse gas pollutants and use methods that will not run out. ‎

There are different methods to creating renewable energy, but many of them use generators ‎just like a typical power plant. Hydroelectric power plants use flowing water to turn the ‎turbines of a generator and while wind turbines use wind. Some methods like geothermal or ‎solar thermal use heat to create steam which turns a turbine, while photovoltaic cells, or solar ‎panels, use sunlight to create electricity through flowing electrons.‎

But of the different forms of renewable energy available, and with the clear benefits for ‎the environment, why does renewable energy account for less than 15% of electricity created in ‎the United States (in 2018)? ‎

IDENTIFY THE PROBLEM

As wind Turbines account for approximately 24% of the renewable energy created In the United ‎States (which is only about 11% of total energy produced), they are one of the most widely used ‎forms of renewable energy worldwide. While there are many benefits to wind energy, there ‎are also, many challenges. The first of which is cost, wind turbines are expensive and as they ‎only create electricity when there’s wind, many companies can’t afford to produce wind ‎turbines that may only be used part of the time. Wind turbines are also often considered to be ‎ugly, loud, and can impact local wildlife negatively.‎

Using an engineering design process, can we design and create our own prototype wind ‎turbines that combat the drawbacks of typical wind turbines such as cost, looks, noise, and or ‎wildlife impact?‎

Challenge Constraints include but are not limited to:

  • You must address at least one of the defined drawbacks for wind turbines
  • You have 1 day to brainstorm, 3 days to build, and 1 day to test & evaluate‎‎
  • You must design your prototype to support the provided DC motor that will act as your ‎generator‎
  • Your 3D Model build volume may not exceed 36 in3
  • You must incorporate at least three different materials‎

typical_4

Typical types of Horizontal (HAWT) and Vertical Axis (VAWT) Wind Turbines

BRAINSTORM POSSIBLE SOLUTIONS

WHY SOLUTIONS AND NOT SOLUTION?‎

The second step of our Engineering Design Process is “Brainstorm Possible Solutions.” A key ‎part of this step is solutions being plural, meaning more than one. Why do designers and ‎engineers think of more than one way to solve a problem?‎

BRAINSTORMING OUR SOLUTIONS ‎

As we work to think of different ways to solve this problem, there are a few things we can ‎consider assisting in our design. The first is learning from existing wind turbine styles. Wind ‎turbines can have either a vertical axis (VAWT) or horizontal axis (HAWT) with different blade ‎configurations for each. Take time to research and learn about the benefits and drawbacks to ‎each type. Which do you think would best suit our needs and why?‎

Remember, we must address at least one of the defined drawbacks for wind turbines in our ‎designed solutions. The drawbacks are Cost, Aesthetics, Noise, and Negative Impacts on Wildlife.‎

After researching the various types of turbines, blades, and drawbacks, begin to brainstorm ‎different ways, you could construct your own turbine under the specifications and constraints of ‎the challenge. Thumbnail sketches are a great way to think of many ideas quickly without ‎getting caught up on the details. Once you’ve completed the thumbnail sketches, narrow your ‎choices down as you create your final design.‎

For your final sketch, create a clear design that is neat and labeled. Consider drawing your ‎design from multiple views (front, top, side, or isometric) to better portray your ideas.‎

RESOURCES:

  • Thumbnail Sketching Document [PDF]
  • Technical Drawing Paper [PDF]

DEVELOP A PROTOTYPE

WHAT IS 3D PRINTING? ‎

Step 3 of the engineering design process is all about constructing our prototype solution! In this ‎step, we are going to get hands-on with software and machinery to create our final design.‎

One of the key prototyping machines used by professional designers, engineers, and scientists is ‎a 3D printer. There are a lot of different types of 3D printers out there, but all 3D printers ‎create physical objects you can touch, and hold based on a 3D design or model. Some 3D ‎printers melt rolls of plastic into the model, while others use light to harden a liquid resin. ‎There are even 3D printers that can print concrete, metal, or living cell tissue!‎

Lulzbot 3D printers use the fused deposition modeling process (FDM) that feeds and melts ‎spools of plastic through a nozzle, kind of like glue traveling through a hot glue gun. The plastic ‎is fed, or extruded, layer by layer to create the model designed in computer aided design (CAD) ‎software. Once we design your wind turbine model in CAD software, we will be able to send ‎them to a 3D printer to be manufactured!‎

DEVELOPING OUR 3D MODELS

Now that we’ve brainstormed our wind turbine designs, it is time to begin to fabricate it! But ‎before we can 3D print our parts; we need a 3D design. To create this, we will use computer ‎aided design software, or CAD. There’s plenty of great free CAD programs out there, we ‎recommend Tinkercad, FreeCAD, Fusion360, or OnShape for students. When designing your ‎model, there’s a few things to consider that will best prepare it for 3D printing:‎

  • Size - Make sure you are keeping track of your dimensions, or measurements as you design
  • Base - Try to design a model with a flat base so it is supported while printing from bottom up
  • Overhangs - When possible, avoid overhangs to reduce the amount of support material needed
  • Tolerances - Where parts fit together or fit with something else, leave some “wiggle” room or ‎a tolerance as the plastic will shrink during printing‎

flawed_4

‎Example of a flawed design created in Tinkercad with overhangs and without a flat base

corrected_5

‎Example of a corrected design created in Tinkercad

blades_6

VAWT Turbine Blades designed in Tinkercad

Printed on a LulzBot Mini 2‎

PRINTING

Once students have completed their designs, it’s time to download and prepare them to use ‎Cura. Cura is not a CAD program in that it allows you to design your models. Instead, Cura ‎‎“slices” models’ layer by layer to create a program file, or Gcode file for the 3D printer to read. ‎This Gcode file is a set of directions that the 3D printer follows as it prints your model.‎

In general, we recommend PLA filament for most classroom uses as it’s a safe plastic to print in ‎schools and prints easily in nearly any setting. PLA works well for most applications, but if you ‎need your prototype to be exceptionally strong, or able to resist the sun or high temperatures, ‎consider looking into other materials that may better suit your needs.‎

When printing your student’s models, a “high speed” setting will probably be best to get all the ‎models printed quickly at good quality. The default layer height for high speed is 0.38mm. If the ‎models are small, detailed, or delicate, consider using a “standard” or “high detail” print ‎setting which uses a smaller layer height. The smaller the layer height, the slower the print but ‎the smoother and more refined the finished model will be. If you students have any overhangs, ‎you should use support material. Support material is automatically drawn by Cura and it fills ‎any gaps or structural flaws. After the model is printed, support material can be carefully ‎removed by peeling it off of the model. When possible, avoid needing supports in your model ‎design as it adds time, uses additional material, and may reduce the quality of the finished print. ‎However, sometimes support material is unavoidable and needed to print designs.‎

Discussing Gcode is a good lesson in itself! Gcode is a list of directions for the machines to ‎follow and can be read using a basic text program. Did you know early CNC machines required ‎people to write Gcode manually? Luckily, we have Cura for that now!‎

preparing_7

Preparing a VAWT design in Cura LulzBot Edition to be 3D Printed on a Mini 2‎

CONSTRUCTING OUR PROTOTYPES

In the final part of this stage in the engineering design process, we must construct our ‎prototypes after all parts have been 3D printed. Depending on available resources and the ‎specifications and constraints of the challenge, this step may involve assembling 3D printed ‎parts together, or gluing other materials like popsicle sticks or skewers to parts that have been ‎‎3D printed.‎

Ensure turbine blades have been securely fastened to the DC motors. Avoid using hot glue, as ‎glue around the motor shaft could prevent the motor from spinning. A hot air gun or blow dryer ‎allows PLA to be softened which may help in installation if some tolerances are a little tight.‎

Remember, proper safety procedures should be introduced to students when working in any ‎makerspace or lab environment. When students are around machines such as 3D printers, or ‎using tools to cut or glue materials, students must be informed of potential hazards and taught ‎how to use these resources safely. For reference, see the safety resources offered by ITEEA.‎

TEST AND EVALUATE

TESTING CRITERIA

Before we test our solutions, we need to determine how we can test and evaluate them! First, ‎we need a source of wind. Large circular fans or box fans work well for creating wind in a ‎classroom but remember lab safety procedures when testing your solutions! In addition to ‎observing how our turbines turn in the wind, we can also measure how much electricity is being ‎creating using a voltmeter or multimeter set to DC Volts. Connect the leads of your voltmeter ‎to the wires of your turbine to monitor its output as you test!‎

If your turbine struggles to turn, don’t give up yet! Can something be added or modified to ‎make it perform better? Consider adding cardboard or notecards to the blades to increase their ‎surface area. Or elevate the base to make the turbine taller and catch more wind. No design ‎is perfect, something we will discuss further in the next step!‎

Test each turbine for 2-3 minutes, moving the turbine around to find the best possible angle ‎and air low. Record the amount of volts measured during testing. Also make notes of any ‎changes or modifications you made, as well as where your turbine best performed.‎

In addition to using a voltmeter to measure voltage, LED lights can be connected to the DC ‎motors to show generated electricity by illuminating. Additionally, larger 5V motors may ‎generate enough electricity to charge a phone using a 5v USB adapter (see Modifications in ‎Lesson Introduction).‎

turbine_8

Example 3D Printed Wind Turbine being tested using a multimeter to measure voltage ‎

EVALUATION CRITERIA

‎In addition to testing the performance of our wind turbines, we also must evaluate how well ‎they addressed the defined drawbacks of real wind turbines. Remember, your turbine prototype ‎must address at least one of the defined drawbacks. These drawbacks are cost, looks, noise, and ‎negative wildlife impact.‎

Analyze your wind turbine prototype. Compare your design to the real wind turbines you ‎research in an earlier step. How do you think your wind turbine compares to existing solutions? ‎Do you think it would work well? Why or why not? Record your findings for a later step.‎

REDESIGN

No design is perfect, nor is it ever truly finished. As new technology is developed improvements ‎like cost, speed, performance, or aesthetics can always be made. Consider your findings from ‎testing and evaluating your wind turbine solutions. What worked well? What could be improved?‎

Create a sketch of an improved wind turbine design with changes you would make to allow your ‎wind turbine to perform better, or better meet the evaluation criteria and solve our real-world ‎problem. Your sketch should be neat and label the changes you are making to improve your ‎turbine’s performance. Include why you’ve chosen these changes and how you think they will ‎improve your turbine.‎

RESOURCES:

  • Graph Paper or Technical Drawing Paper [PDF]

COLLABORATE AND SHARE WHAT WE LEARNED

Create a presentation to share with your classmates that includes the following information:‎

  • Name of your Turbine and what type of turbine it is
  • Initial ideas from your brainstorming stage and why you chose the final idea you constructed
  • Any key features or design characteristics
  • Which defined drawback does your turbine address and how?‎‎
  • How did your turbine perform during testing? What worked well and what could be improved?‎‎
  • What changes would you make to your turbine if you were to complete this project again‎

Where possible, included sketches and visuals to share your ideas with your classmates during ‎your presentation. Record and share feedback to your classmates on their designs as you ‎discuss similarities and differences between your designed prototype solutions.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.