Maker.io main logo

Getting Started with Enviro (Pico W Aboard)

225

2023-07-14 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

Enviro is a family of programmable data logging boards, powered by ‎Raspberry Pi Pico W. They're designed to be easy to use and unobtrusive to ‎have around your house, garden, or workplace. They all have a deep sleep ‎mode so that they can be run off battery for a long time without any ‎annoying wires.

This beginner level tutorial has been written to help folks who are brand new ‎to the Pico/RP2040 ecosystem get to grips with how to assemble Enviro kits ‎and how to communicate with Enviro boards using Thonny. There's also ‎a quick start guide on GitHub, which covers some more advanced usage.

This guide will cover:

  • A quick tour of Enviro's features
  • How to power Enviro
  • How to assemble the Enviro accessory kits
  • How to set up (provision) Enviro boards
  • How to communicate with your Enviro using Thonny and what to do if ‎things go wrong!

What You'll Need

Board Overview

Here's a quick tour of the common functions you can find on all Enviro boards ‎so you can find your way around!

board_1

  1. POKE button: wakes the board from sleep to take a reading (if on ‎battery power)‎
  2. ACTIVITY LED (white): pulses gently when the board is awake, blinks ‎quickly when in provisioning mode
  3. WARNING LED (red): lights up or flashes if an error occurs
  4. Qw/ST connector: a convenient way to add extra sensors
  5. Sensors: the collection of sensors that the board gathers data from ‎‎(these vary depending on board type)‎
  6. RESET button: resets the board
  7. Battery connector: compatible with many battery holders and cells
  8. USB connector: for communicating with the board using your computer

Powering Enviro

AA OR AAA BATTERIES

If you got an Accessory kit with your Enviro, it would come with a suitably ‎sized AA or AAA battery pack and a square of Velcro so you can stick it to ‎the back of Enviro if you want.

power_2

Bear in mind that the Pico W's wireless antenna is also on the back, so if ‎you're planning on putting your Enviro somewhere with a weak wireless ‎signal you might not want to position your battery pack directly over the ‎antenna. Also consider that you will need access to the Pico W's BOOTSEL ‎button in the future if you want to update the firmware.

Once you're happy with the placement of your Velcro, press it down and then ‎wait 10 minutes for the adhesive to set. If you have an on/off switch on your ‎battery holder, make sure it's set to 'on'!

enviro_3

LIPO BATTERIES

Enviro has an accommodating input voltage (5.5V max), so you're not limited ‎to AA and AAA batteries. You can also use LiPo batteries to power it, though ‎you should consider the following things:

  • LiPos are not always the best option for really long battery life, as they ‎discharge naturally over time
  • If you're using a soft LiPo and are putting your Enviro somewhere ‎where it might get knocked or bashed, it's probably a good idea to ‎fashion a backplate or enclosure to protect the battery
  • If you've sourced a battery from elsewhere, check that the connector ‎has the red wire going to + and the black wire going to - on our board. ‎Not all batteries have their connectors attached the same way up!‎
  • Enviro boards don't have battery charging circuitry onboard. You'll need ‎to plug your battery into an external LiPo charger (like a LiPo Amigo) to ‎charge it

USB POWER

You don't have to power Enviro by battery of course, you can just feed it with ‎power using a USB micro-B cable or charger if you have one handy. Its power ‎demands are modest, so any charger will work (maybe you have an old ‎mobile phone one that can be repurposed?)

Assembling Accessory Kits

This section will show you how to put everything in the kits together. For the ‎outdoor Enviros (Urban and Weather) you might want to come back to this ‎section when you've got to grips with the software and are ready to install ‎your Enviro in its final location. Troubleshooting hardware at the top of a pole ‎is no fun at all!

ENVIRO URBAN

Enviro Urban comes with a weatherproof enclosure, so you can put it outside ‎without it getting damaged by the elements. It has a bunch of slots in the ‎side to ensure that the outside air gets to the sensors. We used the Velcro that comes with the enclosure to stick our Enviro Urban and battery combo ‎onto the base of the enclosure.

grow_3a

We then used the cable ties to attach it to the fence outside Pirate Towers, ready for checking up on the particulate emissions of passing shipping.

attach_4

ENVIRO WEATHER

The big white box that comes with Enviro Weather contains the wind and rain ‎sensors; you'll first need to attach them to their pole. The wind sensors ‎mount on the double ended arm that goes on the top of the pole (note that ‎the anemometer has a short cable which plugs into the wind vane, so that ‎both wind sensors can then share the same long cable). The rain sensor is ‎mounted on its own arm that comes out of the side of the pole. If you need ‎step by step instructions (with photos) for assembling the sensors, check ‎out Sparkfun's excellent hook-up guide!

weather_5

We left some space in between the wind and the rain arms so we could ‎attach our enclosure on the pole as well, but you might want to go for a ‎different formation - just make sure nothing overhangs the rain sensor, as ‎this will stop it from reading correctly.

It comes with the same weatherproof enclosure as Urban, but with Weather ‎you'll need to mod it a little to be able to plug in the RJ11 connectors from ‎the wind and rain sensor. We used side cutters to remove a few struts from ‎one of the grills one the base of the enclosure to give us room to poke the ‎connectors through, but you could enlarge the existing cable hole with a ‎Dremel or a drill if you prefer (mind your fingers).

enclosure_6

Plug the wires from the wind and rain sensors into the labelled connectors on ‎Enviro Weather. You can tell which sensors the wires come from by peering ‎at the connectors - the RJ11 connector that comes from the wind sensors ‎will have four wires inside it (two for each sensor!) while the rain sensor connector only has two. The wind cable is a bit thicker than the rain cable, ‎because of the extra wires.

wires_7

We used the Velcro that comes with the enclosure to stick our Enviro ‎Weather and battery combo onto the base of the enclosure...

velcro_8

... and mounted the enclosure bracket onto the wind and rain sensors pole ‎using the cable ties that are included. We also tidied up the wires.

mount_9

We then used Jubilee clips to attach the pole to a structure in front of ‎Pimoroni HQ. When you install the wind/rain sensors in their final location, ‎make sure you align the markings on the wind vane to North and that the rain ‎gauge is level.

attach_10

We're hoping the weather will clear up!

ENVIRO GROW

We're planning on making a separate tutorial on Grow in the future to show ‎you how to set up auto-watering and buzzer alerts and such. For the moment ‎though, know that the moisture sensors plug into the three connectors on top of Enviro using the 3 pin cables. The two pin connectors on the underside are ‎for attaching the pumps.

MicroPython and Enviro

Enviro comes with MicroPython firmware pre-installed. It uses our special ‎custom build of MicroPython which includes some tweaks to support fast ‎wakeup, plus built-in drivers to read the sensors.

It also comes with some software pre-loaded so you can get started logging ‎your data super-fast. A neat thing about Enviro is that all the software is ‎stored on the device as MicroPython scripts, so it's easy to open them up and ‎look at every bit of how they work and change things if you want to!

Adafruit.io?

In this tutorial, we'll be posting our data into adafruit.io, an easy-to-use cloud ‎data service. If you want to do the same, we'd suggest signing up for an ‎adafruit.io account before you start setting up your Enviro. You'll need two ‎things during setup: your username and your Adafruit.io key. You can find ‎both of these by clicking on the yellow key at the top right of the adafruit.io ‎site when you're logged in.

data_11

The key is a long number, so we'd recommend copying it to the clipboard of ‎your device now, so you don't have to write it down/type it in later.

Provisioning

To set Enviro up and start logging/posting data places you'll need to go ‎through the provisioning process. You can do this from your phone or other ‎Wi-Fi-enabled device like a tablet or laptop thanks to Enviro's state of the art ‎captive portal technology.

Make sure Enviro has battery or USB power. If it's not been through the ‎provisioning process already, it should automatically go in to provisioning ‎mode and the white ACTIVITY LED will start flashing rapidly (if it's not doing ‎that, try pressing RESET on the back of the board).

On your phone (or another wireless device) go into your internet/wireless ‎settings and find and connect to the wireless network called "Enviro Setup". ‎Here's what that looks like on an Android phone:

settings_12

For us, a browser window opened automatically once our phone was ‎connected to the Enviro network, but on some devices, you might need to ‎click on a message that says 'sign in to network' or similar to get it to pop up ‎‎(you won't actually have to sign into anything).

signin_13

If you've having trouble with your phone or tablet staying connected to the ‎Enviro network, try turning off your mobile internet connection temporarily - ‎your device might be searching for an internet connection and automatically ‎switching to mobile internet.

Once you're connected, the web pages (which are all being served from the ‎Pico W itself) will walk you through how to set up your Enviro. There's more ‎info about what each step does in the quickstart guide.

In our case, we're:

  • Choosing a nickname for our device
  • Giving Enviro our wireless network details so it can talk to the internet
  • Choosing how often to take readings, and how often to report them to ‎your endpoint. We're choosing to take a reading every 15 minutes and ‎upload every reading for now- this is quite a battery intensive schedule, ‎but good for testing and seeing immediate results! We'll show you how ‎to change it later
  • Telling Enviro what endpoint we want to use, we're choosing Adafruit ‎IO. This is where you'll need your username and key from earlier.

Once you've reached the end of the provisioning process, you'll get a 'Reset ‎the board' button. Once you press that, the board will go to sleep for the ‎interval you specified above, and then wake up and take a reading.

‎You might occasionally find that the provisioning website hangs when you ‎move between steps. If this happens, you can refresh the step you're on by ‎clicking on the Enviro banner at the top of the page.

VIEWING YOUR DATA IN ADAFRUIT.IO

To start seeing your readings in Adafruit IO, you'll need to go onto the ‎Adafruit.io website and, on the 'Feeds' tab, create a new group called 'enviro'. ‎Once you've done that, readings should start showing up on this page when ‎your board next posts them. Simples!

chart_14

(Note that we've got a lot of feeds going on here - if you have a free account, ‎you won't be able to create this many).

CONFIGURING A DASHBOARD

Looking at a list of numbers is all very well, but for our human brains to ‎process them usefully, you'll probably want to set up some graphs.

Open up the 'Dashboards' tab in adafruit.io and create a new dashboard. ‎There's nothing here right now, so let’s make it a bit more interesting! Click ‎on the cog icon in the top right of the screen and select 'Create New Block'. ‎There are a bunch to choose from, here we've got some line charts:

dashboard_15

Once you select a type of block, you'll get asked what feed/s to associate it ‎with. You can move blocks around and resize them with 'edit layout'.

We've also used some gauges here to keep track of external and internal air ‎temperature at Pirate Towers, and a stream block with all our feeds added to ‎it to see exactly what's been posted in:

gauges_16

Adafruit IO's free tier lets you store data for 30 days and lets you post up to ‎‎30 data points a minute. This sounds like a lot but bear in mind Enviro returns ‎‎7 or 8 different sensor readings at a time and it bundles multiple sets of ‎readings together (so you might be submitting readings for a couple of hours, ‎but they're all being posted in the same minute). If you exceed this limit, you ‎may see throttling errors start showing up in Enviro's log.

If you want to learn more about Adafruit IO, check out this getting started ‎tutorial.

Troubleshooting

CONNECTING TO ENVIRO WITH THONNY

But what if something isn't working and you have a red light, a static white ‎light or no readings showing up? Here are some things that might help.

Enviro logs everything it does in a file, so you can plug it into your computer ‎to view any errors. To view the files (and program it in MicroPython) you'll ‎need to talk to it through an interpreter - we're using Thonny, which is ‎available for Windows, Mac, or Linux. Here's how to get Enviro and your ‎computer talking to each other.

  • Install the latest version of Thonny. We'd suggest downloading it from ‎the Thonny website, as package managers don't always have the most ‎up to date versions
  • Plug Enviro into your computer if it's not plugged in already
  • Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)'
  • The MicroPython prompt and >>> in the 'Shell' box tells you that Enviro ‎is talking to your computer and is ready to accept instructions. If you ‎don't see the MicroPython prompt in the shell box, try pressing the red ‎stop button in Thonny to interrupt whatever it's doing
  • You'll want the Files window visible so you can see the files on Enviro. ‎If you can't see it, you can open it up with 'View > Files'

files_17

The files in the top box are the ones on your computer, and the ones in the ‎bottom box are the ones on Enviro.

Couldn't Find the Device Automatically?

If your version of Thonny doesn't manage to detect our board automatically ‎‎(or if you have more than one Pico/RP2040 device connected) you might ‎have to specify what port the device is using manually. You can do this by ‎clicking on 'MicroPython (Raspberry Pi Pico) at the bottom right and selecting ‎‎'Configure Interpreter'. Select your device under 'Port'.

VIEWING THE LOGS

Enviro logs everything it does in a file called log.txt - to view it, double click on it ‎‎(you might need to click the stop button first if Enviro is in the middle of doing ‎something). If you can't find any obvious errors in there, try opening ‎up main.py and running it using the green run button - you will then be able to ‎view the output of the code in the 'Shell' window. main.py is the file that runs ‎every time Enviro wakes up.

RESTARTING THE PROVISIONING PROCESS

Incorrect wi-fi details are a common reason why you might get errors. If you ‎get errors that mention the clock, that might also mean that your Enviro ‎hasn't been able to connect to the internet to set the time. If you want to try ‎entering your details again, you can restart the provisioning process. Hold ‎down the POKE button on the front of Enviro and tap the reset button on the ‎back. Release the POKE button when the ACTIVITY light starts flashing ‎rapidly - you should now be able to reconnect to Enviro with your phone and ‎enter different details. If you've followed our instructions above, you might ‎want to take this opportunity to change your upload schedule to one that will ‎make your battery last longer.

EDITING THE CONFIG FILE MANUALLY

You can also change the provisioning details by manually ‎editing config.py using Thonny. Double click on this file to open it up, and when ‎you're done changing things, make sure to save your changes by clicking the ‎save button in the menu bar.

menu_18

We edited our config.py to change our upload_frequency to uploading every four ‎sets of readings - with readings every 15 minutes, that will post our data to ‎Adafruit.io every hour. That should make our battery last a bit longer!

If you're posting into a free adafruit.io account, we'd recommend ‎setting upload frequency to a maximum of 3 to avoid running into upload limits.

FURTHER TROUBLESHOOTING

You can find more troubleshooting suggestions here.

If they don't solve your issue, we'd recommend downloading and flashing the ‎latest version of the Enviro firmware so that you have access to all the latest ‎bug fixes.

Note that this process will delete all the files from your Enviro, so you might ‎want to back up config.py and any saved readings first. You can also follow ‎these instructions to reset your Enviro to factory settings if you accidentally ‎delete or change something.

Next Steps

We hope this guide helps you get started with Enviro! We'll hopefully have ‎more Enviro content for you in the future, we want to hook them up to all the ‎things. Drop us a line on Twitter or the forums and let us know how you're ‎getting on :)

That's all folks!

מק"ט יצרן # PIM629
ENVIRO URBAN (PICO W ABOARD)
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.