Maker.io main logo

Getting Started with Grow

72

2022-02-10 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

Automatic, systematic and hydromatic, Grow is a smart modular monitoring system ‎designed to help you take the best possible care of your plants. It will tell you how well ‎they're hydrated, attract your attention when they need water and, if you want to go a ‎step further, even give them water!‎

In this tutorial, we’ll show you how everything fits together and how to get ‎started monitoring your plants using our monitor application, as well as ‎explaining a little bit about how Grow works. We’ll be starting from the ‎absolute basics, so if you’re already familiar with how to setup a Raspberry Pi ‎and install software for HATs you might want to skip the first few sections.‎

What You’ll Need

  • One of our Grow kits! The base kit of mini HAT and moisture ‎sensors will do if you’d like to monitor your existing plants, or you ‎could pick up one of our chilli or herb starter kits if you’d like to ‎grow your own from scratch
  • A Raspberry Pi! We’ll be using a Pi Zero WH in this tutorial as we’ve ‎designed the Grow HAT Mini to fit nicely on top of the Zero footprint, ‎and it has a pre-soldered header so you won’t need to do any soldering ‎yourself. Grow HAT Mini will also work with other Raspberry Pis as long ‎as they have a 40 pin GPIO header (it’s only the very early ones that ‎don’t)
  • Power supply for Pi. You’ll need a way of powering your Pi - for a Zero ‎we’d recommend this USB micro-B power supply
  • MicroSD card, 8GB or greater. We sell ones pre-installed with ‎Raspberry Pi OS here, which will save you a step later on
  • Standoffs (Optional) To be extra sure that your Grow Mini HAT stays ‎firmly attached to your Pi Zero, you could use a couple of 10mm M2.5 ‎standoffs to secure the board to your Pi
  • Keyboard, mouse, display cables. We’ll be assuming that you’ll be ‎plugging your Pi into a HDMI monitor and keyboard as that’s the ‎easiest way to set everything up (though it’s also possible to set it up ‎‎‘headlessly’ from another computer - we’ve got a tutorial for how to do ‎that here). The Pi Zero WH has a mini HDMI display port, so you'll need ‎either a mini HDMI cable or a standard HDMI cable and a mini HDMI ‎adaptor (like the one in our Zero adaptor kit). To plug in a USB ‎keyboard, you'll likely need a micro-USB adaptor - there's one of those ‎in our Zero adaptor kit too!‎

Rehydrating the "Soil"‎

If you’re using our Chillies or Herbs kits, you’ll need to rehydrate the ‎Cocopress ‘soil’ - it’s worth doing this as your first order of business so that ‎the moisture levels have time to settle down a bit. Stick the three tablets in a ‎watertight container with 100ml of warm water and leave them there until ‎they’ve sucked it all up. Don’t be tempted to rehydrate the tablets in the plant ‎pots, all the water will escape out of the hole in the bottom (ask us how we ‎know). We had good results leaving our soil overnight before we planted our ‎seeds, as it was a bit on the soggy side when freshly generated.‎

rehydrating_1

rehydrating_2

Planting the Seeds

When you’re ready to plant the seeds, divide most of the soil between the ‎three pots, sprinkle the seeds on the surface and cover them with a bit more ‎soil.‎

planting_3

It’s best to put the seeds somewhere warm and light for best results, and ‎once the seedlings are big enough, you’ll want to transfer them to some ‎bigger pots - you can carry on monitoring your favourites with Grow though! ‎There’s a space on the back of the Grow moisture sensors for keeping track ‎of what you’ve planted in which pot, we’ve found whiteboard markers work ‎nicely for labelling and are easy to erase.‎

seeds_4

How to Attach the Grow HAT to Your Pi

To attach Grow HAT Mini to your Pi, push the female header on Grow down ‎onto the male header on the Raspberry Pi as far as it will go, making sure ‎that you've lined all of the pins up correctly and that it’s the right way round. ‎Powering it up when plugged in to the wrong pins could damage the Pi or the ‎Grow HAT Mini.‎

attach_5

You can unpeel the protective plastic film from the screen using the green ‎tab, or you can leave it on to protect it from errant bits of soil if you prefer.‎

Connecting the Moisture Sensors

The moisture sensors come in sets of three, still attached to their sprues. ‎Side cutters are the best way to separate them if you have them but ‎snapping them by hand along the perforation line will work too. You can tidy ‎up the rough edge with sandpaper or an emery board if you want.‎

connecting_6

The moisture sensor cables have three wires and connect to the three pin ‎ports S1, S2 and S3 on top of the Grow HAT Mini - the connectors will only go ‎in one way round, so if you’re having trouble plugging them in try rotating the ‎connector and trying it the other way round rather than forcing them. If you ‎ever need to unplug these little JST connectors, we’d recommend holding ‎onto the moulded plastic connector and gently wiggling - don’t pull them out ‎by the wires, as they can sometimes be a bit delicate.‎

cables_7

The connectors on the bottom of the HAT (P1, P2 and P3) are squarer and ‎only have two pins. They’re for plugging in 5v devices like pumps - we’ll take ‎a look at those in later tutorials!‎

For the capacitive moisture sensors to work best as much of them will need ‎to be surrounded by soil as possible, so it’s best to position the sensors a ‎little way in from the edge of the pot and push them in as far as they can go. ‎The Under/Ground line should be at or above the level of the soil, to avoid the ‎components at the top of the sensors coming into contact with water.‎

Installing the Grow Software

For this part of the tutorial, you'll need a micro-SD card that's been set up ‎with the Raspberry Pi OS operating system, and to be connected to Wi-Fi. If ‎you’re flashing the SD card yourself, we’d recommend using the Raspberry Pi ‎Imager tool, which is available for Windows, Mac, and Linux - you can ‎download it here and there are detailed instructions here if you need them.‎

software_8

If you're a beginner, it's best to use the full 32-bit desktop version of ‎Raspberry Pi OS as it's a little easier to set up and use and includes all the ‎software dependencies that you'll need.‎

Once Raspberry Pi OS is booted, you can configure Wi-Fi through the menu ‎that appears on first boot or by typing sudo raspi-config in the terminal - the Wi-Fi ‎settings are under Network Options>Wireless LAN and you can navigate with ‎the arrow keys and enter. We'd recommend starting with a fresh install of ‎Raspberry Pi OS if you can, but if you you’re using an older image, we’d ‎recommend that you run sudo apt update and sudo apt upgrade in the terminal to get ‎everything up to date.‎

To download and install the Grow software open a terminal (press control-alt-‎t or find it in the Raspberry Pi menu) and then type the following and press ‎enter.‎

curl -sSL https://get.pimoroni.com/grow | bash

The installer will download the other software dependencies it needs to work, ‎make some changes to your config.txt file that let your Pi interface with ‎Grow’s hardware and then ask whether you’d like to install the examples - ‎say yes! It will also ask you if you’d like to install the plant monitor as a ‎service - if you answer yes to this it will make the monitor start automatically ‎when the Pi is turned on, which means you don't need to permanently have ‎your display and keyboard plugged in!‎

Once everything’s installed, type Y to reboot (or sudo reboot ) to reboot your Pi ‎and apply the config changes.‎

If you're having trouble finding the | (pipe) symbol in the middle of the install ‎command, we made a video on where it might be hiding! If you've found it ‎on your keyboard, but it's coming out as a different symbol you might need to ‎change your keyboard layout to US (sudo raspi-config then Localisation Options > ‎Change Keyboard Layout )‎

Using the Monitor

Once you've rebooted, if everything's gone well you should have a screen that ‎looks something like this (though your lines and bars are likely to be in ‎different places!)‎

monitor_9

You’ll see three bars that correspond to your three moisture sensor channels, ‎the colour and height will show you how hydrated each of your pots is, and ‎the black line will show you at what level the alarm will sound. The button ‎next to the little bell will mute the alarm if it’s going off, the alarm will also ‎auto mute if the light sensor detects it’s dark (so it shouldn’t chirp away at ‎night!) The > (A button) at the top left will cycle through the channels and ‎show you more information about each one, as well as a little graph showing ‎the moisture levels over time.‎

bars_10

The % is the current moisture level of your pot, or saturation. The settings ‎button (X button) within the channel menu will take you to a screen where ‎you can alter the moisture level at which the alarm is triggered or disable the ‎channel altogether. You can also alter the wet and dry points using this ‎screen - more on how those work in the calibration section below!‎

settings_11

From the main screen with the three bars, pressing the settings button (X ‎button) will take you to a screen that will let you change global settings, like ‎disabling the alarm and changing up the beep sound.‎

screen_12

Any of the settings that you change in using the menus in the monitor will be ‎saved in a file on your Pi, which will look something like this:‎

menu_13

Starting and Stopping the Service

If you ever need to stop the monitor from running in the background, you can ‎do that with:‎

sudo systemctl stop grow-monitor.service

If you want to permanently disable it, you can type in the terminal:‎

sudo systemctl stop grow-monitor.service

sudo systemctl disable grow-monitor.service

Or to re-enable it:‎

sudo systemctl enable grow-monitor.service

sudo systemctl start grow-monitor.service

If you’re running the monitor as a service and want to edit your settings file ‎directly you can do that with:‎

cd /etc/default

sudo nano grow

‎(and ctrl-X to exit Nano when you're done editing). It's a good idea to stop the ‎service before you start editing the settings file and start it again afterwards.‎

How the Moisture Sensors Work

Grow's capacitive moisture sensors work using Pulse-Frequency ‎Modulation - they report the moisture level by sending out a regular pattern ‎of on-off electrical pulses, with varying frequency. If you looked at the pattern ‎of pulses with an oscilloscope, you would see a square wave like this:‎

report_14

The Pi (via Grow HAT Mini) interprets the frequency of the pulses as a Hz ‎value between about 0 and 30. A smaller number is wetter, and a larger ‎number is drier.‎

Calibration (Important!)‎

The Hz values that Grow’s sensors report is relative rather than absolute ‎moisture readings, and are likely to vary depending on soil type, pot size, ‎sensor position, and ambient conditions. We’ve included some default values ‎for ‘wet points’ and ‘dry points’ - but you’ll likely get better results if you ‎calibrate the sensors by taking your own base readings. Setting your own wet ‎points and dry points will also mean you can tailor your conditions to different ‎types of plants - a cactus will likely have different opinions about what it ‎considers to be ideal soil conditions to a basil seed!‎

We’d recommend letting your soil dry out to the point where you think it really ‎needs watering, and then setting the ‘dry point’ reading in the channel ‎settings to match. You can then water it to the desired level, and then set the ‎‎‘wet point’ reading. You’ve now got an upper and lower limit of what Grow ‎considers to be acceptable soil conditions!‎

calibrate_15

In the channel settings you can also change the % at which the alarm tells ‎you it’s time for watering to happen - if you want to wait until everything’s at ‎the minimum acceptable moisture level set your alarm level to 0% or set it at ‎‎20% or 40% if you want a bit of a heads up before everything dries up.‎

Next Steps

We hope that gets you started monitoring your plants with Grow - tweet ‎us @pimoroni and let us know what you’ve been planting! We’ve got another ‎tutorial planned to show you how to take your Grow setup to the next level by ‎incorporating pumps and auto-watering, so keep an eye out for that.‎

מק"ט יצרן # PIM510
GROW KIT
Pimoroni Ltd
מק"ט יצרן # SC0251L
32GB NOOBS MICROSD CARD
Raspberry Pi
מק"ט יצרן # SC0532
CBL HDMI-D M-MIC HDMI-A M 2M
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.