Maker.io main logo

Getting Started with Inky Frame

249

2023-01-05 | By Pimoroni

License: See Original Project Wifi

Courtesy of Pimoroni

Guide by Pimoroni

Inky Frame is a luscious, 7 colour, 5.7" (600 x 448 pixel) programmable E Ink ‎display, powered by Raspberry Pi Pico W. It can go into a deep sleep mode ‎between updates to preserve battery and can be woken back up with a ‎button press or on a timer using the onboard Real Time Clock (RTC).‎

This beginner friendly tutorial will cover:‎

  • how to plug everything in
  • how to get started programming Inky Frame with MicroPython and ‎Thonny
  • how to get to grips with our examples
  • how to display images
  • some troubleshooting suggestions

What you'll need

  • An Inky Frame
  • A micro-USB cable (for programming)
  • A micro-SD card (required for some of the wireless examples)
  • Some sort of battery if you want to disconnect Inky Frame from your ‎computer - we'll discuss a few options and their pros and cons!
  • A computer to program from (Windows, Mac or Linux/Raspberry Pi)‎

Batteries

AA OR AAA BATTERIES

The easiest way to supply Inky Frame with power is via some good old-‎fashioned double or triple A batteries, connected in series. You'll need a ‎battery holder with a JST-PH connector to be able to plug it in. We'd ‎recommend a 3 x AA or 3 x AAA battery pack which should give you plenty of ‎juice to keep going for a good long time.‎

LIPO / LIION BATTERIES

Alternatively, you could power Inky Frame from a LiPo battery. Our hard case ‎Galleon LiPo batteries make for a really neat power solution combined with ‎Inky Frame's deep sleep capability, though you might prefer something with ‎more capacity for longer battery life.‎

lipo_1

A few more things you should consider if you're using a LiPo:‎

  • If you're using a soft LiPo battery you might want to consider ‎fashioning a backplate or case to protect it
  • There's no battery protection included on Inky Frame, so you should ‎only use it with LiPo batteries that include internal protection (all ours ‎do)
  • If you've sourced a battery from elsewhere, check that the connector ‎has the red wire going to + and the black wire going to - on our board. ‎Not all batteries have their connectors attached the same way up!
  • Inky Frame doesn't have battery charging circuitry onboard. You'll need ‎to plug your battery into an external LiPo charger (like a LiPo Amigo) to ‎charge it
  • If you wanted to add USB-C battery charging capability (and a power ‎button!) to Inky Frame you could add a LiPo Amigo Pro to the back ‎‎(you'll also need one of these cables)

Assembling the Inky Frame Accessory Kit

assembling_2

Our Accessory Kit contains legs to let your Inky stand up, an AA battery pack ‎and fixings, a USB cable and an SD card. Here's how to put it all together!‎

ATTACHING THE LEGS

From the front, poke the rounded screws through the larger set of holes at ‎the bottom of Inky Frame.‎

attach_3

Then screw the legs onto the screw threads!‎

screw_4

INSERTING THE SD CARD

The SD card goes into the slot on the back of Inky Frame (it will only go in ‎one way). It's a spring-loaded slot, so should you ever want to remove it you'll ‎need to push it in to get it to pop out.‎

ATTACHING THE BATTERY PACK

Our Inky Frame accessory kit comes with some Velcro for sticking the ‎battery pack on. Before you start sticking things down, experiment a little bit ‎with the positioning of the battery pack:‎

  • If you're planning on hanging Inky Frame from a hook, you'll want to ‎make sure the battery pack is balanced in the middle to avoid it ‎hanging lopsided
  • If you want to be able to use the on/off switch on your battery pack, ‎make sure you stick the Velcro to the other side!
  • Make sure the reset button is accessible and not squashed down by ‎the battery pack
  • Once you're happy with the placement, press the squares down ‎‎(avoiding pressing directly on the screen) and then wait 10 minutes for ‎the adhesive to set

pack_5

placement_6

MicroPython and Inky Frame

Our custom MicroPython build is the easiest way to get started with Inky ‎Frame. It comes with a built-in tiny graphics library called PicoGraphics, which ‎contains lots of tools for drawing on Inky Frame's screen, including drawing ‎text and shapes, rendering images, and generating QR codes!‎

Inky Frame ships without firmware (although we do put an image on the ‎screen as part of our testing process) - you'll need to install our custom ‎MicroPython build on it before you can run code on it.‎

INSTALLING MICROPYTHON

First of all, you'll need to download our most recent batteries included ‎MicroPython image, and copy it to the Pico W. We'd recommend ‎using v1.19.6 or later, as it includes a fix for an annoying bug that can crop ‎up when saving code that connects to wireless as main.py.‎

If you're brand new to Raspberry Pi Pico/RP2040s, you might find the step by ‎step instructions in our Getting Started with Raspberry Pi Pico tutorial useful ‎‎- it will show you how to install our custom MicroPython build and goes into ‎more detail about how to use Thonny. Here's a quick TLDR!‎

assets_7

  • Connect Inky Frame to your computer with a USB cable
  • Hold down the BOOT button of Inky Frame, and then tap the RESET ‎button. This will put it into bootloader mode, and it should appear as a ‎drive on your computer called RPI-RP2
  • Copy the .uf2 file to the RPI-RP2 drive - once you've done that Inky ‎Frame will reboot

Programming Inky Frame with Thonny

Once MicroPython is installed, Inky Frame won't show up as a drive on your ‎computer anymore. To program it, you'll need to talk to it through an ‎interpreter - we're using Thonny, which is available for Windows, Mac or Linux.‎

  • Install Thonny
  • Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)'
  • Plug Inky Frame into your computer, if it's not plugged in already
  • The flashing cursor next to the >>> in the 'Shell' box tells you that Inky ‎Frame is talking to your computer and is ready to accept instructions. If ‎you don't see the MicroPython prompt in the shell box, try pressing the ‎red stop button in Thonny to interrupt whatever it's doing

thonny_8

Couldn't find the device automatically?‎

Our version of Thonny didn't manage to detect our board automatically - ‎probably because the Pico W image is based on brand new v1.19 ‎MicroPython. We had to specify the port our device was using; you can do ‎this by clicking on 'MicroPython (Raspberry Pi Pico) at the bottom right and ‎selecting 'Configure Interpreter'. Select your device under 'Port' - ours was ‎showing up as 'COM5.‎

options_9

LIGHTING UP THE ACTIVITY LED

As a test that everything's working OK, let's light up the activity LED (that's ‎the one with the flag next to it). Enter the following code line by line in the ‎REPL (that's the bottom 'Shell' box in Thonny).‎

Copy Code
from machine import Pin

led = Pin(6, Pin.OUT)
led.value(1)

Let's turn off the LED again, to be tidy!‎

Copy Code
led.value(0)

You can light up the other LEDs in the same way, just change the pin number ‎in the code above. Inky Frame's LEDs are connected to the following pins on ‎the Pico W:‎

Activity LED - 6‎

Connect LED - 7

A, B, C, D, E - 11, 12, 13, 14, 15‎

You can also set the brightness of the LEDs to values between 0 and 1 using ‎PWM.‎

WRITING TEXT ON THE SCREEN

Here's a simple example of how to display text on the E Ink screen using the ‎PicoGraphics library. Copy and paste this code into a new tab in Thonny, and ‎then click on the 'run' button.‎

Copy Code
from picographics import PicoGraphics, DISPLAY_INKY_FRAME
display = PicoGraphics(display=DISPLAY_INKY_FRAME)

BLACK = 0
WHITE = 1
GREEN = 2
BLUE = 3
RED = 4
YELLOW = 5
ORANGE = 6
TAUPE = 7

display.set_pen(WHITE)
display.clear()
display.set_pen(BLACK)
display.text("Hello Inky", 0, 0, 600, 4)
display.update()

The first two lines set up the Inky display - you'll need to start any code that ‎uses the screen like this.‎

The rest of the code does this:‎

  • The set_pen line tells your program what pen you want to start writing ‎with. Inky Frame has seven pen colours to choose from (plus a ‎mysterious eighth 'cleaning' colour, taupe)
  • display.clear() fills the whole screen with the last selected pen colour - ‎we're using it here to start with a white background
  • display.text writes text to the screen buffer. When using a bitmap font, ‎the '0, 0' is the x/y co-ordinates of the top left of the text. '600' is when ‎text will start wrapping onto the next line (so needs to be the width of ‎the screen in most cases). The final number '4' is the scale of the text, ‎reduce or increase it to shrink or embiggen!‎
  • display.update updates the screen (you can draw multiple things to your ‎screen buffer before triggering an update)

display_10

The default font is bitmap6, which is all uppercase and a little small and blocky. ‎Switching to bitmap8 gives you upper and lower case and a bit more definition ‎‎(it also includes more special characters like °)‎

Copy Code
from picographics import PicoGraphics, DISPLAY_INKY_FRAME
display = PicoGraphics(display=DISPLAY_INKY_FRAME)

BLACK = 0
WHITE = 1
GREEN = 2
BLUE = 3
RED = 4
YELLOW = 5
ORANGE = 6
TAUPE = 7

display.set_pen(WHITE)
display.clear()
display.set_pen(BLACK)
display.set_font('bitmap8')
display.text("Hello Inky", 0, 0, 600, 4)
display.update()

hello_11

MORE DRAWING FUNCTIONS

There are more functions in the library for using vector fonts and drawing ‎individual pixels, lines, and shapes. Check out the PicoGraphics function ‎reference for more info!‎

Running the Examples

You can find all the Inky Frame examples at the link below:‎

Click on one to open it up and copy and paste the code into a new tab in ‎Thonny (if you click the 'raw' button on GitHub first it will make it easier to ‎copy and paste). Press the green run button in Thonny to run the code.‎

INSTALLING SUPPORTING LIBRARIES

To run the wireless examples (and the ones using the SD card) you'll need to ‎copy some extra libraries to your Pico. You could copy and paste the files ‎from the common folder on GitHub and save them to your Pico one by one if ‎you wanted to, but we're going to download the whole lot as it's easier to ‎move multiple files around.‎

On the front page of the pimoroni-pico repo, click on the green code button ‎and select 'download ZIP' - this will download the whole repo to your ‎computer. Unzip it somewhere where you can find it easily.‎

front_12

Then, switch back to Thonny. For the next step you'll need to have the Files ‎window visible in Thonny, you can open it up with 'View > Files'.‎

The top box can be used to browse the local files in on your computer, and ‎the bottom box shows the files on Inky Frame. Find your unzipped repo and ‎navigate to micropython/examples/common in the top box.‎

top_13

You'll need a bunch of stuff out of the common/lib folder to run the examples, ‎so you might as well grab the whole thing - right click on lib in the top box and ‎select 'Upload to /' to transfer it to your Pico. You'll also ‎need network_manager.py and WIFI_CONFIG.py, so right click on those and upload ‎them to your Pico as well.‎

Once you're done, the files on your Pico W should look something like this:‎

files_14

Note that network_manager.py and WIFI_CONFIG.py should be in the root directory of ‎your Pico W, and the other libraries should be inside a folder called lib.‎

ADDING WI-FI CREDENTIALS

For the examples that use wireless to work, your Pico W will need to know ‎your wireless network details. Double click on the copy of WIFI_CONFIG.py that's ‎on your Pico W to open it up in Thonny. Add your network's SSID, password ‎and country code (if you're in the UK like us then your country code should be ‎‎"GB" - if not check this list). Note that SSID and password are case sensitive! ‎Once that's done, click save.‎

creds_15

If your credentials are correct, the wireless examples should now work!‎

Displaying images

Pirate flavour MicroPython can now decode jpegs, woohaa! Here's how to get ‎an image onto that beautiful Inky Frame screen.‎

You should resize your images to 600 x 448 pixels (or smaller) using an ‎image editor (we're using GIMP) before copying them across to Inky Frame. ‎When exporting your jpeg, we found we had to open up 'advanced options' ‎and untick the 'progressive' option for it to work with jpegdec. We saved our ‎images at 70% quality to help keep the file size down.‎

navigate_16

Navigate to your jpeg in the top Files window, right click on it and upload it to ‎your Pico W. Here's how to show the image:‎

Copy Code
from picographics import PicoGraphics, DISPLAY_INKY_FRAME
from jpegdec import JPEG

display = PicoGraphics(display=DISPLAY_INKY_FRAME)
j = JPEG(display)

j.open_file("jwst1.jpg")
j.decode()
display.update()

You can find demo images to use, plus an offline photo frame example which ‎switches between images and goes to sleep when on battery power here (or ‎in micropython/examples/inky_frame/image_gallery if you downloaded a local copy). ‎Thanks Webb Space Telescope, we really loved your photos. Who'd have ‎thought it would be possible to see the Raspberry Pi Picow from 1.5 million ‎kilometers away?‎

PicoGraphics will dither your image into the eight colours that are available on ‎Inky Frame to save RAM. When prepping our images, we found we got best ‎results by boosting the saturation and black levels up a bit. In GIMP, you can ‎do this with 'Colors' > 'Saturation' and 'Colors' > 'Exposure'.‎

sat_17

sat_18

Next Steps

Hopefully, this tutorial will have helped you grok the basics of getting text and ‎images onto Inky Frame - next stop The Interwebs! Drop us a line on ‎Twitter or on our forums and let us know what you're using it for - we'd love ‎to know!‎

Troubleshooting

HOW DO I MAKE AN EXAMPLE RUN WHENEVER INKY FRAME'S POWERED UP?‎

Save your example as main.py if you want it to run automatically every time ‎Inky Frame is powered up or reset. It's a good idea to test your code is ‎working as expected before you do this, as a malfunctioning main.py can lock ‎up your Pico and stop it from communicating with Thonny.‎

HOW DO I FACTORY RESET?‎

If you do find yourself in a sticky main.py situation, you can delete all your ‎programs from Inky Frame's flash memory and start again from scratch by ‎downloading this special .uf2 file and copying it to Inky Frame whilst it's in ‎bootloader/DFU mode. Once you've done that, you'll need to copy the ‎MicroPython image across again.‎

You may also find clearing the flash to be useful if you encounter problems ‎after upgrading to the newest version of MicroPython - just make sure you ‎save any code you've been working on to your computer first!‎

BATTERY PROBLEMS?‎

If Inky Frame is plugged in via USB, it will never go into deep sleep mode. It ‎will spring into life and attempt to run main.py as soon as it has USB power, ‎just like any Pico/RP2040 board running MicroPython.‎

However, if you're powering Inky Frame by battery things will work a little ‎differently - the hardware level power saving features will kick in, which can ‎be a bit confusing and make it look like you have a duff battery.‎

Once you hit reset on a battery powered Inky, you'll have to press one of the ‎buttons to trigger it to wake up and run main.py. If this doesn't seem to be ‎working, try holding one of the front buttons down for a second or two - it ‎needs a fairly solid press to wake it up (this is because there's a short delay ‎whilst MicroPython starts up, so it can miss quick button presses).‎

You can force Inky Frame to stay awake (which is useful when you're doing ‎things with wireless, for example) by holding the vsys enable pin, like this:‎

Copy Code
import machine

HOLD_VSYS_EN_PIN = 2

# set up and enable vsys hold so we don't go to sleep
hold_vsys_en_pin = machine.Pin(HOLD_VSYS_EN_PIN, machine.Pin.OUT)
hold_vsys_en_pin.value(True)

You can send it back to sleep by reversing the direction of this pin:‎

Copy Code
hold_vsys_en_pin.init(machine.Pin.IN)

SD CARD PROBLEMS?‎

We've found that MicroPython can be slightly fussy with SD cards, especially ‎larger ones. If you're having trouble reading from your SD card, try ‎reformatting it with FAT and a small block size - we managed to get most SD ‎cards we tried working like this (though we did find a few that stubbornly ‎refused to play).‎

RAM PROBLEMS?‎

Using the wireless stack currently uses lots of the Pico W's available RAM - ‎which can be a problem when driving a large display. We're hoping for this ‎situation to improve as MicroPython for Pico W enters a less beta state, but ‎for the moment at least you'll need to be conscious of RAM usage when ‎using wireless and Inky Frame together - the good news is that PicoGraphics ‎is written with conservation of RAM in mind!‎

Things that we've found that help avoid memory errors (like ENOMEM) include:‎

  • making sure you close HTTP sockets after opening them
  • downloading images to your SD card rather than straight into RAM
  • incorporating garbage collection (gc.collect) into your code - see this ‎example for a demonstration!‎

RTC PROBLEMS?‎

Some of our examples use the Real Time Clock's timer function to wake up ‎Inky every so many seconds. If you try and increase the number of seconds ‎over 255, you may see an error like this:

Copy Code
ValueError: ticks out of range. Expected 0 to 255

‎This is because the RTC is only able to keep track of a certain number of ‎‎'ticks'. It is possible to make it sleep for longer though - check out this GitHub ‎issue for some suggestions of how to do that!‎

That's all folks!‎

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.