Maker.io main logo

Getting Started with Tufty 2040

217

2023-08-24 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

Tufty 2040 is a RP2040-powered programmable badge with a swish 2.4" ‎colour LCD screen.‎

This tutorial will show you how to plug things in, how to get to grips with the ‎built in demo programs and how to start programming your Tufty with ‎MicroPython.‎

What you'll need

  • A Tufty 2040
  • A USB-C cable (for programming)
  • Some sort of battery if you want to disconnect Tufty from your ‎computer and update the display on the go - we'll discuss a few options ‎and their pros and cons!
  • A computer to program from (Windows, Mac, or Linux/Raspberry Pi).‎

Batteries

AA OR AAA BATTERIES

The easiest way to supply Tufty with power is via some good old-fashioned ‎double or triple A batteries, connected in series. You'll need a battery holder ‎with a JST-PH connector to be able to plug it in. We'd recommend a 3 x AAA ‎battery pack which should give you enough juice to keep going for a few days ‎conferencing without being too bulky. 3 x AA batteries will also work!‎

‎2 x AA or AAA batteries will only work if you're using non rechargeable ‎batteries - the voltage from 2 rechargeable (NiMH) batteries won't be ‎enough for Tufty's screen.‎

If you're using AA or AAA batteries, you'll see the backlight on the screen ‎dimming when the batteries run low (below 2.9V).‎

ASSEMBLING THE TUFTY ACCESSORY KIT

If you have our Tufty accessory kit, it will come with some Velcro for sticking ‎the battery pack on. Before you start sticking things down, experiment a little ‎bit with the positioning of the battery pack:‎

  • If you're hanging Tufty from a lanyard, you'll want to make sure the ‎battery pack is balanced in the middle to avoid your badge hanging ‎lopsided. We positioned ours so it was just above the JST connector on ‎the board.
  • The on/off switch on the battery pack doesn't need to be accessible as ‎Tufty has its own power button. We put our Velcro on the switch side ‎of the battery pack as it's a little easier to open that way. Just make ‎sure the switch is set to on before you stick it down!
  • Once you're happy with the placement, press em down (avoiding ‎pressing directly on the screen) and then wait 10 minutes for the ‎adhesive to set. Then you're ready to go!‎

battery_1

battery_2

USB BATTERY PACK

USB battery packs are probably a bit heavy for dangling round your neck, but ‎they might be useful for powering Tufty from your pocket or your bag, if you ‎don't want to stick on a battery pack.‎

LIPO/LIION BATTERIES

If the person wearing the badge is an adult who knows what they're doing ‎with LiPo batteries, it's possible to power Tufty from a LiPo battery. Our hard ‎case Galleon LiPo batteries make for a really neat power solution, though ‎you might prefer something larger for longer battery life (400 mAh will only ‎give you around 4 hours battery life, with the screen on at full brightness).‎

pack_3

A few more things you should consider if you're using a LiPo:‎

  • If you're using a soft LiPo battery, it's a very good idea to 3D print (or ‎otherwise fashion) a backplate or case to protect it whilst being worn
  • There's no battery protection included on Tufty 2040, so you should ‎only use it with LiPo batteries that include internal protection (all ours ‎do)
  • If you've sourced a battery from elsewhere, check that the connector ‎has the red wire going to + and the black wire going to - on our board. ‎Not all batteries have their connectors attached the same way up!‎
  • Unlike some of our other boards, Tufty 2040 doesn't have battery ‎charging circuitry onboard. You'll need to plug your battery into an ‎external LiPo charger (like a LiPo Amigo) to charge it

MicroPython and Tufty 2040‎

Our new spruced up Pico Graphics library gives you lots of tools for drawing ‎on Tufty's screen, including drawing text and shapes, rendering images, and ‎generating QR codes!‎

INSTALLING TUFTY FLAVOURED MICROPYTHON

Your Tufty will come preloaded with MicroPython and a suite of examples, ‎but for the all the latest features, tweaks and fixes, download yourself ‎the newest version. You'll need to be running version 1.19.0 or later to have ‎access to all the new Tufty/PicoGraphics stuff.‎

If you're brand new to Raspberry Pi Pico/RP2040s, you might find the step by ‎step instructions in our Getting Started with Raspberry Pi Pico tutorial useful ‎‎- it will show you how to install our custom MicroPython build and goes into ‎more detail about how to use Thonny . Here's a quick TLDR!‎

  • Download the most recent MicroPython .uf2 from the Releases page of ‎our pimoroni-pico Github repository. You'll want to download the ‎special version for Tufty 2040, to give you access to all that lovely extra ‎flash storage
  • Connect Tufty to your computer with a USB-C cable
  • Hold down the BOOT button of Tufty 2040, and then tap the PWR ‎button to turn it on. This will put it into bootloader mode, and it should ‎appear as a drive on your computer called RPI-RP2
  • Copy the .uf2 file to the RPI-RP2 drive - once you've done that Tufty ‎‎2040 will reboot.‎

NAVIGATING THE TUFTY DEMO REEL

We've preloaded Tufty with a little menu program and some examples to ‎show you what's possible. Navigate the menu with the arrow up and down ‎buttons and press A to open up the example. If you save additional ‎MicroPython programs to your Tufty, they'll show up automatically in the ‎menu. You'll need to turn Tufty off and on with the power button to return to ‎the menu once you're done with an example.

‎If you'd like to modify or replace it, the menu program is saved ‎as main.py (MicroPython runs any script named main.py automatically on boot.)‎

Programming Tufty with Thonny

Once MicroPython is installed, Tufty won't show up as a drive on your ‎computer anymore. To program it, you'll need to talk to it through an ‎interpreter - we're using Thonny, which is available for Windows, Mac, or ‎Linux.‎

  • Install Thonny
  • Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)'
  • Plug Tufty into your computer if it's not plugged in already. Because ‎main.py will already be running, you'll need to stop it with the stop ‎button in Thonny before sending it any instructions
  • After you press stop, you should get something like this a MicroPython ‎prompt that looks something like this. The flashing cursor next to ‎the >>> in the 'Shell' box tells you that Tufty 2040 is talking to your ‎computer and is ready to accept instructions

program_4

Couldn't find the device automatically?‎

Thonny didn't manage to detect our board automatically - probably because ‎the Tufty image is based on brand new v1.19 MicroPython . We had to ‎specify the port our device was using, you can do this by clicking ‎on MicroPython (Raspberry Pi Pico) at the bottom right and ‎selecting Configure Interpreter. Select your device under 'Port' - our Tufty ‎was showing up as 'COM20'.

options_5

LIGHTING UP THE ONBOARD LED

You can light up the white onboard LED with the following code - enter it line ‎by line in the REPL (that's the bottom 'Shell' box in Thonny.)‎

Copy Code
from machine import Pin

led = Pin(25, Pin.OUT)
led.value(1)

Let's turn off the LED again, to be tidy!‎

Copy Code
led.value(0)

‎You can also set the brightness of the LED to values between 0 and 1 using ‎PWM.‎

USING THE BUTTONS

The built in example button_test.py shows a simple way to read the buttons on ‎Tufty using one of our helper functions. Fancier, interrupt methods are ‎available! (Get Started with MicroPython on Raspberry Pi Pico covers a few ‎different methods).‎

LIGHT SENSING

The light sensing phototransistor on Tufty is wired up to one of the ADC ‎‎(analog to digital converter) pins. Copy and paste this code into a new tab in ‎Thonny, and then press the green 'run' button.‎

Copy Code
from machine import ADC, Pin
from time import sleep

lux_pwr = Pin(27, Pin.OUT)
lux_pwr.value(1)

lux = ADC(26)

while True:
reading = lux.read_u16()
print(reading)
sleep(1)

Readings should start appearing in the bottom shell box. If you go to View > ‎Plotter in Thonny it will show you the results from the light sensor on a graph.‎

WRITING TEXT ON THE SCREEN

Here's a simple example of how to display text on the screen using our new ‎PicoGraphics library.‎

Copy Code
from picographics import PicoGraphics, DISPLAY_TUFTY_2040
display = PicoGraphics(display=DISPLAY_TUFTY_2040)

WHITE = display.create_pen(255, 255, 255)

display.set_pen(WHITE)
display.text("Hello Tufty", 0, 0, 320, 4)
display.update()

The first two lines set up Tufty's screen, you'll need to start any code that ‎uses the screen like this.‎The rest of the code does this:‎

  • create_pen creates a pen colour to write with (255, 255, 255 is the RGB ‎colour code for white. More colours are available!)
  • The set_pen line tells your program that we want to start writing with the ‎white pen
  • display.text writes text to the screen buffer. When using a bitmap font, ‎the '0, 0' is the x/y co-ordinates of the top left of the text. '320' is when ‎text will start wrapping onto the next line (so needs to be the width of ‎the screen in most cases). The final number '4' is the scale of the text, ‎reduce or increase it to shrink or embiggen!
  • display.update updates the screen (you can draw multiple things to your ‎screen buffer before triggering an update)

screen_6

If you try writing more text to the screen, you will find that things you've ‎drawn to the screen buffer will stick around until you overwrite them. To clear ‎the screen and start with a clean slate (we'll first need to create a new black ‎pen):‎

Copy Code
BLACK = display.create_pen(0, 0, 0)

display.set_pen(BLACK)
display.clear()

The default font is 'bitmap6', which is all uppercase and a little small and ‎blocky. Switching to 'bitmap8' gives you upper and lower case and a bit more ‎definition (it also includes more special characters like °.)

Copy Code
from picographics import PicoGraphics, DISPLAY_TUFTY_2040
display = PicoGraphics(display=DISPLAY_TUFTY_2040)

WHITE = display.create_pen(255, 255, 255)

display.set_pen(WHITE)
display.set_font('bitmap8')
display.text("Hello Tufty", 0, 0, 320, 4)
display.update()

update_7

MORE DRAWING FUNCTIONS

There are more functions in the library for using vector fonts and drawing ‎individual pixels, lines, and shapes. Check out the PicoGraphics function ‎reference for more info!‎

Customising the Examples

To edit the names and other details in the examples, you can open up the .py ‎example files on the device and edit them. To see the files on Tufty, you will ‎need to have the Files window visible in Thonny, you can do this with View > ‎Files.‎

edits_8

The top box can be used to browse the local files in on your computer, and ‎the bottom box shows the files on Tufty. Double click on one of the examples ‎to open it up in Thonny, and 'save' once you're done editing ( or 'run' if you ‎want to run the code straight away). Here's what editing the text ‎in wavy_message.py looks like!

top_9

You can also copy files from your computer to Tufty by right clicking on them ‎in the top window and choosing 'Upload to/' (useful for copying across things ‎like images.)‎

DISPLAYING IMAGES

We are delighted to finally have jpeg decoding included in Pirate flavour ‎MicroPython. Here's how to get some cat pics on your Tufty, stat!‎

You should resize your images to 320 x 240 pixels (or smaller) using an ‎image editor (we're using GIMP) before copying them across to Tufty. When ‎exporting your jpeg, we found we had to open up 'advanced options' and ‎untick the 'progressive' option for it to work with jpegdec.‎

display_10

Navigate to your jpeg in the top Files window, right click on it and upload it to ‎your Tufty. Here's how to show the image:‎

Copy Code
from picographics import PicoGraphics, DISPLAY_TUFTY_2040
from jpegdec import JPEG

display = PicoGraphics(display=DISPLAY_TUFTY_2040)
j = JPEG(display)

j.open_file("jorts.jpg")
j.decode()
display.update()

‎‎(Here is the 320 x 240 photo of Jorts if you would like to test with it. You ‎should also go follow him on Twitter.)‎

The default PicoGraphics colour palette is 8 bit, so your photo will be dithered ‎into 256 colours to save RAM. Other palette options are available - consult ‎the function reference for details.‎

Help - I deleted something!

‎Don't panic! You can find the Python code for all the baked in examples (plus ‎a few extras) on Github.‎

Next steps

Once you've got to grips with Thonny and our examples, why not add one of ‎our breakouts into the mix to give your Tufty some sensor smarts. If your ‎breakout has a Qw/ST connector, you can plug it straight into Tufty with ‎a Qw/ST cable (if not, you can use one of these adaptors.) There's a list of ‎which of our breakouts are currently supported in our MicroPython build here.‎

Drop us a line on Twitter to tell us what you and Tufty get up to - we'd love to ‎know!‎

Troubleshooting

HOW DO I FACTORY RESET?‎

If you need to delete all your programs from Tufty's flash memory and start ‎again from scratch, you can do that by downloading this special .uf2 file and ‎copying it to Tufty whilst it's in bootloader mode. Once you've done that, you'll ‎need to copy the Tufty MicroPython image across again.‎

You may also find clearing the flash to be useful if you encounter problems ‎after upgrading to the newest version of MicroPython - just make sure you ‎save any code you've been working on to your computer first!‎

That's all folks!‎

מק"ט יצרן # MAG71
GET STARTED WITH MICROPYTHON ON
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.