Maker.io main logo

Green Energy-Adding a Solar Panel to the Kitronik Smart Greenhouse

36

2021-06-24 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Greenhouses are used for growing plants. Plants rely on an amount of sunlight to grow, and so we can also use some of this sunlight to power the control system. Harvesting sunlight to product electricity is possible by using solar panels.

green_1

The Kitronik Smart Greenhouse kit includes a 5697 Environmental Control Board is designed to provide both environmental sensor inputs to, and control outputs from a BBC micro:bit.

bit_2

Adding a Solar Panel to the Kitronik Smart Greenhouse:

The board is powered by electricity, and can be powered by a mains adapter, or by batteries. Batteries are ideal if there is no connection to mains electricity available, but they are limited in capacity.

The design includes a solar panel input, which can be used in conjunction with rechargeable batteries to produce a solar powered control board. It has a reverse blocking diode on board - to prevent the discharge of the batteries when the panel is not sufficiently illuminated to charge them. For more information on Solar power see this guide.

The solar add on kit (56113) consists of a Solar Cell and 3 NiMH rechargeable batteries.

battery_3

The solar panel (3608) is capable of outputting up to 130mA. It is generally accepted that NiMH rechargeable batteries can be left on charge indefinitely at a rate of 1/10 of the capacity of the battery. The batteries (2278) are 1300mAH - which is a good match for this 1/10C charge rate.

How to Assemble the Solar Add on Kit:

Firstly, insert the 3 NiMH AA batteries into the battery cage on the reverse of the Environmental Control board.

battery_4

Then connect up the Solar Panel. The Solar panel comes with 2 leads – Red and Black in colour. The Red lead connects to the Solar Panel Input terminal marked +.

connect_5

Tighten the screw terminal and connect the Black lead to the terminal marked -, also tightening its terminal.

tight_6

The Kit is now assembled, and ready to power your environmental control board. You can confirm this by switching the Environmental control board on – its Power LED should light up.

solar_7

A simple stand can be created to hold the solar panel. This DXF contains a simple stand designed to be laser cut from 3mm thick material, such as acrylic or ply.

stand_8

By

David Sanderson,

MEng (hons) DIS, CEng MIMarEST

Technical Director at Kitronik

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof without Kitronik's prior written consent.

מק"ט יצרן # 5697
KITRONIK ENVIRONMENTAL CONTROL B
Kitronik Ltd.
מק"ט יצרן # 56113
SOLAR CELL KIT FOR THE KITRONIK
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.