Maker.io main logo

How To Take Multiple RFID Readings Simultaneously

281

2025-02-11 | By SparkFun Electronics

License: See Original Project RFID / NFC

Courtesy of SparkFun

Guide by Chowdah

Introduction

In this tutorial, we'll show you how to set up the SparkFun Simultaneous RFID Reader to ‎take multiple, if not nearly unlimited, RFID readings simultaneously by connecting either ‎the M7E Hecto or M6E Nano directly to your computer using a USB-C connection and ‎running Universal Reader Assistant (URA) software, which provides a simple and effective ‎interface for configuring and managing your RFID reader. This is really useful for ‎applications like measuring attendance at events, as well livestock management etc.‎

Required Hardware

To complete this project, you will need the following components:‎

For this simple setup, you do not need a microcontroller. However, in many (maybe most) ‎practical applications, it would make sense to connect the RFID Reader to a microcontroller ‎and add an antenna so you could take readings remotely without your computer in front of ‎you and extend the range (which goes up to 3 or 4 feet in this example). Users who prefer to ‎communicate with the RFID reader using the Serial PTH header should solder either wires or ‎header pins to connect them to a 3.3V microcontroller, such as our RedBoard Artemis. ‎Check out our Hookup Guide for instructions on how to do this.‎

Setting Up Your Simultaneous RFID Reader

To connect the RFID reader directly to your computer via USB-C. Follow these steps:‎

  • Connect the USB-C Cable: Plug the USB-C end of the cable into the RFID reader and ‎the USB-A end into your computer. This connection will provide both power and data ‎communication between the RFID reader and your computer.‎

  • Check the UART Selection Switch: Ensure that the UART selection switch on the RFID ‎reader is in the correct position for USB operation. This is crucial for proper ‎communication with the software.‎

How to Download and Install Universal Reader Assistant (URA)‎

With the hardware set up, you can now move on to using the Universal Reader Assistant to ‎interact with your RFID reader.‎

The Universal Reader Assistant (URA) software is a powerful tool designed to help you ‎make full use of the capabilities of your SparkFun Simultaneous RFID Reader. ‎Unfortunately, as mentioned, the URA is only available for Windows.‎

Download URA

Setting Up the URA

  • Download the URA: Visit the ThingMagic website to download the Universal Reader ‎Assistant. Ensure you choose the correct version (32-bit or 64-bit) based on your ‎Windows operating system.‎

  • Install the URA: Once the download is complete, open the installer and follow the ‎instructions provided by the installation wizard.‎

Using the Software

  • Connect Your RFID Reader: Make sure your Simultaneous RFID Reader is connected ‎to your computer via USB. Open the Universal Reader Assistant after the installation ‎is complete.‎

  • Connection Wizard: Upon opening URA, you will be greeted by the Connection ‎Wizard menu. Here, you can select the reader type and the port your RFID reader is ‎connected to. (If you're familiar with the setup, you can skip this selection and move ‎directly to the main menu. Otherwise, select the correct port for your RFID reader ‎and click "Next.")‎

reader_1

  • Connect to the Reader: The Connection Wizard should display your RFID reader's ‎settings. You can click "Connect & Read" to start scanning tags immediately or ‎‎"Connect" to access the main window without starting the read operation.‎

connect_2

URA Features and Tips

Exploring URA Features

explore_3

The main window of the Universal Reader Assistant offers a wide range of settings and ‎status options for the M6E Nano or M7E Hecto RFID readers. Here are some key features ‎you can explore.‎

Read/Write Options: Adjust the RFID reader's power level, read/write settings, and other ‎operational parameters.‎

Practical Tech Tips - most settings can be adjusted on the right drop down menu.

‎Thermal Management: The RFID reader has an internal temperature sensor to prevent ‎damage from overheating. If you encounter a temperature-limit fault, reduce the read ‎power, or improve cooling.

‎Power Level: Start with a moderate power level (e.g., 500 dBm) to prevent the USB port from ‎browning out. You can increase the power as needed but be mindful of thermal limits.

‎Tag Read Efficiency: Experiment with different settings in the URA to optimize the RFID ‎reader's performance for your specific application.‎

Final Thoughts

By following this tutorial, you’ve (hopefully) successfully set up your SparkFun ‎Simultaneous RFID Reader to take multiple RFID readings directly through a USB ‎connection using your computer. The Universal Reader Assistant software allows you to ‎explore the full potential of your RFID reader, making it a powerful tool for various RFID ‎applications. Happy hacking!

מק"ט יצרן # 24738
SIMULTANEOUS RFID READER
SparkFun Electronics
₪ 1,127.27
הצגת עוד Details
מק"ט יצרן # 15426
CBL USB2.0 A PLUG TO C PLG 0.98'
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.