Maker.io main logo

I Made My Own LED Beaded Curtain

221

2023-08-06 | By bekathwia

License: None

 

I built a flexible screen in the form of a beaded curtain encrusted with LEDs that I control remotely. I’ve had this project on my list for quite some time, and the idea is simple: run lots of LEDs in vertical strips, enough to form a curtain.

Supplies

01_microcontroller

I used a pixelBlaze wifi microcontroller so I can control the animations remotely on my computer or phone, but an ESP module with WLED could also work.

Existing curtain attach leds

I started with an existing beaded curtain to use as my substrate. I figured I could use the bead strands to attach the LEDs, so they don’t have too much strain.

04_LED-strands

Here's what I used to make this project:

If you’re a beginner, don’t miss my introductory electronic series on the DigiKey YouTube channel. It’ll bring you up to speed on the wiring and soldering techniques you’ll need to build your own LED curtain.

Wiring the LEDs

05_wiring-sketch

Ideally, there would be a bunch of strands coming down from the top. But these pixels are best wired in a single data chain, so that would require soldering at the top of each strand, as well as a long data wire connecting the end of each strand to the top of the next.

06_big-black-clips

I opted to wire mine in a zigzag pattern, linking two strands at the bottom as well as the top. The strands are pretty close together, which makes for the least soldering possible– only where it’s needed to connect the termination of one strand with the beginning of another. That’s just because I don’t like the look of the big black clips.

circuit diagram

LED curtain

I attached the LED strands to the beaded strands with plain sewing thread, tying individual double knots around one or more of the wires as well as the string in between the beads.

mounting - resized - compressed

I had to set up my soldering iron nearby the curtain and make sure to attach the next strand before the end of the previous one gets too short, or it wouldn’t reach.

08_secondary-power

This process was not too quick, but it was fun to toil over while the LEDs were on. I attached a secondary power and ground to the end of the last LED strand, then connected up all the LEDs to test them and double-check that everything was getting enough power.

09_thread-trimming

Trimming all those threads gave me flashbacks to my DIY Beaded Chandelier project... which still doesn’t have all of its threads trimmed if I’m being honest.

Off-The-Shelf Curtains

When I put this project on my long list of things to make, I could swear there weren’t readymade LED screen-like curtains available for purchase, but now there are.

premade curtain - resized - compressed

So, if you are satisfied with the size and the animations that come preloaded on this thing, maybe buy the off-the-shelf version. But if you want to make entirely custom and very sophisticated-looking animations, the handmade one has the advantage.

Conclusion

walking through - resized - compressed

After hanging it in the doorway and trying it out, it’s pretty obvious that the connections at the bottom impact the ease of walking through it. This could be mitigated by tying threads in between connected strands every so often, so the two strands pull apart more as one. Or just use it against a flat surface like a window instead of a doorway.

showcase curtain - resized - compressed

But it is successful by the metric of projects my 13-year-old self would love.

If I were to take this further, I might try to reverse-engineer the store-bought version to see if it’s possible to replace the microcontroller. Then I’d have the best of both worlds with purpose-built function and high-class algorithmic fashion.

מק"ט יצרן # 4560
ADDRESS LED STRIP SOFT FLEXIBLE
Adafruit Industries LLC
מק"ט יצרן # 368
ADAPT TERM BL 2POS TO 2.1MM JCK
Adafruit Industries LLC
מק"ט יצרן # 32581
SCREWDR SET PHIL SLOT W/HNDL 4PC
Klein Tools, Inc.
מק"ט יצרן # WBNCC633731-2OZ
NO-CLEAN FLUX CORE SOLDER, 63/37
SRA Soldering Products
מק"ט יצרן # 404070001
TWEEZERS POINTED FINE 12 5.32"
Seeed Technology Co., Ltd
מק"ט יצרן # 11228-00000-100
3M VIRTUA PROTECTIVE EYE 1=1PC
3M
מק"ט יצרן # MN35
DIGITAL MINI MULTIMETER
FLIR Extech
מק"ט יצרן # 4559
PRE-CUT MULTI-COLORED HEAT SHRIN
Adafruit Industries LLC
מק"ט יצרן # SOLDERWICK2.0
2.0MM SOLDER WICK NO CLEAN
Chip Quik Inc.
מק"ט יצרן # 17536
DESOLDER PUMP WITH TIP 7.5"
Aven Tools
מק"ט יצרן # 297
SCISSORS - STRAIGHT LONG BLADE -
Excelta Corporation
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.