Maker.io main logo

Illuminated Butterfly Wall Art

131

2025-04-01 | By Adafruit Industries

License: See Original Project Hand Tools LED Strips Microcontrollers Arduino ESP32 Adafruit Feather Qwiic

Courtesy of Adafruit

Guide by Ben Everard

Overview

leds_butterfly_gif_large

Make animated wall art, powered by pebble-style LEDs, and controlled by a Mini Sparkle ‎Motion. The body is made out of corrugated plastic which is easy to work with by hand. This ‎will be mounted behind an artist's canvas, providing excellent LED diffusion and a subtle ‎texture.‎

Parts

The power supply below provides an all-in-one solution. ‎

‎-OR-‎

You can also use an old mobile phone power supply to the wall and an appropriate cable. If ‎the wall power is USB A, the following cable may work well (be careful of length depending ‎on where you mount your art).‎

Additionally, you'll need a stretched artists canvas, some corrugated plastic (for example ‎Coroplast), duct tape, four small screws, and a USB C power supply. Some optional black ‎cardstock will help make your art more defined if you have white corrugated plastic.‎

Optional

Tools & Materials

You'll need:‎

  • craft knife

  • soldering iron

  • screwdriver

  • Duct tape

  • Artist's canvas

  • Small wood screws x4‎

Electronics

To make the butterfly wing pattern symmetrical, the LEDs are placed in identical, but ‎mirrored, layouts. You can get display the same pattern in both halves by connecting the ‎two strands to the same data line. In order to connect both halves of the Pebble stands to ‎the power and data pins, you first need to combine their wires.‎

The power of one strip should be connected to the power of the other. The two grounds ‎should also be connected, as should the two data-in lines.‎

This image shows how you'll connect them:‎

connect_1

Finding which wires are which can be tricky. For the LED Pebbles, there are no very obvious ‎markings. Erin St. Blaine has written a guide page which helps identify which wires are ‎which.‎

Sparkle Motion Skirt with 2D Mapping

By Erin St Blaine

Electronics Assembly

View Guide

skirt_2

As shown in the Fritzing diagram above, you'll want to trim some wire back on each input ‎side of the Pebble LED line and twist the same lines together such that you now have each ‎like wire connected on the input sides of each strand. These three wires are then connected ‎to the respective pads on the Mini Sparkle Motion: 5V, G/Ground and the Pebble Data in to ‎pin 32.‎

You can solder straight onto the Mini Sparkle Motion or add a screw terminal block ‎connector (not included, sold separately) to the Mini Sparkle Motion and screw in the wires ‎to make it easy to attach or detach the controller.‎

There are troubleshooting steps on Erin's page if later in the build the lights are not acting as ‎intended.‎

terminal_3

The build above shows three colored wires connected to each Pebble LED strand end and ‎then leading to the Mini Sparkle Motion, without a terminal block.‎

Build

The physical build is made up of two parts:‎

  • a mask that slots into the back of your canvas

  • a box that holds the LEDs

The box is cut from one sheet of corrugated plastic. It will fold up and slot into the back of ‎the canvas and secured with four screws.

Cut the Mask

A butterfly shape will be used to mask out some of the light from the LEDs, leaving just an ‎image of a butterfly -- a little like a reverse silhouette.‎

First, you need an image of a butterfly. Below is one that you can download, or you can ‎search for your own. You'll need to scale this to the appropriate size for your canvas and ‎print it out on a sheet of paper.‎

butterfly_shape.svg

butterfly_4

Cut a sheet of your corrugated plastic to fit inside the back of the canvas. This should be ‎very snug, and if anything, slightly oversized.‎

Once you have this cut out, tape the butterfly shape in the middle, and use a craft knife to ‎cut out the shape. It is easiest to do several light passes with a craft knife rather than a ‎single hard pass.‎

If your corrugated plastic is translucent, you might want to cut the same shape out of dark ‎paper or card to block more of the light. Here you can see that I've used a bit of tape to hold ‎the dark paper and corrugated plastic together.

corrugated_5

Be careful when using a craft knife to avoid cuts. Suitable eye protection would be prudent ‎also.‎

Build the box

You can 'score' the corrugated plastic using a light pass of a craft knife -- this makes it bend ‎easily in exactly the place you want. It takes a bit of practice to get this right, and the bits ‎you cut out from the butterfly are ideal for cutting practice.

score_6

‎The cuts you need to make for the box are shown in the image below.‎

  • Red lines are scores on the front

  • Blue lines are scores on the back

  • Black lines are through cuts

Exact dimensions aren't given as it's based off the actual size of the canvas, which will vary ‎a bit from manufacturer to manufacturer. This will be detailed shortly.‎

The length of the two side folds isn't critical. These are used for screwing the plastic sheet to ‎the canvas.‎

folds_7

Start by scoring the inner rectangle. This is the same size as the mask, so you can use it as ‎a template. The outer square should be about 1.25 inches (3cm) bigger, so make sure ‎there's space for this.‎

Tape the mask to the middle of a section of corrugated plastic making sure that there is ‎sufficient space on all sides. Once you've scored this, you can work outwards by measuring ‎and cutting.‎

The two blue scores on the side should be approximately half the length of the side, leaving ‎about a quarter at the top and bottom. The blue scores need to sit on the wood of the ‎canvas, so they need to be the same distance in as the wood is thick.

wood_8

Attach the LEDs

Corrugated plastic is, in some ways, easy to work with, but it does have one problem: not ‎much sticks to it. CA glue holds a bit, and there are some specialized adhesives. However, ‎I've had the most success with duct tape.‎

Your two strings of LEDs should be positioned in an exact mirror image of each other. This ‎way whatever pattern you display will be mirrored perfectly on each wing. Zig zag the strands ‎up the sheet in the way shown in the photo. Ideally, you want the LEDs on one layer to fall ‎between the LEDs on the layer below. This will prevent any dark spots.

leds_9

Bringing Everything Together

The control board can be held in place by a bit of tape that's stuck back on itself.

tape_10

Your USB cable for powering the project needs to run from the wall USB power source and ‎pass through the plastic sheet to the Mini Sparkle Motion board. Cut a cross in at the ‎appropriate place for passing the cable (don't forget to account for the fact that part of the ‎plastic will be covered by the wood of the canvas).‎

cable_11

You'll need a way of hanging your art on the wall. I used picture wire, but you could use ‎string or even regular hookup wire. You'll need to make two small cuts on either side of the ‎picture that you can thread the wire through and twist it to keep it secure.

secure_12

Fold the sheet in to make a box. This should fit snugly inside the canvas.‎

box_13

With the box now inside the canvas, it just needs some screws to hold it in place.‎

canvas_14

Your butterfly is now ready for software and then to hang on the wall, plug in, and enjoy.‎

butterfly_15

Next, we'll take a look at the software. WLED is a software package that you'll load onto the ‎Mini Sparkle Motion and then configure via your computer.‎

WLED Setup

The following pages will walk you through installing WLED, setting up the various features ‎within the software and getting your lights turned on and responding to sound or IR control. ‎We'll also show you how to connect sensors via the onboard Stemma port and add button ‎control. And we'll show you how to set up multiple strands and multiple controllers and ‎sync them together for larger scale projects.‎

Ready? Set? Let's go.‎

setup_16

WLED Software

Board Choices

WLED runs on several different boards in Adafruit's collection. There are different benefits ‎to each, but the installation process is largely the same. This page contains instructions for ‎multiple boards -- be sure to use the pinouts and installation instructions for the one you're ‎using,‎

Sparkle Motion

This is our flagship ESP32 board, designed with WLED and Xlights in mind. It has 4 outputs ‎and is set up to drive either 5v, 12v or 24v pixels. It's a workhorse of a board and for larger ‎projects it's the clear winner. It has an onboard microphone for instant sound-reactive ‎support, and an IR sensor built in, to make it easy to control your project with an infrared ‎remote. It also has a couple stemma ports so you can add your own sensors or peripherals.‎

Sparkle Motion Mini

The Sparkle Motion Mini is a smaller version of the Sparkle Motion board. It has two LED ‎outputs, a microphone, and two stemma ports that make it easy to add an IR sensor or ‎other peripherals. It's got an onboard NeoPixel and a small footprint, making it perfect for ‎wearables or smaller projects. It will power a whole lot of pixels through the onboard USB ‎port: it's safe to draw up to 4A through this port, giving you plenty of power for most ‎wearable projects.‎

At this time, the Sparkle Motion Mini works best with WLED 0.15.1 -- the extra GPIO for ‎the microphone pins are not supported in WLED 0.15.0. This should be fixed with the ‎release of version 16.‎

To get mic support now, the following combined .bin file can be used. Get it by downloading ‎this zip file:‎

esp32_bootloader_v4_WLED_0.16.0-alpha_ESP32.zip

To install, extract the .bin file from the zip and then follow the same ESB Web Flasher ‎process used for installing CircuitPython. At the "Programming the Board" step, choose ‎the .bin file and leave offset as 0x0.‎

QT Py Pico ESP32‎

The QT Py Pico is small and affordable, so usually my go-to for smaller costumes or ‎wearables. It also has a range of BFF add-on boards that add functionality. Here's a guide ‎with more QT Py info. The QT Py will drive up to around 30 pixels through the onboard USB ‎port, so if you have more LEDs than that you may want to consider the Sparkle Motion Mini ‎instead, or you can power the board through the +5v pin.‎

Note: WLED works on the QT Py Pico but NOT on the S2 or S3 versions, at the time of writing.‎

Feather Huzzah ESP32 ‎

The Feather Huzzah ESP32 the top of the line. It's a great choice for projects where you want ‎to add sensors, interaction, or drive a whole lot of LEDs. It's the most reliable as well -- I've ‎run these for two months straight with no power cycling and they just keep on truckin. ‎Adafruit has a very wide selection of Feather Wing boards that connect to the Feather ‎microcontroller line. The sky is the limit with these boards.‎

It also comes in a version with a high-powered WiFi range extender! If you're trying to sync ‎multiple instances across distance, check this one out. Feather Huzzah ESP32 V2 w.FL ‎Antenna.

Feather Huzzah ESP8266‎

The Feather Huzzah ESP8266 will run WLED as well but won't drive as many pixels: the ‎ESP32 limit on WLED is around 1000 pixels per input, but the ESP8266 tops out at around ‎‎500. It's about $5 cheaper though, so for smaller projects it's a great way to save a little ‎money and still have access to all the FeatherWing options in the Adafruit store.‎

Driver Update

Some versions of our controllers have a new serial chip which needs a driver installed ‎before we can install WLED. Head over to our How to Install Drivers for WCH USB to Serial ‎Chips tutorial and download and install the new driver.‎

If you have an older QT Py with CP2102 USB-to-Serial bridge, use SiLabs’ driver instead.‎

‎Install WLED

These next steps require a Web Serial-compatible browser. As of this writing, that ‎means Google Chrome, Microsoft Edge, or Opera “desktop” browsers. Other browsers ‎‎(Safari, Firefox, Explorer, and anything mobile) won’t work.‎

Visit https://install.wled.me/‎

Plug your microcontroller into your computer with a known good USB cable. Click "Install" ‎and select the port for your board.‎

Depending on the USB-to-serial bridge chip on the board, you might see one or two serial ‎ports. On Mac, for instance, there might be both ‎‎“/dev/cu.usbmodem[number]” and “/dev/cu.wchusbserial[number]”. Use the ‎‎“wchusbserial” one.‎

install_17

After successful installation, enter your WiFi network name and password when prompted. ‎This must be a 2.4 GHz WiFi network; ESP32 does not support 5 GHz networks. If it can’t ‎connect, then as a fallback WLED will create its own 2.4 GHz WiFi access point.‎

install_18

If you don't see the "Connect to Wi-Fi" prompt, you'll need to set up your WiFi network using ‎AP (access point) mode. Open up your WiFi settings and look for a WiFi network ‎called WLED-AP. Connect to this network using the default password wled1234. The WLED ‎interface will pop up in its own browser.‎

From here, go into Config/Wifi Settings and enter your WiFi credentials near the top. Give ‎your project a name in the mDNS field a little further down the page. Now you can type in ‎‎"projectname.local" (where "projectname" is your mDNS name) into any web browser on ‎the same wifi network to access your microcontroller.‎

You can also scan the QR code below to open access point mode. ‎

For more help and troubleshooting tips visit the Getting Started page on the WLED ‎knowledge base.‎

install_19

install_20

code_21

Setup & Preferences

WiFi Setup

Head to the WiFi Setup screen under Config and create a good URL so you can control your ‎project from any web-enabled device. Call it something you'll remember, that's easy to type ‎into any web browser on your WiFi network in order to connect to your project.‎

In Safari or Chrome on your phone or computer, type in this web address to access the ‎WLED interface: http://projectname.local (where "projectname" is whatever you put into ‎this field).‎

Check out the Additional Settings page for more info on accessing your project. WLED has ‎an "access point mode" that doesn't require a WiFi network for when you're out on the go. ‎It's also helpful to download one of the WLED apps to help manage and organize your ‎projects.‎

config_22

config_23

LED Preferences

Next, head to the LED Preferences tab under the Config menu.‎

Scroll down to Hardware Setup. Put your total number of LEDs into the "Length" field and ‎change GPIO to the pin number associated with the pin you soldered to. Check the pinout ‎diagram for the board you're using (it's the number in yellow).‎

config_24

Use It

use_25

Now you can use any computer or handheld device to control your LEDs. ‎

Make sure your device is on the same WiFi network as your board. Navigate to your custom ‎URL (projectname.local/ ) in a web browser. You'll see a color picker above a whole bunch of ‎color palette choices.‎

Choose a color, choose an effect, and watch your lights animate and glow!‎

Save your favorite combinations as presets, create playlists, control the speed and intensity ‎of the animations, and lots more. This web app is incredibly intuitive and easy to use.‎

Head over to the WLED wiki at https://kno.wled.ge/ to delve into all the particulars.‎

WLED Config

Next, we'll tell WLED about our physical setup. We'll give our project a name and easy-to-‎remember URL and tell the software how many LEDs we have set up on each pin.‎

WiFi Setup

Head to the WiFi Setup screen under Config. This is where your network credentials live, so ‎you can change them if needed. Scroll down to the mDNS field and create a good URL so ‎you can control your project from any web-enabled device. Call it something you'll ‎remember, that's easy to type into any web browser on your WiFi network in order to connect ‎to your project. ‎

In this example, I'd go to my web browser on my phone, iPad, or computer, and type in ‎‎"http://projectname.local" to open up the WLED interface on my screen. Your device must ‎be on the same WiFi network as your board.‎

credentials_26

credentials_27

LED Preferences

Next, head to the LED Preferences tab under the Config menu.‎

Scroll down to Hardware Setup. The Sparkle Motion Mini board has 2 outputs to attach ‎LED strips: GPIO pins 32 and 33.‎

WLED allows up to 3 strips to be connected at once. The strips can be of different types, ‎lengths, and color order. Select your LED type, length, and GPIO pin. If you have multiple ‎strips connected, click the + button and enter the additional strips in the same way. ‎

wifi_27a

Click "save" and if you've done everything correctly, your light strands should come on in a ‎warm, cheerful yellow color. Success! Time to start making pretty light animations. ‎

Troubleshooting

If your lights didn't come on, here are a few things to try:‎

  1. Head back to WLED and check your pinout configuration under LED Preferences. Be ‎sure the pin number is the correct GPIO for the attachment point you used.‎

  2. Check your wiring! Be sure you connected to the IN end of the LED strip. These strips ‎can be inconsistent, so this is a pretty common problem. Use an alligator clip to try ‎connecting the data wire on the other end (the power and ground wires should work ‎from either end).‎

  3. Try re-uploading the WLED software. ‎

  4. If the lights come on but you can't control them: i.e. you type in "projectname.local" ‎into your browser and it won't connect, make sure you're on the correct WiFi network. ‎If you're on a different network than the one you set up the sofware on, you won't see ‎the WLED connection.‎

  5. If your lights came on in blue or green instead of yellow, your color order is wrong. ‎See below to fix.‎

  6. If only half your lights came on, be sure you've got the correct number in the "length" ‎field under LED preferences.‎

  7. If your lights came on in a variety of weird colors and looking like a 1950s diner ‎interior, you may have the wrong LED strip type selected. RGBW strips and RGB ‎strips are not the same, so be sure you've got the correct strip type, or you'll get very ‎odd behavior.‎

  8. If your microcontroller hangs or keeps rebooting, or gets really hot, you may have the ‎power and ground lines switched. Unplug right away and check: this is a fast way to ‎brick your controller.‎

Color Order

If your lights have come on in any color other than a warm yellow, there's one more setting ‎to change. LED strips and pixels are not all standardized, and sometimes the red, green, ‎and blue LEDs inside are connected in a different order. ‎

In the main interface window, choose "solid" as your effect and red as your color from the ‎color picker. ‎

If your lights come on in any color other than red, your color order is set incorrectly. This is ‎an easy fix. Head back to the LED settings tab and find the Hardware Setup section (this is ‎where you set up your pin number earlier). Choose BRG from the dropdown, click save, and ‎see if your pixel colors match your color picker now. If not, try another combo until the lights ‎look correct.‎

color_28

color_29

Setting the Light Pattern

Now that the electronics and software are set up, it's time to create the WLED pattern to light ‎up the butterfly. There aren't any hard-and-fast rules here, and you can illuminate your ‎butterfly however you like.‎

Personally, I like a blue butterfly with a shimmer of purple to give the effect of iridescence. ‎This is inspired by butterflies such as the Common Blue and Holly Blue. Another common ‎color pallet in nature is orange and red. However, you don't have to be limited by real life ‎butterflies, you can pick whatever you like.‎

To create the effect for a Common Blue inspired butterfly, first you have to make some ‎settings in the Colors tab in WLED. Pick a blue for color 1 and purple for color 2, then ‎select Colors 1&2 in the pallet type list.‎

light_30

You can now switch to the effects tab and select your effect. I like the Blends effect.‎

effects_31

Finally, in order to make your butterfly start with the same pattern when it's powered on, you ‎need to save the setup as a preset.‎

In the Presets tab, click Create Preset, give it a name, and click Save Preset. This will give ‎it a preset ID. Remember this as you'll need it in the next step.‎

presets_32

Go to Config > LED Preferences and scroll down. Near the bottom you'll find ‎the Defaults section, and in this section, you'll see the option to Apply Preset x At Boot. ‎Change the number to the ID of the preset you just created and scroll back to the top to save ‎the settings. Now, each time you power on your device, it'll start with the correct lighting.‎

מק"ט יצרן # 6024
ADAFRUIT NEOPIXEL PEBBLE / SEED
Adafruit Industries LLC
מק"ט יצרן # 5044
CABLE A PLUG TO C PLUG 6.5'
Adafruit Industries LLC
מק"ט יצרן # 2137
TERM BLK 4P SIDE ENT 2.54MM PCB
Adafruit Industries LLC
PANEL MOUNT 1K POTENTIOMETER (BR
מק"ט יצרן # 1789
PANEL MOUNT 1K POTENTIOMETER (BR
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.