Maker.io main logo

Infrared Hand Gesture Robot Control Glove

49

2019-06-27 | By Adafruit Industries

License: See Original Project Programmers Circuit Playground

Courtesy of Adafruit

Guide by Dave Astels

Overview

With a wave of your hand, a robot obeys your command!

This project will take a Circuit Playground Express based robot such as the CRICKIT Snake Bot or Crickit Carnival Bumper Bot and add wireless hand gesture control with the built in Infrared.

2_blinka

We'll be using CircuitPython for this project. Are you new to using CircuitPython? No worries, there is a full getting started guide here.

Adafruit suggests using the Mu editor to edit your code and have an interactive REPL in CircuitPython. You can learn about Mu and its installation in this tutorial.

We'll be making use of the IR transmit and receive capabilities of the Circuit Playground Express to send commands from the controller to the robot. We have a guide that covers working with Circuit Playground Express IR in detail. There are other project guides that make use of it such as the Treasure Hunt and Zombie games.

Parts

You'll need two Circuit Playground Expresses - one on your hand and one for your robot.

Tools and Supplies

A glove onto which you can sew a Circuit Playground Express.

Sewing supplies: needle, thread, scissors. Alternatively, you could use self-adhesive Velcro.

Build a Robot

3_robotics

Before you get started with the infrared glove part, we'll need a robot to control.

We recommend building our simple Circuit Playground + Crickit bumper bot. You don't need the speaker and servo flag, the most important parts are the two motors, two wheels, and the Crickit with CPX on top.

Visit the Bumper Bot guide to build it

Motion Control

The only construction required for this guide (beyond a robot) is attaching a Circuit Playground Express to the palm of a glove. A biking glove works well, as you can see in the photos. The alligator clip pads are ideal for sewing; use a few to attach the board to the glove. Regular thread is all that is required, we're sewing it to attach it, not to make any connections.

Attach the Circuit Playground Express so that the battery connector is closest to your wrist, as shown in the photo below. Not only does this align with the accelerometer data expected by the code, it also makes it easy to slip an attached LiPo battery into the glove.

4_circuit

The controller recognizes 9 different hand positions/commands:

STOP

5_flat

6_stop

Hold your hand flat with your palm facing down.

The robot stops all motion.

ROTATE_LEFT

8_tilt

7_counterclockwise

With your hand flat, palm facing down, rotate your wrist counterclockwise.

The robot rotates counterclockwise.

ROTATE_RIGHT

10_right

9_rotate

With your hand flat, palm facing down, rotate your wrist clockwise.

The robot rotates clockwise.

FORWARD

11_up

12_forward

Hold your hand with your palm facing away from you.

The robot will move forward.

FORWARD_LEFT

13_left

 14_forward-left

With your handheld palm outward, rotate your wrist clockwise. 

The robot will veer to the left while moving forward.

FORWARD_RIGHT

15_clockwise

16_forward-right

With your handheld palm outward, rotate your wrist clockwise.

The robot will veer to the right while moving forward.

REVERSE

17_down

18_reverse

Hold your hand, wrist bent, with your palm facing toward you.

The robot will move in reverse.

Depending on the reflectivity of the surfaces in the area, the reverse commands might not be reliable.

REVERSE_LEFT

19_lef

20_reverse-left

With your handheld wrist bent and palm facing you, rotate your wrist clockwise.

The robot will veer to the left while moving in reverse.

REVERSE_RIGHT

22_reverse-right

21_reverse 

With your handheld wrist bent and palm facing you, rotate your wrist counterclockwise.

The robot will veer to the right while moving in reverse.

Controller Code

The controller code continually reads the 3 axes of the accelerometer and, based on those readings, sends the appropriate code via the IR transmitter.

Since accelerometers can detect gravity, they're great for calculating the tilt of your hand. But sometimes it's hard to visualize what the motion translates to X-Y-Z values. For that, we recommend using the CircuitPython plotter.

Check our motion-plotting guide and video to see how you can read the x, y, and z accelerations and get values for use in detecting tilt.

 

 Sensor Plotting Motion with Mu and CircuitPython

There are three primary hand positions that correspond to stop, forward, and reverse:

1. palm down: z is a high negative value,

2. hand up with palm facing away from you: y has a high positive value, and

3. hand down with palm facing toward you: y has a high negative value.

For each of these three hand positions, wrist rotation adds a turn to the basic stop/forward/reverse motion: rotating in place if the robot is stopped or veering left/right if the robot is moving forward or reversing. The X component of the accelerometer reading indicates wrist rotation: a large negative value for a counterclockwise rotation, and a large positive value for clockwise rotation.

After configuring the hardware and libraries, the main loop reads the accelerometer and a 2 level conditional decides what should be sent to the robot.

Below is the code for the control glove. Save it to the Circuit Playground Express on the glove as code.py.

Download: Project Zip or glove.py | View on Github

Copy Code
import time
import busio
import board
import pulseio
import adafruit_irremote
import adafruit_lis3dh

# Control debug output: it takes time so don't unless you're debugging
DEBUG_LOG = False

# Control codes
STOP = 0x01
ROTATE_LEFT = 0x02
ROTATE_RIGHT = 0x03
FORWARD = 0x04
FORWARD_LEFT = 0x05
FORWARD_RIGHT = 0x06
REVERSE = 0x07
REVERSE_LEFT = 0x08
REVERSE_RIGHT = 0x09

TRANSMIT_DELAY = 0.1

# Setup accelerometer
i2c = busio.I2C(board.ACCELEROMETER_SCL, board.ACCELEROMETER_SDA)
sensor = adafruit_lis3dh.LIS3DH_I2C(i2c, address=0x19)

# Create a 'pulseio' output, to send infrared signals on the IR transmitter @ 38KHz
pwm = pulseio.PWMOut(board.IR_TX, frequency=38000, duty_cycle=2 ** 15)
pulseout = pulseio.PulseOut(pwm)

# Create an encoder that will take numbers and turn them into IR pulses
encoder = adafruit_irremote.GenericTransmit(header=[9500, 4500],
one=[550, 550],
zero=[550, 1700],
trail=0)

def log(s):
"""Optionally output some text.
:param string s: test to output
"""
if DEBUG_LOG:
print(s)


while True:
x, y, z = sensor.acceleration
log("{0: 0.3f} {1: 0.3f} {2: 0.3f}".format(x, y, z))
if z < -5.0 and abs(y) < 3.0: # palm down
if x < -5.0: # tipped counterclockwise
log("ROTATE_LEFT")
encoder.transmit(pulseout, [ROTATE_LEFT] * 4)
elif x > 5.0: # tipped clockwise
log("ROTATE_RIGHT")
encoder.transmit(pulseout, [ROTATE_RIGHT] * 4)
else: # level
log("STOP")
encoder.transmit(pulseout, [STOP] * 4)
elif y > 5.0: # palm facing away
if x < -5.0: # tipped counterclockwise
log("FORWARD_LEFT")
encoder.transmit(pulseout, [FORWARD_LEFT] * 4)
elif x > 5.0: # tipped clockwise
log("FORWARD_RIGHT")
encoder.transmit(pulseout, [FORWARD_RIGHT] * 4)
else: # straight up
log("FORWARD")
encoder.transmit(pulseout, [FORWARD] * 4)
elif y < -5.0: # palm facing toward (hand down)
if x < -5.0: # tipped counterclockwise
log("REVERSE_RIGHT")
encoder.transmit(pulseout, [REVERSE_RIGHT] * 4)
elif x > 5.0: # tipped clockwise
log("REVERSE_LEFT")
encoder.transmit(pulseout, [REVERSE_LEFT] * 4)
else: #straight down
log("REVERSE")
encoder.transmit(pulseout, [REVERSE] * 4)

time.sleep(TRANSMIT_DELAY)

Robot Code

The robot code is pretty simple: it continually reads data from the IR receiver and based on what it reads, controls the motor direction and speed.

The robot code is below. Save it to the Circuit Playground Express on the robot as code.py.

Download: Project Zip or robot.py | View on Github

Copy Code
import board
import pulseio
import adafruit_irremote
from adafruit_crickit import crickit

# Control debug output: it takes time so don't unless you're debugging
DEBUG_LOG = False

# Control codes
STOP = 0x01
ROTATE_LEFT = 0x02
ROTATE_RIGHT = 0x03
FORWARD = 0x04
FORWARD_LEFT = 0x05
FORWARD_RIGHT = 0x06
REVERSE = 0x07
REVERSE_LEFT = 0x08
REVERSE_RIGHT = 0x09

left_wheel = crickit.dc_motor_1
right_wheel = crickit.dc_motor_2


def log(s):
"""Optionally output some text.
:param string s: test to output
"""
if DEBUG_LOG:
print(s)


# These allow easy correction for motor speed variation.
# Factors are determined by observation and fiddling.
# Start with both having a factor of 1.0 (i.e. none) and
# adjust until the bot goes more or less straight
def set_right(speed):
right_wheel.throttle = speed * 0.9

def set_left(speed):
left_wheel.throttle = speed


# Uncomment this to find the above factors
# set_right(1.0)
# set_left(1.0)
# while True:
# pass


# Create a 'pulseio' input, to listen to infrared signals on the IR receiver
pulsein = pulseio.PulseIn(board.IR_RX, maxlen=120, idle_state=True)

# Create a decoder that will take pulses and turn them into numbers
decoder = adafruit_irremote.GenericDecode()

while True:
# Listen for incoming IR pulses
pulses = decoder.read_pulses(pulsein)

# Try and decode them
try:
# Attempt to convert received pulses into numbers
received_code = decoder.decode_bits(pulses)
except adafruit_irremote.IRNECRepeatException:
# We got an unusual short code, probably a 'repeat' signal
log("NEC repeat!")
continue
except adafruit_irremote.IRDecodeException as e:
# Something got distorted or maybe its not an NEC-type remote?
log("Failed to decode: {}".format(e.args))
continue


if received_code == [STOP] * 4:
log("STOP")
set_left(0.0)
set_right(0.0)
elif received_code == [ROTATE_LEFT] * 4:
log("ROTATE_LEFT")
set_left(-0.25)
set_right(0.25)
elif received_code == [ROTATE_RIGHT] * 4:
log("ROTATE_RIGHT")
set_left(0.25)
set_right(-0.25)
elif received_code == [FORWARD] * 4:
log("FORWARD")
set_left(0.5)
set_right(0.5)
elif received_code == [FORWARD_LEFT] * 4:
log("FORWARD_LEFT")
set_left(0.0)
set_right(0.5)
elif received_code == [FORWARD_RIGHT] * 4:
log("FORWARD_RIGHT")
set_left(0.5)
set_right(0.0)
elif received_code == [REVERSE] * 4:
log("REVERSE")
set_left(-0.5)
set_right(-0.5)
elif received_code == [REVERSE_LEFT] * 4:
log("REVERSE_LEFT")
set_left(-0.25)
set_right(-0.5)
elif received_code == [REVERSE_RIGHT] * 4:
log("REVERSE_RIGHT")
set_left(-0.5)
set_right(-0.25)
else:
log("UNKNOWN")

Wrapup

This project is pretty simple: send commands via IR based on accelerometer readings (i.e. hand position) and manipulate a CRICKIT based on commands received via IR. Even so, this can be the basis of many different projects. This just controls two motors connected to the CRICKIT, but the same approach could be applied to anything connected to the CRICKIT or Circuit Playground Express.

It could be taken further by adding simple gestures in addition to static hand position. This could be done by examining changes in accelerometer values over time.

מק"ט יצרן # 3333
CIRCUIT PLAYGROUND EXPRESS
Adafruit Industries LLC
מק"ט יצרן # 3093
CRICKIT CIRCUIT PLAYGROUND EXP
Adafruit Industries LLC
מק"ט יצרן # 3777
GEARMOTOR 200 RPM 3-6V DC
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.