Maker.io main logo

Integrating BleuIO with Teensy 4.1 for Seamless BLE Applications

52

2026-02-16 | By Sheikh Shuhad

License: GNU Lesser General Public License Bluetooth / BLE Arduino Teensy

In this project, we will build a high-performance embedded Bluetooth Low Energy (BLE) host system using the Teensy 4.1 microcontroller and the BleuIO USB BLE dongle. The goal is to turn the Teensy into a USB Host controller that communicates directly with BleuIO through a simple Arduino sketch, allowing us to create BLE applications without implementing a full BLE stack on the microcontroller.

By the end of this project, you will have a fully functional embedded BLE platform where Teensy 4.1 acts as the application controller and BleuIO handles all Bluetooth Low Energy communication internally. You will be able to send AT commands from Teensy to scan for BLE devices, connect to them, read characteristics, and build your own BLE-based solutions. More importantly, you will gain a reusable architecture that can serve as the foundation for industrial gateways, IoT devices, monitoring systems, or custom embedded products.

Why We Chose Teensy 4.1

The Teensy 4.1 is built around the powerful NXP i.MX RT1062 ARM Cortex-M7 processor running at 600 MHz. This makes it one of the fastest microcontrollers compatible with the Arduino ecosystem. Its high clock speed, large memory capacity, and hardware floating-point support allow it to handle complex logic, real-time data processing, and communication tasks with ease.

What makes Teensy 4.1 particularly ideal for this project is its USB Host capability. Since BleuIO is a USB device, it requires a host controller to operate independently of a PC. Teensy 4.1 provides exactly that. It allows us to connect BleuIO directly to the microcontroller and build a fully standalone BLE system. The board’s performance headroom ensures stable communication, fast response handling, and scalability for advanced applications.

Rather than choosing a minimal low-power MCU, we selected Teensy 4.1 because it bridges the gap between traditional microcontrollers and more complex application processors. It gives developers flexibility, speed, and reliability in embedded BLE projects.

Project Requirements

To build this project, you will need:

Project Architecture Overview

The system architecture is straightforward. Teensy 4.1 operates as a USB Host and communicates directly with the BleuIO dongle over serial. BleuIO then manages all Bluetooth Low Energy communication with nearby BLE devices. This separation of responsibilities simplifies development significantly. Teensy focuses on application logic, while BleuIO handles the BLE stack internally.

Teensy 4.1 (USB Host)
        ↓
BleuIO USB Dongle
        ↓
BLE Devices

How the Project Works – Step-by-Step

Step 1: Install Arduino IDE and Teensy Support

First, download the Arduino 2.x.x IDE from Arduino’s website. All versions 2.0.4 and later are supported. Versions 2.3.0 or later are recommended, due to improvements in Boards Manager. 

To install Teensy on Arduino IDE 2.x, click File > Preferences (on MacOS, click Arduino IDE > Settings). 

In the main Arduino window, open Boards Manager by clicking the left-side board icon, search for “teensy”, and click “Install”. 

Step 2: Configure USB Type

Teensy supports multiple USB configurations. Under Tools → USB Type, select the appropriate mode so the board can manage serial communication while operating with USB Host functionality. Teensyduino is also compatible with many Arduino libraries

Step 3: Upload the Sketch

The source code for this project, USBtoUSBHostSerial.ino sketch, is publicly available on GitHub: https://github.com/smart-sensor-devices-ab/bleuio_Teensy_host

Upload the provided USBtoUSBHostSerial.ino sketch to the Teensy 4.1 using the Arduino IDE. This sketch initializes the USB Host interface and establishes a communication bridge between the Teensy and the BleuIO dongle. Once programmed, the Teensy essentially becomes a serial terminal for BleuIO, allowing you to type AT commands through the Arduino Serial Monitor and receive responses in real time.

Instead of embedding complex BLE logic in the microcontroller firmware, the sketch focuses on maintaining stable USB communication and forwarding user commands to the dongle. BleuIO processes these commands internally and returns structured responses. This design keeps the firmware clean, modular, and easy to expand.

Why This Approach Is Powerful

Developing BLE applications directly on microcontrollers traditionally requires integrating a BLE stack, managing connection states, handling security layers, parsing protocol events, and debugging complex timing issues. This process can be time-consuming and hardware-dependent. Each microcontroller family often requires a different SDK, stack configuration, and maintenance strategy.

By using BleuIO, this complexity is dramatically reduced. BLE functionality is abstracted behind a simple AT command interface. The microcontroller does not need to manage low-level BLE operations. Instead, it communicates using straightforward serial commands while BleuIO takes care of scanning, connecting, reading characteristics, and maintaining protocol compliance internally. This modular architecture makes the system portable across hardware platforms and reduces firmware complexity, development time, and maintenance effort.

GitHub Repository

The source code for this project, USBtoUSBHostSerial.ino sketch, is publicly available on GitHub:

https://github.com/smart-sensor-devices-ab/bleuio_Teensy_host

This project is shared as a public example to demonstrate how BleuIO can be integrated into high-performance embedded systems. It is intentionally simple in structure so that developers can clearly understand the architecture and reuse it in their own applications.

By combining the computational power of Teensy 4.1 with the modular BLE capabilities of BleuIO, we created a clean and scalable embedded architecture. This project highlights how BLE integration does not need to be complicated. With the right approach, developers can focus on innovation and application logic rather than low-level protocol management.

מק"ט יצרן # 20359
TEENSY 4.1 WITHOUT ETHERNET
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.