Maker.io main logo

LED Crystal Goddess Crown

23

2017-10-12 | By SparkFun Electronics

License: See Original Project Wearables

Courtesy of SparkFun

Introduction

Design and build time: 2 Days (using 7 molds)

In this project, we’ll create a wearable LED Crystal Crown using a simple circuit made of 7x Super Bright White LEDs wired in parallel and powered by two coin cell batteries wired in series.

Suggested Reading

Before you get started, take some time to familiarize yourself with the following:

Materials and Tools

Let’s go over all of the things you’ll need to solder your project together.

You Will Also Need:

Understanding Your Circuit

The LED Crystal Goddess Crown project is an example of a basic circuit – an electrical loop that travels from a power source along a path (i.e. wires, traces, or any conductive material), through one or more component(s), and then back to the power source. For our project, we’ll use LEDs (Light-Emitting Diodes). This electrical loop for the project is completed by soldering the LED’s leads together. In order to light the LEDs, electricity from the power source must flow from the positive (+) side of the battery through an LED and back to the negative (–) side of the battery. This electric flow is called current.

In this circuit, the LEDs are soldered in parallel while the two coin cell batteries are attached in series. Take a look at the LEDs, current limiting resistors, and batteries in the circuit diagram below. When the LEDs are connected in parallel, all the positive leads will be connected together. The bent leads on the right of the LEDs (anodes +) are connected to VCC or + on the power source and to each other. Additionally, the negative leads will share a common connection. Notice that the leads on the left of the LEDs (cathodes -) are connected to ground on the power source via a resistor. We suggest using a low-value resistor (i.e. a 1.5Ω with brown green gold color bands) as the current limiting resistor in this project to maximize the brightness of the LEDs.

It’s important to keep in mind that certain electronic components (like LEDs) have polarity - meaning electric current can only flow through them in one direction. If hooked up incorrectly, the LEDs will not light up. The battery is also polarized; it has a positive and negative side. Always check to make sure that all your parts are correctly oriented before soldering together a circuit.

check all your parts are oriented before soldering

Having a hard time seeing the circuit? Click on the wiring diagram for a closer look.

Putting It Together

STEP 1:

Stuff your crystal mold with glitter.

Stuff your crystal mold with glitter

STEP 2:

Prepare the resin according to the instructions on the box. Use a paper clip to mix.

Prepare resin according to the instructions

STEP 3:

Pour the prepared resin into your crystal mold. Squeeze, tap, and shake the mold lightly to make sure all air bubbles reach the surface. The resin should be almost to the top, with some extra room left over.

Pour the prepared resin into your crystal mold

STEP 4:

Place the LED into the resin-filled mold with the electrical leads completely out of the resin and pointing towards the sky. If the LED is falling or leaning in any direction, add some tape to the leads and the side of the mold to keep it straight.

Place LED into resin-filled mold with electrical leads

STEP 5:

Let this sit for 24 hours to harden.

Let this sit for 24 hours to harden

STEP 6:

Remove the resin crystal from the mold and repeat step 4-6 another 6 times. This can either be done over the course of 7 days (one full 24 hour period per crystal), or in one 24 hour time period with seven separate molds.

Remove resin crystal from mold and repeat

STEP 7:

Bend the electrical leads of each crystal perpendicular to their natural position, and hot glue the crystals at the base to your headband.

hot glue the crystals at the base to headband

STEP 8:

Solder the resistors to the LED cathodes according to the circuit diagram provided above.

Solder resistors to LED cathodes

STEP 9:

If necessary, use some hook-up wire to connect the LED terminals together in parallel. Cut a piece of the wire from a spool and strip a piece of the wire. Otherwise, bend the LED terminals so that they connect to each other in parallel. Continue to solder the LEDs together in parallel according to the circuit diagram.

Continue to solder the LEDs together in parallel

STEP 10:

Solder the two battery holders together in series (i.e. positive lead connects to negative lead).

Solder the two battery holders together in series

STEP 11:

Hot glue the battery holders to the base of the headband.

Hot glue battery holders to base of the headband

STEP 12:

Use the hook-up wire to connect the battery holder leads to the LED leads according to the circuit diagram.

connect battery holder leads to LED leads

At this point, try inserting the batteries into the battery holders to test. If the LEDs are not lighting up, try checking your circuit and connections. If the LEDs are lighting up as expected, remove the batteries and move on to the next step!

STEP 13:

Thoroughly insulate all exposed wire with hot glue.

Thoroughly insulate all exposed wire with hot glue

*PLEASE NOTE: The wires need to be completely covered in hot glue. Make sure that metal pins on the anode and cathode side have some space between each other. This is to prevent a circuit short which can cause a fire. It is important for your safety to completely cover any exposed wire with glue.

STEP 14:

Re-insert the batteries and enjoy!

Re-insert the batteries and enjoy

Finished Crown

מק"ט יצרן # 08026
HOOK-UP SOLID 22AWG WHITE 25'
SparkFun Electronics
מק"ט יצרן # BA2032SM
BATTERY HOLDER COIN 20MM SMD
MPD (Memory Protection Devices)
מק"ט יצרן # 4900-112G
SOLDER LF SN96 21GAUGE .25LBS
MG Chemicals
מק"ט יצרן # 10969
RESISTOR KIT - 1/4W (500 TOTAL)
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.