Maker.io main logo

MicroMod Main Board Hookup Guide V2

215

2024-02-16 | By SparkFun Electronics

License: See Original Project MicroMod

Courtesy of SparkFun

Guide by BBOYHO, ELIAS THE SPARKIEST

Introduction

Note: This tutorial is for the MicroMod Main Board - Single V2.1 and Double V2.2. For users with ‎the older versions of the Main Boards, make sure to check out the older tutorial.‎

The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to ‎interface a Processor Board with a Function Board(s). The modular system allows you to add an ‎additional feature(s) to a Processor Board with the help of a Function Board(s).‎

Required Materials

To follow along with this tutorial, you will need the following materials at a minimum. You may not ‎need everything though depending on what you have. Add it to your cart, read through the guide, ‎and adjust the cart, as necessary.‎

Minimum Wishlist with MicroMod Main Board - Single SparkFun Wish List

VIEW MINIMUM WISHLIST WITH MICROMOD MAIN BOARD - SINGLE ON ‎SPARKFUN.COM

MicroMod Main Board

To hold the Processor and Function boards, you will need one Main Board. Depending on your ‎application, you may choose to have either one or two Function Boards.‎

MicroMod Processor Board

There are a variety of MicroMod Processor Boards available to choose from. You will probably want ‎to avoid having the same Processor and Function Board since there is an ESP32 on both types of ‎boards.‎

MicroMod Function Board

To add additional functionality to your Processor Board, you'll want to include one or two Function ‎Boards when connecting them to the Main Board. Make sure to check out the catalog for other ‎function boards.‎

Tools

You will need a screwdriver to secure the Processor and Function Boards. The MicroMod ‎Screwdriver is an excellent option for those looking for a low-cost tool. The SparkFun Mini ‎Screwdriver and Pocket Screwdriver Set can work as well. For users using a microSD card and ‎want to easily read the contents of the memory card, you will need a microSD card adapter or USB ‎reader.‎

Suggested Reading

If you aren't familiar with the MicroMod ecosystem, we recommend reading here for an overview. ‎We recommend reading here for an overview if you decide to take advantage of the Qwiic ‎connector.‎

micro_1

MicroMod Ecosystem               Qwiic Connect System

If you aren’t familiar with the following concepts, we also recommend checking out a few of these ‎tutorials before continuing. Make sure to check the respective hookup guides for your Processor ‎board and Function Board to ensure that you are installing the correct USB-to-serial converter. You ‎may also need to follow additional instructions that are not outlined in this tutorial to install the ‎appropriate software.‎

  • What is an Arduino? What is this 'Arduino' thing anyway? This tutorial dives into what an ‎Arduino is and along with Arduino projects and widgets.‎

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software on ‎Windows, Mac, and Linux.‎

  • How to Install CH340 Drivers: How to install CH340 drivers (if you need them) on Windows, ‎Mac OS X, and Linux.‎

  • Getting Started with MicroMod: Dive into the world of MicroMod - a compact interface to ‎connect a microcontroller to various peripherals via the M.2 Connector!‎

Hardware Overview

The overall functionality of the Single and Double Main Boards are the same. We'll use the Single ‎Main Board more in this section to highlight the features since this is also included in the Double ‎Main Board. We'll switch to the Double Main Board when necessary to highlight the features that ‎are only included in the Double Main Board.‎

The differences are that the Double Main Board includes:‎

  • ‎3x switches‎

    • two for the 3.3V power enable pins

    • one for the secondary SPI CS pin

  • ability to add a second MicroMod Function Board to the mix

  • board's width

main_2

Main Board - Single V2.1‎

main_3

Main Board - Double V2.2

Revision Changes

The following changes to the Main Board Single V2.1 and Main Board Double V2.2 include:

  • Rotate silkscreen for the connectors and a majority of the labels.‎

  • Add TVS diodes for ESD protection on the USB pins.‎

  • Add SHLD jumper to isolate the USB Type C connector's shield pin.‎

  • Add a 5V MEAS PTH jumper as a measurement for 5V.‎

  • Remove the 500mA/100mA selector for the LiPo charge circuit. The board now charges at a ‎default rate of 500mA only.‎

  • Add a DIVIDER jumper to remove the resistor divider that is connected to processor's ‎‎"BATT_VIN/3" pin for low power applications.

  • Add a dedicated 3.3V/500mA voltage regulator for the Qwiic port.

  • Add GPIO control of 3.3V voltage regulator (I2C_SCL1-Processor.)

  • Add a LED for the 3.3V Qwiic port with a QWIIC LED jumper to disable.‎

  • Add a transistor to disable power to the microSD socket (can be controlled using I2C_SCL1-‎Processor.)‎

  • Add multiplexed primary UART pins to send serial data to Function Board(s).‎

  • Add PTH pins for multiplexed UART (Main Board Single v2.1 only.)

  • Move PWR_EN0 from SDIO_Data2_Processor to PWM1 (Main Board - Single v2.1 only.)

  • Add two 2.2kΩ I2C pull-ups to the primary I2C pins with jumpers (I2C) to disable.‎

  • Replace male header pins and 2-pin shunt with SMD switches to adjust the Function Board ‎Power enable pins (Main Board - Double v2.2 only.)‎

  • Add option to adjust Function Board One's secondary SPI CS pin (i.e., "CS1-processor" and ‎‎"A1-processor") with a SMD switch (Main Board - Double V2.2 only.)‎

Note: Outboard Device Firmware Updates only work with the STM32 Processor Board ‎v20 and Cellular Function Board - Blues Wireless Notecarrier on either the SparkFun MicroMod ‎Main Board - Single V2.1 or the SparkFun MicroMod Main Board - Double V2.2. Other Processors ‎may be supported in the future but are beyond the scope of this tutorial.‎

Power

There are two ways to power the Main Boards, Processor Board, and Function Board(s).

  • USB

  • Single Cell LiPo Battery

It is fine to connect a power source to the USB connector and LiPo battery's JST connector at the ‎same time. The MicroMod Main Board has power-control circuitry to automatically select the best ‎power source.‎

Power USB

One option of powering the board is through the USB Type C connector. You will need a USB Type ‎C cable to power the board with 5V. Power connected to the board's USB C connector will go ‎through a resettable PTC fuse (rated at 2A max) and then the AP7361C 3.3V voltage regulator ‎‎(rated at 1A max). The little green component close to the USB connector is the resettable PTC ‎fuse while the square IC is the voltage regulator. The voltage regulator accepts voltages ‎between ~2.2V to 6.0V. For Main Boards V2+, there are now ESD protection diodes (the 6-pin IC ‎next to the fuse) on the USB data lines. There is also now an additional AP7347DQ 3.3V voltage ‎regulator (rated at 500mA) for the Qwiic connectors. The voltage regulator accepts voltages ‎between ~1.7V to 5.5V.‎

power_4

Power LiPo

The other option is to connect a single cell LiPo battery (i.e., nominal 3.7V, 4.2V fully charged) to ‎the 2-pin JST connector as shown below. For users interested in soldering headers, wire, or ‎measuring a LiPo battery, the VBAT and GND is broken out next to the connector. A MCP73831 ‎charge IC is included on the boards to safely charge the LiPo batteries via USB Type C connector. ‎A corresponding status LED (labeled as CHG, not highlighted in the image below) will indicate when ‎the board is charging or is fully charged. More information on the LED status is highlighted in the ‎LEDs section. For Main Boards V2+, the default charge rate is now set to 500mA only. We ‎recommend that users only use a single cell LiPo battery with a capacity of 500mAh or higher to ‎safely charge the battery. There is also a small cutout on the edge of the board allowing users to ‎place a LiPo battery underneath the board if they decide to place the board in an enclosure.‎

lipo_5

The voltage from the LiPo battery is then regulated down to 3.3V as it goes through the AP7361C ‎‎3.3V voltage regulator (rated at 1A max) for the rest of the board. The voltage is regulated down ‎to 3.3V as it goes through the Qwiic connector's AP7347DQ 3.3V voltage regulator (rated at 500mA ‎max) as well.‎

Note: For more information on proper handling of LiPo batteries, check out the LilyPad Basics: ‎Powering Your Project - LiPo Battery Safety Care.

battery_6

MicroMod Processor Board

The MicroMod ecosystem allows you to easily swap out processors depending on your application. ‎The location of the M.2 connector labeled as Processor is where you would connect and secure a ‎MicroMod Processor Board.‎

processor_7

MicroMod Function Board

Beside the MicroMod Processor's socket is another M.2 connector for MicroMod Function Boards, ‎which allow you to add additional functionality to your Processor Board. The Single Main Board ‎includes one M.2 connector for a single Function Board while the Double Main Board includes two ‎M.2 connectors for up two Function Boards.‎

location_8

Main Board - Single Function Board Location

location_8a

Main Board - Double Function Board Location

Reset and Boot Buttons

Each board includes one button for the RESET and another button for the BOOT. There is an ‎additional reset and GND PTH pin next to the reset button. Hitting the reset button will restart your ‎Processor Board. Hitting the boot button will put the Processor Board into a special boot mode. ‎Depending on the Processor Board, this boot pin may not be connected.‎

buttons_9

SWD Pins

For advanced users, we broke out the 2x5 SWD programming pins. Note that this is not populated ‎so you will need a compatible header and compatible JTAG programmer to connect.‎

swd_10

MicroSD Card Socket

The board includes a microSD socket if your application requires you to log and save data to ‎a memory card. The primary SPI pins (SDO, SDI, SCK) from your Processor and Function Board ‎are connected to the microSD card socket. The cs_10a pin for the microSD card socket is different on ‎each board:‎

  • The MicroMod Main Board - Single v2.1 is on Processor Board's pin D1.‎

  • The MicroMod Main Board - Double v2.2 is on Processor Board's pin G4.‎

socket_11

For Main Boards V2+, there is a transistor (the tiny three pin IC below the microSD card socket) to ‎toggle power to the microSD card socket's VCC pin. This is connected the Processor Board's ‎secondary I2C clock pin (i.e., "I2C_SCL1") and is active low. For users using the Main Boards in low ‎power applications, you can define the pin and set it to a logic HIGH to disconnect power connected ‎to the microSD card socket. Setting the pin to a logic LOW will power the microSD card socket. Just ‎make sure to close the file to avoid any corrupt data.‎

LEDs

There are four LEDs on the board:‎

  • VIN - The VIN LED lights up to indicate when power available from the USB connector.‎

  • QWC - The QWC LED lights up to indicate when there is a 3.3V available to the Qwiic ‎connector after power is regulated down from the USB connector or LiPo battery. This is a ‎new feature that was added in Main Boards v2+.‎

  • ‎3V3 - The 3V3 LED lights up to indicate when there is a 3.3V available for the MicroMod ‎Processor Board and Function Boards after power is regulated down from the USB connector ‎or LiPo battery.‎

  • CHG - The on-board yellow CHG LED can be used to get an indication of the charge ‎status of your battery. Below is a table of other status indicators depending on the state of ‎the charge IC.‎‎

table_12

leds_13

Jumpers

Note: If this is your first time working with jumpers, check out the How to Work with Jumper Pads ‎and PCB Traces tutorial for more information.‎

The following ten jumpers are included on both the Single and Double Main Boards.‎

  • SHLD - By default, the jumper is closed and located on the bottom side of the board. This ‎jumper connects the USB Type C connector's shield pin to GND. Cut this to isolate the USB ‎Type C connector's shield pin. This is a new feature that was added in Main Boards v2+.‎

  • ‎5V5 MEAS - By default, the jumper is closed and located on the top side of the board. This ‎jumper is used to measure your system's current consumption. You can cut this jumper's trace ‎and connect the PTHs to a ammeter/multimeter to probe the input into the 3.3V voltage ‎regulator. Check out our How to Use a Multimeter tutorial for more information on measuring ‎current. This is a new feature that was added in Main Boards V2+.

  • ‎3V3 MEAS - By default, the jumper is closed and located on the top side of the board. This ‎jumper is used to measure your system's current consumption. You can cut this jumper's trace ‎and connect the PTHs to a ammeter/multimeter to probe the output from the 3.3V voltage ‎regulator.‎

  • PTC - By default, the jumper is open and located on the bottom of the board. For advanced ‎users, add a solder blob to the jumper to bypass the resettable PTC fuse to pull more than 2A ‎from the USB source.‎

  • 3V3 EN - By default, this jumper is open and located on the bottom of the board. Closing this ‎jumper enables processor control of the 3.3V bus.‎

  • VIN LED - By default, this jumper is closed and located on the bottom of the board. Cut this ‎trace to disable the LED that is connected to the input of the USB.‎

  • QWIIC LED - By default, this jumper is closed and located on the bottom of the board. Cut this ‎trace to disable the LED that is connected to the output of the Qwiic connector's 3.3V voltage ‎regulator. This is a new feature that was added in Main Boards V2+.‎

  • 3V3 LED - By default, this jumper is closed and located on the bottom of the board. Cut this ‎trace to disable the LED that is connected to the output of the 3.3V voltage regulator.‎

  • DIVIDER - By default, this jumper is closed and located on the bottom of the board. This is ‎connected to processor's "BATT_VIN/3" pin. This is for advanced users that want to remove ‎the resistor divider in low power applications.‎

  • I2C - By default, this 3-pad jumper is closed by default and located on the bottom of the board. ‎The 2.2kΩ pull-up resistors are attached to the primary I2C bus; if multiple devices are ‎connected to the bus with the pull-up resistors enabled, the parallel equivalent resistance will ‎create too strong of a pull-up for the bus to operate correctly. As a general rule of ‎thumb, disable all but one pair of pull-up resistors if multiple devices are connected to the bus. ‎This is a new feature that was added in Main Boards V2+.‎

view_14

Main Board - Single Top View Jumpers

view_14a

Main Board - Single Bottom View Jumpers

Switches

Certain processors have limited GPIO (e.g., SAMD51, ESP32, and STM32 to name a few) and so ‎these alternative powers enable pins to have been provided. The previous version of the Main ‎Board Double used male jumper pins and 2-pin shunts for each Function Board power enable pin. ‎For the Main Board Double v2.2, these are now replaced with SMD switches. There is an additional ‎switch for the CS pin for users that require the use of more than one SPI chip select pin. Simply ‎move the switch toward the side that fits your project's needs. The list below explains where the ‎pins are routed when the switch set to each side. Make sure to check the hookup guide for your ‎Processor and Function Board for more information about the pin definitions.‎

  • G6

    • EN1_ALT - Setting the G5 switch toward the EN1_ALT position will route the ‎Processor Board's G6 to SDIO_DATA1. As stated earlier, this is needed for Processor ‎Boards that do not have a SDIO_DATA1 pin. Thus, a general-purpose pin was used as ‎an alternative pin.

    • G6 PROC - Setting the switch toward the G6 PROC position will route the Processor ‎Board's G6 pin to the Function Board One's general-purpose pin (i.e., FC1's "F4" pin.)‎

  • G5

    • EN0_ALT - Setting the G5 switch toward the EN0_ALT position will route the ‎Processor Board's G5 to SDIO_DATA2. As stated earlier, this is needed for Processor ‎Boards that do not have a SDIO_DATA2 pin. Thus, a general-purpose pin was used as ‎an alternative pin.‎

    • G5 PROC - Setting the switch toward the G5 PROC position will route the Processor ‎Board's G5 pin to the Function Board One's general-purpose pin (i.e., FC1's "F3" pin.)‎

  • CS

    • CS_ALT - Setting the CS switch toward the CS_ALT position will route the Processor ‎Board's secondary SPI chip select pin cs1_15 pin to A1. As stated earlier, this is needed ‎for Processor Boards that do not have a SDIO_DATA3 pin. In this case, an analog pin ‎was used for the alternative pin.‎

    • CS DEF - Setting the switch toward the CS DEF position will route the Processor ‎Board's CS1 pin to the Function Board One's chip select pin (i.e., FC1's "F1/cs_16" pin.)‎

switches_17

Multiplexed Primary UART

For Main Boards V2+, a multiplexer was added after the Processor Board's primary UART pins (i.e., ‎TX1 and RX1). Most users will not need to worry about using the multiplexer, which should be ‎connected to Function Card 0's default UART pins (i.e., FC0's "Rx" and "TX" pins.)‎

main_18

MicroMod Main Board - Single Mux and PTH Pins

 main_18

MicroMod Main Board - Double Mux

For those that have certain Function Boards that require device firmware updates (DFU), users will ‎need to configure the multiplexer's input pins "1IN" and "2IN" by pulling either pin low. Setting "1IN" ‎to LOW will route primary UART lines to Function Card Zero's multiplexed pins (i.e., FC0's ‎‎"DFU_FC_TX and "DFU_FC_RX" pins). Setting "2IN" to LOW will route primary UART lines to ‎Function Card One's multiplexed pins (i.e., FC1's "DFU_FC_TX and "DFU_FC_RX" pins). ‎The MicroMod Cellular Function Board - Blues Wireless Notecarrier is one board that takes ‎advantage of this feature. Since the Main Board Single V2.1 only has one location for a Function ‎Board, the second set of multiplexed pins are broken out to a row of PTH pins (i.e., GND, sel_18b, RXI, ‎TXO). Below is the truth table for the multiplexer. For more information, make sure to check out the ‎respective schematics to view where the pins are connected.‎

scheme_19

Screenshot of the UART Multiplexer from the Main Board Single V2.1 Schematic

scheme_20

Screenshot of the UART Multiplexer from the Main Board Double V2.2 Schematic

Qwiic and I2C

The board includes a vertical and horizontal Qwiic connector. These are connected to the primary ‎I2C bus on both the Processor and Function Board connectors allowing you to easily add a Qwiic-‎enabled device to your application. For Main Boards that are V2+, the 3.3V pin is connected to its ‎own dedicated 3.3V voltage regulator as explained earlier. The I2C data and clock lines are also tied ‎to 2.2kΩ pull-up resistors.‎

qwiic_21

Note: Not highlighted are the Processor Board's secondary I2C pins. Note that the "I2C_SCL1" pin ‎is also connected to the Qwiic connector's 3.3V voltage regulator (i.e., "QWIIC_EN"). Additionally, ‎the I2C_SDA1 is connected to the microSD card socket's transistor to toggle power ‎‎(i.e., SD_ENABLE_22).‎

Note that there are two mounting holes for Qwiic-enabled boards that have a standard 1.0"x1.0" ‎size board. The image below highlighted with a black square is where you would place the board.‎

square_23

MicroMod Pinout

Depending on your window size, you may need to use the horizontal scroll bar at the bottom of the ‎table to view the additional pin functions. Note that the M.2 connector pins on opposing sides are ‎offset from each other as indicated by the bottom pins where it says (Not Connected)*. There is no ‎connection to pins that have a "-" under the primary function.‎

MICROMOD MAIN BOARD - SINGLE

table_24

MICROMOD MAIN BOARD - DOUBLE

table_25

MICROMOD GENERAL FUNCTION BOARD

table_26

MICROMOD GENERAL PROCESSOR BOARD

table_27

MICROMOD GENERAL PIN DESCRIPTIONS

table_28

Low Power Considerations

For users using the Main Board for low power applications, there are a few methods to reduce ‎power for your system. It was briefly explained earlier but we will compile a short list as shown ‎below. The first would be to disable the status LEDs by cutting the jumpers on the back of the ‎board. Of course, you could also disable the LEDs on any Qwiic-enabled boards that are connected ‎as well. Using a Processor Board's GPIO, you could also toggle the voltage regulator on the Qwiic ‎port and Function Boards when not in use. For users with Main Boards V2+, you could toggle ‎power on the microSD card socket by pulling the transistor low using a GPIO.‎

  • Manually disable the LEDs by cutting the following jumpers

    • VIN LED

    • ‎3V3 LED

    • Qwiic LED

  • Manually disabling any LEDs on any Qwiic-enabled boards used with the Main Boards

  • GPIO control of the following

    • Qwiic"s voltage regulator

    • Voltage Enable on the Function Board (EN0 and EN1)

    • Transistor connected to the microSD card socket VCC pin

Dimensions

The board dimension of the MicroMod Main Board - Single V2.1 is 2.90" x 3.40" while the ‎MicroMod Main Board - Double v2.2 is 2.90" x 4.90". Both boards include 5x mounting holes. Four ‎are located on the edge of each board. The fifth mounting hole is located 0.80" away from another ‎mounting hole to mount Qwiic-enabled boards that have the standard 1.0"x1.0" size board.‎

dimensions_29

MicroMod Main Board - Single

dimensions_30

MicroMod Main Board - Double

Note: You'll notice that the Main Boards have the USB C connector, microSD card socket, and ‎Qwiic connector on one side of the board. This is part of the design for users that decide to place ‎the MicroMod Main Board in an enclosure!

Hardware Hookup

If you have not already, make sure to check out the Getting Started with MicroMod: Hardware ‎Hookup for information on inserting your Processor and Function Boards to the Main Board.‎

getting_31

Getting Started with MicroMod

‎Dive into the world of MicroMod - a compact interface to connect a microcontroller to various ‎peripherals via the M.2 Connector!‎

USB

To program and power the Main Board, you will need to insert the USB-C cable into the USB ‎connector. We will leave the other end disconnected when connecting a Processor or Function ‎board to the Main Board.‎

When the boards are secure, insert the other end to a computer. When you are finished ‎programming the processor, you can use a USB battery via the USB connector or LiPo battery via ‎the JST connector to power the board.‎

usb_32

Processor Board

Align the Processor Board's key into its M.2 connector's socket. Insert the board at an angle (~25°), ‎push down, and tighten the screw. In this case, we had the MicroMod Artemis Processor Board ‎secured in the M.2 connector socket. Depending on your application, you may have a different ‎Processor Board.‎

board_33

Function Boards

Align the Function Board's key into its M.2 connector's socket. Insert the board at an angle (~25°), ‎push down, and tighten one of the screws to hold the board down. Attach the second screw on the ‎other side of the board. Once the board is aligned, tighten both screws fully to secure the board.‎

function_32

In this case, we had the Environmental Function Board secured in the M.2 connector socket. ‎Depending on your application, you may have a different Function Board.‎

secure_33

If you decide to have two function boards attached to the Main Board - Double, we recommend ‎tightening the screw between the two Function Boards first to hold them down before attaching the ‎remaining screws on either side of the Function Boards. Again, once the boards are aligned, tighten ‎all three screws fully to secure the board. In this case, we had the Single Pair Ethernet Function ‎Board and the Environmental Function Board secured in the M.2 connector sockets. Depending on ‎your application, you may have different function boards.‎

two_34

Once the Function Boards are secure, attach any remaining cables, antennas, or components that ‎your application may need. In this case, we would have attached a Single Pair Ethernet cable to the ‎SPE Function Board.‎

attached_35

attached_35a

Attach Any Additional Cables and Antennas

Single Cell LiPo Battery

For mobile applications, attach a single cell LiPo battery to the 2-pin JST connector. Attach a USB ‎cable to a USB port or charger when the battery is low to begin charging.‎

battery_36

To remove the LiPo battery, you can pull the white JST connector away from the socket while also ‎wiggling the connector side to side using your thumb and index finger.‎

Note: For more information on proper handling of LiPo batteries, check out the LilyPad Basics: ‎Powering Your Project - LiPo Battery Safety Care.

battery_6

Qwiic-Enabled Devices

To Qwiic-ly connect I2C devices, simply insert a Qwiic cable between one of the MicroMod Main ‎Board's Qwiic ports and your Qwiic device. Of course, you can also daisy chain boards for ‎applications that require more than one Qwiic-enabled device.‎

device_37

If you need to mount a Qwiic-enabled board to the MicroMod Main Board, you can grab ‎some standoffs and mount a standard Qwiic 1.0"x1.0" sized board using the two mounting holes ‎near the USB Type C connector. Place the standoff between the boards and tighten the screws to ‎mount. The image below used standoffs with built-in threads.‎

standoffs_38

MicroSD Card

With power removed from the board, insert a microSD card (with the pins facing toward the board) ‎into the socket. You'll hear a nice click indicating that the microSD card is locked in place.‎

card_39

To remove, make sure power is off and press the microSD card into the socket to eject. You'll hear ‎a nice click indicating that the card is ready to be removed from the socket.‎

Software Installation

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. ‎If this is your first-time using Arduino, please review the following tutorials.

Arduino Board Definitions and Driver

We'll assume that you installed the necessary board files and drivers for your Processor Board. In ‎this case, we used the MicroMod Artemis Processor Board which uses the CH340 USB-to-serial ‎converter. If you are using a different Processor Board, make sure to check out its hookup guide ‎for your Processor Board.‎

install_40

Installing Board Definitions in the Arduino IDE

SEPTEMBER 9, 2020

‎How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an ‎Arduino board definition using the Arduino Board Manager. We will also go over manually installing ‎third-party cores, such as the board definitions required for many of the SparkFun development ‎boards.‎

guide_41

MicroMod Artemis Processor Board Hookup Guide

‎Get started with the Artemis MicroMod Processor Board in this tutorial!‎

driver_42

How to Install CH340 Drivers

‎How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.‎

Arduino Examples

Let's go over a few basic examples to get started with the MicroMod Main Board Single and Double. ‎We'll toggle the 3.3V voltage regulators and log data to a microSD card on both boards.‎

Example 1: MicroMod Main Board - Single Enable Function ‎Board

If you have not already, select your Board (in this case the MicroMod Artemis), and associated ‎COM port. Copy and paste the code below in your Arduino IDE. Hit the upload button.‎

Copy Code
/******************************************************************************

  WRITTEN BY: Ho Yun "Bobby" Chan
  @ SparkFun Electronics
  UPDATED: 1/3/2023
  DATE: 10/19/2021
  GITHUB REPO: https://github.com/sparkfun/SparkFun_MicroMod_Main_Board_Single
  DEVELOPMENT ENVIRONMENT SPECIFICS:
    Firmware developed using Arduino IDE v1.8.12

  ========== DESCRIPTION==========
  This example code toggles the Function Board's AP2112 3.3V voltage 
  regulator's enable pin. The Function Boards built-in power LED should blink.
  This example is based on Arduino's built-in Blink Example:

      https://www.arduino.cc/en/Tutorial/BuiltInExamples/Blink

  Note that this example code uses the MicroMod Main Board - Single. The MicroMod
  Main Board - Double routes the PWR_EN# pins slightly different for the
  two function boards. 

  ========== HARDWARE CONNECTIONS ==========
  MicroMod Artemis Processor Board => MicroMod Main Board - Single => Function Board

  Feel like supporting open source hardware?
  Buy a board from SparkFun!
       MicroMod Artemis Processor Board - https://www.sparkfun.com/products/16401
       MicroMod Main Board - Single - https://www.sparkfun.com/products/20748
       MicroMod Environmental Function Board - https://www.sparkfun.com/products/18632

  LICENSE: This code is released under the MIT License (http://opensource.org/licenses/MIT)

******************************************************************************/

/*Define the power enable pins for the processor board with either SDIO_DATA2 or A1.
  Depending on the processor board, the Arduino pin may be different. 

  Note: For MicroMod Main Board - Single v2.1, there is now only one GPIO available 
        to toggle the Power Enable 0 (PWR_EN0) pin. The previous defines for a few 
        Processor Boards are still available for those that have v1.1.

        For MicroMod Main Board - Single v1.1, certain Processor Boards like the 
        Artemis have SDIO_DATA2 and A1 available to control the Function Board's
        voltage regulator. SAMD51, ESP32, and STM32 Processor Board pins do not 
        have SDIO_DATA2, so users will need to reference the Processor Pin A1.
        Below are a few examples.*/



//==========ARTEMIS==========
//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v2.1 PWM1 => Artemis Processor Board (D45)
#define PWR_EN0 45

//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v1.1 SDIO_DATA2 => Artemis Processor Board (D4)
//#define PWR_EN0 4

//Alternative option that does the same thing. Make sure to just choose one for PWR_EN0
//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v1.1 A1 => Artemis Processor Board (A35)
//#define PWR_EN0 35



//==========TEENSY==========
//Function Board 0's "PWR_EN0" pin <= MicroMod Main- Single v2.1 PWM1 => Teensy Processor Board (2)
//#define PWR_EN0 2

//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v1.1 SDIO_DATA2 => Teensy Processor Board (39)
//#define PWR_EN0 39

//Alternative option that does the same thing. Make sure to just choose one for PWR_EN0
//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v1.1 A1 => Teensy Processor Board (A1)
//#define PWR_EN0 15



//Note: For those using Main - Single v1.1;
//      SAMD51, ESP32, and STM32 Processor Board Pins
//      do not have SDIO_DATA2 and SDIO_DATA1.

//==========SAMD51==========
//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v2.1 PWM1 => SAMD51 Processor Board (20)
//#define PWR_EN0 20

//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v1.1 A1 => SAMD51 Processor Board (18)
//#define PWR_EN0 18


//==========ESP32==========
//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v2.1 PWM1 => ESP32 Processor Board (12)
//#define PWR_EN0 12

//Function Board 0's "PWR_EN0" pin <= MicroMod Main - Single v1.1 A1 => ESP32 Processor Board (35)
//#define PWR_EN0 35



void setup() {
  // initialize the digital pin as an output.
    pinMode(PWR_EN0, OUTPUT);
}



void loop() {
  digitalWrite(PWR_EN0, HIGH); // turn the 3.3V regulator on (HIGH is the voltage level)
  delay(5000);                 // wait for a few seconds to do something with the function boards

  digitalWrite(PWR_EN0, LOW);  // turn the 3.3V regulator off by making the voltage LOW
  delay(5000);                 // wait for a few seconds before turning function boards back on

}

After uploading, take a look at your Function Board's PWR LED. The LED will be on for about 5 ‎seconds and then turn off for another 5 seconds. It will continue to repeat until power is removed ‎from the MicroMod Main Board - Single.

‎Example 2: MicroMod Main Board - Double Enable Function ‎Boards

If you have not already, select your Board (in this case the MicroMod Artemis), and associated ‎COM port. Copy and paste the code below in your Arduino IDE. Hit the upload button.‎

Copy Code
/******************************************************************************

  WRITTEN BY: Ho Yun "Bobby" Chan
  @ SparkFun Electronics
  UPDATED: 1/3/2023
  DATE: 10/19/2021
  GITHUB REPO: https://github.com/sparkfun/SparkFun_MicroMod_Main_Board_Double
  DEVELOPMENT ENVIRONMENT SPECIFICS:
    Firmware developed using Arduino IDE v1.8.12

  ========== DESCRIPTION==========
  This example code toggles the Function Board's AP2112 3.3V voltage
  regulator's enable pin. The Function Boards built-in power LED should blink.
   This example is based on Arduino's built-in Blink Example:

      https://www.arduino.cc/en/Tutorial/BuiltInExamples/Blink

  Note that this example code uses the MicroMod Main Board - Double. The MicroMod
  Main Board - Single routes the PWR_EN0 pin slightly different for the
  function board. 

  ========== HARDWARE CONNECTIONS ==========
  MicroMod Artemis Processor Board => MicroMod Main Board - Double => Function Boards

  Feel like supporting open source hardware?
  Buy a board from SparkFun!
       MicroMod Artemis Processor Board - https://www.sparkfun.com/products/16401
       MicroMod Main Board - Double - https://www.sparkfun.com/products/20595
       MicroMod Environmental Function Board - https://www.sparkfun.com/products/18632

  LICENSE: This code is released under the MIT License (http://opensource.org/licenses/MIT)

******************************************************************************/

/*Define the power enable pins for the processor board with SDIO_DATA2 and SDIO_DATA1.
  Depending on the processor board, the Arduino pin may be different. 

  Note: Certain Processor Boards like the Artemis have more than one pin available 
        to control the Function Board's voltage regulator (e.g. SDIO_DATA2 and G5).
        SAMD51, ESP32, and STM32 Processor Board pins do not have SDIO_DATA2, so
        users will need to reference the Processor Pin G5. Below are a few examples. */

//==========ARTEMIS==========
// We suggest flipping the switch to the G5 PROC and G6 PROC. The volrage regulators will work reguardless
// since SDIO_DATA2 and SDIO_DATA1 are connected regardless of what side the switch is on.
// Function Board 0's "PWR_EN0" pin <= MicroMod Main - Double SDIO_DATA2 => Artemis Processor Board (D4)  
#define PWR_EN0 4
// Function Board 1's "PWR_EN1" pin <= MicroMod Main - Double SDIO_DATA1 => Artemis Processor Board (D26)
#define PWR_EN1 26

// Make sure switch is flipped over to the EN0 ALT and & EN1 ALT. 
// Alternative option that does the same thing. Make sure to just choose one for PWR_EN0 and PWR_EN1.
// Function Board 0's "PWR_EN0" pin <= MicroMod Main - Double G5 => Artemis Processor Board (A29)
//#define PWR_EN0 29
// Function Board 1's "PWR_EN0" pin <= MicroMod Main - Double G6 => Artemis Processor Board (D14)
//#define PWR_EN1 14


//==========TEENSY==========
// We suggest flipping the switch to the G5 PROC and G6 PROC. The volrage regulators will work reguardless
// since SDIO_DATA2 and SDIO_DATA1 are connected regardless of what side the switch is on.
// Function Board 0's "PWR_EN0" pin <= MicroMod Main - Double SDIO_DATA2 => Teensy Processor Board (D39)
//#define PWR_EN0 39
// Function Board 1's "PWR_EN1" pin <= MicroMod Main - Double SDIO_DATA1 => Teensy Processor Board (D34)
//#define PWR_EN1 34

// Make sure switch is flipped over to the EN0 ALT and & EN1 ALT. 
// Alternative option that does the same thing. Make sure to just choose one for PWR_EN0 and PWR_EN1
// Function Board 0's "PWR_EN0" pin <= MicroMod Main - Double G5 => Teensy Processor Board (45)
//#define PWR_EN0 45
// Function Board 1's "PWR_EN1" pin <= MicroMod Main - Double G6 => Teensy Processor Board (6)
//#define PWR_EN1 6



//Note: The SAMD51, ESP32, and STM32 Processor Board Pins do not have SDIO_DATA2 and SDIO_DATA1.

//==========SAMD51==========
// Make sure switch is flipped over to the EN0 ALT and & EN1 ALT. 
// Function Board 0's "PWR_EN0" pin <= MicroMod Main - Double G5 => SAMD51 Processor Board (D7)
//#define PWR_EN0 7
//Function Board 1's"PWR_EN1" pin <= MicroMod Main - Double G6 => SAMD51 Processor Board (D8)
//#define PWR_EN1 8


//==========ESP32==========
// Make sure switch is flipped over to the EN0 ALT and & EN1 ALT. 
// Function Board 0's "PWR_EN0" pin <= MicroMod Main - Double G5 => ESP32 Processor Board (32)
//#define PWR_EN0  32
// Function Board 1's"PWR_EN1" pin <= MicroMod Main - Double G6 => ESP32 Processor Board (33)
//#define PWR_EN1  33



void setup() {
  // initialize the digital pins as an output.
  pinMode(PWR_EN0, OUTPUT); 
  pinMode(PWR_EN1, OUTPUT);

}



void loop() {

  digitalWrite(PWR_EN0, HIGH); // turn the 3.3V regulator on (HIGH is the voltage level)
  digitalWrite(PWR_EN1, HIGH); // turn the 3.3V regulator on (HIGH is the voltage level)
  delay(5000);                 // wait for a few seconds to do something with the function boards 

  digitalWrite(PWR_EN0, LOW);  // turn the 3.3V regulator off by making the voltage LOW
  digitalWrite(PWR_EN1, LOW);  // turn the 3.3V regulator off by making the voltage LOW
  delay(5000);                 // wait for a few seconds before turning function boards back on

}

After uploading, take a look at the PWR LEDs on the Function Boards. The LEDs will be on for ‎about 5 seconds and then turn off for another 5 seconds. It will continue to repeat until power is ‎removed from the MicroMod Main Board - Double.‎

Example 3: Reading and Writing to a MicroSD Card‎

Note: For the MicroMod Teensy, make sure to check out the SdFat library included with the ‎Teensyduino add-on. Once the board is selected, head to the menu to open the examples ‎‎(File > Examples > SD). You'll need to modify the defined pin from:

Copy Code
const int chipSelect = 10;

To one of the following values. ‎

Copy Code
//==========TEENSY==========
// default value used in Teensy SD Example Code
//const int chipSelect = 10; 
// The microSD Card CS pin is D1 for the MicroMod Main Board - Single and Teensy Processor (5). Adjust for your processor if necessary.
const int chipSelect 5;
// The microSD Card's CS pin is G4 for the MicroMod Main Board - Double and Teensy Processor (44). Adjust for your processor if necessary.
//const int chipSelect 44;

The example below uses the built-in SD Arduino library. The only difference in the code is the CS ‎pin for the microSD card, which you will need to adjust for your processor board (in this case we ‎use the Artemis Processor Board). Make sure to reference your Processor Board's CS pin for ‎either the Main Board - Single (D1) or Main Board - Double (G4).‎

Note: The SPI pins will be defined as macros with your processor's board definitions, so we won't ‎need to define PICO, POCI, or CLK pins. Sweet!‎

If you have not already, select your Board (in this case the MicroMod Artemis), and associated ‎COM port. Copy and paste the code below in your Arduino IDE. Hit the upload button.‎

Copy Code
/*
  SD Card Read/Write

  This example shows how to read and write data to and from an SD card file
  The circuit:

  SD card attached to SPI bus as follows:

   SD Card   <=> MicroMod Main Board <=> Artemis Processor Board
   -----------------------------------------------------------------
   SD ENABLE <=>  I2C_SDA1-PROCESSOR <=> pin 9
   PICO/SDO  <=>  SPI_PROCESSOR_SDO  <=> pin 38
   POCI/SDI  <=>  SPI_PROCESSOR_SDI  <=> pin 43
   CLK       <=>  SPI_PROCESSOR_CLK  <=> pin 42
   CS        <=>  D1_PROCESSOR       <=> pin 1 (Main Board - Single)
   or ...
   CS        <=>  G4_PROCESSOR       <=> pin 28 (Main Board - Double)

  created   Nov 2010
  by David A. Mellis
  modified 9 Apr 2012
  by Tom Igoe

  This example code is in the public domain.

*/

#include <SPI.h>
#include <SD.h>

//==========ARTEMIS==========
// The microSD Card CS pin is D1 for the MicroMod Main Board - Single and Artemis Processor (D1). Adjust for your processor if necessary.
const int SD_CS_PIN = 1;
// The microSD Card's CS pin is G4 for the MicroMod Main Board - Double and Artemis Processor (D28). Adjust for your processor if necessary.
//const int SD_CS_PIN = 28; 

File myFile;

void setup() {
  // Open serial communications and wait for port to open:
  Serial.begin(9600);
  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }


  Serial.print("Initializing SD card...");

  if (!SD.begin(SD_CS_PIN)) {
    Serial.println("initialization failed!");
    while (1);
  }
  Serial.println("initialization done.");

  // open the file. note that only one file can be open at a time,
  // so you have to close this one before opening another.
  myFile = SD.open("test.txt", FILE_WRITE);

  // if the file opened okay, write to it:
  if (myFile) {
    Serial.print("Writing to test.txt...");
    myFile.println("testing 1, 2, 3.");
    // close the file:
    myFile.close();
    Serial.println("done.");
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }

  // re-open the file for reading:
  myFile = SD.open("test.txt");
  if (myFile) {
    Serial.println("test.txt:");

    // read from the file until there's nothing else in it:
    while (myFile.available()) {
      Serial.write(myFile.read());
    }
    // close the file:
    myFile.close();
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }
}

void loop() {
  // nothing happens after setup
}

Open the Arduino Serial Monitor at 9600 baud. If all goes well, you should see the following output ‎if this is the first time writing to the card! Note that you may see "testing 1, 2, 3." written a few times ‎if you hit the reset button.‎

Copy Code
Initializing SD card...initialization done.
Writing to test.txt...done.
test.txt:
testing 1, 2, 3.

com_43

If you are looking to go the extra mile to see if data was saved, close the Serial Monitor and remove ‎power from the MicroMod Main Board. Eject your microSD card from the socket and insert into a ‎microSD card adapter. Then insert the microSD card into your computer's card reader or USB port. ‎Open the test.txt file in a text editor. You should see an output similar to what you saw in the Serial ‎Monitor after the file was opened as shown below. If you let the program run a few times by hitting ‎the reset button or opening the Serial Monitor, you may see it written a few times.‎

Copy Code
testing 1, 2, 3.

Besides verifying the data in the file, this step is also useful if you adjust the code to continuously ‎log data in a CSV format. After logging data, you could the open text document in a spreadsheet ‎and graph the values!‎

Example 4: Reading and Writing to a MicroSD Card (Low ‎Power)‎

The example below uses the built-in SD Arduino library like the previous example. However, it ‎toggles the power for the microSD card socket with SD_ENABLE. The pin is active low so by setting ‎the pin HIGH, power will be disconnected. Make sure to close the file before removing power.‎

If you have not already, select your Board (in this case the MicroMod Artemis), and associated ‎COM port. Copy and paste the code below in your Arduino IDE. Hit the upload button.‎

Copy Code
/*
  SD Card Read/Write

  This example shows how to read and write data to and from an SD card file
  The circuit:

  SD card attached to SPI bus as follows:

   SD Card   <=> MicroMod Main Board <=> Artemis Processor Board
   -----------------------------------------------------------------
   SD ENABLE <=>  I2C_SDA1-PROCESSOR <=> pin 9
   PICO/SDO  <=>  SPI_PROCESSOR_SDO  <=> pin 38
   POCI/SDI  <=>  SPI_PROCESSOR_SDI  <=> pin 43
   CLK       <=>  SPI_PROCESSOR_SCK  <=> pin 42
   CS        <=>  D1_PROCESSOR       <=> pin 1 (Main Board - Single)
   or ...
   CS        <=>  G4_PROCESSOR       <=> pin 28 (Main Board - Double)

  created   Nov 2010
  by David A. Mellis
  modified 9 Apr 2012
  by Tom Igoe

  This example code is in the public domain.

*/

#include <SPI.h>
#include <SD.h>

//==========ARTEMIS==========
// The microSD Card CS pin is D1 for the MicroMod Main Board - Single and Artemis Processor (D1). Adjust for your processor if necessary.
const int SD_CS_PIN = 1;
// The microSD Card's CS pin is G4 for the MicroMod Main Board - Double and Artemis Processor (D28). Adjust for your processor if necessary.
//const int SD_CS_PIN = 28; 

// The microSD Card CS pin is SDA1 for the MicroMod Main Board - Single and Artemis Processor (D9). Adjust for your processor if necessary.
const int SD_ENABLE = 9;

File myFile;

void setup() {

  pinMode(SD_ENABLE, OUTPUT);  //sets the digital pin as output
  digitalWrite(SD_ENABLE, LOW);  //Power MicroSD card socket, pin is active low

  // Open serial communications and wait for port to open:
  Serial.begin(9600);
  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }


  Serial.print("Initializing SD card...");

  if (!SD.begin(SD_CS_PIN)) {
    Serial.println("initialization failed!");
    while (1);
  }
  Serial.println("initialization done.");

  // open the file. note that only one file can be open at a time,
  // so you have to close this one before opening another.
  myFile = SD.open("test.txt", FILE_WRITE);

  // if the file opened okay, write to it:
  if (myFile) {
    Serial.print("Writing to test.txt...");
    myFile.println("testing 1, 2, 3.");
    // close the file:
    myFile.close();
    Serial.println("done.");
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }

  // re-open the file for reading:
  myFile = SD.open("test.txt");
  if (myFile) {
    Serial.println("test.txt:");

    // read from the file until there's nothing else in it:
    while (myFile.available()) {
      Serial.write(myFile.read());
    }
    // close the file:
    myFile.close();
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }

  digitalWrite(SD_ENABLE, HIGH);  //remove power from MicroSD card socket for low power applications

}// end setup()

void loop() {
  // nothing happens after setup

}//end loop()

Open the Arduino Serial Monitor at 9600 baud. If all goes well, you should see the same output in ‎the Serial Monitor and data written to the microSD card.‎

Example 5: MicroMod Main Enable Qwiic Boards

If you have not already, select your Board (in this case the MicroMod Artemis), and associated ‎COM port. Copy and paste the code below in your Arduino IDE. Hit the upload button.‎

Copy Code
/******************************************************************************

  WRITTEN BY: Ho Yun "Bobby" Chan
  @ SparkFun Electronics
  DATE: 1/3/2023
  GITHUB REPO: https://github.com/sparkfun/SparkFun_MicroMod_Main_Board_Single
  DEVELOPMENT ENVIRONMENT SPECIFICS:
    Firmware developed using Arduino IDE v1.8.12

  ========== DESCRIPTION==========
  This example code toggles the Qwiic Port's AP7347DQ 3.3V voltage 
  regulator's enable pin. The Qwiic-enabled boards with built-in
  power LED should blink. The Main Board's QWC LED will also blink
  as well. This example is based on Arduino's built-in Blink Example:

      https://www.arduino.cc/en/Tutorial/BuiltInExamples/Blink

  Note that this example code works for both the MicroMod Main Board - Single v2.1
  and Double v2.2. 

  ========== HARDWARE CONNECTIONS ==========
  MicroMod Artemis Processor Board => MicroMod Main Board - Single => Qwiic Board

  Feel like supporting open source hardware?
  Buy a board from SparkFun!
       MicroMod Artemis Processor Board - https://www.sparkfun.com/products/16401
       MicroMod Main Board - Single - https://www.sparkfun.com/products/20748
       MicroMod Environmental Function Board - https://www.sparkfun.com/products/18632
       SparkFun GPS Breakout - Chip Antenna, SAM-M8Q - https://www.sparkfun.com/products/15210

  LICENSE: This code is released under the MIT License (http://opensource.org/licenses/MIT)

******************************************************************************/

/*Define the power enable pin for the processor board for I2C_SCL1-PROCESSOR.
  Depending on the processor board, the Arduino pin may be different.*/


//==========ARTEMIS==========
// Qwiic Port's "Qwiic EN" pin <= MicroMod Main Board I2C_SCL1-PROCESSOR => Artemis Processor Board (D8)
#define QWIIC_EN 8 


//==========TEENSY==========
// Qwiic Port's "QWIIC_EN" pin <= MicroMod Main Board I2C_SCL1-PROCESSOR => Teensy Processor Board (24)
//#define QWIIC_EN 24


//==========SAMD51==========
// Qwiic Port's "QWIIC_EN" pin <= MicroMod Main Board I2C_SCL1-PROCESSOR => SAMD51 Processor Board (36)
//#define QWIIC_EN 36


//==========ESP32==========
// Qwiic Port's "QWIIC_EN" pin <= MicroMod Main Board I2C_SCL1-PROCESSOR => ESP32 Processor Board (?25??)
//#define QWIIC_EN 25


void setup() {
  // initialize the digital pin as an output.
    pinMode(QWIIC_EN, OUTPUT);
}



void loop() {
  digitalWrite(QWIIC_EN, HIGH); // turn the 3.3V regulator on (HIGH is the voltage level)
  delay(5000);                 // wait for a few seconds to do something with the Qwiic-enabled board(s)

  digitalWrite(QWIIC_EN, LOW);  // turn the 3.3V regulator off by making the voltage LOW
  delay(5000);                 // wait for a few seconds before turning Qwiic-enabled board(s) back on

}

Once uploaded, check out your Qwiic-enabled board to see if the power LED turns on/off every 5 ‎seconds. Not all boards have an LED populated for power. In that case, you can also check your ‎Main Board's built-in LED labeled as QWC. The LED will also turn on and off.‎

More Examples!‎

Sweet! Now that we know that we can read and write to the microSD card, try exploring the other ‎examples in either the SD or SdFat Arduino libraries. Or check out the following MicroMod tutorials ‎that have a built-in microSD card socket for ideas on data logging. Better yet, try adding a sensor ‎and write some code to log some data!‎

MicroMod Weather Carrier Board Hookup Guide: A quick guide to help to create your ‎own MicroMod weather station using the MicroMod Weather Carrier Board and Processor of your ‎choice.‎

MicroMod Data Logging Carrier Board Hookup Guide: Get started with some ‎customizable MicroMod data logging with the Data Logging Carrier Board.‎

MicroMod Asset Tracker Carrier Board Hookup Guide: Get started with the SparkFun ‎MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-‎blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.

‎Looking for more examples with a Function Board? Below are a few Function Board examples from ‎our tutorials that are tagged with MicroMod.‎

1W LoRa MicroMod Function Board Hookup Guide: Everything you need to get ‎started with the 1W LoRa MicroMod function board; a MicroMod function board that provides LoRa ‎capabilities for your MicroMod project. Must be used in conjunction with a MicroMod main board ‎and processor.‎

MicroMod WiFi Function Board - ESP32 Hookup Guide: The MicroMod ESP32 ‎Function Board adds additional wireless options to MicroMod Processor Boards that do not have ‎that capability. This special function board acts as a coprocessor that takes advantage of Espressif's ‎ESP32 WROOM to add WiFi and Bluetooth® to your applications.‎

MicroMod Environmental Function Board Hookup Guide: The SparkFun MicroMod ‎Environmental Function Board adds additional sensing options to the MicroMod Processor Boards. ‎This function board includes three sensors to monitor air quality (SGP40), humidity & temperature ‎‎(SHTC3), and CO2 concentrations (STC31) in your indoor environment. To make it even easier to ‎use, all communication is over the MicroMod's I2C bus! In this tutorial, we will go over how to ‎connect the board and read the sensors.‎

MicroMod WiFi Function Board - DA16200 Hookup Guide: Add IoT functionality to ‎any MicroMod project with the MicroMod WiFi function Board - DA16200!‎

Better yet, try connecting a Qwiic-enabled device to the Main Board's Qwiic connector. Below are a ‎few examples from our tutorials that are tagged with Qwiic.‎

Capacitive Touch Slider (CAP1203) Hookup Guide: An easy and Qwiic way to add ‎capacitive touch to any of your projects using the CAP1203! In this guide, we go over how to ‎connect and set up your Capacitive Touch Slider so you can start playing with it right away.‎

SparkFun Top pHAT Hookup Guide: The pHAT to sit above your other HATs. Does that ‎make it the "king" of the pHATs? This guide will help you get started using the Top pHAT with the ‎Raspberry Pi.‎

Qwiic ToF Imager - VL53L5CX Hookup Guide: Hookup Guide for the Qwiic ToF Imager - ‎VL53L5CX

SparkFun Arduino UNO R4 WiFi Qwiic Kit Hookup Guide: The SparkFun Arduino ‎UNO R4 WiFi Qwiic Kit is a great way to get started with Arduino and the Qwiic-connect system - ‎use this guide to get started!‎

Troubleshooting

Not working as expected and need help?‎‎ ‎

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE‎ ‎

If you don't find what you need there, the SparkFun Forums: MicroMod are a great place to find ‎and ask for help. If this is your first visit, you'll need to create a Forum Account to search product ‎forums and post questions.

SPARKFUN FORUMS: MICROMOD

Resources and Going Further

Now that you've successfully got your MicroMod Main Board with a Processor Board, it's time to ‎incorporate it into your own project! For more information, check out the resources below:‎

מק"ט יצרן # 20748
SPARKFUN MICROMOD MAIN BOARD - S
SparkFun Electronics
מק"ט יצרן # 20595
SPARKFUN MICROMOD MAIN BOARD - D
SparkFun Electronics
מק"ט יצרן # 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
מק"ט יצרן # 16401
MICROMOD ARTEMIS PROCESSOR
SparkFun Electronics
מק"ט יצרן # 16791
MICROMOD SAMD51 PROCESSOR
SparkFun Electronics
מק"ט יצרן # 17713
SPARKFUN MICROMOD STM32 PROCESSO
SparkFun Electronics
מק"ט יצרן # 19935
SPARKFUN MICROMOD MIKROBUS START
SparkFun Electronics
מק"ט יצרן # COM-19038
MICROMOD SINGLEPAIR ETHERNET BRD
SparkFun Electronics
מק"ט יצרן # 18378
SPARKFUN MICROMOD GNSS FUNCTION
SparkFun Electronics
מק"ט יצרן # 18632
MICROMOD ENVIRONMENTAL FUNCTION
SparkFun Electronics
מק"ט יצרן # 13004
MICROSD USB READER
SparkFun Electronics
מק"ט יצרן # 19012
MICROMOD SCREWDRIVER
SparkFun Electronics
מק"ט יצרן # 21326
SPARKFUN MICROMOD STM32 PROCESSO
SparkFun Electronics
מק"ט יצרן # 20409
SPARKFUN MICROMOD CELLULAR FUNCT
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.